summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: c586bd9)
raw | patch | inline | side by side (parent: c586bd9)
author | Chase Maupin <Chase.Maupin@ti.com> | |
Mon, 11 Mar 2013 20:03:31 +0000 (15:03 -0500) | ||
committer | Denys Dmytriyenko <denys@ti.com> | |
Mon, 11 Mar 2013 21:17:04 +0000 (17:17 -0400) |
* Moved the setup-defconfig.inc file from meta-arago to meta-ti.
This functionality is used by the SDKs to allow the option for
using an in-tree configuration file for the kernel build.
* This option was chosen to make it easy for other layers to
override the config with their own using the normal OE method
of specifying a defconfig file in their layer rather than having
to use some custom variable setting.
Signed-off-by: Chase Maupin <Chase.Maupin@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
This functionality is used by the SDKs to allow the option for
using an in-tree configuration file for the kernel build.
* This option was chosen to make it easy for other layers to
override the config with their own using the normal OE method
of specifying a defconfig file in their layer rather than having
to use some custom variable setting.
Signed-off-by: Chase Maupin <Chase.Maupin@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
recipes-kernel/linux/setup-defconfig.inc | [new file with mode: 0644] | patch | blob |
diff --git a/recipes-kernel/linux/setup-defconfig.inc b/recipes-kernel/linux/setup-defconfig.inc
--- /dev/null
@@ -0,0 +1,26 @@
+# Check the defconfig file and see if it points to an in kernel
+# defconfig that should be used, or if it is a complete config file
+
+addtask setup_defconfig before do_configure after do_patch
+do_setup_defconfig() {
+ # Always copy the defconfig file to .config to keep consistency
+ # between the case where there is a real config and the in kernel
+ # tree config
+ cp ${WORKDIR}/defconfig ${S}/.config
+}
+
+# define our own do_configure that will:
+# 1. Check the .config file and see if string use-kernel-config= is present
+# 2. If the use-kernel-config string is present parse out the config to use
+# and run make ${config}
+# 3. else run yes '' | oe_runmake oldconfig like the default do_configure
+# does
+do_configure() {
+ config=`cat ${S}/.config | grep use-kernel-config | cut -d= -f2`
+ if [ "x${config}" != "x" ]
+ then
+ oe_runmake ${config}
+ else
+ yes '' | oe_runmake oldconfig
+ fi
+}