u-boot_2011.09, u-boot_2011.12: Always use gnu ld for LD
authorKhem Raj <raj.khem@gmail.com>
Thu, 12 Jan 2012 20:15:05 +0000 (12:15 -0800)
committerKoen Kooi <koen@dominion.thruhere.net>
Fri, 13 Jan 2012 11:30:50 +0000 (12:30 +0100)
u-boot wants GNU ld and cant link with gold
so when default linker is gold we make sure
that it still uses good old GNU ld

Signed-off-by: Khem Raj <raj.khem@gmail.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
recipes-bsp/u-boot/u-boot/0001-config-Always-use-GNU-ld.patch [new file with mode: 0644]
recipes-bsp/u-boot/u-boot_2011.09.bb
recipes-bsp/u-boot/u-boot_2011.12.bb

diff --git a/recipes-bsp/u-boot/u-boot/0001-config-Always-use-GNU-ld.patch b/recipes-bsp/u-boot/u-boot/0001-config-Always-use-GNU-ld.patch
new file mode 100644 (file)
index 0000000..2564d1d
--- /dev/null
@@ -0,0 +1,43 @@
+From dff01fc9346e6f4e3386536df309d2e78f03f3ee Mon Sep 17 00:00:00 2001
+From: Khem Raj <raj.khem@gmail.com>
+Date: Wed, 21 Dec 2011 08:53:02 -0800
+Subject: [PATCH] config: Always use GNU ld
+
+This patch makes sure that we always use the GNU ld. u-boot uses certain
+construct e.g. OVERLAY which are not implemented in gold therefore it
+always needs GNU ld for linking. It works well if default linker in
+toolchain is GNU ld but in some cases we can have gold to be the
+default linker and also ship GNU ld but not as default in such cases
+its called $(PREFIX)ld.bfd, with this patch we make sure that if
+$(PREFIX)ld.bfd exists than we use that for our ld. This way it
+does not matter what the default ld is.
+
+Upstream-status: Pending
+
+Signed-off-by: Khem Raj <raj.khem@gmail.com>
+---
+ config.mk |    4 +++-
+ 1 files changed, 3 insertions(+), 1 deletions(-)
+
+diff --git a/config.mk b/config.mk
+index ddaa477..59b3e71 100644
+--- a/config.mk
++++ b/config.mk
+@@ -126,11 +126,13 @@ cc-option = $(strip $(if $(findstring $1,$(CC_OPTIONS)),$1,\
+               $(if $(call cc-option-sys,$1),$1,$2)))
+ endif
++exists_bfd_ld = $(shell if $(CROSS_COMPILE)ld.bfd -v >& /dev/null; \
++              then echo "$(1)"; else echo "$(2)"; fi; )
+ #
+ # Include the make variables (CC, etc...)
+ #
+ AS    = $(CROSS_COMPILE)as
+-LD    = $(CROSS_COMPILE)ld
++LD    = $(call exists_bfd_ld, "$(CROSS_COMPILE)ld.bfd", "$(CROSS_COMPILE)ld")
+ CC    = $(CROSS_COMPILE)gcc
+ CPP   = $(CC) -E
+ AR    = $(CROSS_COMPILE)ar
+-- 
+1.7.5.4
+
index 74c8518f794fa2d4f2f2c083a18ab826eaa87703..4a9d3cb137c60ba47160803cc8b62240ea730401 100644 (file)
@@ -1,6 +1,6 @@
 require u-boot.inc
 
-PR = "r5"
+PR = "r6"
 
 # SPL build
 UBOOT_BINARY = "u-boot.img"
@@ -32,6 +32,7 @@ SRC_URI = "git://www.denx.de/git/u-boot.git;protocol=git \
            file://2011.09/0019-BeagleBoard-config-Really-switch-to-ttyO2.patch \
            file://2011.09/0020-beagleboard-add-support-for-TCT-Beacon-board.patch \
            file://2011.09/0021-beagleboard-add-support-for-scanning-loop-through-ex.patch \
+           file://0001-config-Always-use-GNU-ld.patch \
            file://fw_env.config \
           "
 
index d776c38c7611b9ec3acac1e98e375f5079deafcd..7554badc912bfb1e2f765d291b48efb4d2cd6edf 100644 (file)
@@ -6,7 +6,7 @@ UBOOT_IMAGE = "u-boot-${MACHINE}-${PV}-${PR}.img"
 UBOOT_SYMLINK = "u-boot-${MACHINE}.img"
 
 PV = "2011.12"
-PR = "r1"
+PR = "r2"
 
 # No patches for other machines yet
 COMPATIBLE_MACHINE = "(beagleboard|pandaboard|hawkboard|am3517-evm|am37x-evm|omap3evm)"
@@ -18,6 +18,7 @@ SRC_URI = "git://www.denx.de/git/u-boot.git;protocol=git \
            file://2011.12/0004-omap4-common-mount-root-RO.patch \
            file://2011.12/0005-omap4-common-use-ext4-by-default.patch \
            file://2011.12/U-Boot-OMAP-MMC-Add-delay-before-waiting-for-status.patch \
+           file://0001-config-Always-use-GNU-ld.patch \
           "
 
 # v2011.12 tag