From: Denys Dmytriyenko Date: Thu, 28 Feb 2013 21:52:53 +0000 (-0500) Subject: u-boot 2012.10: add the latest SDK 05.06 version from meta-arago X-Git-Url: https://git.ti.com/gitweb?p=glsdk%2Fmeta-ti-glsdk.git;a=commitdiff_plain;h=a80ec1d7bec835a743701a8f19c87efdaf92a6ba u-boot 2012.10: add the latest SDK 05.06 version from meta-arago Signed-off-by: Denys Dmytriyenko --- diff --git a/recipes-bsp/u-boot/u-boot_2012.10.bb b/recipes-bsp/u-boot/u-boot_2012.10.bb new file mode 100644 index 0000000..89d646c --- /dev/null +++ b/recipes-bsp/u-boot/u-boot_2012.10.bb @@ -0,0 +1,32 @@ +# Use the version of u-boot.inc in oe-core not the meta-ti version +require ${COREBASE}/meta/recipes-bsp/u-boot/u-boot.inc + +# Reset OEMAKE. Current u-boot.inc sets -02 which breaks this version of u-boot's build. +# This issue was fixed in oe-core master by removing the -02 statement. +EXTRA_OEMAKE = 'CROSS_COMPILE=${TARGET_PREFIX} CC="${TARGET_PREFIX}gcc ${TOOLCHAIN_OPTIONS}"' + +DESCRIPTION = "u-boot bootloader for ARM MPU devices" +LICENSE = "GPLv2+" +LIC_FILES_CHKSUM = "file://COPYING;md5=1707d6db1d42237583f50183a5651ecb" + +COMPATIBLE_MACHINE = "ti33x|omap3" + +DEFAULT_PREFERENCE = "-1" + +PACKAGE_ARCH = "${MACHINE_ARCH}" + +PR = "r7+gitr${SRCPV}" + +SRC_URI = "git://arago-project.org/git/projects/u-boot-am33x.git;protocol=git;branch=${BRANCH} \ +" + +BRANCH = "amsdk-05.06.00.00" + +SRCREV = "6536bfa6b7f16bb49fdea8c72959e3ed54e77a82" + +S = "${WORKDIR}/git" + +UBOOT_SUFFIX = "img" + +# Set the name of the SPL that will built so that it is also packaged with u-boot. +SPL_BINARY = "MLO"