Revert "linux-omap3: Add supported kernel recipe for am37x-evm and am3517-evm"
The same recipe already exists under linux-omap-psp name.
This reverts commit 153b5ed063c0bc2b16b938409027794a8dad908e.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
The same recipe already exists under linux-omap-psp name.
This reverts commit 153b5ed063c0bc2b16b938409027794a8dad908e.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
machine configs: Add SGX to MACHINE_FEATURES
* Add sgx to MACHINE_FEATURES to indicate that a particular machine supports
sgx.
* TI chips are available in multiple variants including some that supports sgx
while others do not.
* By adding sgx as a machine feature other layers can create generic
packagegroups or images for a particular soc but will only include sgx
dependencies if the particular machine has sgx support.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Add sgx to MACHINE_FEATURES to indicate that a particular machine supports
sgx.
* TI chips are available in multiple variants including some that supports sgx
while others do not.
* By adding sgx as a machine feature other layers can create generic
packagegroups or images for a particular soc but will only include sgx
dependencies if the particular machine has sgx support.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux: Add kernel version 3.3.7 for beagleboard
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-omap3: Add supported kernel recipe for am37x-evm and am3517-evm
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
mesa-dri: update to 9.0.2 to follow oe-core
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3: ignore QA errors
This patch allows libgles-omap3 to build on the danny branch. The following
warnings are not addressed:
WARNING: libgles-omap3: No generic license file exists for: proprietary-binary in any provider
WARNING: QA Issue: libgles-omap3: Files/directories were installed but not shipped
/usr/lib/ES2.0
WARNING: libgles-omap3: The compile log indicates that host include and/or library paths were used.
Please check the log '/prj/oe/omap/build-gumstix-community-danny/tmp/work/armv7a-vfp-neon-poky-linux-gnueabi/libgles-omap3-4.05.00.03-r35/temp/log.do_compile' for more information.
Signed-off-by: Peter A. Bigot <pab@pabigot.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
This patch allows libgles-omap3 to build on the danny branch. The following
warnings are not addressed:
WARNING: libgles-omap3: No generic license file exists for: proprietary-binary in any provider
WARNING: QA Issue: libgles-omap3: Files/directories were installed but not shipped
/usr/lib/ES2.0
WARNING: libgles-omap3: The compile log indicates that host include and/or library paths were used.
Please check the log '/prj/oe/omap/build-gumstix-community-danny/tmp/work/armv7a-vfp-neon-poky-linux-gnueabi/libgles-omap3-4.05.00.03-r35/temp/log.do_compile' for more information.
Signed-off-by: Peter A. Bigot <pab@pabigot.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
omap3-sgx-modules: Add v4.08.00.01 of the SGX modules
* Add version 4.08.00.01 of the SGX modules.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Add version 4.08.00.01 of the SGX modules.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3: Add v4.08.00.01 of the Graphics SDK
* Add version v4.08.00.01 of the Graphics SDK.
* Add X11 support via DRI/DRM Xorg driver
* Replace pvrsrvinit with pvrsrvctl (Imagination Technologies based change)
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Add version v4.08.00.01 of the Graphics SDK.
* Add X11 support via DRI/DRM Xorg driver
* Replace pvrsrvinit with pvrsrvctl (Imagination Technologies based change)
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
machines: set default virtual/bootloader for remaining machines
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
am335x-evm: Increase UBI max size to 500MB
* Based on the EVM and beaglebone + NAND memory cape we can
increase the base file system size to 500MB since by default
there is about 504MB of space allocated to the file system
partition in the NAND.
* The max size in LEBs was determined using the formula at
http://processors.wiki.ti.com/index.php/UBIFS_Support
Signed-off-by: Chase Maupin <Chase.Maupin@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Based on the EVM and beaglebone + NAND memory cape we can
increase the base file system size to 500MB since by default
there is about 504MB of space allocated to the file system
partition in the NAND.
* The max size in LEBs was determined using the formula at
http://processors.wiki.ti.com/index.php/UBIFS_Support
Signed-off-by: Chase Maupin <Chase.Maupin@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-mainline 3.2: update beagleboard defconfig
Link the TLC59108 driver statically so ULCD7 initialization occurs
automatically as it did before f0e2305c7e1 which removed the initialization
from u-boot. (Angstrom-v2012.12 does not include this module by default.)
Signed-off-by: Peter A. Bigot <pab@pabigot.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Link the TLC59108 driver statically so ULCD7 initialization occurs
automatically as it did before f0e2305c7e1 which removed the initialization
from u-boot. (Angstrom-v2012.12 does not include this module by default.)
Signed-off-by: Peter A. Bigot <pab@pabigot.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
u-boot_2012.04.01: Add latest u-boot recipe for am37x-evm
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
ti-ocf-crypto-module: Port ti-ocf-crypto-module from Arago
* Recipe pulls in ti-ocf-crypto-module from gforge
* For am37x, this module allows access to the crypto hardware accelerators
through OCF-Linux.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Recipe pulls in ti-ocf-crypto-module from gforge
* For am37x, this module allows access to the crypto hardware accelerators
through OCF-Linux.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
u-boot_2010.12-psp03.21.00.04.sdk: Add latest u-boot recipe for am180x-evm
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
ti-pru-sw-edma-driver: Port PRU SW edma driver from Arago
* Add PRU SW edma driver recipe for the omapl138 machines
* This recipe builds and installs an edma driver module that supports the
edma user space libraries built by the ti-pru-sw-edma-library recipe.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Add PRU SW edma driver recipe for the omapl138 machines
* This recipe builds and installs an edma driver module that supports the
edma user space libraries built by the ti-pru-sw-edma-library recipe.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-omapl138-psp: Add latest linux-omapl138 patches
* Add latest patches to linux-omapl138 that were added since this recipe was
added to meta-ti.
* Update to latest am180x-evm defconfig
* Mimic the following commits from arago:
linux-davinci: update to add mmc patches
* Optimizations to reduce overhead on weak platforms
linux: disable DMA for MUSB
* For the am3517, am180x, and am335x devices the CPPI 4.1 DMA
should NOT be used for the MUSB controller. Using this DMA
can cause the controller to lockup.
* Updated the defconfigs to set the use of PIO mode
* Added a patch to updated the PIO mode description to make it
easier to determine when it can be used.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Add latest patches to linux-omapl138 that were added since this recipe was
added to meta-ti.
* Update to latest am180x-evm defconfig
* Mimic the following commits from arago:
linux-davinci: update to add mmc patches
* Optimizations to reduce overhead on weak platforms
linux: disable DMA for MUSB
* For the am3517, am180x, and am335x devices the CPPI 4.1 DMA
should NOT be used for the MUSB controller. Using this DMA
can cause the controller to lockup.
* Updated the defconfigs to set the use of PIO mode
* Added a patch to updated the PIO mode description to make it
easier to determine when it can be used.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-omapl138-psp_2.6.37: Add MACHINE_KERNEL_PR and fix white space issues.
* Add MACHINE_KERNEL_PR variable to enable future tweaks to this recipe.
* Convert tabs to whitespaces
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Add MACHINE_KERNEL_PR variable to enable future tweaks to this recipe.
* Convert tabs to whitespaces
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
machine config: Correct SERIAL_CONSOLE variable for am3517-evm and am37x-evm
* When testing on am37x-evm I noticed that no prompt to login was ever shown
when connected via serial port.
* I finally noticed that the SERIAL_CONSOLE variable was set incorrectly and
didn't match the value in the old Arago layer.
* After using the values specific in the machine file in the Arago layer I was
able to login via serial port.
* This has been verified on both the am37x-evm and am3517-evm.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* When testing on am37x-evm I noticed that no prompt to login was ever shown
when connected via serial port.
* I finally noticed that the SERIAL_CONSOLE variable was set incorrectly and
didn't match the value in the old Arago layer.
* After using the values specific in the machine file in the Arago layer I was
able to login via serial port.
* This has been verified on both the am37x-evm and am3517-evm.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
am335x-evm, omap3*: drop remaining TARGET_ARCH, wrecking sstate
Bump MACHINE_KERNEL_PR to rebuild the correct sstate.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Bump MACHINE_KERNEL_PR to rebuild the correct sstate.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
keystone: update defconfig with latest for mcsdk alpha7
Signed-off-by: Murali Karicheri <m-karicheri2@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Murali Karicheri <m-karicheri2@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
keystone: update kernel and bootloaders recipes for mcsdk alpha7 release
Signed-off-by: Murali Karicheri <m-karicheri2@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Murali Karicheri <m-karicheri2@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
keystone: boot-monitor: add initial recipe
This adds recipe to build boot monitor image. Boot monitor is
a standalone image that is loaded and executed from u-boot to
replace the RBL provided monitor code in ARM with Linux boot
specific code.
Signed-off-by: Murali Karicheri <m-karicheri2@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
This adds recipe to build boot monitor image. Boot monitor is
a standalone image that is loaded and executed from u-boot to
replace the RBL provided monitor code in ARM with Linux boot
specific code.
Signed-off-by: Murali Karicheri <m-karicheri2@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
multi-kernel.inc: drop use of KERNEL_CCSUFFIX to match oe-core
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
multi-kernel.inc: repeat do_configure after do_compileconfigs
Populate default defconfig into .config and process with oldconfig target
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Populate default defconfig into .config and process with oldconfig target
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beagleboard.conf: add additional sound modules
require for audio to function
Signed-off-by: Cliff Brake <cbrake@bec-systems.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
require for audio to function
Signed-off-by: Cliff Brake <cbrake@bec-systems.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux_3.1: add extra '#' to multi-line comment
Bitbake is getting more particular:
ERROR: There is a confusing multiline, partially commented expression on
line 27 of file /scratch/oe/oe-build-core-3/sources/meta-ti/...
Please clarify whether this is all a comment or should be parsed.
Signed-off-by: Cliff Brake <cbrake@bec-systems.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Bitbake is getting more particular:
ERROR: There is a confusing multiline, partially commented expression on
line 27 of file /scratch/oe/oe-build-core-3/sources/meta-ti/...
Please clarify whether this is all a comment or should be parsed.
Signed-off-by: Cliff Brake <cbrake@bec-systems.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-keystone: update to the latest dev release for keystone
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
u-boot: update to the latest dev release for keystone
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
netbase: fix file search path for 'interfaces' file
This .bbappend file is used to override the 'interfaces' file for certain
targets. The current version is broken in that it does not search the correct
path(s).
Thanks to Robert P. J. Day and Gary Thomas for spotting the issue and providing
patches.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
This .bbappend file is used to override the 'interfaces' file for certain
targets. The current version is broken in that it does not search the correct
path(s).
Thanks to Robert P. J. Day and Gary Thomas for spotting the issue and providing
patches.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
mesa-dri: update to 9.0.1 to match oe-core
this makes Cliff Brake's unapplied patch obsolete
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
this makes Cliff Brake's unapplied patch obsolete
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-keystone: update from version 3.6-rc6 to 3.6.6
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
keystone: bump MACHINE_KERNEL_PR for previous changes
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
keystone-evm: update serial port and virtual terminal settings
Keystone uses the old ttyS0 serial name instead of the new ttyO0.
Also disable spawning gettys on virtual terminals.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Keystone uses the old ttyS0 serial name instead of the new ttyO0.
Also disable spawning gettys on virtual terminals.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
conf/machine: omap4: update configs after xorg upgrade
There were some changes in the xserver-xorg upstream project that need
to be reflected here too:
* extmod module was removed completely as it became empty;
* DRI1, DRI2, DBE (among others) were made built-in;
(see poky rev: 5cea09e3d010d4799eab296b2a0cb83a0af09c76)
Signed-off-by: Nicolas Dechesne <n-dechesne@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
There were some changes in the xserver-xorg upstream project that need
to be reflected here too:
* extmod module was removed completely as it became empty;
* DRI1, DRI2, DBE (among others) were made built-in;
(see poky rev: 5cea09e3d010d4799eab296b2a0cb83a0af09c76)
Signed-off-by: Nicolas Dechesne <n-dechesne@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Revert "xf86-video-omap: add new recipe for OMAP4/5 X11 video driver"
This reverts commit 410dc026f2ee24a2346e7563a83f0181c79809cf.
Because this recipe was integrated in oe-core (then poky master).
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
This reverts commit 410dc026f2ee24a2346e7563a83f0181c79809cf.
Because this recipe was integrated in oe-core (then poky master).
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Revert "libdrm: enable omap experimental api support"
This reverts commit cce5a7aea905d2e2b167ab51b132ec43ed519a12.
Because oe-core (then poky master) was upgraded to libdrm 2.40,
and because OMAP experimental support was enabled there too.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
This reverts commit cce5a7aea905d2e2b167ab51b132ec43ed519a12.
Because oe-core (then poky master) was upgraded to libdrm 2.40,
and because OMAP experimental support was enabled there too.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
keystone-evm.conf: enable cpio images by default
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
u-boot: add version 2012.07 for keystone machines
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3: Verify pvrsrvkm module was found
* Check to see if the pvrsrvkm.ko module was found and that the insmod
for that module was successful.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Check to see if the pvrsrvkm.ko module was found and that the insmod
for that module was successful.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3: Adjust for non X11 distros
* Non X11 base distros are unable to build this Graphics SDK.
* This patch tweaks the libgles-omap3 include file to always build the
Graphics SDK in Raw mode and also build in X11 mode only if X11 is
a part of the DISTRO_FEATURE. Components are built, installed and packaged
based on which mode the Graphics SDK is built in.
* Create a new variable PVR_INIT that is by default set to pvrsrvinit. This is
needed for newer version of the Graphics SDK that replaced this file.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Non X11 base distros are unable to build this Graphics SDK.
* This patch tweaks the libgles-omap3 include file to always build the
Graphics SDK in Raw mode and also build in X11 mode only if X11 is
a part of the DISTRO_FEATURE. Components are built, installed and packaged
based on which mode the Graphics SDK is built in.
* Create a new variable PVR_INIT that is by default set to pvrsrvinit. This is
needed for newer version of the Graphics SDK that replaced this file.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
conf/machine: Update the FSTYPES for AMSDK machines
* Updated the IMAGE_FSTYPES to ubi and tar.gz for the AMSDK
machine types as the base file system type.
* This was done to speed up compression/decompression time at
the expense of file size.
Signed-off-by: Chase Maupin <Chase.Maupin@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Updated the IMAGE_FSTYPES to ubi and tar.gz for the AMSDK
machine types as the base file system type.
* This was done to speed up compression/decompression time at
the expense of file size.
Signed-off-by: Chase Maupin <Chase.Maupin@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-omap4-3.1.0: Add sched_process_exec tracing
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-omap-psp 2.6.37: add more recent version of OMAP3 kernel
Ported from Arago the kernel that corresponds to PSP version 04.02.00.07 with
corresponding SDK patches applied on top.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Ported from Arago the kernel that corresponds to PSP version 04.02.00.07 with
corresponding SDK patches applied on top.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-keystone: add kernel for keystone SOC
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
conf/machine: add keystone SOC and keystone-evm machine
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
tune-cortexa7: add tunes for ARM Cortex-A7
http://www.arm.com/products/processors/cortex-a/cortex-a7.php
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
http://www.arm.com/products/processors/cortex-a/cortex-a7.php
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
tune-cortexa15: add tunes for ARM Cortex-A15
http://www.arm.com/products/processors/cortex-a/cortex-a15.php
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
http://www.arm.com/products/processors/cortex-a/cortex-a15.php
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
pandaboard: use xf86-video-omap by default in XSERVER config
Also we need to pull in module-exa as xf86-video-omap relies
on it, at run time.
And replaced the default xorg.conf for 'omap4' machine to take
new driver into account. Do not enable HWcursor (e.g. mouse
using DSS overlay) to keep things simple for now..
Signed-off-by: Nicolas Dechesne <n-dechesne@ti.com>
Signed-off-by: Hervé Fache <h-fache@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Also we need to pull in module-exa as xf86-video-omap relies
on it, at run time.
And replaced the default xorg.conf for 'omap4' machine to take
new driver into account. Do not enable HWcursor (e.g. mouse
using DSS overlay) to keep things simple for now..
Signed-off-by: Nicolas Dechesne <n-dechesne@ti.com>
Signed-off-by: Hervé Fache <h-fache@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
xf86-video-omap: add new recipe for OMAP4/5 X11 video driver
Since this component is still actively being developed, let's use
a _git.bb recipe. We can introduce 'x.y' version later.
Even though xf-video-omap can be combined with private/restricted
EXA sub-driver for SGX/PVR, it can also work without it. In which
case EXA aren't using SGX, but all standard driver features still
work, and it is a replacement for xf-video-fbdev.
Signed-off-by: Nicolas Dechesne <n-dechesne@ti.com>
Signed-off-by: Hervé Fache <h-fache@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Since this component is still actively being developed, let's use
a _git.bb recipe. We can introduce 'x.y' version later.
Even though xf-video-omap can be combined with private/restricted
EXA sub-driver for SGX/PVR, it can also work without it. In which
case EXA aren't using SGX, but all standard driver features still
work, and it is a replacement for xf-video-fbdev.
Signed-off-by: Nicolas Dechesne <n-dechesne@ti.com>
Signed-off-by: Hervé Fache <h-fache@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libdrm: enable omap experimental api support
This is needed to build gst-plugin-ducati.
Signed-off-by: Enrico Butera <ebutera@users.berlios.de>
Signed-off-by: Nicolas Dechesne <n-dechesne@ti.com>
Signed-off-by: Hervé Fache <h-fache@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
This is needed to build gst-plugin-ducati.
Signed-off-by: Enrico Butera <ebutera@users.berlios.de>
Signed-off-by: Nicolas Dechesne <n-dechesne@ti.com>
Signed-off-by: Hervé Fache <h-fache@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-omap4: update to 3.4 from GLP 1.6.6 release
Used Herve's version as a base with some mods from Enrico and additional fixes
on top, defconfig is the validated one from GLP release.
Signed-off-by: Hervé Fache <h-fache@ti.com>
Cc: Enrico Butera <ebutera@users.berlios.de>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Used Herve's version as a base with some mods from Enrico and additional fixes
on top, defconfig is the validated one from GLP release.
Signed-off-by: Hervé Fache <h-fache@ti.com>
Cc: Enrico Butera <ebutera@users.berlios.de>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-am335x-3.2.0-psp04.06.00.08: Add PSP v04.06.00.08 of the Linux kernel
* Add the PSP release version of the Linux kernel for the am335x-evm
* Include a variable called KERNEL_PATCHES which can be used to add
patches on top of the PSP release of the Linux kernel. Currently used
to apply various patches that add functionality or fixes bugs.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Add the PSP release version of the Linux kernel for the am335x-evm
* Include a variable called KERNEL_PATCHES which can be used to add
patches on top of the PSP release of the Linux kernel. Currently used
to apply various patches that add functionality or fixes bugs.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
recipes: Fix ti-eula-unpack issue. Tweak sgx modules and libgles recipes.
* Commit d8fc4a686262c50fd0053afa7240020909ec430b addressed an issue where
too many newlines characters were being sent since print by default already
sends a newline character. This commit however resulted in bin files being
installed in the WORKDIR and broke other recipes which commit
a94f765b9867abefd5f0bd262b5dddb8782b3187 addressed. This lead to a very
cluttered WORKDIR.
* This patch updates ti-eula-unpack.inc to switch from using a print to a write.
Since write doesn't automatically send newlines it is a bit more obvious when
newlines are sent.
* Part of the reason that bin files were being installed in the WORKDIR was
due to TI_BIN_UNPK_WDEXT being blank for some recipes. For instance in the
libgles-omap3 recipes, when the workdir command is set in TI_BIN_UNPK_CMDS the
directory that the Graphics SDK will be installed into is
workdir+TI_BIN_UNPK_WDEXT. A blank TI_BIN_UNPK_WDEXT means the SDK will be
installed in WORKDIR. By setting TI_BIN_UNPK_WDEXT to a proper value the
recipes can be sure it is installed in the proper directory.
* Determine which file to download based on the defined BINFILE and not a
hardcoded value. This idea was taken from arago.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Acked-by: Chase Maupin <chase.maupin@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Commit d8fc4a686262c50fd0053afa7240020909ec430b addressed an issue where
too many newlines characters were being sent since print by default already
sends a newline character. This commit however resulted in bin files being
installed in the WORKDIR and broke other recipes which commit
a94f765b9867abefd5f0bd262b5dddb8782b3187 addressed. This lead to a very
cluttered WORKDIR.
* This patch updates ti-eula-unpack.inc to switch from using a print to a write.
Since write doesn't automatically send newlines it is a bit more obvious when
newlines are sent.
* Part of the reason that bin files were being installed in the WORKDIR was
due to TI_BIN_UNPK_WDEXT being blank for some recipes. For instance in the
libgles-omap3 recipes, when the workdir command is set in TI_BIN_UNPK_CMDS the
directory that the Graphics SDK will be installed into is
workdir+TI_BIN_UNPK_WDEXT. A blank TI_BIN_UNPK_WDEXT means the SDK will be
installed in WORKDIR. By setting TI_BIN_UNPK_WDEXT to a proper value the
recipes can be sure it is installed in the proper directory.
* Determine which file to download based on the defined BINFILE and not a
hardcoded value. This idea was taken from arago.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Acked-by: Chase Maupin <chase.maupin@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
u-boot_2011.09-psp04.06.00.08: Add PSP v04.06.00.08 of u-boot
* Add the PSP release version 04.06.00.08 of u-boot.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Add the PSP release version 04.06.00.08 of u-boot.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3.inc: Tweak PLATFORM variable.
* Newer versions of libgles-omap3 utilize a different PLATFORM value. This
patch allows the PLATFORM variable to be easily overridden if needed.
* Replace the hardcoded usage of LinuxOMAP3 with the PLATFORM variable.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Newer versions of libgles-omap3 utilize a different PLATFORM value. This
patch allows the PLATFORM variable to be easily overridden if needed.
* Replace the hardcoded usage of LinuxOMAP3 with the PLATFORM variable.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
ti-hw-bringup-image: remove duplicate timestamp-service, as it's in systemd-image
Since systemd-image from meta-angstrom already includes timestamp-service, remove
the duplicate from ti-hw-bringup-image recipe, which uses the former as a base.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Since systemd-image from meta-angstrom already includes timestamp-service, remove
the duplicate from ti-hw-bringup-image recipe, which uses the former as a base.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
layer.conf: lower layer priority from 10 to 6
Lowering layer priority from 10 to 6 aligns meta-ti with other BSP layers
and also allows distributions to override our recipes.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Lowering layer priority from 10 to 6 aligns meta-ti with other BSP layers
and also allows distributions to override our recipes.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3: fix for latest oe-core mesa changes
* add virtual/libgles1 virtual/libgles2 to PROVIDES
* add RREPLACES_{PN}* for mesa's libegl* libgles1* libgles2*
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* add virtual/libgles1 virtual/libgles2 to PROVIDES
* add RREPLACES_{PN}* for mesa's libegl* libgles1* libgles2*
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
mesa: add appends to avoid providing conflicts
For libgles-omap3 compatible machines mesa should only provide libgl.
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Rebased to squash removal of mesa-xlib.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
For libgles-omap3 compatible machines mesa should only provide libgl.
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Rebased to squash removal of mesa-xlib.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beaglebone-tester: FTDI eeprom test, v2
Check descriptor instead of VID/PID
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Check descriptor instead of VID/PID
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beaglebone tester: bump SRCREV for FTDI test
An extra test for the FTDI eeprom was added to catch programming errors that would break CCS.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
An extra test for the FTDI eeprom was added to catch programming errors that would break CCS.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beaglebone-tester: ship testaudio, fix depends
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: update beaglebone defconfig
* Add more RTC modules
* Disable cgroup controllers with a lot of overhead
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Add more RTC modules
* Disable cgroup controllers with a lot of overhead
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-mainline: update to 3.2.28
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: update to 3.2.28 and add motorcape support
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti335x-psp 3.2: mux orientation detect for camera sensor to gpio instead of gpmc
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: update to 3.2.25
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: LCD7 A3 support, eMMC cape support, camera cape improvements
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
recipes: Use 'packagegroup' instead of 'task'
bring recipes in sync with OE-Core, task bbclass
is now replaced by packagegroup.
and task recipes are now called packagegroup_something
Signed-off-by: Khem Raj <raj.khem@gmail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
bring recipes in sync with OE-Core, task bbclass
is now replaced by packagegroup.
and task recipes are now called packagegroup_something
Signed-off-by: Khem Raj <raj.khem@gmail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
u-boot_2011.09[.10rc]: Always use gnu ld for LD
- Pull in gnu ld patch for 2011.10rc recipe
- Bump PR
Signed-off-by: Roger Monk <r-monk@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
- Pull in gnu ld patch for 2011.10rc recipe
- Bump PR
Signed-off-by: Roger Monk <r-monk@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
u-boot 2011.09+git: update to latest version of Tom Rini's tree
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
ti-dmai.inc: fix 'proto='-warning on recipe parsing
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
am-sysinfo: switch 'proto' to 'protocol' in SRC_URI
Signed-off-by: Roger Monk <r-monk@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Roger Monk <r-monk@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
gstreamer-ti: convert proto to protocol in SRC_URI
Signed-off-by: Roger Monk <r-monk@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Roger Monk <r-monk@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: update to 3.2.23
Regenerate all beaglebone patches and add one vfs tracer patch for powertop
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Regenerate all beaglebone patches and add one vfs tracer patch for powertop
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: enable more tracing features for beaglebone
This makes powertop 2.0 happy
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
This makes powertop 2.0 happy
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: add fixed for cssp, fbset and OPP50
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
u-boot 2011.09+git: update to latest version of Tom Rini's tree
All patches have been rediffed and boot tested
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
All patches have been rediffed and boot tested
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: add support for audio cape and disable LBO gpio for battery cape
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: add camera driver for beaglebone
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beaglebone-capes: use backlight hack for all LCD4 variants
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: fix audio/spidev clash on beaglebone
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: update to 3.2.21, add libertas fixes
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beaglebone-tester: re-enable pmic test
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beaglebone-tester: bump SRCREV to fix serial console race
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
netbase: follow oe-core to v5.0
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux.inc: remove unused variable RPSRC
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux.inc: remove require linux-tools.inc
linux-tools.inc was removed in oe-core (perf has own package) [1].
[1] http://cgit.openembedded.org/openembedded-core/commit/?id=b485f3e0e55ad62079ed0913970ff0620f4808ea
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-tools.inc was removed in oe-core (perf has own package) [1].
[1] http://cgit.openembedded.org/openembedded-core/commit/?id=b485f3e0e55ad62079ed0913970ff0620f4808ea
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beaglebone-tester: bump SRCREV to fix failure reporting
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: turn on CONFIG_USB_SUSPEND to fix usb mass storage
Many thanks to Arkadiusz Karas <arkkar13@googlemail.com> for figuring that out
and sharing the info.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Many thanks to Arkadiusz Karas <arkkar13@googlemail.com> for figuring that out
and sharing the info.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beaglebone-capes: add support for weatherstation cape
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beaglebone-capes: add support for 4.3" LCD cape
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: backport PM and USB fixes from PSP
The complete patchset will get rebased to the tip of the PSP tree soon, but the
conflicts take a lot of time to resolve.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
The complete patchset will get rebased to the tip of the PSP tree soon, but the
conflicts take a lot of time to resolve.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: fix buttons on LCD capes
One patch to add button layout for the a1 revision of the 3.5" LCD cape and
another patch to stop spidev from loading when SPI1_D1 is used as gpio
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
One patch to add button layout for the a1 revision of the 3.5" LCD cape and
another patch to stop spidev from loading when SPI1_D1 is used as gpio
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp: enable TSL2550 driver for beaglebone weatherstation cape
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: switch ADC to 16x averaging, disable 275MHz, add 4.3" LCD support
* The switch to 16x averaging is done to combat the excessive noise in the
signal. It's still *very* bad, but the TS cursor jitter has decreased a bit
* The OPP for 275MHz was disabled due to all the errata. Both the EMIF and MUSB
don't seem to like that OPP.
* The resistive touch version of the 4.3" LCD cape is supported in 24 bit mode.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* The switch to 16x averaging is done to combat the excessive noise in the
signal. It's still *very* bad, but the TS cursor jitter has decreased a bit
* The OPP for 275MHz was disabled due to all the errata. Both the EMIF and MUSB
don't seem to like that OPP.
* The resistive touch version of the 4.3" LCD cape is supported in 24 bit mode.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-mainline 3.2.18: build in usbhid and tsc2007 and run 'make oldconfig'
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: set PV accordingly, when not using tipspkernel
The patchset in PATCHES_OVER_PSP updates the kernel to 3.2.x, so make PV match.
This doesn't need PR or MACHINE_KERNEL_PR bumps since both the kernel ABI and
file locations remain the same.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Acked-by: Koen Kooi <koen@circuitco.com>
The patchset in PATCHES_OVER_PSP updates the kernel to 3.2.x, so make PV match.
This doesn't need PR or MACHINE_KERNEL_PR bumps since both the kernel ABI and
file locations remain the same.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Acked-by: Koen Kooi <koen@circuitco.com>
tipspkernel: add extra level to FILESPATH with major version in the name
Add PMV variable to contain major version by extracting first 2 numbers from PV
Insert new level to FILESPATH - PN-PV-PR:PN-PV:PN-PMV:PN:files:.
Allow keeping patches and configs generic for the series (i.e. 3.2) while
incrementing stable releases (i.e. 3.2.18)
Drop use of BP and BPN, as they don't change for the kernel
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Acked-by: Koen Kooi <koen@circuitco.com>
Add PMV variable to contain major version by extracting first 2 numbers from PV
Insert new level to FILESPATH - PN-PV-PR:PN-PV:PN-PMV:PN:files:.
Allow keeping patches and configs generic for the series (i.e. 3.2) while
incrementing stable releases (i.e. 3.2.18)
Drop use of BP and BPN, as they don't change for the kernel
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Acked-by: Koen Kooi <koen@circuitco.com>
linux-ti33x-psp 3.2: fix pin free check once and for all
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>