glsdk/meta-ti-glsdk.git
9 years agolinux-omap-psp 2.6.37: add more recent version of OMAP3 kernel
Denys Dmytriyenko [Fri, 2 Nov 2012 02:50:53 +0000 (22:50 -0400)]
linux-omap-psp 2.6.37: add more recent version of OMAP3 kernel

Ported from Arago the kernel that corresponds to PSP version 04.02.00.07 with
corresponding SDK patches applied on top.

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-keystone: add kernel for keystone SOC
Denys Dmytriyenko [Fri, 2 Nov 2012 00:44:13 +0000 (20:44 -0400)]
linux-keystone: add kernel for keystone SOC

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agoconf/machine: add keystone SOC and keystone-evm machine
Denys Dmytriyenko [Fri, 2 Nov 2012 00:43:07 +0000 (20:43 -0400)]
conf/machine: add keystone SOC and keystone-evm machine

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agotune-cortexa7: add tunes for ARM Cortex-A7
Denys Dmytriyenko [Thu, 18 Oct 2012 22:28:06 +0000 (18:28 -0400)]
tune-cortexa7: add tunes for ARM Cortex-A7

http://www.arm.com/products/processors/cortex-a/cortex-a7.php

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agotune-cortexa15: add tunes for ARM Cortex-A15
Denys Dmytriyenko [Thu, 18 Oct 2012 22:27:27 +0000 (18:27 -0400)]
tune-cortexa15: add tunes for ARM Cortex-A15

http://www.arm.com/products/processors/cortex-a/cortex-a15.php

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agopandaboard: use xf86-video-omap by default in XSERVER config
Nicolas Dechesne [Fri, 19 Oct 2012 13:51:26 +0000 (15:51 +0200)]
pandaboard: use xf86-video-omap by default in XSERVER config

Also we need to pull in module-exa as xf86-video-omap relies
on it, at run time.

And replaced the default xorg.conf for 'omap4' machine to take
new driver into account. Do not enable HWcursor (e.g. mouse
using DSS overlay) to keep things simple for now..

Signed-off-by: Nicolas Dechesne <n-dechesne@ti.com>
Signed-off-by: Hervé Fache <h-fache@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agoxf86-video-omap: add new recipe for OMAP4/5 X11 video driver
Nicolas Dechesne [Fri, 19 Oct 2012 13:51:25 +0000 (15:51 +0200)]
xf86-video-omap: add new recipe for OMAP4/5 X11 video driver

Since this component is still actively being developed, let's use
a _git.bb recipe. We can introduce 'x.y' version later.

Even though xf-video-omap can be combined with private/restricted
EXA sub-driver for SGX/PVR, it can also work without it. In which
case EXA aren't using SGX, but all standard driver features still
work, and it is a replacement for xf-video-fbdev.

Signed-off-by: Nicolas Dechesne <n-dechesne@ti.com>
Signed-off-by: Hervé Fache <h-fache@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolibdrm: enable omap experimental api support
Enrico Butera [Fri, 19 Oct 2012 13:51:24 +0000 (15:51 +0200)]
libdrm: enable omap experimental api support

This is needed to build gst-plugin-ducati.

Signed-off-by: Enrico Butera <ebutera@users.berlios.de>
Signed-off-by: Nicolas Dechesne <n-dechesne@ti.com>
Signed-off-by: Hervé Fache <h-fache@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-omap4: update to 3.4 from GLP 1.6.6 release
Hervé Fache [Fri, 5 Oct 2012 12:57:42 +0000 (14:57 +0200)]
linux-omap4: update to 3.4 from GLP 1.6.6 release

Used Herve's version as a base with some mods from Enrico and additional fixes
on top, defconfig is the validated one from GLP release.

Signed-off-by: Hervé Fache <h-fache@ti.com>
Cc: Enrico Butera <ebutera@users.berlios.de>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-am335x-3.2.0-psp04.06.00.08: Add PSP v04.06.00.08 of the Linux kernel
Franklin S. Cooper Jr [Fri, 12 Oct 2012 05:14:45 +0000 (00:14 -0500)]
linux-am335x-3.2.0-psp04.06.00.08: Add PSP v04.06.00.08 of the Linux kernel

* Add the PSP release version of the Linux kernel for the am335x-evm
* Include a variable called KERNEL_PATCHES which can be used to add
  patches on top of the PSP release of the Linux kernel. Currently used
  to apply various patches that add functionality or fixes bugs.

Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agorecipes: Fix ti-eula-unpack issue. Tweak sgx modules and libgles recipes.
Franklin S. Cooper Jr [Sat, 1 Sep 2012 17:45:03 +0000 (12:45 -0500)]
recipes: Fix ti-eula-unpack issue. Tweak sgx modules and libgles recipes.

* Commit d8fc4a686262c50fd0053afa7240020909ec430b addressed an issue where
  too many newlines characters were being sent since print by default already
  sends a newline character. This commit however resulted in bin files being
  installed in the WORKDIR and broke other recipes which commit
  a94f765b9867abefd5f0bd262b5dddb8782b3187 addressed. This lead to a very
  cluttered WORKDIR.
* This patch updates ti-eula-unpack.inc to switch from using a print to a write.
  Since write doesn't automatically send newlines it is a bit more obvious when
  newlines are sent.
* Part of the reason that bin files were being installed in the WORKDIR was
  due to TI_BIN_UNPK_WDEXT being blank for some recipes. For instance in the
  libgles-omap3 recipes, when the workdir command is set in TI_BIN_UNPK_CMDS the
  directory that the Graphics SDK will be installed into is
  workdir+TI_BIN_UNPK_WDEXT. A blank TI_BIN_UNPK_WDEXT means the SDK will be
  installed in WORKDIR. By setting TI_BIN_UNPK_WDEXT to a proper value the
  recipes can be sure it is installed in the proper directory.
* Determine which file to download based on the defined BINFILE and not a
  hardcoded value. This idea was taken from arago.

Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Acked-by: Chase Maupin <chase.maupin@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agou-boot_2011.09-psp04.06.00.08: Add PSP v04.06.00.08 of u-boot
Franklin S. Cooper Jr [Fri, 5 Oct 2012 05:07:28 +0000 (00:07 -0500)]
u-boot_2011.09-psp04.06.00.08: Add PSP v04.06.00.08 of u-boot

* Add the PSP release version 04.06.00.08 of u-boot.

Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolibgles-omap3.inc: Tweak PLATFORM variable.
Franklin S. Cooper Jr [Fri, 31 Aug 2012 23:19:57 +0000 (18:19 -0500)]
libgles-omap3.inc: Tweak PLATFORM variable.

* Newer versions of libgles-omap3 utilize a different PLATFORM value. This
  patch allows the PLATFORM variable to be easily overridden if needed.
* Replace the hardcoded usage of LinuxOMAP3 with the PLATFORM variable.

Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agoti-hw-bringup-image: remove duplicate timestamp-service, as it's in systemd-image
Denys Dmytriyenko [Fri, 14 Sep 2012 04:57:22 +0000 (00:57 -0400)]
ti-hw-bringup-image: remove duplicate timestamp-service, as it's in systemd-image

Since systemd-image from meta-angstrom already includes timestamp-service, remove
the duplicate from ti-hw-bringup-image recipe, which uses the former as a base.

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolayer.conf: lower layer priority from 10 to 6
Denys Dmytriyenko [Fri, 14 Sep 2012 04:40:55 +0000 (00:40 -0400)]
layer.conf: lower layer priority from 10 to 6

Lowering layer priority from 10 to 6 aligns meta-ti with other BSP layers
and also allows distributions to override our recipes.

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolibgles-omap3: fix for latest oe-core mesa changes
Andreas Müller [Tue, 4 Sep 2012 16:20:58 +0000 (18:20 +0200)]
libgles-omap3: fix for latest oe-core mesa changes

* add virtual/libgles1 virtual/libgles2 to PROVIDES
* add RREPLACES_{PN}* for mesa's libegl* libgles1* libgles2*

Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agomesa: add appends to avoid providing conflicts
Andreas Müller [Tue, 4 Sep 2012 16:20:57 +0000 (18:20 +0200)]
mesa: add appends to avoid providing conflicts

For libgles-omap3 compatible machines mesa should only provide libgl.

Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Rebased to squash removal of mesa-xlib.

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agobeaglebone-tester: FTDI eeprom test, v2
Koen Kooi [Sat, 1 Sep 2012 11:46:43 +0000 (13:46 +0200)]
beaglebone-tester: FTDI eeprom test, v2

Check descriptor instead of VID/PID

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agobeaglebone tester: bump SRCREV for FTDI test
Koen Kooi [Fri, 31 Aug 2012 07:16:45 +0000 (09:16 +0200)]
beaglebone tester: bump SRCREV for FTDI test

An extra test for the FTDI eeprom was added to catch programming errors that would break CCS.

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agobeaglebone-tester: ship testaudio, fix depends
Koen Kooi [Sun, 12 Aug 2012 08:11:12 +0000 (10:11 +0200)]
beaglebone-tester: ship testaudio, fix depends

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: update beaglebone defconfig
Koen Kooi [Thu, 30 Aug 2012 07:56:13 +0000 (09:56 +0200)]
linux-ti33x-psp 3.2: update beaglebone defconfig

* Add more RTC modules
* Disable cgroup controllers with a lot of overhead

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-mainline: update to 3.2.28
Koen Kooi [Fri, 24 Aug 2012 07:20:38 +0000 (09:20 +0200)]
linux-mainline: update to 3.2.28

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: update to 3.2.28 and add motorcape support
Koen Kooi [Wed, 22 Aug 2012 12:29:17 +0000 (14:29 +0200)]
linux-ti33x-psp 3.2: update to 3.2.28 and add motorcape support

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti335x-psp 3.2: mux orientation detect for camera sensor to gpio instead of...
Koen Kooi [Thu, 16 Aug 2012 09:18:35 +0000 (11:18 +0200)]
linux-ti335x-psp 3.2: mux orientation detect for camera sensor to gpio instead of gpmc

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: update to 3.2.25
Koen Kooi [Wed, 8 Aug 2012 08:41:23 +0000 (10:41 +0200)]
linux-ti33x-psp 3.2: update to 3.2.25

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: LCD7 A3 support, eMMC cape support, camera cape improvements
Koen Kooi [Mon, 30 Jul 2012 18:41:14 +0000 (20:41 +0200)]
linux-ti33x-psp 3.2: LCD7 A3 support, eMMC cape support, camera cape improvements

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agorecipes: Use 'packagegroup' instead of 'task'
Khem Raj [Sun, 9 Sep 2012 17:07:47 +0000 (10:07 -0700)]
recipes: Use 'packagegroup' instead of 'task'

bring recipes in sync with OE-Core, task bbclass
is now replaced by packagegroup.

and task recipes are now called packagegroup_something

Signed-off-by: Khem Raj <raj.khem@gmail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agou-boot_2011.09[.10rc]: Always use gnu ld for LD
Roger Monk [Fri, 3 Aug 2012 22:20:08 +0000 (23:20 +0100)]
u-boot_2011.09[.10rc]: Always use gnu ld for LD

   - Pull in gnu ld patch for 2011.10rc recipe
   - Bump PR

Signed-off-by: Roger Monk <r-monk@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agou-boot 2011.09+git: update to latest version of Tom Rini's tree
Koen Kooi [Thu, 26 Jul 2012 10:40:43 +0000 (12:40 +0200)]
u-boot 2011.09+git: update to latest version of Tom Rini's tree

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agoti-dmai.inc: fix 'proto='-warning on recipe parsing
Andreas Müller [Wed, 1 Aug 2012 09:35:48 +0000 (11:35 +0200)]
ti-dmai.inc: fix 'proto='-warning on recipe parsing

Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agoam-sysinfo: switch 'proto' to 'protocol' in SRC_URI
Roger Monk [Thu, 19 Jul 2012 12:52:19 +0000 (13:52 +0100)]
am-sysinfo: switch 'proto' to 'protocol' in SRC_URI

Signed-off-by: Roger Monk <r-monk@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agogstreamer-ti: convert proto to protocol in SRC_URI
Roger Monk [Thu, 19 Jul 2012 12:49:01 +0000 (13:49 +0100)]
gstreamer-ti: convert proto to protocol in SRC_URI

Signed-off-by: Roger Monk <r-monk@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: update to 3.2.23
Koen Kooi [Tue, 17 Jul 2012 07:23:14 +0000 (09:23 +0200)]
linux-ti33x-psp 3.2: update to 3.2.23

Regenerate all beaglebone patches and add one vfs tracer patch for powertop

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: enable more tracing features for beaglebone
Koen Kooi [Sat, 14 Jul 2012 13:38:07 +0000 (15:38 +0200)]
linux-ti33x-psp 3.2: enable more tracing features for beaglebone

This makes powertop 2.0 happy

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: add fixed for cssp, fbset and OPP50
Koen Kooi [Fri, 13 Jul 2012 10:19:44 +0000 (12:19 +0200)]
linux-ti33x-psp 3.2: add fixed for cssp, fbset and OPP50

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agou-boot 2011.09+git: update to latest version of Tom Rini's tree
Koen Kooi [Wed, 11 Jul 2012 09:53:27 +0000 (11:53 +0200)]
u-boot 2011.09+git: update to latest version of Tom Rini's tree

All patches have been rediffed and boot tested

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: add support for audio cape and disable LBO gpio for battery...
Koen Kooi [Wed, 4 Jul 2012 05:58:33 +0000 (07:58 +0200)]
linux-ti33x-psp 3.2: add support for audio cape and disable LBO gpio for battery cape

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: add camera driver for beaglebone
Koen Kooi [Mon, 2 Jul 2012 04:22:09 +0000 (06:22 +0200)]
linux-ti33x-psp 3.2: add camera driver for beaglebone

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agobeaglebone-capes: use backlight hack for all LCD4 variants
Koen Kooi [Thu, 28 Jun 2012 09:53:55 +0000 (11:53 +0200)]
beaglebone-capes: use backlight hack for all LCD4 variants

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: fix audio/spidev clash on beaglebone
Koen Kooi [Tue, 26 Jun 2012 07:47:54 +0000 (09:47 +0200)]
linux-ti33x-psp 3.2: fix audio/spidev clash on beaglebone

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: update to 3.2.21, add libertas fixes
Koen Kooi [Wed, 20 Jun 2012 10:42:22 +0000 (12:42 +0200)]
linux-ti33x-psp 3.2: update to 3.2.21, add libertas fixes

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agobeaglebone-tester: re-enable pmic test
Koen Kooi [Thu, 14 Jun 2012 22:07:20 +0000 (00:07 +0200)]
beaglebone-tester: re-enable pmic test

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agobeaglebone-tester: bump SRCREV to fix serial console race
Koen Kooi [Fri, 8 Jun 2012 14:37:46 +0000 (16:37 +0200)]
beaglebone-tester: bump SRCREV to fix serial console race

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agonetbase: follow oe-core to v5.0
Andreas Müller [Mon, 9 Jul 2012 12:35:36 +0000 (14:35 +0200)]
netbase: follow oe-core to v5.0

Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux.inc: remove unused variable RPSRC
Andreas Müller [Thu, 21 Jun 2012 23:19:38 +0000 (01:19 +0200)]
linux.inc: remove unused variable RPSRC

Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux.inc: remove require linux-tools.inc
Andreas Müller [Thu, 21 Jun 2012 23:19:37 +0000 (01:19 +0200)]
linux.inc: remove require linux-tools.inc

linux-tools.inc was removed in oe-core (perf has own package) [1].

[1] http://cgit.openembedded.org/openembedded-core/commit/?id=b485f3e0e55ad62079ed0913970ff0620f4808ea

Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agobeaglebone-tester: bump SRCREV to fix failure reporting
Koen Kooi [Fri, 8 Jun 2012 09:37:44 +0000 (11:37 +0200)]
beaglebone-tester: bump SRCREV to fix failure reporting

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: turn on CONFIG_USB_SUSPEND to fix usb mass storage
Koen Kooi [Thu, 7 Jun 2012 15:40:45 +0000 (17:40 +0200)]
linux-ti33x-psp 3.2: turn on CONFIG_USB_SUSPEND to fix usb mass storage

Many thanks to Arkadiusz Karas <arkkar13@googlemail.com> for figuring that out
and sharing the info.

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agobeaglebone-capes: add support for weatherstation cape
Koen Kooi [Thu, 7 Jun 2012 15:40:44 +0000 (17:40 +0200)]
beaglebone-capes: add support for weatherstation cape

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agobeaglebone-capes: add support for 4.3" LCD cape
Koen Kooi [Thu, 7 Jun 2012 15:40:43 +0000 (17:40 +0200)]
beaglebone-capes: add support for 4.3" LCD cape

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: backport PM and USB fixes from PSP
Koen Kooi [Thu, 7 Jun 2012 15:40:42 +0000 (17:40 +0200)]
linux-ti33x-psp 3.2: backport PM and USB fixes from PSP

The complete patchset will get rebased to the tip of the PSP tree soon, but the
conflicts take a lot of time to resolve.

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: fix buttons on LCD capes
Koen Kooi [Thu, 7 Jun 2012 15:40:41 +0000 (17:40 +0200)]
linux-ti33x-psp 3.2: fix buttons on LCD capes

One patch to add button layout for the a1 revision of the 3.5" LCD cape and
another patch to stop spidev from loading when SPI1_D1 is used as gpio

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp: enable TSL2550 driver for beaglebone weatherstation cape
Koen Kooi [Thu, 7 Jun 2012 15:40:40 +0000 (17:40 +0200)]
linux-ti33x-psp: enable TSL2550 driver for beaglebone weatherstation cape

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: switch ADC to 16x averaging, disable 275MHz, add 4.3" LCD support
Koen Kooi [Thu, 7 Jun 2012 15:40:39 +0000 (17:40 +0200)]
linux-ti33x-psp 3.2: switch ADC to 16x averaging, disable 275MHz, add 4.3" LCD support

* The switch to 16x averaging is done to combat the excessive noise in the
  signal. It's still *very* bad, but the TS cursor jitter has decreased a bit
* The OPP for 275MHz was disabled due to all the errata. Both the EMIF and MUSB
  don't seem to like that OPP.
* The resistive touch version of the 4.3" LCD cape is supported in 24 bit mode.

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-mainline 3.2.18: build in usbhid and tsc2007 and run 'make oldconfig'
Koen Kooi [Tue, 29 May 2012 07:42:19 +0000 (09:42 +0200)]
linux-mainline 3.2.18: build in usbhid and tsc2007 and run 'make oldconfig'

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: set PV accordingly, when not using tipspkernel
Denys Dmytriyenko [Wed, 30 May 2012 22:14:14 +0000 (18:14 -0400)]
linux-ti33x-psp 3.2: set PV accordingly, when not using tipspkernel

The patchset in PATCHES_OVER_PSP updates the kernel to 3.2.x, so make PV match.
This doesn't need PR or MACHINE_KERNEL_PR bumps since both the kernel ABI and
file locations remain the same.

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Acked-by: Koen Kooi <koen@circuitco.com>
10 years agotipspkernel: add extra level to FILESPATH with major version in the name
Denys Dmytriyenko [Wed, 30 May 2012 22:01:41 +0000 (18:01 -0400)]
tipspkernel: add extra level to FILESPATH with major version in the name

Add PMV variable to contain major version by extracting first 2 numbers from PV
Insert new level to FILESPATH - PN-PV-PR:PN-PV:PN-PMV:PN:files:.
Allow keeping patches and configs generic for the series (i.e. 3.2) while
incrementing stable releases (i.e. 3.2.18)
Drop use of BP and BPN, as they don't change for the kernel

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Acked-by: Koen Kooi <koen@circuitco.com>
10 years agolinux-ti33x-psp 3.2: fix pin free check once and for all
Koen Kooi [Wed, 23 May 2012 16:05:58 +0000 (18:05 +0200)]
linux-ti33x-psp 3.2: fix pin free check once and for all

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: sgx fix from PSP + dvi cape audio fix
Koen Kooi [Wed, 23 May 2012 14:18:16 +0000 (16:18 +0200)]
linux-ti33x-psp 3.2: sgx fix from PSP + dvi cape audio fix

Also move more things to modules to speed up boot.

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: update to 3.2.18
Koen Kooi [Wed, 23 May 2012 09:20:07 +0000 (11:20 +0200)]
linux-ti33x-psp 3.2: update to 3.2.18

Duplicate patches between PSP and 3.2.17 have been dropped from the 3.2.17 series

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: i2c and cape fixes
Koen Kooi [Tue, 22 May 2012 12:42:55 +0000 (14:42 +0200)]
linux-ti33x-psp 3.2: i2c and cape fixes

* Fix I2C prescaler to run at full speed instead of 1/4 speed
* fix led/spidev/w1 check
* move RS232 cape to ttyO2

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-mainline: Add patches to enable libertas firmware loading asynchronously
Andreas Müller [Fri, 25 May 2012 09:11:57 +0000 (11:11 +0200)]
linux-mainline: Add patches to enable libertas firmware loading asynchronously

When using udev >=177 libertas driver does not load properly the firmware [1].
The patches 0001-0016 were taken from [2] and can be viewed at [3]. Patch 0017
I created to fix compiler complaining for missing symbol is_interrupt when
DEBUG set.
The patch series was tested with meta-gumstix on overo with udev-175 and
udev-182.

[1] http://www.spinics.net/lists/linux-wireless/msg85541.html
[2] git://git.kernel.org/pub/scm/linux/kernel/git/linville/wireless-next.git
[3] http://git.kernel.org/?p=linux/kernel/git/linville/wireless-next.git;a=history;f=drivers/net/wireless/libertas;hb=HEAD

Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-mainline: update to 3.2.18
Koen Kooi [Wed, 23 May 2012 11:57:15 +0000 (13:57 +0200)]
linux-mainline: update to 3.2.18

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agoti-hw-bringup-image: disable sdcard image class
Koen Kooi [Fri, 25 May 2012 07:31:47 +0000 (09:31 +0200)]
ti-hw-bringup-image: disable sdcard image class

The class breaks with the current genext2fs in oe-core.

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: merge in 6 musb patches from PSP
Koen Kooi [Tue, 22 May 2012 06:06:26 +0000 (08:06 +0200)]
linux-ti33x-psp 3.2: merge in 6 musb patches from PSP

Updating the SRCREV would require redoing all boardfile patches due to the
EVM-SK changes. So cherry-pick the 6 patches we need.

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti335x-psp 3.2: cape enhancements and patch cleanups
Koen Kooi [Tue, 22 May 2012 06:06:25 +0000 (08:06 +0200)]
linux-ti335x-psp 3.2: cape enhancements and patch cleanups

* add support for revision A2 of the 7" Beagleboardtoys cape
* allow capes to disable w1-gpio
* add stub for the Beagleboardtoys camera cape
* Fill in more entries in the am335x mux table
* switch to 4x oversampling in the tsadc driver to reduce jitter (or cursor hula
  dancing as Gerald describes it)
* Add a function to set the pinmux from the eeprom data instead of the boardfile
* Add support for the Bebopr cape

All beaglebone patches have been rediffed and renumbered to avoid confusion

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: silence useless omap4 hwmod warning
Koen Kooi [Tue, 22 May 2012 06:06:24 +0000 (08:06 +0200)]
linux-ti33x-psp 3.2: silence useless omap4 hwmod warning

This fixes the last remaining debug print shown when booting with 'quiet'

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: demote cpsw PHY message to INFO
Koen Kooi [Thu, 17 May 2012 10:07:06 +0000 (12:07 +0200)]
linux-ti33x-psp 3.2: demote cpsw PHY message to INFO

This keeps them from appearing on the screen during quiet boots. They are still
being reported, so no info is lost.

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agobeaglebone-capes: add a powerdown script as well
Koen Kooi [Fri, 18 May 2012 14:11:39 +0000 (16:11 +0200)]
beaglebone-capes: add a powerdown script as well

The current powerdown script disables the PMIC backlight

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agoomapfbplay: import from OE classic + api tweak
Roger Monk [Thu, 10 May 2012 14:18:27 +0000 (15:18 +0100)]
omapfbplay: import from OE classic + api tweak

Signed-off-by: Roger Monk <r-monk@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agoREADME: by popular demand add comment on how to avoid systemd breakage
Denys Dmytriyenko [Fri, 18 May 2012 03:47:35 +0000 (23:47 -0400)]
README: by popular demand add comment on how to avoid systemd breakage

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agoREADME: no longer depend on toolchain-layer, remove references to older gcc/binutils
Denys Dmytriyenko [Fri, 18 May 2012 03:36:52 +0000 (23:36 -0400)]
README: no longer depend on toolchain-layer, remove references to older gcc/binutils

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: make st7735fb DMA safe
Koen Kooi [Wed, 16 May 2012 13:27:00 +0000 (15:27 +0200)]
linux-ti33x-psp 3.2: make st7735fb DMA safe

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agobeagleboard-getting-started: update for revision A6 release
Koen Kooi [Wed, 16 May 2012 06:45:48 +0000 (08:45 +0200)]
beagleboard-getting-started: update for revision A6 release

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: updates
Koen Kooi [Mon, 14 May 2012 14:34:35 +0000 (16:34 +0200)]
linux-ti33x-psp 3.2: updates

* Fix LEDs on 3.5", 7" and DVI capes
* Add support for rev A2 DVI capes
* Minor warning fixes to the boardfile
* All PWMs are initialized, but not pinmuxed
* Debugfs output for mux direction has been fixed
* When no capes claim the SPI bus /dev/spidev2.0 will appear

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: avoid gold linker for Thumb2 kernel
Denys Dmytriyenko [Fri, 11 May 2012 01:55:15 +0000 (21:55 -0400)]
linux-ti33x-psp 3.2: avoid gold linker for Thumb2 kernel

BeagleBone kernel is required to be built in Thumb2 mode for fast boot.
Gold linker is not yet perfect for this, giving an internal error:

| arm-linux-gnueabi-ld: internal error in thumb_branch_common, at .../binutils-cross-2.22-r6/binutils-2.22/gold/arm.cc:4149

While this fix can be put in generic linux.inc for all the kernels, it's
better to test the Gold linker out as much as possible and only disable it
for known issues, like this one (until it gets fixed, of course).

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agoomap3-sgx-modules, ti-staging.inc, ti-linuxutils: change PACKAGE_STRIP = "no" to...
Koen Kooi [Thu, 10 May 2012 13:45:24 +0000 (15:45 +0200)]
omap3-sgx-modules, ti-staging.inc, ti-linuxutils: change PACKAGE_STRIP = "no" to the proper INHIBIT_PACKAGE_STRIP = "1"

PACKAGE_STRIP doesn't exit in oe-core (anymore)

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: for beaglebone set default Asm architecture to armv7-a
Denys Dmytriyenko [Thu, 3 May 2012 21:20:32 +0000 (17:20 -0400)]
linux-ti33x-psp 3.2: for beaglebone set default Asm architecture to armv7-a

Beaglebone kernel needs to be built in Thumb2 mode to achieve fast boot
times. Unfortunately, that build is broken under newer binutils-2.22 with
the below Assembler error. The fix is to pass the specific -march=armv7-a
flag to the Assembler to make it work.

| arch/arm/boot/compressed/head.S: Assembler messages:
| arch/arm/boot/compressed/head.S:127: Error: selected processor does not support requested special purpose register -- `mrs r2,cpsr'
| arch/arm/boot/compressed/head.S:134: Error: selected processor does not support requested special purpose register -- `mrs r2,cpsr'
| arch/arm/boot/compressed/head.S:136: Error: selected processor does not support requested special purpose register -- `msr cpsr_c,r2'
| make[2]: *** [arch/arm/boot/compressed/head.o] Error 1
| make[1]: *** [arch/arm/boot/compressed/vmlinux] Error 2

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Acked-by: Koen Kooi <koen@circuitco.com>
10 years agouim: userspace app to manage wl12xx firmware loading
Koen Kooi [Mon, 7 May 2012 15:57:40 +0000 (17:57 +0200)]
uim: userspace app to manage wl12xx firmware loading

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: rebase patches onto latest git
Koen Kooi [Tue, 8 May 2012 14:29:09 +0000 (16:29 +0200)]
linux-ti33x-psp 3.2: rebase patches onto latest git

The psp tree added a patch to limit the beaglebone to 500MHz when powered by USB, which triggered conflicts in the patches. The 3.2.16 series has been rediffed as well, no functional changes.

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti33x-psp 3.2: bump SRCREV for 2 CPPI1.4 fixes
Koen Kooi [Tue, 8 May 2012 13:10:19 +0000 (15:10 +0200)]
linux-ti33x-psp 3.2: bump SRCREV for 2 CPPI1.4 fixes

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti335x-psp 3.2: switch to userspace governor for beaglebone, ondemand seems...
Koen Kooi [Mon, 7 May 2012 12:09:16 +0000 (14:09 +0200)]
linux-ti335x-psp 3.2: switch to userspace governor for beaglebone, ondemand seems to cause problems on a small percentage of boards

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti335x-psp 3.2: add patch to disable heartbeat LED trigger on shutdown
Koen Kooi [Mon, 7 May 2012 11:39:56 +0000 (13:39 +0200)]
linux-ti335x-psp 3.2: add patch to disable heartbeat LED trigger on shutdown

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti335x-psp 3.2: use proper irq fix from Vaibhav
Koen Kooi [Sat, 5 May 2012 07:19:13 +0000 (09:19 +0200)]
linux-ti335x-psp 3.2: use proper irq fix from Vaibhav

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti335x-psp 3.2: add support for CAN, RS232 and Battery beaglebone capes
Koen Kooi [Fri, 4 May 2012 11:29:46 +0000 (13:29 +0200)]
linux-ti335x-psp 3.2: add support for CAN, RS232 and Battery beaglebone capes

Also change defconfig to prepare for audio support and fix lcd35 pinmux

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti335x-psp 3.2: update to 3.2.16
Koen Kooi [Fri, 4 May 2012 09:05:58 +0000 (11:05 +0200)]
linux-ti335x-psp 3.2: update to 3.2.16

3.2.16 is the final release in the 3.2-stable series by Greg KH.

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-ti335x-psp 3.2: bump SRCREV to head of v3.2-staging and add 2 irq patches
Koen Kooi [Fri, 4 May 2012 09:02:11 +0000 (11:02 +0200)]
linux-ti335x-psp 3.2: bump SRCREV to head of v3.2-staging and add 2 irq patches

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-mainline 3.2: shut down heartbeat LED on halt/reboot/panic
Koen Kooi [Thu, 10 May 2012 08:53:45 +0000 (10:53 +0200)]
linux-mainline 3.2: shut down heartbeat LED on halt/reboot/panic

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-mainline 3.2: add ASoC fixes for beagleboard
Koen Kooi [Fri, 4 May 2012 06:45:54 +0000 (08:45 +0200)]
linux-mainline 3.2: add ASoC fixes for beagleboard

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-mainline 3.2: add support for beagleboard wifi expansion board
Koen Kooi [Fri, 4 May 2012 06:40:06 +0000 (08:40 +0200)]
linux-mainline 3.2: add support for beagleboard wifi expansion board

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agosdcard_image bbclass: make ext4 the default
Koen Kooi [Fri, 4 May 2012 06:40:01 +0000 (08:40 +0200)]
sdcard_image bbclass: make ext4 the default

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agou-boot 2011.12: switch beagleboard to ext4 to match beaglebone
Koen Kooi [Tue, 1 May 2012 19:06:52 +0000 (21:06 +0200)]
u-boot 2011.12: switch beagleboard to ext4 to match beaglebone

Also add patch to increase ext2 read speed.

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Acked-by: Tom Rini <trini@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agou-boot 2011.12: don't poke at uLCD7 settings from u-boot, it's handled in the kernel now
Koen Kooi [Tue, 1 May 2012 19:06:51 +0000 (21:06 +0200)]
u-boot 2011.12: don't poke at uLCD7 settings from u-boot, it's handled in the kernel now

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Acked-by: Tom Rini <trini@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-mainline 3.2: fix build of external SGX modules
Koen Kooi [Tue, 1 May 2012 19:06:50 +0000 (21:06 +0200)]
linux-mainline 3.2: fix build of external SGX modules

Patch downloaded from https://github.com/RobertCNelson/stable-kernel/tree/master/patches/sgx

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agobeagleboard: switch to linux-mainline and drag in more modules
Koen Kooi [Tue, 1 May 2012 19:06:49 +0000 (21:06 +0200)]
beagleboard: switch to linux-mainline and drag in more modules

also bump MACHINE_KERNEL_PR to force rebuild of external modules like sgx and dsp.

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolinux-mainline 3.2: kernel recipe based on mainline 3.2.16 with additional patches...
Koen Kooi [Tue, 1 May 2012 19:06:48 +0000 (21:06 +0200)]
linux-mainline 3.2: kernel recipe based on mainline 3.2.16 with additional patches for e.g. beagleboard on top

This patchset is managed in https://github.com/beagleboard/kernel/tree/beagleboard-3.2 by Robert Nelson and myself.

Tested on beagleboard-xM/Angstrom

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agobonescript: silence systemd bbclass WARNING, ${PN}-systemd is unwanted
Denys Dmytriyenko [Thu, 3 May 2012 22:21:13 +0000 (18:21 -0400)]
bonescript: silence systemd bbclass WARNING, ${PN}-systemd is unwanted

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agobeaglebone: re-enable THUMB2_KERNEL in defconfig, as it affects boot time by .5s
Denys Dmytriyenko [Thu, 3 May 2012 19:16:55 +0000 (15:16 -0400)]
beaglebone: re-enable THUMB2_KERNEL in defconfig, as it affects boot time by .5s

This reverts commit 3c693c26087aa148b944166083b5336f05d1c15b.

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolibgles-omap3: enable for ti814x SOC family
Denys Dmytriyenko [Thu, 3 May 2012 06:13:57 +0000 (02:13 -0400)]
libgles-omap3: enable for ti814x SOC family

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agolibgles-omap3: work around bug in opkg
Koen Kooi [Wed, 2 May 2012 12:33:26 +0000 (14:33 +0200)]
libgles-omap3: work around bug in opkg

All the EGL_BADALLOC failures that user have been reporting turn out to be
a bug in opkg:
http://groups.google.com/group/opkg-devel/browse_thread/thread/741d18b0ef31435e#

Opkg decides to relink symlinks to the wrong files. As a workaround we check
the symlink during every bootup and fix it if needed.

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>