glsdk/meta-ti-glsdk.git
8 years agokeystone-evm config: add ubifs support
Hao Zhang [Tue, 26 Feb 2013 19:48:50 +0000 (14:48 -0500)]
keystone-evm config: add ubifs support

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agoRevert "linux-omap3: Add supported kernel recipe for am37x-evm and am3517-evm"
Denys Dmytriyenko [Thu, 28 Feb 2013 19:57:26 +0000 (14:57 -0500)]
Revert "linux-omap3: Add supported kernel recipe for am37x-evm and am3517-evm"

The same recipe already exists under linux-omap-psp name.

This reverts commit 153b5ed063c0bc2b16b938409027794a8dad908e.

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agomachine configs: Add SGX to MACHINE_FEATURES
Franklin S. Cooper Jr [Tue, 19 Feb 2013 04:45:16 +0000 (22:45 -0600)]
machine configs: Add SGX to MACHINE_FEATURES

* Add sgx to MACHINE_FEATURES to indicate that a particular machine supports
  sgx.
* TI chips are available in multiple variants including some that supports sgx
  while others do not.
* By adding sgx as a machine feature other layers can create generic
  packagegroups or images for a particular soc but will only include sgx
  dependencies if the particular machine has sgx support.

Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agolinux: Add kernel version 3.3.7 for beagleboard
Franklin S. Cooper Jr [Sun, 17 Feb 2013 22:00:32 +0000 (16:00 -0600)]
linux: Add kernel version 3.3.7 for beagleboard

Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agolinux-omap3: Add supported kernel recipe for am37x-evm and am3517-evm
Franklin S. Cooper Jr [Sun, 17 Feb 2013 22:00:31 +0000 (16:00 -0600)]
linux-omap3: Add supported kernel recipe for am37x-evm and am3517-evm

Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agomesa-dri: update to 9.0.2 to follow oe-core
Denys Dmytriyenko [Mon, 18 Feb 2013 21:47:16 +0000 (16:47 -0500)]
mesa-dri: update to 9.0.2 to follow oe-core

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agolibgles-omap3: ignore QA errors
Peter A. Bigot [Mon, 14 Jan 2013 19:41:01 +0000 (13:41 -0600)]
libgles-omap3: ignore QA errors

This patch allows libgles-omap3 to build on the danny branch.  The following
warnings are not addressed:

 WARNING: libgles-omap3: No generic license file exists for: proprietary-binary in any provider
 WARNING: QA Issue: libgles-omap3: Files/directories were installed but not shipped
  /usr/lib/ES2.0
 WARNING: libgles-omap3: The compile log indicates that host include and/or library paths were used.
         Please check the log '/prj/oe/omap/build-gumstix-community-danny/tmp/work/armv7a-vfp-neon-poky-linux-gnueabi/libgles-omap3-4.05.00.03-r35/temp/log.do_compile' for more information.

Signed-off-by: Peter A. Bigot <pab@pabigot.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agoomap3-sgx-modules: Add v4.08.00.01 of the SGX modules
Franklin S. Cooper Jr [Wed, 6 Feb 2013 06:57:52 +0000 (00:57 -0600)]
omap3-sgx-modules: Add v4.08.00.01 of the SGX modules

* Add version 4.08.00.01 of the SGX modules.

Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agolibgles-omap3: Add v4.08.00.01 of the Graphics SDK
Franklin S. Cooper Jr [Wed, 6 Feb 2013 06:57:51 +0000 (00:57 -0600)]
libgles-omap3: Add v4.08.00.01 of the Graphics SDK

* Add version v4.08.00.01 of the Graphics SDK.
* Add X11 support via DRI/DRM Xorg driver
* Replace pvrsrvinit with pvrsrvctl (Imagination Technologies based change)

Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agomachines: set default virtual/bootloader for remaining machines
Denys Dmytriyenko [Sun, 17 Feb 2013 21:49:28 +0000 (16:49 -0500)]
machines: set default virtual/bootloader for remaining machines

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agoam335x-evm: Increase UBI max size to 500MB
Chase Maupin [Fri, 16 Nov 2012 16:53:55 +0000 (10:53 -0600)]
am335x-evm: Increase UBI max size to 500MB

* Based on the EVM and beaglebone + NAND memory cape we can
  increase the base file system size to 500MB since by default
  there is about 504MB of space allocated to the file system
  partition in the NAND.
* The max size in LEBs was determined using the formula at
  http://processors.wiki.ti.com/index.php/UBIFS_Support

Signed-off-by: Chase Maupin <Chase.Maupin@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agolinux-mainline 3.2: update beagleboard defconfig
Peter A. Bigot [Thu, 6 Dec 2012 18:04:15 +0000 (12:04 -0600)]
linux-mainline 3.2: update beagleboard defconfig

Link the TLC59108 driver statically so ULCD7 initialization occurs
automatically as it did before f0e2305c7e1 which removed the initialization
from u-boot.  (Angstrom-v2012.12 does not include this module by default.)

Signed-off-by: Peter A. Bigot <pab@pabigot.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agou-boot_2012.04.01: Add latest u-boot recipe for am37x-evm
Franklin S. Cooper Jr [Tue, 12 Feb 2013 01:04:42 +0000 (19:04 -0600)]
u-boot_2012.04.01: Add latest u-boot recipe for am37x-evm

Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agoti-ocf-crypto-module: Port ti-ocf-crypto-module from Arago
Franklin S. Cooper Jr [Tue, 12 Feb 2013 01:04:41 +0000 (19:04 -0600)]
ti-ocf-crypto-module: Port ti-ocf-crypto-module from Arago

* Recipe pulls in ti-ocf-crypto-module from gforge
* For am37x, this module allows access to the crypto hardware accelerators
  through OCF-Linux.

Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agou-boot_2010.12-psp03.21.00.04.sdk: Add latest u-boot recipe for am180x-evm
Franklin S. Cooper Jr [Tue, 12 Feb 2013 01:04:40 +0000 (19:04 -0600)]
u-boot_2010.12-psp03.21.00.04.sdk: Add latest u-boot recipe for am180x-evm

Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agoti-pru-sw-edma-driver: Port PRU SW edma driver from Arago
Franklin S. Cooper Jr [Tue, 12 Feb 2013 01:04:39 +0000 (19:04 -0600)]
ti-pru-sw-edma-driver: Port PRU SW edma driver from Arago

* Add PRU SW edma driver recipe for the omapl138 machines

* This recipe builds and installs an edma driver module that supports the
  edma user space libraries built by the ti-pru-sw-edma-library recipe.

Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agolinux-omapl138-psp: Add latest linux-omapl138 patches
Franklin S. Cooper Jr [Tue, 12 Feb 2013 01:04:38 +0000 (19:04 -0600)]
linux-omapl138-psp: Add latest linux-omapl138 patches

* Add latest patches to linux-omapl138 that were added since this recipe was
  added to meta-ti.
* Update to latest am180x-evm defconfig
* Mimic the following commits from arago:

  linux-davinci: update to add mmc patches

    * Optimizations to reduce overhead on weak platforms

  linux: disable DMA for MUSB

    * For the am3517, am180x, and am335x devices the CPPI 4.1 DMA
      should NOT be used for the MUSB controller.  Using this DMA
      can cause the controller to lockup.
    * Updated the defconfigs to set the use of PIO mode
    * Added a patch to updated the PIO mode description to make it
      easier to determine when it can be used.

Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agolinux-omapl138-psp_2.6.37: Add MACHINE_KERNEL_PR and fix white space issues.
Franklin S. Cooper Jr [Tue, 12 Feb 2013 01:04:37 +0000 (19:04 -0600)]
linux-omapl138-psp_2.6.37: Add MACHINE_KERNEL_PR and fix white space issues.

* Add MACHINE_KERNEL_PR variable to enable future tweaks to this recipe.
* Convert tabs to whitespaces

Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agomachine config: Correct SERIAL_CONSOLE variable for am3517-evm and am37x-evm
Franklin S. Cooper Jr [Tue, 12 Feb 2013 01:04:36 +0000 (19:04 -0600)]
machine config: Correct SERIAL_CONSOLE variable for am3517-evm and am37x-evm

* When testing on am37x-evm I noticed that no prompt to login was ever shown
  when connected via serial port.
* I finally noticed that the SERIAL_CONSOLE variable was set incorrectly and
  didn't match the value in the old Arago layer.
* After using the values specific in the machine file in the Arago layer I was
  able to login via serial port.
* This has been verified on both the am37x-evm and am3517-evm.

Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agoam335x-evm, omap3*: drop remaining TARGET_ARCH, wrecking sstate
Denys Dmytriyenko [Thu, 7 Feb 2013 21:44:37 +0000 (16:44 -0500)]
am335x-evm, omap3*: drop remaining TARGET_ARCH, wrecking sstate

Bump MACHINE_KERNEL_PR to rebuild the correct sstate.

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agokeystone: update defconfig with latest for mcsdk alpha7
Murali Karicheri [Tue, 29 Jan 2013 17:15:25 +0000 (12:15 -0500)]
keystone: update defconfig with latest for mcsdk alpha7

Signed-off-by: Murali Karicheri <m-karicheri2@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agokeystone: update kernel and bootloaders recipes for mcsdk alpha7 release
Murali Karicheri [Tue, 29 Jan 2013 17:14:57 +0000 (12:14 -0500)]
keystone: update kernel and bootloaders recipes for mcsdk alpha7 release

Signed-off-by: Murali Karicheri <m-karicheri2@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agokeystone: boot-monitor: add initial recipe
Murali Karicheri [Fri, 18 Jan 2013 23:15:21 +0000 (18:15 -0500)]
keystone: boot-monitor: add initial recipe

This adds recipe to build boot monitor image. Boot monitor is
a standalone image that is loaded and executed from u-boot to
replace the RBL provided monitor code in ARM with Linux boot
specific code.

Signed-off-by: Murali Karicheri <m-karicheri2@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agomulti-kernel.inc: drop use of KERNEL_CCSUFFIX to match oe-core
Denys Dmytriyenko [Fri, 25 Jan 2013 08:02:18 +0000 (03:02 -0500)]
multi-kernel.inc: drop use of KERNEL_CCSUFFIX to match oe-core

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agomulti-kernel.inc: repeat do_configure after do_compileconfigs
Denys Dmytriyenko [Tue, 22 Jan 2013 02:19:32 +0000 (21:19 -0500)]
multi-kernel.inc: repeat do_configure after do_compileconfigs

Populate default defconfig into .config and process with oldconfig target

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agobeagleboard.conf: add additional sound modules
Cliff Brake [Tue, 22 Jan 2013 22:40:55 +0000 (17:40 -0500)]
beagleboard.conf: add additional sound modules

require for audio to function

Signed-off-by: Cliff Brake <cbrake@bec-systems.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agolinux_3.1: add extra '#' to multi-line comment
Cliff Brake [Tue, 22 Jan 2013 17:13:20 +0000 (12:13 -0500)]
linux_3.1: add extra '#' to multi-line comment

Bitbake is getting more particular:
ERROR: There is a confusing multiline, partially commented expression on
line 27 of file /scratch/oe/oe-build-core-3/sources/meta-ti/...
Please clarify whether this is all a comment or should be parsed.

Signed-off-by: Cliff Brake <cbrake@bec-systems.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agolinux-keystone: update to the latest dev release for keystone
Denys Dmytriyenko [Tue, 22 Jan 2013 02:38:27 +0000 (21:38 -0500)]
linux-keystone: update to the latest dev release for keystone

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agou-boot: update to the latest dev release for keystone
Denys Dmytriyenko [Tue, 22 Jan 2013 02:37:18 +0000 (21:37 -0500)]
u-boot: update to the latest dev release for keystone

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agonetbase: fix file search path for 'interfaces' file
Denys Dmytriyenko [Wed, 16 Jan 2013 17:29:57 +0000 (12:29 -0500)]
netbase: fix file search path for 'interfaces' file

This .bbappend file is used to override the 'interfaces' file for certain
targets. The current version is broken in that it does not search the correct
path(s).

Thanks to Robert P. J. Day and Gary Thomas for spotting the issue and providing
patches.

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agomesa-dri: update to 9.0.1 to match oe-core
Andreas Müller [Fri, 11 Jan 2013 07:52:53 +0000 (08:52 +0100)]
mesa-dri: update to 9.0.1 to match oe-core

this makes Cliff Brake's unapplied patch obsolete

Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agolinux-keystone: update from version 3.6-rc6 to 3.6.6
Denys Dmytriyenko [Mon, 3 Dec 2012 20:45:01 +0000 (15:45 -0500)]
linux-keystone: update from version 3.6-rc6 to 3.6.6

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agokeystone: bump MACHINE_KERNEL_PR for previous changes
Denys Dmytriyenko [Fri, 30 Nov 2012 16:44:24 +0000 (11:44 -0500)]
keystone: bump MACHINE_KERNEL_PR for previous changes

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agokeystone-evm: update serial port and virtual terminal settings
Denys Dmytriyenko [Fri, 30 Nov 2012 16:31:07 +0000 (11:31 -0500)]
keystone-evm: update serial port and virtual terminal settings

Keystone uses the old ttyS0 serial name instead of the new ttyO0.
Also disable spawning gettys on virtual terminals.

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agoconf/machine: omap4: update configs after xorg upgrade
Nicolas Dechesne [Thu, 22 Nov 2012 14:35:59 +0000 (15:35 +0100)]
conf/machine: omap4: update configs after xorg upgrade

There were some changes in the xserver-xorg upstream project that need
to be reflected here too:
 * extmod module was removed completely as it became empty;
 * DRI1, DRI2, DBE (among others) were made built-in;

(see poky rev: 5cea09e3d010d4799eab296b2a0cb83a0af09c76)

Signed-off-by: Nicolas Dechesne <n-dechesne@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agoRevert "xf86-video-omap: add new recipe for OMAP4/5 X11 video driver"
Nicolas Dechesne [Thu, 22 Nov 2012 14:35:58 +0000 (15:35 +0100)]
Revert "xf86-video-omap: add new recipe for OMAP4/5 X11 video driver"

This reverts commit 410dc026f2ee24a2346e7563a83f0181c79809cf.

Because this recipe was integrated in oe-core (then poky master).

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agoRevert "libdrm: enable omap experimental api support"
Nicolas Dechesne [Thu, 22 Nov 2012 14:35:57 +0000 (15:35 +0100)]
Revert "libdrm: enable omap experimental api support"

This reverts commit cce5a7aea905d2e2b167ab51b132ec43ed519a12.

Because oe-core (then poky master) was upgraded to libdrm 2.40,
and because OMAP experimental support was enabled there too.

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agokeystone-evm.conf: enable cpio images by default
Denys Dmytriyenko [Tue, 27 Nov 2012 16:40:06 +0000 (11:40 -0500)]
keystone-evm.conf: enable cpio images by default

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agou-boot: add version 2012.07 for keystone machines
Denys Dmytriyenko [Sat, 17 Nov 2012 03:58:02 +0000 (22:58 -0500)]
u-boot: add version 2012.07 for keystone machines

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agolibgles-omap3: Verify pvrsrvkm module was found
Franklin S. Cooper Jr [Fri, 16 Nov 2012 19:19:42 +0000 (13:19 -0600)]
libgles-omap3: Verify pvrsrvkm module was found

* Check to see if the pvrsrvkm.ko module was found and that the insmod
  for that module was successful.

Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agolibgles-omap3: Adjust for non X11 distros
Franklin S. Cooper Jr [Fri, 16 Nov 2012 19:19:41 +0000 (13:19 -0600)]
libgles-omap3: Adjust for non X11 distros

* Non X11 base distros are unable to build this Graphics SDK.
* This patch tweaks the libgles-omap3 include file to always build the
  Graphics SDK in Raw mode and also build in X11 mode only if X11 is
  a part of the DISTRO_FEATURE. Components are built, installed and packaged
  based on which mode the Graphics SDK is built in.
* Create a new variable PVR_INIT that is by default set to pvrsrvinit. This is
  needed for newer version of the Graphics SDK that replaced this file.

Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agoconf/machine: Update the FSTYPES for AMSDK machines
Chase Maupin [Thu, 15 Nov 2012 21:15:03 +0000 (15:15 -0600)]
conf/machine: Update the FSTYPES for AMSDK machines

* Updated the IMAGE_FSTYPES to ubi and tar.gz for the AMSDK
  machine types as the base file system type.
* This was done to speed up compression/decompression time at
  the expense of file size.

Signed-off-by: Chase Maupin <Chase.Maupin@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agolinux-omap4-3.1.0: Add sched_process_exec tracing
Paul Woegerer [Fri, 12 Oct 2012 07:40:24 +0000 (00:40 -0700)]
linux-omap4-3.1.0: Add sched_process_exec tracing

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agolinux-omap-psp 2.6.37: add more recent version of OMAP3 kernel
Denys Dmytriyenko [Fri, 2 Nov 2012 02:50:53 +0000 (22:50 -0400)]
linux-omap-psp 2.6.37: add more recent version of OMAP3 kernel

Ported from Arago the kernel that corresponds to PSP version 04.02.00.07 with
corresponding SDK patches applied on top.

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agolinux-keystone: add kernel for keystone SOC
Denys Dmytriyenko [Fri, 2 Nov 2012 00:44:13 +0000 (20:44 -0400)]
linux-keystone: add kernel for keystone SOC

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agoconf/machine: add keystone SOC and keystone-evm machine
Denys Dmytriyenko [Fri, 2 Nov 2012 00:43:07 +0000 (20:43 -0400)]
conf/machine: add keystone SOC and keystone-evm machine

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agotune-cortexa7: add tunes for ARM Cortex-A7
Denys Dmytriyenko [Thu, 18 Oct 2012 22:28:06 +0000 (18:28 -0400)]
tune-cortexa7: add tunes for ARM Cortex-A7

http://www.arm.com/products/processors/cortex-a/cortex-a7.php

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agotune-cortexa15: add tunes for ARM Cortex-A15
Denys Dmytriyenko [Thu, 18 Oct 2012 22:27:27 +0000 (18:27 -0400)]
tune-cortexa15: add tunes for ARM Cortex-A15

http://www.arm.com/products/processors/cortex-a/cortex-a15.php

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agopandaboard: use xf86-video-omap by default in XSERVER config
Nicolas Dechesne [Fri, 19 Oct 2012 13:51:26 +0000 (15:51 +0200)]
pandaboard: use xf86-video-omap by default in XSERVER config

Also we need to pull in module-exa as xf86-video-omap relies
on it, at run time.

And replaced the default xorg.conf for 'omap4' machine to take
new driver into account. Do not enable HWcursor (e.g. mouse
using DSS overlay) to keep things simple for now..

Signed-off-by: Nicolas Dechesne <n-dechesne@ti.com>
Signed-off-by: Hervé Fache <h-fache@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agoxf86-video-omap: add new recipe for OMAP4/5 X11 video driver
Nicolas Dechesne [Fri, 19 Oct 2012 13:51:25 +0000 (15:51 +0200)]
xf86-video-omap: add new recipe for OMAP4/5 X11 video driver

Since this component is still actively being developed, let's use
a _git.bb recipe. We can introduce 'x.y' version later.

Even though xf-video-omap can be combined with private/restricted
EXA sub-driver for SGX/PVR, it can also work without it. In which
case EXA aren't using SGX, but all standard driver features still
work, and it is a replacement for xf-video-fbdev.

Signed-off-by: Nicolas Dechesne <n-dechesne@ti.com>
Signed-off-by: Hervé Fache <h-fache@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agolibdrm: enable omap experimental api support
Enrico Butera [Fri, 19 Oct 2012 13:51:24 +0000 (15:51 +0200)]
libdrm: enable omap experimental api support

This is needed to build gst-plugin-ducati.

Signed-off-by: Enrico Butera <ebutera@users.berlios.de>
Signed-off-by: Nicolas Dechesne <n-dechesne@ti.com>
Signed-off-by: Hervé Fache <h-fache@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agolinux-omap4: update to 3.4 from GLP 1.6.6 release
Hervé Fache [Fri, 5 Oct 2012 12:57:42 +0000 (14:57 +0200)]
linux-omap4: update to 3.4 from GLP 1.6.6 release

Used Herve's version as a base with some mods from Enrico and additional fixes
on top, defconfig is the validated one from GLP release.

Signed-off-by: Hervé Fache <h-fache@ti.com>
Cc: Enrico Butera <ebutera@users.berlios.de>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agolinux-am335x-3.2.0-psp04.06.00.08: Add PSP v04.06.00.08 of the Linux kernel
Franklin S. Cooper Jr [Fri, 12 Oct 2012 05:14:45 +0000 (00:14 -0500)]
linux-am335x-3.2.0-psp04.06.00.08: Add PSP v04.06.00.08 of the Linux kernel

* Add the PSP release version of the Linux kernel for the am335x-evm
* Include a variable called KERNEL_PATCHES which can be used to add
  patches on top of the PSP release of the Linux kernel. Currently used
  to apply various patches that add functionality or fixes bugs.

Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agorecipes: Fix ti-eula-unpack issue. Tweak sgx modules and libgles recipes.
Franklin S. Cooper Jr [Sat, 1 Sep 2012 17:45:03 +0000 (12:45 -0500)]
recipes: Fix ti-eula-unpack issue. Tweak sgx modules and libgles recipes.

* Commit d8fc4a686262c50fd0053afa7240020909ec430b addressed an issue where
  too many newlines characters were being sent since print by default already
  sends a newline character. This commit however resulted in bin files being
  installed in the WORKDIR and broke other recipes which commit
  a94f765b9867abefd5f0bd262b5dddb8782b3187 addressed. This lead to a very
  cluttered WORKDIR.
* This patch updates ti-eula-unpack.inc to switch from using a print to a write.
  Since write doesn't automatically send newlines it is a bit more obvious when
  newlines are sent.
* Part of the reason that bin files were being installed in the WORKDIR was
  due to TI_BIN_UNPK_WDEXT being blank for some recipes. For instance in the
  libgles-omap3 recipes, when the workdir command is set in TI_BIN_UNPK_CMDS the
  directory that the Graphics SDK will be installed into is
  workdir+TI_BIN_UNPK_WDEXT. A blank TI_BIN_UNPK_WDEXT means the SDK will be
  installed in WORKDIR. By setting TI_BIN_UNPK_WDEXT to a proper value the
  recipes can be sure it is installed in the proper directory.
* Determine which file to download based on the defined BINFILE and not a
  hardcoded value. This idea was taken from arago.

Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Acked-by: Chase Maupin <chase.maupin@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
8 years agou-boot_2011.09-psp04.06.00.08: Add PSP v04.06.00.08 of u-boot
Franklin S. Cooper Jr [Fri, 5 Oct 2012 05:07:28 +0000 (00:07 -0500)]
u-boot_2011.09-psp04.06.00.08: Add PSP v04.06.00.08 of u-boot

* Add the PSP release version 04.06.00.08 of u-boot.

Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolibgles-omap3.inc: Tweak PLATFORM variable.
Franklin S. Cooper Jr [Fri, 31 Aug 2012 23:19:57 +0000 (18:19 -0500)]
libgles-omap3.inc: Tweak PLATFORM variable.

* Newer versions of libgles-omap3 utilize a different PLATFORM value. This
  patch allows the PLATFORM variable to be easily overridden if needed.
* Replace the hardcoded usage of LinuxOMAP3 with the PLATFORM variable.

Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agoti-hw-bringup-image: remove duplicate timestamp-service, as it's in systemd-image
Denys Dmytriyenko [Fri, 14 Sep 2012 04:57:22 +0000 (00:57 -0400)]
ti-hw-bringup-image: remove duplicate timestamp-service, as it's in systemd-image

Since systemd-image from meta-angstrom already includes timestamp-service, remove
the duplicate from ti-hw-bringup-image recipe, which uses the former as a base.

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolayer.conf: lower layer priority from 10 to 6
Denys Dmytriyenko [Fri, 14 Sep 2012 04:40:55 +0000 (00:40 -0400)]
layer.conf: lower layer priority from 10 to 6

Lowering layer priority from 10 to 6 aligns meta-ti with other BSP layers
and also allows distributions to override our recipes.

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolibgles-omap3: fix for latest oe-core mesa changes
Andreas Müller [Tue, 4 Sep 2012 16:20:58 +0000 (18:20 +0200)]
libgles-omap3: fix for latest oe-core mesa changes

* add virtual/libgles1 virtual/libgles2 to PROVIDES
* add RREPLACES_{PN}* for mesa's libegl* libgles1* libgles2*

Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agomesa: add appends to avoid providing conflicts
Andreas Müller [Tue, 4 Sep 2012 16:20:57 +0000 (18:20 +0200)]
mesa: add appends to avoid providing conflicts

For libgles-omap3 compatible machines mesa should only provide libgl.

Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Rebased to squash removal of mesa-xlib.

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agobeaglebone-tester: FTDI eeprom test, v2
Koen Kooi [Sat, 1 Sep 2012 11:46:43 +0000 (13:46 +0200)]
beaglebone-tester: FTDI eeprom test, v2

Check descriptor instead of VID/PID

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agobeaglebone tester: bump SRCREV for FTDI test
Koen Kooi [Fri, 31 Aug 2012 07:16:45 +0000 (09:16 +0200)]
beaglebone tester: bump SRCREV for FTDI test

An extra test for the FTDI eeprom was added to catch programming errors that would break CCS.

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agobeaglebone-tester: ship testaudio, fix depends
Koen Kooi [Sun, 12 Aug 2012 08:11:12 +0000 (10:11 +0200)]
beaglebone-tester: ship testaudio, fix depends

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-ti33x-psp 3.2: update beaglebone defconfig
Koen Kooi [Thu, 30 Aug 2012 07:56:13 +0000 (09:56 +0200)]
linux-ti33x-psp 3.2: update beaglebone defconfig

* Add more RTC modules
* Disable cgroup controllers with a lot of overhead

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-mainline: update to 3.2.28
Koen Kooi [Fri, 24 Aug 2012 07:20:38 +0000 (09:20 +0200)]
linux-mainline: update to 3.2.28

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-ti33x-psp 3.2: update to 3.2.28 and add motorcape support
Koen Kooi [Wed, 22 Aug 2012 12:29:17 +0000 (14:29 +0200)]
linux-ti33x-psp 3.2: update to 3.2.28 and add motorcape support

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-ti335x-psp 3.2: mux orientation detect for camera sensor to gpio instead of...
Koen Kooi [Thu, 16 Aug 2012 09:18:35 +0000 (11:18 +0200)]
linux-ti335x-psp 3.2: mux orientation detect for camera sensor to gpio instead of gpmc

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-ti33x-psp 3.2: update to 3.2.25
Koen Kooi [Wed, 8 Aug 2012 08:41:23 +0000 (10:41 +0200)]
linux-ti33x-psp 3.2: update to 3.2.25

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-ti33x-psp 3.2: LCD7 A3 support, eMMC cape support, camera cape improvements
Koen Kooi [Mon, 30 Jul 2012 18:41:14 +0000 (20:41 +0200)]
linux-ti33x-psp 3.2: LCD7 A3 support, eMMC cape support, camera cape improvements

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agorecipes: Use 'packagegroup' instead of 'task'
Khem Raj [Sun, 9 Sep 2012 17:07:47 +0000 (10:07 -0700)]
recipes: Use 'packagegroup' instead of 'task'

bring recipes in sync with OE-Core, task bbclass
is now replaced by packagegroup.

and task recipes are now called packagegroup_something

Signed-off-by: Khem Raj <raj.khem@gmail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agou-boot_2011.09[.10rc]: Always use gnu ld for LD
Roger Monk [Fri, 3 Aug 2012 22:20:08 +0000 (23:20 +0100)]
u-boot_2011.09[.10rc]: Always use gnu ld for LD

   - Pull in gnu ld patch for 2011.10rc recipe
   - Bump PR

Signed-off-by: Roger Monk <r-monk@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agou-boot 2011.09+git: update to latest version of Tom Rini's tree
Koen Kooi [Thu, 26 Jul 2012 10:40:43 +0000 (12:40 +0200)]
u-boot 2011.09+git: update to latest version of Tom Rini's tree

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agoti-dmai.inc: fix 'proto='-warning on recipe parsing
Andreas Müller [Wed, 1 Aug 2012 09:35:48 +0000 (11:35 +0200)]
ti-dmai.inc: fix 'proto='-warning on recipe parsing

Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agoam-sysinfo: switch 'proto' to 'protocol' in SRC_URI
Roger Monk [Thu, 19 Jul 2012 12:52:19 +0000 (13:52 +0100)]
am-sysinfo: switch 'proto' to 'protocol' in SRC_URI

Signed-off-by: Roger Monk <r-monk@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agogstreamer-ti: convert proto to protocol in SRC_URI
Roger Monk [Thu, 19 Jul 2012 12:49:01 +0000 (13:49 +0100)]
gstreamer-ti: convert proto to protocol in SRC_URI

Signed-off-by: Roger Monk <r-monk@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-ti33x-psp 3.2: update to 3.2.23
Koen Kooi [Tue, 17 Jul 2012 07:23:14 +0000 (09:23 +0200)]
linux-ti33x-psp 3.2: update to 3.2.23

Regenerate all beaglebone patches and add one vfs tracer patch for powertop

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-ti33x-psp 3.2: enable more tracing features for beaglebone
Koen Kooi [Sat, 14 Jul 2012 13:38:07 +0000 (15:38 +0200)]
linux-ti33x-psp 3.2: enable more tracing features for beaglebone

This makes powertop 2.0 happy

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-ti33x-psp 3.2: add fixed for cssp, fbset and OPP50
Koen Kooi [Fri, 13 Jul 2012 10:19:44 +0000 (12:19 +0200)]
linux-ti33x-psp 3.2: add fixed for cssp, fbset and OPP50

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agou-boot 2011.09+git: update to latest version of Tom Rini's tree
Koen Kooi [Wed, 11 Jul 2012 09:53:27 +0000 (11:53 +0200)]
u-boot 2011.09+git: update to latest version of Tom Rini's tree

All patches have been rediffed and boot tested

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-ti33x-psp 3.2: add support for audio cape and disable LBO gpio for battery...
Koen Kooi [Wed, 4 Jul 2012 05:58:33 +0000 (07:58 +0200)]
linux-ti33x-psp 3.2: add support for audio cape and disable LBO gpio for battery cape

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-ti33x-psp 3.2: add camera driver for beaglebone
Koen Kooi [Mon, 2 Jul 2012 04:22:09 +0000 (06:22 +0200)]
linux-ti33x-psp 3.2: add camera driver for beaglebone

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agobeaglebone-capes: use backlight hack for all LCD4 variants
Koen Kooi [Thu, 28 Jun 2012 09:53:55 +0000 (11:53 +0200)]
beaglebone-capes: use backlight hack for all LCD4 variants

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-ti33x-psp 3.2: fix audio/spidev clash on beaglebone
Koen Kooi [Tue, 26 Jun 2012 07:47:54 +0000 (09:47 +0200)]
linux-ti33x-psp 3.2: fix audio/spidev clash on beaglebone

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-ti33x-psp 3.2: update to 3.2.21, add libertas fixes
Koen Kooi [Wed, 20 Jun 2012 10:42:22 +0000 (12:42 +0200)]
linux-ti33x-psp 3.2: update to 3.2.21, add libertas fixes

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agobeaglebone-tester: re-enable pmic test
Koen Kooi [Thu, 14 Jun 2012 22:07:20 +0000 (00:07 +0200)]
beaglebone-tester: re-enable pmic test

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agobeaglebone-tester: bump SRCREV to fix serial console race
Koen Kooi [Fri, 8 Jun 2012 14:37:46 +0000 (16:37 +0200)]
beaglebone-tester: bump SRCREV to fix serial console race

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agonetbase: follow oe-core to v5.0
Andreas Müller [Mon, 9 Jul 2012 12:35:36 +0000 (14:35 +0200)]
netbase: follow oe-core to v5.0

Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux.inc: remove unused variable RPSRC
Andreas Müller [Thu, 21 Jun 2012 23:19:38 +0000 (01:19 +0200)]
linux.inc: remove unused variable RPSRC

Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux.inc: remove require linux-tools.inc
Andreas Müller [Thu, 21 Jun 2012 23:19:37 +0000 (01:19 +0200)]
linux.inc: remove require linux-tools.inc

linux-tools.inc was removed in oe-core (perf has own package) [1].

[1] http://cgit.openembedded.org/openembedded-core/commit/?id=b485f3e0e55ad62079ed0913970ff0620f4808ea

Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agobeaglebone-tester: bump SRCREV to fix failure reporting
Koen Kooi [Fri, 8 Jun 2012 09:37:44 +0000 (11:37 +0200)]
beaglebone-tester: bump SRCREV to fix failure reporting

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-ti33x-psp 3.2: turn on CONFIG_USB_SUSPEND to fix usb mass storage
Koen Kooi [Thu, 7 Jun 2012 15:40:45 +0000 (17:40 +0200)]
linux-ti33x-psp 3.2: turn on CONFIG_USB_SUSPEND to fix usb mass storage

Many thanks to Arkadiusz Karas <arkkar13@googlemail.com> for figuring that out
and sharing the info.

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agobeaglebone-capes: add support for weatherstation cape
Koen Kooi [Thu, 7 Jun 2012 15:40:44 +0000 (17:40 +0200)]
beaglebone-capes: add support for weatherstation cape

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agobeaglebone-capes: add support for 4.3" LCD cape
Koen Kooi [Thu, 7 Jun 2012 15:40:43 +0000 (17:40 +0200)]
beaglebone-capes: add support for 4.3" LCD cape

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-ti33x-psp 3.2: backport PM and USB fixes from PSP
Koen Kooi [Thu, 7 Jun 2012 15:40:42 +0000 (17:40 +0200)]
linux-ti33x-psp 3.2: backport PM and USB fixes from PSP

The complete patchset will get rebased to the tip of the PSP tree soon, but the
conflicts take a lot of time to resolve.

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-ti33x-psp 3.2: fix buttons on LCD capes
Koen Kooi [Thu, 7 Jun 2012 15:40:41 +0000 (17:40 +0200)]
linux-ti33x-psp 3.2: fix buttons on LCD capes

One patch to add button layout for the a1 revision of the 3.5" LCD cape and
another patch to stop spidev from loading when SPI1_D1 is used as gpio

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-ti33x-psp: enable TSL2550 driver for beaglebone weatherstation cape
Koen Kooi [Thu, 7 Jun 2012 15:40:40 +0000 (17:40 +0200)]
linux-ti33x-psp: enable TSL2550 driver for beaglebone weatherstation cape

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-ti33x-psp 3.2: switch ADC to 16x averaging, disable 275MHz, add 4.3" LCD support
Koen Kooi [Thu, 7 Jun 2012 15:40:39 +0000 (17:40 +0200)]
linux-ti33x-psp 3.2: switch ADC to 16x averaging, disable 275MHz, add 4.3" LCD support

* The switch to 16x averaging is done to combat the excessive noise in the
  signal. It's still *very* bad, but the TS cursor jitter has decreased a bit
* The OPP for 275MHz was disabled due to all the errata. Both the EMIF and MUSB
  don't seem to like that OPP.
* The resistive touch version of the 4.3" LCD cape is supported in 24 bit mode.

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-mainline 3.2.18: build in usbhid and tsc2007 and run 'make oldconfig'
Koen Kooi [Tue, 29 May 2012 07:42:19 +0000 (09:42 +0200)]
linux-mainline 3.2.18: build in usbhid and tsc2007 and run 'make oldconfig'

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
9 years agolinux-ti33x-psp 3.2: set PV accordingly, when not using tipspkernel
Denys Dmytriyenko [Wed, 30 May 2012 22:14:14 +0000 (18:14 -0400)]
linux-ti33x-psp 3.2: set PV accordingly, when not using tipspkernel

The patchset in PATCHES_OVER_PSP updates the kernel to 3.2.x, so make PV match.
This doesn't need PR or MACHINE_KERNEL_PR bumps since both the kernel ABI and
file locations remain the same.

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Acked-by: Koen Kooi <koen@circuitco.com>
9 years agotipspkernel: add extra level to FILESPATH with major version in the name
Denys Dmytriyenko [Wed, 30 May 2012 22:01:41 +0000 (18:01 -0400)]
tipspkernel: add extra level to FILESPATH with major version in the name

Add PMV variable to contain major version by extracting first 2 numbers from PV
Insert new level to FILESPATH - PN-PV-PR:PN-PV:PN-PMV:PN:files:.
Allow keeping patches and configs generic for the series (i.e. 3.2) while
incrementing stable releases (i.e. 3.2.18)
Drop use of BP and BPN, as they don't change for the kernel

Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Acked-by: Koen Kooi <koen@circuitco.com>