libdrm: enable omap experimental api support
This is needed to build gst-plugin-ducati.
Signed-off-by: Enrico Butera <ebutera@users.berlios.de>
Signed-off-by: Nicolas Dechesne <n-dechesne@ti.com>
Signed-off-by: Hervé Fache <h-fache@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
This is needed to build gst-plugin-ducati.
Signed-off-by: Enrico Butera <ebutera@users.berlios.de>
Signed-off-by: Nicolas Dechesne <n-dechesne@ti.com>
Signed-off-by: Hervé Fache <h-fache@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-omap4: update to 3.4 from GLP 1.6.6 release
Used Herve's version as a base with some mods from Enrico and additional fixes
on top, defconfig is the validated one from GLP release.
Signed-off-by: Hervé Fache <h-fache@ti.com>
Cc: Enrico Butera <ebutera@users.berlios.de>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Used Herve's version as a base with some mods from Enrico and additional fixes
on top, defconfig is the validated one from GLP release.
Signed-off-by: Hervé Fache <h-fache@ti.com>
Cc: Enrico Butera <ebutera@users.berlios.de>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-am335x-3.2.0-psp04.06.00.08: Add PSP v04.06.00.08 of the Linux kernel
* Add the PSP release version of the Linux kernel for the am335x-evm
* Include a variable called KERNEL_PATCHES which can be used to add
patches on top of the PSP release of the Linux kernel. Currently used
to apply various patches that add functionality or fixes bugs.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Add the PSP release version of the Linux kernel for the am335x-evm
* Include a variable called KERNEL_PATCHES which can be used to add
patches on top of the PSP release of the Linux kernel. Currently used
to apply various patches that add functionality or fixes bugs.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
recipes: Fix ti-eula-unpack issue. Tweak sgx modules and libgles recipes.
* Commit d8fc4a686262c50fd0053afa7240020909ec430b addressed an issue where
too many newlines characters were being sent since print by default already
sends a newline character. This commit however resulted in bin files being
installed in the WORKDIR and broke other recipes which commit
a94f765b9867abefd5f0bd262b5dddb8782b3187 addressed. This lead to a very
cluttered WORKDIR.
* This patch updates ti-eula-unpack.inc to switch from using a print to a write.
Since write doesn't automatically send newlines it is a bit more obvious when
newlines are sent.
* Part of the reason that bin files were being installed in the WORKDIR was
due to TI_BIN_UNPK_WDEXT being blank for some recipes. For instance in the
libgles-omap3 recipes, when the workdir command is set in TI_BIN_UNPK_CMDS the
directory that the Graphics SDK will be installed into is
workdir+TI_BIN_UNPK_WDEXT. A blank TI_BIN_UNPK_WDEXT means the SDK will be
installed in WORKDIR. By setting TI_BIN_UNPK_WDEXT to a proper value the
recipes can be sure it is installed in the proper directory.
* Determine which file to download based on the defined BINFILE and not a
hardcoded value. This idea was taken from arago.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Acked-by: Chase Maupin <chase.maupin@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Commit d8fc4a686262c50fd0053afa7240020909ec430b addressed an issue where
too many newlines characters were being sent since print by default already
sends a newline character. This commit however resulted in bin files being
installed in the WORKDIR and broke other recipes which commit
a94f765b9867abefd5f0bd262b5dddb8782b3187 addressed. This lead to a very
cluttered WORKDIR.
* This patch updates ti-eula-unpack.inc to switch from using a print to a write.
Since write doesn't automatically send newlines it is a bit more obvious when
newlines are sent.
* Part of the reason that bin files were being installed in the WORKDIR was
due to TI_BIN_UNPK_WDEXT being blank for some recipes. For instance in the
libgles-omap3 recipes, when the workdir command is set in TI_BIN_UNPK_CMDS the
directory that the Graphics SDK will be installed into is
workdir+TI_BIN_UNPK_WDEXT. A blank TI_BIN_UNPK_WDEXT means the SDK will be
installed in WORKDIR. By setting TI_BIN_UNPK_WDEXT to a proper value the
recipes can be sure it is installed in the proper directory.
* Determine which file to download based on the defined BINFILE and not a
hardcoded value. This idea was taken from arago.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Acked-by: Chase Maupin <chase.maupin@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
u-boot_2011.09-psp04.06.00.08: Add PSP v04.06.00.08 of u-boot
* Add the PSP release version 04.06.00.08 of u-boot.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Add the PSP release version 04.06.00.08 of u-boot.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3.inc: Tweak PLATFORM variable.
* Newer versions of libgles-omap3 utilize a different PLATFORM value. This
patch allows the PLATFORM variable to be easily overridden if needed.
* Replace the hardcoded usage of LinuxOMAP3 with the PLATFORM variable.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Newer versions of libgles-omap3 utilize a different PLATFORM value. This
patch allows the PLATFORM variable to be easily overridden if needed.
* Replace the hardcoded usage of LinuxOMAP3 with the PLATFORM variable.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
ti-hw-bringup-image: remove duplicate timestamp-service, as it's in systemd-image
Since systemd-image from meta-angstrom already includes timestamp-service, remove
the duplicate from ti-hw-bringup-image recipe, which uses the former as a base.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Since systemd-image from meta-angstrom already includes timestamp-service, remove
the duplicate from ti-hw-bringup-image recipe, which uses the former as a base.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
layer.conf: lower layer priority from 10 to 6
Lowering layer priority from 10 to 6 aligns meta-ti with other BSP layers
and also allows distributions to override our recipes.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Lowering layer priority from 10 to 6 aligns meta-ti with other BSP layers
and also allows distributions to override our recipes.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3: fix for latest oe-core mesa changes
* add virtual/libgles1 virtual/libgles2 to PROVIDES
* add RREPLACES_{PN}* for mesa's libegl* libgles1* libgles2*
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* add virtual/libgles1 virtual/libgles2 to PROVIDES
* add RREPLACES_{PN}* for mesa's libegl* libgles1* libgles2*
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
mesa: add appends to avoid providing conflicts
For libgles-omap3 compatible machines mesa should only provide libgl.
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Rebased to squash removal of mesa-xlib.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
For libgles-omap3 compatible machines mesa should only provide libgl.
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Rebased to squash removal of mesa-xlib.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beaglebone-tester: FTDI eeprom test, v2
Check descriptor instead of VID/PID
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Check descriptor instead of VID/PID
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beaglebone tester: bump SRCREV for FTDI test
An extra test for the FTDI eeprom was added to catch programming errors that would break CCS.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
An extra test for the FTDI eeprom was added to catch programming errors that would break CCS.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beaglebone-tester: ship testaudio, fix depends
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: update beaglebone defconfig
* Add more RTC modules
* Disable cgroup controllers with a lot of overhead
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Add more RTC modules
* Disable cgroup controllers with a lot of overhead
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-mainline: update to 3.2.28
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: update to 3.2.28 and add motorcape support
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti335x-psp 3.2: mux orientation detect for camera sensor to gpio instead of gpmc
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: update to 3.2.25
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: LCD7 A3 support, eMMC cape support, camera cape improvements
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
recipes: Use 'packagegroup' instead of 'task'
bring recipes in sync with OE-Core, task bbclass
is now replaced by packagegroup.
and task recipes are now called packagegroup_something
Signed-off-by: Khem Raj <raj.khem@gmail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
bring recipes in sync with OE-Core, task bbclass
is now replaced by packagegroup.
and task recipes are now called packagegroup_something
Signed-off-by: Khem Raj <raj.khem@gmail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
u-boot_2011.09[.10rc]: Always use gnu ld for LD
- Pull in gnu ld patch for 2011.10rc recipe
- Bump PR
Signed-off-by: Roger Monk <r-monk@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
- Pull in gnu ld patch for 2011.10rc recipe
- Bump PR
Signed-off-by: Roger Monk <r-monk@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
u-boot 2011.09+git: update to latest version of Tom Rini's tree
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
ti-dmai.inc: fix 'proto='-warning on recipe parsing
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
am-sysinfo: switch 'proto' to 'protocol' in SRC_URI
Signed-off-by: Roger Monk <r-monk@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Roger Monk <r-monk@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
gstreamer-ti: convert proto to protocol in SRC_URI
Signed-off-by: Roger Monk <r-monk@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Roger Monk <r-monk@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: update to 3.2.23
Regenerate all beaglebone patches and add one vfs tracer patch for powertop
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Regenerate all beaglebone patches and add one vfs tracer patch for powertop
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: enable more tracing features for beaglebone
This makes powertop 2.0 happy
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
This makes powertop 2.0 happy
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: add fixed for cssp, fbset and OPP50
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
u-boot 2011.09+git: update to latest version of Tom Rini's tree
All patches have been rediffed and boot tested
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
All patches have been rediffed and boot tested
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: add support for audio cape and disable LBO gpio for battery cape
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: add camera driver for beaglebone
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beaglebone-capes: use backlight hack for all LCD4 variants
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: fix audio/spidev clash on beaglebone
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: update to 3.2.21, add libertas fixes
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beaglebone-tester: re-enable pmic test
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beaglebone-tester: bump SRCREV to fix serial console race
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
netbase: follow oe-core to v5.0
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux.inc: remove unused variable RPSRC
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux.inc: remove require linux-tools.inc
linux-tools.inc was removed in oe-core (perf has own package) [1].
[1] http://cgit.openembedded.org/openembedded-core/commit/?id=b485f3e0e55ad62079ed0913970ff0620f4808ea
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-tools.inc was removed in oe-core (perf has own package) [1].
[1] http://cgit.openembedded.org/openembedded-core/commit/?id=b485f3e0e55ad62079ed0913970ff0620f4808ea
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beaglebone-tester: bump SRCREV to fix failure reporting
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: turn on CONFIG_USB_SUSPEND to fix usb mass storage
Many thanks to Arkadiusz Karas <arkkar13@googlemail.com> for figuring that out
and sharing the info.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Many thanks to Arkadiusz Karas <arkkar13@googlemail.com> for figuring that out
and sharing the info.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beaglebone-capes: add support for weatherstation cape
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beaglebone-capes: add support for 4.3" LCD cape
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: backport PM and USB fixes from PSP
The complete patchset will get rebased to the tip of the PSP tree soon, but the
conflicts take a lot of time to resolve.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
The complete patchset will get rebased to the tip of the PSP tree soon, but the
conflicts take a lot of time to resolve.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: fix buttons on LCD capes
One patch to add button layout for the a1 revision of the 3.5" LCD cape and
another patch to stop spidev from loading when SPI1_D1 is used as gpio
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
One patch to add button layout for the a1 revision of the 3.5" LCD cape and
another patch to stop spidev from loading when SPI1_D1 is used as gpio
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp: enable TSL2550 driver for beaglebone weatherstation cape
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: switch ADC to 16x averaging, disable 275MHz, add 4.3" LCD support
* The switch to 16x averaging is done to combat the excessive noise in the
signal. It's still *very* bad, but the TS cursor jitter has decreased a bit
* The OPP for 275MHz was disabled due to all the errata. Both the EMIF and MUSB
don't seem to like that OPP.
* The resistive touch version of the 4.3" LCD cape is supported in 24 bit mode.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* The switch to 16x averaging is done to combat the excessive noise in the
signal. It's still *very* bad, but the TS cursor jitter has decreased a bit
* The OPP for 275MHz was disabled due to all the errata. Both the EMIF and MUSB
don't seem to like that OPP.
* The resistive touch version of the 4.3" LCD cape is supported in 24 bit mode.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-mainline 3.2.18: build in usbhid and tsc2007 and run 'make oldconfig'
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: set PV accordingly, when not using tipspkernel
The patchset in PATCHES_OVER_PSP updates the kernel to 3.2.x, so make PV match.
This doesn't need PR or MACHINE_KERNEL_PR bumps since both the kernel ABI and
file locations remain the same.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Acked-by: Koen Kooi <koen@circuitco.com>
The patchset in PATCHES_OVER_PSP updates the kernel to 3.2.x, so make PV match.
This doesn't need PR or MACHINE_KERNEL_PR bumps since both the kernel ABI and
file locations remain the same.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Acked-by: Koen Kooi <koen@circuitco.com>
tipspkernel: add extra level to FILESPATH with major version in the name
Add PMV variable to contain major version by extracting first 2 numbers from PV
Insert new level to FILESPATH - PN-PV-PR:PN-PV:PN-PMV:PN:files:.
Allow keeping patches and configs generic for the series (i.e. 3.2) while
incrementing stable releases (i.e. 3.2.18)
Drop use of BP and BPN, as they don't change for the kernel
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Acked-by: Koen Kooi <koen@circuitco.com>
Add PMV variable to contain major version by extracting first 2 numbers from PV
Insert new level to FILESPATH - PN-PV-PR:PN-PV:PN-PMV:PN:files:.
Allow keeping patches and configs generic for the series (i.e. 3.2) while
incrementing stable releases (i.e. 3.2.18)
Drop use of BP and BPN, as they don't change for the kernel
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Acked-by: Koen Kooi <koen@circuitco.com>
linux-ti33x-psp 3.2: fix pin free check once and for all
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: sgx fix from PSP + dvi cape audio fix
Also move more things to modules to speed up boot.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Also move more things to modules to speed up boot.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: update to 3.2.18
Duplicate patches between PSP and 3.2.17 have been dropped from the 3.2.17 series
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Duplicate patches between PSP and 3.2.17 have been dropped from the 3.2.17 series
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: i2c and cape fixes
* Fix I2C prescaler to run at full speed instead of 1/4 speed
* fix led/spidev/w1 check
* move RS232 cape to ttyO2
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Fix I2C prescaler to run at full speed instead of 1/4 speed
* fix led/spidev/w1 check
* move RS232 cape to ttyO2
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-mainline: Add patches to enable libertas firmware loading asynchronously
When using udev >=177 libertas driver does not load properly the firmware [1].
The patches 0001-0016 were taken from [2] and can be viewed at [3]. Patch 0017
I created to fix compiler complaining for missing symbol is_interrupt when
DEBUG set.
The patch series was tested with meta-gumstix on overo with udev-175 and
udev-182.
[1] http://www.spinics.net/lists/linux-wireless/msg85541.html
[2] git://git.kernel.org/pub/scm/linux/kernel/git/linville/wireless-next.git
[3] http://git.kernel.org/?p=linux/kernel/git/linville/wireless-next.git;a=history;f=drivers/net/wireless/libertas;hb=HEAD
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
When using udev >=177 libertas driver does not load properly the firmware [1].
The patches 0001-0016 were taken from [2] and can be viewed at [3]. Patch 0017
I created to fix compiler complaining for missing symbol is_interrupt when
DEBUG set.
The patch series was tested with meta-gumstix on overo with udev-175 and
udev-182.
[1] http://www.spinics.net/lists/linux-wireless/msg85541.html
[2] git://git.kernel.org/pub/scm/linux/kernel/git/linville/wireless-next.git
[3] http://git.kernel.org/?p=linux/kernel/git/linville/wireless-next.git;a=history;f=drivers/net/wireless/libertas;hb=HEAD
Signed-off-by: Andreas Müller <schnitzeltony@googlemail.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-mainline: update to 3.2.18
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
ti-hw-bringup-image: disable sdcard image class
The class breaks with the current genext2fs in oe-core.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
The class breaks with the current genext2fs in oe-core.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: merge in 6 musb patches from PSP
Updating the SRCREV would require redoing all boardfile patches due to the
EVM-SK changes. So cherry-pick the 6 patches we need.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Updating the SRCREV would require redoing all boardfile patches due to the
EVM-SK changes. So cherry-pick the 6 patches we need.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti335x-psp 3.2: cape enhancements and patch cleanups
* add support for revision A2 of the 7" Beagleboardtoys cape
* allow capes to disable w1-gpio
* add stub for the Beagleboardtoys camera cape
* Fill in more entries in the am335x mux table
* switch to 4x oversampling in the tsadc driver to reduce jitter (or cursor hula
dancing as Gerald describes it)
* Add a function to set the pinmux from the eeprom data instead of the boardfile
* Add support for the Bebopr cape
All beaglebone patches have been rediffed and renumbered to avoid confusion
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* add support for revision A2 of the 7" Beagleboardtoys cape
* allow capes to disable w1-gpio
* add stub for the Beagleboardtoys camera cape
* Fill in more entries in the am335x mux table
* switch to 4x oversampling in the tsadc driver to reduce jitter (or cursor hula
dancing as Gerald describes it)
* Add a function to set the pinmux from the eeprom data instead of the boardfile
* Add support for the Bebopr cape
All beaglebone patches have been rediffed and renumbered to avoid confusion
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: silence useless omap4 hwmod warning
This fixes the last remaining debug print shown when booting with 'quiet'
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
This fixes the last remaining debug print shown when booting with 'quiet'
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: demote cpsw PHY message to INFO
This keeps them from appearing on the screen during quiet boots. They are still
being reported, so no info is lost.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
This keeps them from appearing on the screen during quiet boots. They are still
being reported, so no info is lost.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beaglebone-capes: add a powerdown script as well
The current powerdown script disables the PMIC backlight
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
The current powerdown script disables the PMIC backlight
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
omapfbplay: import from OE classic + api tweak
Signed-off-by: Roger Monk <r-monk@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Roger Monk <r-monk@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
README: by popular demand add comment on how to avoid systemd breakage
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
README: no longer depend on toolchain-layer, remove references to older gcc/binutils
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: make st7735fb DMA safe
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beagleboard-getting-started: update for revision A6 release
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: updates
* Fix LEDs on 3.5", 7" and DVI capes
* Add support for rev A2 DVI capes
* Minor warning fixes to the boardfile
* All PWMs are initialized, but not pinmuxed
* Debugfs output for mux direction has been fixed
* When no capes claim the SPI bus /dev/spidev2.0 will appear
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* Fix LEDs on 3.5", 7" and DVI capes
* Add support for rev A2 DVI capes
* Minor warning fixes to the boardfile
* All PWMs are initialized, but not pinmuxed
* Debugfs output for mux direction has been fixed
* When no capes claim the SPI bus /dev/spidev2.0 will appear
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: avoid gold linker for Thumb2 kernel
BeagleBone kernel is required to be built in Thumb2 mode for fast boot.
Gold linker is not yet perfect for this, giving an internal error:
| arm-linux-gnueabi-ld: internal error in thumb_branch_common, at .../binutils-cross-2.22-r6/binutils-2.22/gold/arm.cc:4149
While this fix can be put in generic linux.inc for all the kernels, it's
better to test the Gold linker out as much as possible and only disable it
for known issues, like this one (until it gets fixed, of course).
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
BeagleBone kernel is required to be built in Thumb2 mode for fast boot.
Gold linker is not yet perfect for this, giving an internal error:
| arm-linux-gnueabi-ld: internal error in thumb_branch_common, at .../binutils-cross-2.22-r6/binutils-2.22/gold/arm.cc:4149
While this fix can be put in generic linux.inc for all the kernels, it's
better to test the Gold linker out as much as possible and only disable it
for known issues, like this one (until it gets fixed, of course).
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
omap3-sgx-modules, ti-staging.inc, ti-linuxutils: change PACKAGE_STRIP = "no" to the proper INHIBIT_PACKAGE_STRIP = "1"
PACKAGE_STRIP doesn't exit in oe-core (anymore)
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
PACKAGE_STRIP doesn't exit in oe-core (anymore)
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: for beaglebone set default Asm architecture to armv7-a
Beaglebone kernel needs to be built in Thumb2 mode to achieve fast boot
times. Unfortunately, that build is broken under newer binutils-2.22 with
the below Assembler error. The fix is to pass the specific -march=armv7-a
flag to the Assembler to make it work.
| arch/arm/boot/compressed/head.S: Assembler messages:
| arch/arm/boot/compressed/head.S:127: Error: selected processor does not support requested special purpose register -- `mrs r2,cpsr'
| arch/arm/boot/compressed/head.S:134: Error: selected processor does not support requested special purpose register -- `mrs r2,cpsr'
| arch/arm/boot/compressed/head.S:136: Error: selected processor does not support requested special purpose register -- `msr cpsr_c,r2'
| make[2]: *** [arch/arm/boot/compressed/head.o] Error 1
| make[1]: *** [arch/arm/boot/compressed/vmlinux] Error 2
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Acked-by: Koen Kooi <koen@circuitco.com>
Beaglebone kernel needs to be built in Thumb2 mode to achieve fast boot
times. Unfortunately, that build is broken under newer binutils-2.22 with
the below Assembler error. The fix is to pass the specific -march=armv7-a
flag to the Assembler to make it work.
| arch/arm/boot/compressed/head.S: Assembler messages:
| arch/arm/boot/compressed/head.S:127: Error: selected processor does not support requested special purpose register -- `mrs r2,cpsr'
| arch/arm/boot/compressed/head.S:134: Error: selected processor does not support requested special purpose register -- `mrs r2,cpsr'
| arch/arm/boot/compressed/head.S:136: Error: selected processor does not support requested special purpose register -- `msr cpsr_c,r2'
| make[2]: *** [arch/arm/boot/compressed/head.o] Error 1
| make[1]: *** [arch/arm/boot/compressed/vmlinux] Error 2
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Acked-by: Koen Kooi <koen@circuitco.com>
uim: userspace app to manage wl12xx firmware loading
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: rebase patches onto latest git
The psp tree added a patch to limit the beaglebone to 500MHz when powered by USB, which triggered conflicts in the patches. The 3.2.16 series has been rediffed as well, no functional changes.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
The psp tree added a patch to limit the beaglebone to 500MHz when powered by USB, which triggered conflicts in the patches. The 3.2.16 series has been rediffed as well, no functional changes.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti33x-psp 3.2: bump SRCREV for 2 CPPI1.4 fixes
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti335x-psp 3.2: switch to userspace governor for beaglebone, ondemand seems to cause problems on a small percentage of boards
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti335x-psp 3.2: add patch to disable heartbeat LED trigger on shutdown
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti335x-psp 3.2: use proper irq fix from Vaibhav
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti335x-psp 3.2: add support for CAN, RS232 and Battery beaglebone capes
Also change defconfig to prepare for audio support and fix lcd35 pinmux
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Also change defconfig to prepare for audio support and fix lcd35 pinmux
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti335x-psp 3.2: update to 3.2.16
3.2.16 is the final release in the 3.2-stable series by Greg KH.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
3.2.16 is the final release in the 3.2-stable series by Greg KH.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti335x-psp 3.2: bump SRCREV to head of v3.2-staging and add 2 irq patches
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-mainline 3.2: shut down heartbeat LED on halt/reboot/panic
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-mainline 3.2: add ASoC fixes for beagleboard
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-mainline 3.2: add support for beagleboard wifi expansion board
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
sdcard_image bbclass: make ext4 the default
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
u-boot 2011.12: switch beagleboard to ext4 to match beaglebone
Also add patch to increase ext2 read speed.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Acked-by: Tom Rini <trini@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Also add patch to increase ext2 read speed.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Acked-by: Tom Rini <trini@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
10 years agou-boot 2011.12: don't poke at uLCD7 settings from u-boot, it's handled in the kernel now
u-boot 2011.12: don't poke at uLCD7 settings from u-boot, it's handled in the kernel now
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Acked-by: Tom Rini <trini@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Acked-by: Tom Rini <trini@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-mainline 3.2: fix build of external SGX modules
Patch downloaded from https://github.com/RobertCNelson/stable-kernel/tree/master/patches/sgx
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Patch downloaded from https://github.com/RobertCNelson/stable-kernel/tree/master/patches/sgx
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beagleboard: switch to linux-mainline and drag in more modules
also bump MACHINE_KERNEL_PR to force rebuild of external modules like sgx and dsp.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
also bump MACHINE_KERNEL_PR to force rebuild of external modules like sgx and dsp.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-mainline 3.2: kernel recipe based on mainline 3.2.16 with additional patches for e.g. beagleboard on top
This patchset is managed in https://github.com/beagleboard/kernel/tree/beagleboard-3.2 by Robert Nelson and myself.
Tested on beagleboard-xM/Angstrom
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
This patchset is managed in https://github.com/beagleboard/kernel/tree/beagleboard-3.2 by Robert Nelson and myself.
Tested on beagleboard-xM/Angstrom
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
bonescript: silence systemd bbclass WARNING, ${PN}-systemd is unwanted
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beaglebone: re-enable THUMB2_KERNEL in defconfig, as it affects boot time by .5s
This reverts commit 3c693c26087aa148b944166083b5336f05d1c15b.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
This reverts commit 3c693c26087aa148b944166083b5336f05d1c15b.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3: enable for ti814x SOC family
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3: work around bug in opkg
All the EGL_BADALLOC failures that user have been reporting turn out to be
a bug in opkg:
http://groups.google.com/group/opkg-devel/browse_thread/thread/741d18b0ef31435e#
Opkg decides to relink symlinks to the wrong files. As a workaround we check
the symlink during every bootup and fix it if needed.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
All the EGL_BADALLOC failures that user have been reporting turn out to be
a bug in opkg:
http://groups.google.com/group/opkg-devel/browse_thread/thread/741d18b0ef31435e#
Opkg decides to relink symlinks to the wrong files. As a workaround we check
the symlink during every bootup and fix it if needed.
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3: package dri files into driwsegl subpackages
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3: move X related binaries into X11WSEGL subpackages to avoid dragging in libx11 and friends
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3: copy over all binaries and abstract install process
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beaglebone: disable THUMB2_KERNEL in defconfig for newer binutils
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3: add missing libdrm dependency
dpkg-deb -I shows:
Package: libgles-omap3
Version: 4.05.00.03-r26
Depends: libgles-omap3-flipwsegl, devmem2, update-rc.d, libdrm2 (>= 2.4.31), libgles-omap3-linuxfbwsegl, fbset, libc6 (>= 2.12), libgles-omap3-blitwsegl, libgles-omap3-frontwsegl
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
dpkg-deb -I shows:
Package: libgles-omap3
Version: 4.05.00.03-r26
Depends: libgles-omap3-flipwsegl, devmem2, update-rc.d, libdrm2 (>= 2.4.31), libgles-omap3-linuxfbwsegl, fbset, libc6 (>= 2.12), libgles-omap3-blitwsegl, libgles-omap3-frontwsegl
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
cloud9-gnome-image: same as cloud9-image, but with GNOME added to it
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
bonescript: update to latest git
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>