From 13f54d47c948a2f89fd5e1f543d039e39a880962 Mon Sep 17 00:00:00 2001 From: Denys Dmytriyenko Date: Fri, 26 Apr 2013 15:55:47 -0400 Subject: [PATCH] linux-ti-staging: update to ti2013.04.00 release Also, remove do_deploy_append() fix, as it's in oe-core now. Signed-off-by: Denys Dmytriyenko --- recipes-kernel/linux/linux-ti-staging_3.8.bb | 20 +++----------------- 1 file changed, 3 insertions(+), 17 deletions(-) diff --git a/recipes-kernel/linux/linux-ti-staging_3.8.bb b/recipes-kernel/linux/linux-ti-staging_3.8.bb index 622fa3e..6fe52e2 100644 --- a/recipes-kernel/linux/linux-ti-staging_3.8.bb +++ b/recipes-kernel/linux/linux-ti-staging_3.8.bb @@ -6,21 +6,6 @@ KERNEL_IMAGETYPE = "uImage" inherit kernel -# This function must be here BEFORE the require of linux-dtb.inc below. -# There is a "bug" in the base kernel.bbclass that after it's do_deploy -# step it does not return back to the ${S} directory but stays in the -# DEPLOY_DIR. However, the do_deploy_append defined in linux-dtb.inc -# assumes that it is being run in the ${S} directory. A patch is -# being submitted to fix this issue by either changing the do_deploy -# in the kernel.bbclass to do "cd -" as the last step or to add -# "cd ${S}" as the first line of do_deploy in linux-dtb.inc and this -# function can be removed once that change is available. -# If the function is not placed BEFORE the require then the change -# directory is not appended before the linux-dtb.inc changes. -do_deploy_append() { - cd ${S} -} - require recipes-kernel/linux/linux-dtb.inc require recipes-kernel/linux/setup-defconfig.inc @@ -40,11 +25,12 @@ S = "${WORKDIR}/git" BRANCH = "ti-linux-3.8.y" -SRCREV = "1de3616c36710b6949844738f9c63b96e307c49f" +# This commit corresponds to ti2013.04.00 release tag +SRCREV = "23e7f725a6af4ca44660c06bc3569f6ce705d1d0" PV = "3.8.8" # Append to the MACHINE_KERNEL_PR so that a new SRCREV will cause a rebuild -MACHINE_KERNEL_PR_append = "a+gitr${SRCPV}" +MACHINE_KERNEL_PR_append = "b+gitr${SRCPV}" SRC_URI = "git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git;protocol=git;branch=${BRANCH} \ file://defconfig \ -- 2.26.2