add missing #include's for config.h
[glsdk/omapdrmtest.git] / util / display-x11.c
1 /*
2  * Copyright (C) 2011 Texas Instruments
3  * Author: Rob Clark <rob.clark@linaro.org>
4  *
5  * This program is free software; you can redistribute it and/or modify it
6  * under the terms of the GNU General Public License version 2 as published by
7  * the Free Software Foundation.
8  *
9  * This program is distributed in the hope that it will be useful, but WITHOUT
10  * ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or
11  * FITNESS FOR A PARTICULAR PURPOSE.  See the GNU General Public License for
12  * more details.
13  *
14  * You should have received a copy of the GNU General Public License along with
15  * this program.  If not, see <http://www.gnu.org/licenses/>.
16  */
18 #ifdef HAVE_CONFIG_H
19 #include "config.h"
20 #endif
22 #include "util.h"
24 #include <X11/Xlib.h>
25 #include <X11/Xmd.h>
26 #include <X11/Xregion.h>
27 #include <X11/extensions/dri2proto.h>
28 #include <X11/extensions/dri2.h>
30 #include <sys/types.h>
31 #include <sys/stat.h>
32 #include <fcntl.h>
35 #define to_display_x11(x) container_of(x, struct display_x11, base)
36 struct display_x11 {
37         struct display base;
38         Display *dpy;
39         Window win;
40 };
42 #define to_buffer_x11(x) container_of(x, struct buffer_x11, base)
43 struct buffer_x11 {
44         struct buffer base;
45         DRI2Buffer *dri2buf;
46 };
49 #define MAX_BUFFERS 32
51 static struct buffer **
52 get_buffers(struct display *disp, uint32_t n)
53 {
54         ERROR("unimplemented");
55         return NULL;
56 }
58 static struct buffer **
59 get_vid_buffers(struct display *disp, uint32_t n,
60                 uint32_t fourcc, uint32_t w, uint32_t h)
61 {
62         struct display_x11 *disp_x11 = to_display_x11(disp);
63         struct buffer **bufs;
64         unsigned attachments[MAX_BUFFERS+1] = {
65                         DRI2BufferFrontLeft, 32, /* always requested, never returned */
66         };
67         DRI2Buffer *dri2bufs;
68         uint32_t i, j, nbufs = 1;
70         for (i = 0; i < n; i++) {
71                 attachments[ nbufs * 2     ] = i + 1;
72                 attachments[(nbufs * 2) + 1] = fourcc;
73                 nbufs++;
74         }
76         dri2bufs = DRI2GetBuffersVid(disp_x11->dpy, disp_x11->win,
77                         w, h, attachments, nbufs, &nbufs);
78         if (!dri2bufs) {
79                 ERROR("DRI2GetBuffersVid failed");
80                 return NULL;
81         }
83         MSG("DRI2GetBuffers: nbufs=%d", nbufs);
85         if (nbufs != n) {
86                 ERROR("wrong number of bufs: %d vs %d", nbufs, n);
87                 return NULL;
88         }
90         bufs = calloc(nbufs, sizeof(struct buffer *));
92         for (i = 0; i < nbufs; i++) {
93                 struct buffer *buf;
94                 struct buffer_x11 *buf_x11;
96                 buf_x11 = calloc(1, sizeof(*buf_x11));
97                 if (!buf_x11) {
98                         ERROR("allocation failed");
99                         return NULL;
100                 }
102                 buf_x11->dri2buf = &dri2bufs[i];
104                 buf = &buf_x11->base;
106                 buf->fourcc = fourcc;
107                 buf->width = w;
108                 buf->height = h;
110                 for (j = 0; dri2bufs[i].names[j]; j++) {
111                         buf->bo[j] = omap_bo_from_name(disp->dev, dri2bufs[i].names[j]);
112                 }
113                 buf->nbo = j;
115                 bufs[i] = buf;
116         }
118         return bufs;
121 static int
122 post_buffer(struct display *disp, struct buffer *buf)
124         MSG("unimplemented");
125         return -1;
128 static int
129 post_vid_buffer(struct display *disp, struct buffer *buf,
130                 uint32_t x, uint32_t y, uint32_t w, uint32_t h)
132         struct display_x11 *disp_x11 = to_display_x11(disp);
133         struct buffer_x11 *buf_x11 = to_buffer_x11(buf);
134         CARD64 count;
135         BoxRec b = {
136                         .x1 = x,
137                         .y1 = y,
138                         .x2 = x + w,
139                         .y2 = y + h,
140         };
142         DRI2SwapBuffersVid(disp_x11->dpy, disp_x11->win, 0, 0, 0, &count,
143                         buf_x11->dri2buf->attachment, &b);
144         MSG("DRI2SwapBuffersVid[%u]: count=%llu",
145                         buf_x11->dri2buf->attachment, count);
147         return 0;
150 void
151 disp_x11_usage(void)
153         MSG("X11 Display Options:");
154         MSG("\t-w WxH\tset window dimensions");
157 /*** Move these somewhere common ***/
158 #include <ctype.h>
159 static Bool is_fourcc(unsigned int val)
161         char *str = (char *)&val;
162         return isalnum(str[0]) && isalnum(str[1]) && isalnum(str[2]) && isalnum(str[3]);
164 #define ATOM(name) XInternAtom(dpy, name, False)
165 static inline void print_hex(int len, const unsigned char *val)
167         char buf[33];
168         int i, j;
169         for (i = 0; i < len; i += j) {
170                 for (j = 0; (j < 16) && ((i + j) < len); ++j)
171                         sprintf(&buf[j * 2], "%02x", val[i + j]);
172                 fprintf(stderr, "\t%s\n", buf);
173         }
175 /***********************************/
178 static Bool WireToEvent(Display *dpy, XExtDisplayInfo *info,
179                 XEvent *event, xEvent *wire)
181         switch ((wire->u.u.type & 0x7f) - info->codes->first_event) {
183         case DRI2_BufferSwapComplete:
184         {
185 //              xDRI2BufferSwapComplete *awire = (xDRI2BufferSwapComplete *)wire;
186                 MSG("BufferSwapComplete");
187                 return True;
188         }
189         default:
190                 /* client doesn't support server event */
191                 break;
192         }
194         return False;
197 static Status EventToWire(Display *dpy, XExtDisplayInfo *info,
198                 XEvent *event, xEvent *wire)
200    switch (event->type) {
201    default:
202       /* client doesn't support server event */
203       break;
204    }
206    return Success;
209 static const DRI2EventOps ops = {
210                 .WireToEvent = WireToEvent,
211                 .EventToWire = EventToWire,
212 };
214 struct display *
215 disp_x11_open(int argc, char **argv)
217         struct display_x11 *disp_x11 = NULL;
218         struct display *disp;
219         Display *dpy;
220         Window root, win;
221         drm_magic_t magic;
222         int eventBase, errorBase, major, minor;
223         char *driver, *device;
224         unsigned int nformats, *formats;
225         unsigned int i, width = 500, height = 500;
226         CARD32 *pval;
228         MSG("attempting to open X11 connection");
229         dpy = XOpenDisplay(NULL);
230         if (!dpy) {
231                 ERROR("Could not open display");
232                 goto no_x11;
233         }
235         if (!DRI2InitDisplay(dpy, &ops)) {
236                 ERROR("DRI2InitDisplay failed");
237                 goto no_x11;
238         }
240         if (!DRI2QueryExtension(dpy, &eventBase, &errorBase)) {
241                 ERROR("DRI2QueryExtension failed");
242                 goto no_x11;
243         }
245         MSG("DRI2QueryExtension: eventBase=%d, errorBase=%d", eventBase, errorBase);
247         if (!DRI2QueryVersion(dpy, &major, &minor)) {
248                 ERROR("DRI2QueryVersion failed");
249                 goto no_x11;
250         }
252         MSG("DRI2QueryVersion: major=%d, minor=%d", major, minor);
254         root = RootWindow(dpy, DefaultScreen(dpy));
256         if (!DRI2Connect(dpy, root, DRI2DriverDRI, &driver, &device)) {
257                 MSG("DRI2Connect failed");
258                 goto no_x11;
259         }
261         MSG("DRI2Connect: driver=%s, device=%s", driver, device);
263         disp_x11 = calloc(1, sizeof(*disp_x11));
264         if (!disp_x11) {
265                 ERROR("allocation failed");
266                 goto no_x11;
267         }
269         disp = &disp_x11->base;
271         disp->fd = open(device, O_RDWR);
272         if (disp->fd < 0) {
273                 ERROR("could not open drm device: %s (%d)", strerror(errno), errno);
274                 goto no_x11_free;
275         }
277         if (drmGetMagic(disp->fd, &magic)) {
278                 ERROR("drmGetMagic failed");
279                 goto no_x11_free;
280         }
282         if (!DRI2Authenticate(dpy, root, magic)) {
283                 ERROR("DRI2Authenticate failed");
284                 goto no_x11_free;
285         }
287         disp->dev = omap_device_new(disp->fd);
288         if (!disp->dev) {
289                 ERROR("couldn't create device");
290                 goto no_x11_free;
291         }
293         disp->get_buffers = get_buffers;
294         disp->get_vid_buffers = get_vid_buffers;
295         disp->post_buffer = post_buffer;
296         disp->post_vid_buffer = post_vid_buffer;
298         /* note: set args to NULL after we've parsed them so other modules know
299          * that it is already parsed (since the arg parsing is decentralized)
300          */
301         for (i = 1; i < argc; i++) {
302                 if (!argv[i]) {
303                         continue;
304                 }
305                 if (!strcmp("-w", argv[i])) {
306                         argv[i++] = NULL;
307                         if (sscanf(argv[i], "%dx%d", &width, &height) != 2) {
308                                 ERROR("invalid arg: %s", argv[i]);
309                                 goto no_x11_free;
310                         }
311                 } else {
312                         /* ignore */
313                         continue;
314                 }
315                 argv[i] = NULL;
316         }
318         win = XCreateSimpleWindow(dpy, RootWindow(dpy, 0), 1, 1,
319                         width, height, 0, BlackPixel (dpy, 0), BlackPixel(dpy, 0));
320         XMapWindow(dpy, win);
321         XFlush(dpy);
323         disp_x11->dpy = dpy;
324         disp_x11->win = win;
326         if (!DRI2GetFormats(dpy, RootWindow(dpy, DefaultScreen(dpy)),
327                         &nformats, &formats)) {
328                 ERROR("DRI2GetFormats failed");
329                 goto no_x11_free;
330         }
332         if (nformats == 0) {
333                 ERROR("no formats!");
334                 goto no_x11_free;
335         }
337         /* print out supported formats */
338         MSG("Found %d supported formats:", nformats);
339         for (i = 0; i < nformats; i++) {
340                 if (is_fourcc(formats[i])) {
341                         MSG("  %d: %08x (\"%.4s\")", i, formats[i], (char *)&formats[i]);
342                 } else {
343                         MSG("  %d: %08x (device dependent)", i, formats[i]);
344                 }
345         }
347         DRI2CreateDrawable(dpy, win);
349         /* check some attribute.. just to exercise the code-path: */
350         if (!DRI2GetAttribute(dpy, win, ATOM("XV_CSC_MATRIX"), &i, &pval)) {
351                 ERROR("DRI2GetAttribute failed");
352                 goto no_x11_free;
353         }
355         MSG("Got CSC matrix:");
356         print_hex(i*4, (const unsigned char *)pval);
358         // XXX
360         return disp;
362 no_x11_free:
363         XFree(driver);
364         XFree(device);
365 no_x11:
366         ERROR("unimplemented");
367         return NULL;