/* * Copyright (C) 2011 Texas Instruments * Author: Rob Clark * * This program is free software; you can redistribute it and/or modify it * under the terms of the GNU General Public License version 2 as published by * the Free Software Foundation. * * This program is distributed in the hope that it will be useful, but WITHOUT * ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or * FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public License for * more details. * * You should have received a copy of the GNU General Public License along with * this program. If not, see . */ #include "util.h" #define NBUF 3 #define CNT 500 static void usage(char *name) { MSG("Usage: %s [OPTION]...", name); MSG("Simple page-flip test, similar to 'modetest' but with option to use tiled buffers."); MSG(""); disp_usage(); } int main(int argc, char **argv) { struct display *disp; struct buffer **buffers; int ret, i; MSG("Opening Display.."); disp = disp_open(argc, argv); if (!disp) { usage(argv[0]); return 1; } if (check_args(argc, argv)) { /* remaining args.. print usage msg */ usage(argv[0]); return 0; } buffers = disp_get_buffers(disp, NBUF); if (!buffers) { return 1; } for (i = 0; i < CNT; i++) { struct buffer *buf = buffers[i % NBUF]; fill(buf, i * 2); ret = disp_post_buffer(disp, buf); if (ret) { return ret; } } MSG("Ok!"); return 0; }