/* * Copyright (C) 2011 Texas Instruments * Author: Rob Clark * * This program is free software; you can redistribute it and/or modify it * under the terms of the GNU General Public License version 2 as published by * the Free Software Foundation. * * This program is distributed in the hope that it will be useful, but WITHOUT * ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or * FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public License for * more details. * * You should have received a copy of the GNU General Public License along with * this program. If not, see . */ #ifdef HAVE_CONFIG_H #include "config.h" #endif #include "util.h" #include #include /* NOTE: healthy dose of recycling from libdrm modetest app.. */ /* * Mode setting with the kernel interfaces is a bit of a chore. * First you have to find the connector in question and make sure the * requested mode is available. * Then you need to find the encoder attached to that connector so you * can bind it with a free crtc. */ struct connector { uint32_t id; char mode_str[64]; drmModeModeInfo *mode; drmModeEncoder *encoder; int crtc; int pipe; }; #define to_display_kms(x) container_of(x, struct display_kms, base) struct display_kms { struct display base; uint32_t connectors_count; struct connector connector[10]; drmModePlane *ovr[10]; int scheduled_flips, completed_flips; uint32_t bo_flags; drmModeResPtr resources; drmModePlaneRes *plane_resources; struct buffer *current; }; #define to_buffer_kms(x) container_of(x, struct buffer_kms, base) struct buffer_kms { struct buffer base; uint32_t fb_id; }; static struct omap_bo * alloc_bo(struct display *disp, uint32_t bpp, uint32_t width, uint32_t height, uint32_t *bo_handle, uint32_t *pitch) { struct display_kms *disp_kms = to_display_kms(disp); struct omap_bo *bo; uint32_t bo_flags = disp_kms->bo_flags; if ((bo_flags & OMAP_BO_TILED) == OMAP_BO_TILED) { bo_flags &= ~OMAP_BO_TILED; if (bpp == 8) { bo_flags |= OMAP_BO_TILED_8; } else if (bpp == 16) { bo_flags |= OMAP_BO_TILED_16; } else if (bpp == 32) { bo_flags |= OMAP_BO_TILED_32; } } bo_flags |= OMAP_BO_WC; if (bo_flags & OMAP_BO_TILED) { bo = omap_bo_new_tiled(disp->dev, ALIGN2(width,7), height, bo_flags); } else { bo = omap_bo_new(disp->dev, width * height * bpp / 8, bo_flags); } if (bo) { *bo_handle = omap_bo_handle(bo); *pitch = width * bpp / 8; if (bo_flags & OMAP_BO_TILED) *pitch = ALIGN2(*pitch, PAGE_SHIFT); } return bo; } static struct buffer * alloc_buffer(struct display *disp, uint32_t fourcc, uint32_t w, uint32_t h) { struct buffer_kms *buf_kms; struct buffer *buf; uint32_t bo_handles[4] = {0}, offsets[4] = {0}; int ret; buf_kms = calloc(1, sizeof(*buf_kms)); if (!buf_kms) { ERROR("allocation failed"); return NULL; } buf = &buf_kms->base; buf->fourcc = fourcc; buf->width = w; buf->height = h; buf->multiplanar = true; buf->nbo = 1; if (!fourcc) fourcc = FOURCC('A','R','2','4'); switch(fourcc) { case FOURCC('A','R','2','4'): buf->nbo = 1; buf->bo[0] = alloc_bo(disp, 32, buf->width, buf->height, &bo_handles[0], &buf->pitches[0]); break; case FOURCC('U','Y','V','Y'): case FOURCC('Y','U','Y','V'): buf->nbo = 1; buf->bo[0] = alloc_bo(disp, 16, buf->width, buf->height, &bo_handles[0], &buf->pitches[0]); break; case FOURCC('N','V','1','2'): if (disp->multiplanar) { buf->nbo = 2; buf->bo[0] = alloc_bo(disp, 8, buf->width, buf->height, &bo_handles[0], &buf->pitches[0]); buf->fd[0] = omap_bo_dmabuf(buf->bo[0]); buf->bo[1] = alloc_bo(disp, 16, buf->width/2, buf->height/2, &bo_handles[1], &buf->pitches[1]); buf->fd[1] = omap_bo_dmabuf(buf->bo[1]); } else { buf->nbo = 1; buf->bo[0] = alloc_bo(disp, 8, buf->width, buf->height * 3 / 2, &bo_handles[0], &buf->pitches[0]); buf->fd[0] = omap_bo_dmabuf(buf->bo[0]); bo_handles[1] = bo_handles[0]; buf->pitches[1] = buf->pitches[0]; offsets[1] = buf->width * buf->height; buf->multiplanar = false; } break; case FOURCC('I','4','2','0'): buf->nbo = 3; buf->bo[0] = alloc_bo(disp, 8, buf->width, buf->height, &bo_handles[0], &buf->pitches[0]); buf->bo[1] = alloc_bo(disp, 8, buf->width/2, buf->height/2, &bo_handles[1], &buf->pitches[1]); buf->bo[2] = alloc_bo(disp, 8, buf->width/2, buf->height/2, &bo_handles[2], &buf->pitches[2]); break; default: ERROR("invalid format: 0x%08x", fourcc); goto fail; } ret = drmModeAddFB2(disp->fd, buf->width, buf->height, fourcc, bo_handles, buf->pitches, offsets, &buf_kms->fb_id, 0); if (ret) { ERROR("drmModeAddFB2 failed: %s (%d)", strerror(errno), ret); goto fail; } return buf; fail: // XXX cleanup return NULL; } void free_buffers(struct display *disp, uint32_t n) { uint32_t i; for (i = 0; i < n; i++) { if (disp->buf[i]) { omap_bo_del(disp->buf[i]->bo[0]); if(disp->multiplanar){ omap_bo_del(disp->buf[i]->bo[1]); } } } free(disp->buf); } static struct buffer ** alloc_buffers(struct display *disp, uint32_t n, uint32_t fourcc, uint32_t w, uint32_t h) { struct buffer **bufs; uint32_t i = 0; bufs = calloc(n, sizeof(*bufs)); if (!bufs) { ERROR("allocation failed"); goto fail; } for (i = 0; i < n; i++) { bufs[i] = alloc_buffer(disp, fourcc, w, h); if (!bufs[i]) { ERROR("allocation failed"); goto fail; } } disp->buf=bufs; return bufs; fail: // XXX cleanup return NULL; } static struct buffer ** get_buffers(struct display *disp, uint32_t n) { return alloc_buffers(disp, n, 0, disp->width, disp->height); } static struct buffer ** get_vid_buffers(struct display *disp, uint32_t n, uint32_t fourcc, uint32_t w, uint32_t h) { return alloc_buffers(disp, n, fourcc, w, h); } static void page_flip_handler(int fd, unsigned int frame, unsigned int sec, unsigned int usec, void *data) { struct display *disp = data; struct display_kms *disp_kms = to_display_kms(disp); disp_kms->completed_flips++; MSG("Page flip: frame=%d, sec=%d, usec=%d, remaining=%d", frame, sec, usec, disp_kms->scheduled_flips - disp_kms->completed_flips); } static int post_buffer(struct display *disp, struct buffer *buf) { struct display_kms *disp_kms = to_display_kms(disp); struct buffer_kms *buf_kms = to_buffer_kms(buf); int ret, last_err = 0, x = 0; uint32_t i; for (i = 0; i < disp_kms->connectors_count; i++) { struct connector *connector = &disp_kms->connector[i]; if (! connector->mode) { continue; } if (! disp_kms->current) { /* first buffer we flip to, setup the mode (since this can't * be done earlier without a buffer to scanout) */ MSG("Setting mode %s on connector %d, crtc %d", connector->mode_str, connector->id, connector->crtc); ret = drmModeSetCrtc(disp->fd, connector->crtc, buf_kms->fb_id, x, 0, &connector->id, 1, connector->mode); x += connector->mode->hdisplay; } else { ret = drmModePageFlip(disp->fd, connector->crtc, buf_kms->fb_id, DRM_MODE_PAGE_FLIP_EVENT, disp); disp_kms->scheduled_flips++; } if (ret) { ERROR("Could not post buffer on crtc %d: %s (%d)", connector->crtc, strerror(errno), ret); last_err = ret; /* well, keep trying the reset of the connectors.. */ } } /* if we flipped, wait for all flips to complete! */ while (disp_kms->scheduled_flips > disp_kms->completed_flips) { drmEventContext evctx = { .version = DRM_EVENT_CONTEXT_VERSION, .page_flip_handler = page_flip_handler, }; struct timeval timeout = { .tv_sec = 3, .tv_usec = 0, }; fd_set fds; FD_ZERO(&fds); FD_SET(disp->fd, &fds); ret = select(disp->fd + 1, &fds, NULL, NULL, &timeout); if (ret <= 0) { if (errno == EAGAIN) { continue; /* keep going */ } else { ERROR("Timeout waiting for flip complete: %s (%d)", strerror(errno), ret); last_err = ret; break; } } drmHandleEvent(disp->fd, &evctx); } disp_kms->current = buf; return last_err; } static int post_vid_buffer(struct display *disp, struct buffer *buf, uint32_t x, uint32_t y, uint32_t w, uint32_t h) { struct display_kms *disp_kms = to_display_kms(disp); struct buffer_kms *buf_kms = to_buffer_kms(buf); int ret = 0; uint32_t i, j; /* ensure we have the overlay setup: */ for (i = 0; i < disp_kms->connectors_count; i++) { struct connector *connector = &disp_kms->connector[i]; uint32_t used_planes = 0; drmModeModeInfo *mode = connector->mode; if (! mode) { continue; } if (! disp_kms->ovr[i]) { for (j = 0; j < disp_kms->plane_resources->count_planes; j++) { drmModePlane *ovr = drmModeGetPlane(disp->fd, disp_kms->plane_resources->planes[j]); if ((ovr->possible_crtcs & (1 << connector->pipe)) && !(used_planes & (1 << j))) { disp_kms->ovr[i] = ovr; used_planes |= (1 << j); break; } } } if (! disp_kms->ovr[i]) { MSG("Could not find plane for crtc %d", connector->crtc); ret = -1; /* carry on and see if we can find at least one usable plane */ continue; } ret = drmModeSetPlane(disp->fd, disp_kms->ovr[i]->plane_id, connector->crtc, buf_kms->fb_id, 0, /* make video fullscreen: */ 0, 0, mode->hdisplay, mode->vdisplay, /* source/cropping coordinates are given in Q16 */ x << 16, y << 16, w << 16, h << 16); if (ret) { ERROR("failed to enable plane %d: %s", disp_kms->ovr[i]->plane_id, strerror(errno)); } } return ret; } static void close_kms(struct display *disp) { } static void connector_find_mode(struct display *disp, struct connector *c) { struct display_kms *disp_kms = to_display_kms(disp); drmModeConnector *connector; int i, j; /* First, find the connector & mode */ c->mode = NULL; for (i = 0; i < disp_kms->resources->count_connectors; i++) { connector = drmModeGetConnector(disp->fd, disp_kms->resources->connectors[i]); if (!connector) { ERROR("could not get connector %i: %s", disp_kms->resources->connectors[i], strerror(errno)); drmModeFreeConnector(connector); continue; } if (!connector->count_modes) { drmModeFreeConnector(connector); continue; } if (connector->connector_id != c->id) { drmModeFreeConnector(connector); continue; } for (j = 0; j < connector->count_modes; j++) { c->mode = &connector->modes[j]; if (!strcmp(c->mode->name, c->mode_str)) break; } /* Found it, break out */ if (c->mode) break; drmModeFreeConnector(connector); } if (!c->mode) { ERROR("failed to find mode \"%s\"", c->mode_str); return; } /* Now get the encoder */ for (i = 0; i < disp_kms->resources->count_encoders; i++) { c->encoder = drmModeGetEncoder(disp->fd, disp_kms->resources->encoders[i]); if (!c->encoder) { ERROR("could not get encoder %i: %s", disp_kms->resources->encoders[i], strerror(errno)); drmModeFreeEncoder(c->encoder); continue; } if (c->encoder->encoder_id == connector->encoder_id) break; drmModeFreeEncoder(c->encoder); } if (c->crtc == -1) c->crtc = c->encoder->crtc_id; /* and figure out which crtc index it is: */ for (i = 0; i < disp_kms->resources->count_crtcs; i++) { if (c->crtc == (int)disp_kms->resources->crtcs[i]) { c->pipe = i; break; } } } void disp_kms_usage(void) { MSG("KMS Display Options:"); MSG("\t-1 \t\tforce single-plane buffers"); MSG("\t-t \t8, 16, 32, or auto"); MSG("\t-s :\tset a mode"); MSG("\t-s @:\tset a mode"); } struct display * disp_kms_open(int argc, char **argv) { struct display_kms *disp_kms = NULL; struct display *disp; int i; disp_kms = calloc(1, sizeof(*disp_kms)); if (!disp_kms) { ERROR("allocation failed"); goto fail; } disp = &disp_kms->base; disp->fd = drmOpen("omapdrm", NULL); if (disp->fd < 0) { ERROR("could not open drm device: %s (%d)", strerror(errno), errno); goto fail; } disp->dev = omap_device_new(disp->fd); if (!disp->dev) { ERROR("couldn't create device"); goto fail; } disp->get_buffers = get_buffers; disp->get_vid_buffers = get_vid_buffers; disp->post_buffer = post_buffer; disp->post_vid_buffer = post_vid_buffer; disp->close = close_kms; disp->disp_free_buf = free_buffers ; disp_kms->resources = drmModeGetResources(disp->fd); if (!disp_kms->resources) { ERROR("drmModeGetResources failed: %s", strerror(errno)); goto fail; } disp_kms->plane_resources = drmModeGetPlaneResources(disp->fd); if (!disp_kms->plane_resources) { ERROR("drmModeGetPlaneResources failed: %s", strerror(errno)); goto fail; } disp->multiplanar = true; /* note: set args to NULL after we've parsed them so other modules know * that it is already parsed (since the arg parsing is decentralized) */ for (i = 1; i < argc; i++) { if (!argv[i]) { continue; } if (!strcmp("-1", argv[i])) { disp->multiplanar = false; } else if (!strcmp("-t", argv[i])) { int n; argv[i++] = NULL; if (!strcmp(argv[i], "auto")) { n = 0; } else if (sscanf(argv[i], "%d", &n) != 1) { ERROR("invalid arg: %s", argv[i]); goto fail; } disp_kms->bo_flags &= ~OMAP_BO_TILED; if (n == 8) { disp_kms->bo_flags |= OMAP_BO_TILED_8; } else if (n == 16) { disp_kms->bo_flags |= OMAP_BO_TILED_16; } else if (n == 32) { disp_kms->bo_flags |= OMAP_BO_TILED_32; } else if (n == 0) { disp_kms->bo_flags |= OMAP_BO_TILED; } else { ERROR("invalid arg: %s", argv[i]); goto fail; } } else if (!strcmp("-s", argv[i])) { struct connector *connector = &disp_kms->connector[disp_kms->connectors_count++]; connector->crtc = -1; argv[i++] = NULL; if (sscanf(argv[i], "%d:%64s", &connector->id, connector->mode_str) != 2 && sscanf(argv[i], "%d@%d:%64s", &connector->id, &connector->crtc, connector->mode_str) != 3) { // TODO: we could support connector specified as a name too, I suppose ERROR("invalid arg: %s", argv[i]); goto fail; } disp_kms->bo_flags |= OMAP_BO_SCANOUT; } else { /* ignore */ continue; } argv[i] = NULL; } disp->width = 0; disp->height = 0; for (i = 0; i < (int)disp_kms->connectors_count; i++) { struct connector *c = &disp_kms->connector[i]; connector_find_mode(disp, c); if (c->mode == NULL) continue; /* setup side-by-side virtual display */ disp->width += c->mode->hdisplay; if (disp->height < c->mode->vdisplay) { disp->height = c->mode->vdisplay; } } MSG("using %d connectors, %dx%d display, multiplanar: %d", disp_kms->connectors_count, disp->width, disp->height, disp->multiplanar); return disp; fail: // XXX cleanup return NULL; }