/* * Copyright (C) 2011 Texas Instruments * Author: Rob Clark * * This program is free software; you can redistribute it and/or modify it * under the terms of the GNU General Public License version 2 as published by * the Free Software Foundation. * * This program is distributed in the hope that it will be useful, but WITHOUT * ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or * FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public License for * more details. * * You should have received a copy of the GNU General Public License along with * this program. If not, see . */ #ifndef UTIL_H_ #define UTIL_H_ #include #include #include #include #include #include #include #include #include /* align x to next highest multiple of 2^n */ #define ALIGN2(x,n) (((x) + ((1 << (n)) - 1)) & ~((1 << (n)) - 1)) #ifndef __cplusplus typedef enum { false = 0, true = 1 } bool; #endif #include "list.h" /* Display Interface: * * Could be either KMS or X11 depending on build and * environment. Some of details of opening/connecting, allocating buffers, * etc, differ. The intention is just to provide as simple as possible * abstraction to avoid lots of duplication in each test app to handle * both cases. */ struct buffer { uint32_t fourcc, width, height; int nbo; struct omap_bo *bo[4]; uint32_t pitches[4]; struct list unlocked; bool multiplanar; /* True when Y and U/V are in separate buffers. */ int fd[4]; /* dmabuf */ bool noScale; }; /* State variables, used to maintain the playback rate. */ struct rate_control { int fps; /* When > zero, we maintain playback rate. */ long last_frame_mark; /* The time when the last frame was displayed, * as returned by the mark() function. */ int usecs_to_sleep; /* Number of useconds we have slep last frame. */ }; struct display { int fd; uint32_t width, height; struct omap_device *dev; struct list unlocked; struct rate_control rtctl; struct buffer ** (*get_buffers)(struct display *disp, uint32_t n); struct buffer ** (*get_vid_buffers)(struct display *disp, uint32_t n, uint32_t fourcc, uint32_t w, uint32_t h); int (*post_buffer)(struct display *disp, struct buffer *buf); int (*post_vid_buffer)(struct display *disp, struct buffer *buf, uint32_t x, uint32_t y, uint32_t w, uint32_t h); void (*close)(struct display *disp); void (*disp_free_buf) (struct display *disp, uint32_t n); bool multiplanar; /* True when Y and U/V are in separate buffers. */ struct buffer **buf; }; /* Print display related help */ void disp_usage(void); /* Open display.. X11 or KMS depending on cmdline args, environment, * and build args */ struct display * disp_open(int argc, char **argv); /* free allocated buffer */ void disp_free_buffers(struct display *disp, uint32_t n); /* Close display */ static inline void disp_close(struct display *disp) { disp->close(disp); } /* Get normal RGB/UI buffers (ie. not scaled, not YUV) */ static inline struct buffer ** disp_get_buffers(struct display *disp, uint32_t n) { return disp->get_buffers(disp, n); } /* Get video/overlay buffers (ie. can be YUV, scaled, etc) */ struct buffer ** disp_get_vid_buffers(struct display *disp, uint32_t n, uint32_t fourcc, uint32_t w, uint32_t h); /* flip to / post the specified buffer */ int disp_post_buffer(struct display *disp, struct buffer *buf); /* flip to / post the specified video buffer */ int disp_post_vid_buffer(struct display *disp, struct buffer *buf, uint32_t x, uint32_t y, uint32_t w, uint32_t h); /* Get plane (id = 1) for every connector and update the overlay */ int get_overlay_plane(struct display *disp, struct buffer *buf); /* allocate a buffer from pool created by disp_get_vid_buffers() */ struct buffer * disp_get_vid_buffer(struct display *disp); /* free to video buffer pool */ void disp_put_vid_buffer(struct display *disp, struct buffer *buf); /* helper to setup the display for apps that just need video with * no flipchain on the GUI layer */ struct buffer * disp_get_fb(struct display *disp); /* V4L2 utilities: */ struct v4l2; /* Print v4l2 related help */ void v4l2_usage(void); /* Open v4l2 (and media0??) XXX */ struct v4l2 * v4l2_open(int argc, char **argv, uint32_t *fourcc, uint32_t *width, uint32_t *height); /* Share the buffers w/ v4l2 via dmabuf */ int v4l2_reqbufs(struct v4l2 *v4l2, struct buffer **bufs, uint32_t n); int v4l2_streamon(struct v4l2 *v4l2); int v4l2_streamoff(struct v4l2 *v4l2); /* Queue a buffer to the camera */ int v4l2_qbuf(struct v4l2 *v4l2, struct buffer *buf); /* Dequeue buffer from camera */ struct buffer * v4l2_dqbuf(struct v4l2 *v4l2); /* Other utilities.. */ extern int debug; int check_args(int argc, char **argv); void fill(struct buffer *buf, int i); #define FOURCC(a, b, c, d) ((uint32_t)(uint8_t)(a) | ((uint32_t)(uint8_t)(b) << 8) | ((uint32_t)(uint8_t)(c) << 16) | ((uint32_t)(uint8_t)(d) << 24 )) #define FOURCC_STR(str) FOURCC(str[0], str[1], str[2], str[3]) /* Dynamic debug. */ #define DBG(fmt, ...) \ do { if (debug) fprintf(stderr, fmt "\n", ##__VA_ARGS__); } while (0) #define MSG(fmt, ...) \ do { fprintf(stderr, fmt "\n", ##__VA_ARGS__); } while (0) #define ERROR(fmt, ...) \ do { fprintf(stderr, "ERROR:%s:%d: " fmt "\n", __func__, __LINE__, ##__VA_ARGS__); } while (0) #ifndef container_of #define container_of(ptr, type, member) \ (type *)((char *)(ptr) - (char *) &((type *)0)->member) #endif #ifndef MIN # define MIN(a,b) (((a) < (b)) ? (a) : (b)) #endif #ifndef MAX # define MAX(a,b) (((a) > (b)) ? (a) : (b)) #endif #ifndef PAGE_SHIFT # define PAGE_SHIFT 12 #endif #ifndef PAGE_SIZE # define PAGE_SIZE (1 << PAGE_SHIFT) #endif /* align x to next highest multiple of 2^n */ #define ALIGN2(x,n) (((x) + ((1 << (n)) - 1)) & ~((1 << (n)) - 1)) #include static inline long mark(long *last) { struct timeval t; gettimeofday(&t, NULL); if (last) { long delta = t.tv_usec - *last; /* Handle the case, where the seconds have changed. * TODO: keep the whole timeval struct, to be able to cope with * more than one second deltas? */ if (t.tv_usec < *last) delta += 1000000; *last = t.tv_usec; return delta; } return t.tv_usec; } #endif /* UTIL_H_ */