glsdk/omapdrmtest.git
9 years agodisp: new option --no-post to disable buffers posting
Vincent Stehlé [Mon, 13 Aug 2012 12:37:09 +0000 (14:37 +0200)]
disp: new option --no-post to disable buffers posting

This allows to disable display updates from command line for benchmarking
purposes. This is done by overriding the display post_buffer() and
post_vid_buffer() functions with empty ones. Note that rate control does still
work.

Signed-off-by: Vincent Stehlé <v-stehle@ti.com>
9 years agodisp: new option --fps to maintain playback rate
Vincent Stehlé [Fri, 10 Aug 2012 14:45:50 +0000 (16:45 +0200)]
disp: new option --fps to maintain playback rate

Add a new rate control mechanism to the generic display, to allow forcing the
playback rate from command line.

We add rate control calls in the generic display functions disp_post_buffer()
and disp_post_vid_buffer(). As this is in the generic display part, x11 and kms
(and future) displays benefit from that mechanism.

We use the mark() and usleep() functions for the rate control implementation,
and we do also filter a bit the sleep duration, to avoid being too "choppy".

Signed-off-by: Vincent Stehlé <v-stehle@ti.com>
9 years agomark(): handle one second change properly
Vincent Stehlé [Fri, 10 Aug 2012 15:59:40 +0000 (17:59 +0200)]
mark(): handle one second change properly

We handle one second change properly. Two seconds and more will still lead to
erroneous deltas.

Signed-off-by: Vincent Stehlé <v-stehle@ti.com>
9 years agoviddec3test: -h, --help command line options
Vincent Stehlé [Fri, 10 Aug 2012 12:00:51 +0000 (14:00 +0200)]
viddec3test: -h, --help command line options

Signed-off-by: Vincent Stehlé <v-stehle@ti.com>
9 years agoIgnore tags
Vincent Stehlé [Thu, 5 Jul 2012 13:12:07 +0000 (15:12 +0200)]
Ignore tags

Signed-off-by: Vincent Stehlé <v-stehle@ti.com>
9 years agoAdd disp_close, disp_x11_close
Vincent Stehlé [Wed, 6 Jun 2012 16:33:15 +0000 (18:33 +0200)]
Add disp_close, disp_x11_close

Signed-off-by: Vincent Stehlé <v-stehle@ti.com>
9 years agoviddec3test: better initialization of buffer fields
Vincent Stehlé [Mon, 4 Jun 2012 08:01:43 +0000 (10:01 +0200)]
viddec3test: better initialization of buffer fields

We zero the allocated structures and initialize more fields to their correct
values. This, to avoid complaints from the codec.

Signed-off-by: Vincent Stehlé <v-stehle@ti.com>
9 years agoadd NOCONFIGURE support to autogen.sh
Rob Clark [Fri, 11 May 2012 01:38:10 +0000 (20:38 -0500)]
add NOCONFIGURE support to autogen.sh

9 years agoadd --disable-x11 option
Rob Clark [Thu, 10 May 2012 18:03:11 +0000 (13:03 -0500)]
add --disable-x11 option

For example, if you have x11/libdri2 but don't want to build x11
support, or if you have a pre-dri2video version of libdri2.

9 years agoPreserve user $CFLAGS
Vincent Stehlé [Tue, 8 May 2012 09:12:42 +0000 (11:12 +0200)]
Preserve user $CFLAGS

Do not override the $CFLAGS variable internally to allow specifying it at
configure time. Keep the Linux kernel include path flags in a separate
LIN_CFLAGS variable.

Signed-off-by: Vincent Stehlé <v-stehle@ti.com>
9 years agoutil: silence the compiler
Víctor Manuel Jáquez Leal [Mon, 16 Apr 2012 10:39:01 +0000 (12:39 +0200)]
util: silence the compiler

The compiler complains about this:

util.c: In function 'disp_get_vid_buffers':
util.c:76:17: warning: comparison between signed and unsigned integer expressions [-Wsign-compare]

This patch makes the counter variable unsigned too.

Signed-off-by: Víctor Manuel Jáquez Leal <vjaquez@igalia.com>
9 years agoconfigure.ac: pass kernel source path
Víctor Manuel Jáquez Leal [Mon, 2 Apr 2012 17:03:47 +0000 (19:03 +0200)]
configure.ac: pass kernel source path

By default the configure.ac only checked for videodev2.h in
/usr/src/linux-headers-$kversion.

With this patch the user can pass the kernel source path with the parameter
--with-kernel-source.

Signed-off-by: Víctor Manuel Jáquez Leal <vjaquez@igalia.com>
9 years agofliptest: request OMAP_BO_SCANOUT buffers
Vincent Stehlé [Fri, 30 Mar 2012 15:03:25 +0000 (17:03 +0200)]
fliptest: request OMAP_BO_SCANOUT buffers

Works on OMAP5 µEVM.

Signed-off-by: Vincent Stehlé <v-stehle@ti.com>
9 years agoAdd linux-headers include dir
Xavier Boudet [Fri, 30 Mar 2012 09:52:55 +0000 (09:52 +0000)]
Add linux-headers include dir

Signed-off-by: Xavier Boudet <x-boudet@ti.com>
9 years agofixes for proper stride for tiled buffers
Rob Clark [Thu, 1 Mar 2012 17:14:02 +0000 (11:14 -0600)]
fixes for proper stride for tiled buffers

9 years agoviddec: support for multiple decoder instances
Rob Clark [Thu, 1 Mar 2012 17:10:43 +0000 (11:10 -0600)]
viddec: support for multiple decoder instances

Enable support for testing multiple decoders in a single process.

9 years agox11: only open driver once
Rob Clark [Thu, 1 Mar 2012 17:01:15 +0000 (11:01 -0600)]
x11: only open driver once

This is needed if you have multiple dri2video windows in a single
process, since GEM handles only have meaning within the context of
a single file-open.

9 years agoviddec3test: add profiling for render times
Rob Clark [Tue, 31 Jan 2012 16:27:26 +0000 (10:27 -0600)]
viddec3test: add profiling for render times

9 years agocamera/v4l2 fixes
Rob Clark [Tue, 31 Jan 2012 16:27:01 +0000 (10:27 -0600)]
camera/v4l2 fixes

9 years agoadd missing #include's for config.h
Rob Clark [Thu, 26 Jan 2012 20:03:54 +0000 (14:03 -0600)]
add missing #include's for config.h

9 years agoWIP: x11/dri2video support
Rob Clark [Thu, 26 Jan 2012 20:02:06 +0000 (14:02 -0600)]
WIP: x11/dri2video support

9 years agofix typo in checking for libdri2
Rob Clark [Sat, 21 Jan 2012 19:55:37 +0000 (13:55 -0600)]
fix typo in checking for libdri2

9 years agoOnly enable v4l2/dmabuf tests if supported
Rob Clark [Sat, 21 Jan 2012 19:47:39 +0000 (13:47 -0600)]
Only enable v4l2/dmabuf tests if supported

Test v4l2 headers, and only enable v4l2/dmabuf tests if dmabuf support
is detected.

9 years agoadd viddec3 decoder test
Rob Clark [Thu, 26 Jan 2012 20:24:26 +0000 (14:24 -0600)]
add viddec3 decoder test

9 years agoadd video buffer lock/unlock API
Rob Clark [Thu, 26 Jan 2012 20:24:13 +0000 (14:24 -0600)]
add video buffer lock/unlock API

Intended to make life easier for clients like video decode test, which
needs a pool of buffers it can allocate from, and later free back to.

9 years agoadd video buffer support
Rob Clark [Sat, 21 Jan 2012 00:09:13 +0000 (18:09 -0600)]
add video buffer support

9 years agov4l2: add mcf pipeline setup
Rob Clark [Sat, 17 Dec 2011 01:45:30 +0000 (19:45 -0600)]
v4l2: add mcf pipeline setup

The MEDIA_IOC_SETUP_LINK sometimes fails with a timeout msg, and DQBUF
still hangs, but at least now it isn't failing at STREAMON.

9 years agoInitial commit
Rob Clark [Mon, 5 Dec 2011 21:13:10 +0000 (15:13 -0600)]
Initial commit