Adding fixes from Linaro
* debian/patches/111_armel-drv-fallbacks.patch:
- Make Panda able to load the omap video driver without the need of a
config
* debian/patches/516-randr-first-check-pScrPriv-before-using-the-pointer.patch
* debian/patches/517-randr-Catch-two-more-potential-unset-rrScrPriv-uses.patch:
- Add upstream patches to avoid seg fault in case the user is running with
multiple screens and xrandr is only enabled at one (LP: #1015292)
Signed-off-by: Ricardo Salveti de Araujo <ricardo.salveti@linaro.org>
- [DH] debian/patches/111_armel-drv-fallbacks.patch
- [DH] debian/patches/516-randr-first-check-pScrPriv-before-using-the-pointer.patch
- [DH] debian/patches/517-randr-Catch-two-more-potential-unset-rrScrPriv-uses.patch
- [DH] debian/patches/series