]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/xserver.git/blob - depcomp
Imported Debian patch 2:1.11.4-0ubuntu10.2
[glsdk/xserver.git] / depcomp
1 #! /bin/sh
2 # depcomp - compile a program generating dependencies as side-effects
4 scriptversion=2006-10-15.18
6 # Copyright (C) 1999, 2000, 2003, 2004, 2005, 2006 Free Software
7 # Foundation, Inc.
9 # This program is free software; you can redistribute it and/or modify
10 # it under the terms of the GNU General Public License as published by
11 # the Free Software Foundation; either version 2, or (at your option)
12 # any later version.
14 # This program is distributed in the hope that it will be useful,
15 # but WITHOUT ANY WARRANTY; without even the implied warranty of
16 # MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
17 # GNU General Public License for more details.
19 # You should have received a copy of the GNU General Public License
20 # along with this program; if not, write to the Free Software
21 # Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA
22 # 02110-1301, USA.
24 # As a special exception to the GNU General Public License, if you
25 # distribute this file as part of a program that contains a
26 # configuration script generated by Autoconf, you may include it under
27 # the same distribution terms that you use for the rest of that program.
29 # Originally written by Alexandre Oliva <oliva@dcc.unicamp.br>.
31 case $1 in
32   '')
33      echo "$0: No command.  Try \`$0 --help' for more information." 1>&2
34      exit 1;
35      ;;
36   -h | --h*)
37     cat <<\EOF
38 Usage: depcomp [--help] [--version] PROGRAM [ARGS]
40 Run PROGRAMS ARGS to compile a file, generating dependencies
41 as side-effects.
43 Environment variables:
44   depmode     Dependency tracking mode.
45   source      Source file read by `PROGRAMS ARGS'.
46   object      Object file output by `PROGRAMS ARGS'.
47   DEPDIR      directory where to store dependencies.
48   depfile     Dependency file to output.
49   tmpdepfile  Temporary file to use when outputing dependencies.
50   libtool     Whether libtool is used (yes/no).
52 Report bugs to <bug-automake@gnu.org>.
53 EOF
54     exit $?
55     ;;
56   -v | --v*)
57     echo "depcomp $scriptversion"
58     exit $?
59     ;;
60 esac
62 if test -z "$depmode" || test -z "$source" || test -z "$object"; then
63   echo "depcomp: Variables source, object and depmode must be set" 1>&2
64   exit 1
65 fi
67 # Dependencies for sub/bar.o or sub/bar.obj go into sub/.deps/bar.Po.
68 depfile=${depfile-`echo "$object" |
69   sed 's|[^\\/]*$|'${DEPDIR-.deps}'/&|;s|\.\([^.]*\)$|.P\1|;s|Pobj$|Po|'`}
70 tmpdepfile=${tmpdepfile-`echo "$depfile" | sed 's/\.\([^.]*\)$/.T\1/'`}
72 rm -f "$tmpdepfile"
74 # Some modes work just like other modes, but use different flags.  We
75 # parameterize here, but still list the modes in the big case below,
76 # to make depend.m4 easier to write.  Note that we *cannot* use a case
77 # here, because this file can only contain one case statement.
78 if test "$depmode" = hp; then
79   # HP compiler uses -M and no extra arg.
80   gccflag=-M
81   depmode=gcc
82 fi
84 if test "$depmode" = dashXmstdout; then
85    # This is just like dashmstdout with a different argument.
86    dashmflag=-xM
87    depmode=dashmstdout
88 fi
90 case "$depmode" in
91 gcc3)
92 ## gcc 3 implements dependency tracking that does exactly what
93 ## we want.  Yay!  Note: for some reason libtool 1.4 doesn't like
94 ## it if -MD -MP comes after the -MF stuff.  Hmm.
95 ## Unfortunately, FreeBSD c89 acceptance of flags depends upon
96 ## the command line argument order; so add the flags where they
97 ## appear in depend2.am.  Note that the slowdown incurred here
98 ## affects only configure: in makefiles, %FASTDEP% shortcuts this.
99   for arg
100   do
101     case $arg in
102     -c) set fnord "$@" -MT "$object" -MD -MP -MF "$tmpdepfile" "$arg" ;;
103     *)  set fnord "$@" "$arg" ;;
104     esac
105     shift # fnord
106     shift # $arg
107   done
108   "$@"
109   stat=$?
110   if test $stat -eq 0; then :
111   else
112     rm -f "$tmpdepfile"
113     exit $stat
114   fi
115   mv "$tmpdepfile" "$depfile"
116   ;;
118 gcc)
119 ## There are various ways to get dependency output from gcc.  Here's
120 ## why we pick this rather obscure method:
121 ## - Don't want to use -MD because we'd like the dependencies to end
122 ##   up in a subdir.  Having to rename by hand is ugly.
123 ##   (We might end up doing this anyway to support other compilers.)
124 ## - The DEPENDENCIES_OUTPUT environment variable makes gcc act like
125 ##   -MM, not -M (despite what the docs say).
126 ## - Using -M directly means running the compiler twice (even worse
127 ##   than renaming).
128   if test -z "$gccflag"; then
129     gccflag=-MD,
130   fi
131   "$@" -Wp,"$gccflag$tmpdepfile"
132   stat=$?
133   if test $stat -eq 0; then :
134   else
135     rm -f "$tmpdepfile"
136     exit $stat
137   fi
138   rm -f "$depfile"
139   echo "$object : \\" > "$depfile"
140   alpha=ABCDEFGHIJKLMNOPQRSTUVWXYZabcdefghijklmnopqrstuvwxyz
141 ## The second -e expression handles DOS-style file names with drive letters.
142   sed -e 's/^[^:]*: / /' \
143       -e 's/^['$alpha']:\/[^:]*: / /' < "$tmpdepfile" >> "$depfile"
144 ## This next piece of magic avoids the `deleted header file' problem.
145 ## The problem is that when a header file which appears in a .P file
146 ## is deleted, the dependency causes make to die (because there is
147 ## typically no way to rebuild the header).  We avoid this by adding
148 ## dummy dependencies for each header file.  Too bad gcc doesn't do
149 ## this for us directly.
150   tr ' ' '
151 ' < "$tmpdepfile" |
152 ## Some versions of gcc put a space before the `:'.  On the theory
153 ## that the space means something, we add a space to the output as
154 ## well.
155 ## Some versions of the HPUX 10.20 sed can't process this invocation
156 ## correctly.  Breaking it into two sed invocations is a workaround.
157     sed -e 's/^\\$//' -e '/^$/d' -e '/:$/d' | sed -e 's/$/ :/' >> "$depfile"
158   rm -f "$tmpdepfile"
159   ;;
161 hp)
162   # This case exists only to let depend.m4 do its work.  It works by
163   # looking at the text of this script.  This case will never be run,
164   # since it is checked for above.
165   exit 1
166   ;;
168 sgi)
169   if test "$libtool" = yes; then
170     "$@" "-Wp,-MDupdate,$tmpdepfile"
171   else
172     "$@" -MDupdate "$tmpdepfile"
173   fi
174   stat=$?
175   if test $stat -eq 0; then :
176   else
177     rm -f "$tmpdepfile"
178     exit $stat
179   fi
180   rm -f "$depfile"
182   if test -f "$tmpdepfile"; then  # yes, the sourcefile depend on other files
183     echo "$object : \\" > "$depfile"
185     # Clip off the initial element (the dependent).  Don't try to be
186     # clever and replace this with sed code, as IRIX sed won't handle
187     # lines with more than a fixed number of characters (4096 in
188     # IRIX 6.2 sed, 8192 in IRIX 6.5).  We also remove comment lines;
189     # the IRIX cc adds comments like `#:fec' to the end of the
190     # dependency line.
191     tr ' ' '
192 ' < "$tmpdepfile" \
193     | sed -e 's/^.*\.o://' -e 's/#.*$//' -e '/^$/ d' | \
194     tr '
195 ' ' ' >> $depfile
196     echo >> $depfile
198     # The second pass generates a dummy entry for each header file.
199     tr ' ' '
200 ' < "$tmpdepfile" \
201    | sed -e 's/^.*\.o://' -e 's/#.*$//' -e '/^$/ d' -e 's/$/:/' \
202    >> $depfile
203   else
204     # The sourcefile does not contain any dependencies, so just
205     # store a dummy comment line, to avoid errors with the Makefile
206     # "include basename.Plo" scheme.
207     echo "#dummy" > "$depfile"
208   fi
209   rm -f "$tmpdepfile"
210   ;;
212 aix)
213   # The C for AIX Compiler uses -M and outputs the dependencies
214   # in a .u file.  In older versions, this file always lives in the
215   # current directory.  Also, the AIX compiler puts `$object:' at the
216   # start of each line; $object doesn't have directory information.
217   # Version 6 uses the directory in both cases.
218   stripped=`echo "$object" | sed 's/\(.*\)\..*$/\1/'`
219   tmpdepfile="$stripped.u"
220   if test "$libtool" = yes; then
221     "$@" -Wc,-M
222   else
223     "$@" -M
224   fi
225   stat=$?
227   if test -f "$tmpdepfile"; then :
228   else
229     stripped=`echo "$stripped" | sed 's,^.*/,,'`
230     tmpdepfile="$stripped.u"
231   fi
233   if test $stat -eq 0; then :
234   else
235     rm -f "$tmpdepfile"
236     exit $stat
237   fi
239   if test -f "$tmpdepfile"; then
240     outname="$stripped.o"
241     # Each line is of the form `foo.o: dependent.h'.
242     # Do two passes, one to just change these to
243     # `$object: dependent.h' and one to simply `dependent.h:'.
244     sed -e "s,^$outname:,$object :," < "$tmpdepfile" > "$depfile"
245     sed -e "s,^$outname: \(.*\)$,\1:," < "$tmpdepfile" >> "$depfile"
246   else
247     # The sourcefile does not contain any dependencies, so just
248     # store a dummy comment line, to avoid errors with the Makefile
249     # "include basename.Plo" scheme.
250     echo "#dummy" > "$depfile"
251   fi
252   rm -f "$tmpdepfile"
253   ;;
255 icc)
256   # Intel's C compiler understands `-MD -MF file'.  However on
257   #    icc -MD -MF foo.d -c -o sub/foo.o sub/foo.c
258   # ICC 7.0 will fill foo.d with something like
259   #    foo.o: sub/foo.c
260   #    foo.o: sub/foo.h
261   # which is wrong.  We want:
262   #    sub/foo.o: sub/foo.c
263   #    sub/foo.o: sub/foo.h
264   #    sub/foo.c:
265   #    sub/foo.h:
266   # ICC 7.1 will output
267   #    foo.o: sub/foo.c sub/foo.h
268   # and will wrap long lines using \ :
269   #    foo.o: sub/foo.c ... \
270   #     sub/foo.h ... \
271   #     ...
273   "$@" -MD -MF "$tmpdepfile"
274   stat=$?
275   if test $stat -eq 0; then :
276   else
277     rm -f "$tmpdepfile"
278     exit $stat
279   fi
280   rm -f "$depfile"
281   # Each line is of the form `foo.o: dependent.h',
282   # or `foo.o: dep1.h dep2.h \', or ` dep3.h dep4.h \'.
283   # Do two passes, one to just change these to
284   # `$object: dependent.h' and one to simply `dependent.h:'.
285   sed "s,^[^:]*:,$object :," < "$tmpdepfile" > "$depfile"
286   # Some versions of the HPUX 10.20 sed can't process this invocation
287   # correctly.  Breaking it into two sed invocations is a workaround.
288   sed 's,^[^:]*: \(.*\)$,\1,;s/^\\$//;/^$/d;/:$/d' < "$tmpdepfile" |
289     sed -e 's/$/ :/' >> "$depfile"
290   rm -f "$tmpdepfile"
291   ;;
293 hp2)
294   # The "hp" stanza above does not work with aCC (C++) and HP's ia64
295   # compilers, which have integrated preprocessors.  The correct option
296   # to use with these is +Maked; it writes dependencies to a file named
297   # 'foo.d', which lands next to the object file, wherever that
298   # happens to be.
299   # Much of this is similar to the tru64 case; see comments there.
300   dir=`echo "$object" | sed -e 's|/[^/]*$|/|'`
301   test "x$dir" = "x$object" && dir=
302   base=`echo "$object" | sed -e 's|^.*/||' -e 's/\.o$//' -e 's/\.lo$//'`
303   if test "$libtool" = yes; then
304     tmpdepfile1=$dir$base.d
305     tmpdepfile2=$dir.libs/$base.d
306     "$@" -Wc,+Maked
307   else
308     tmpdepfile1=$dir$base.d
309     tmpdepfile2=$dir$base.d
310     "$@" +Maked
311   fi
312   stat=$?
313   if test $stat -eq 0; then :
314   else
315      rm -f "$tmpdepfile1" "$tmpdepfile2"
316      exit $stat
317   fi
319   for tmpdepfile in "$tmpdepfile1" "$tmpdepfile2"
320   do
321     test -f "$tmpdepfile" && break
322   done
323   if test -f "$tmpdepfile"; then
324     sed -e "s,^.*\.[a-z]*:,$object:," "$tmpdepfile" > "$depfile"
325     # Add `dependent.h:' lines.
326     sed -ne '2,${; s/^ *//; s/ \\*$//; s/$/:/; p;}' "$tmpdepfile" >> "$depfile"
327   else
328     echo "#dummy" > "$depfile"
329   fi
330   rm -f "$tmpdepfile" "$tmpdepfile2"
331   ;;
333 tru64)
334    # The Tru64 compiler uses -MD to generate dependencies as a side
335    # effect.  `cc -MD -o foo.o ...' puts the dependencies into `foo.o.d'.
336    # At least on Alpha/Redhat 6.1, Compaq CCC V6.2-504 seems to put
337    # dependencies in `foo.d' instead, so we check for that too.
338    # Subdirectories are respected.
339    dir=`echo "$object" | sed -e 's|/[^/]*$|/|'`
340    test "x$dir" = "x$object" && dir=
341    base=`echo "$object" | sed -e 's|^.*/||' -e 's/\.o$//' -e 's/\.lo$//'`
343    if test "$libtool" = yes; then
344       # With Tru64 cc, shared objects can also be used to make a
345       # static library.  This mechanism is used in libtool 1.4 series to
346       # handle both shared and static libraries in a single compilation.
347       # With libtool 1.4, dependencies were output in $dir.libs/$base.lo.d.
348       #
349       # With libtool 1.5 this exception was removed, and libtool now
350       # generates 2 separate objects for the 2 libraries.  These two
351       # compilations output dependencies in $dir.libs/$base.o.d and
352       # in $dir$base.o.d.  We have to check for both files, because
353       # one of the two compilations can be disabled.  We should prefer
354       # $dir$base.o.d over $dir.libs/$base.o.d because the latter is
355       # automatically cleaned when .libs/ is deleted, while ignoring
356       # the former would cause a distcleancheck panic.
357       tmpdepfile1=$dir.libs/$base.lo.d   # libtool 1.4
358       tmpdepfile2=$dir$base.o.d          # libtool 1.5
359       tmpdepfile3=$dir.libs/$base.o.d    # libtool 1.5
360       tmpdepfile4=$dir.libs/$base.d      # Compaq CCC V6.2-504
361       "$@" -Wc,-MD
362    else
363       tmpdepfile1=$dir$base.o.d
364       tmpdepfile2=$dir$base.d
365       tmpdepfile3=$dir$base.d
366       tmpdepfile4=$dir$base.d
367       "$@" -MD
368    fi
370    stat=$?
371    if test $stat -eq 0; then :
372    else
373       rm -f "$tmpdepfile1" "$tmpdepfile2" "$tmpdepfile3" "$tmpdepfile4"
374       exit $stat
375    fi
377    for tmpdepfile in "$tmpdepfile1" "$tmpdepfile2" "$tmpdepfile3" "$tmpdepfile4"
378    do
379      test -f "$tmpdepfile" && break
380    done
381    if test -f "$tmpdepfile"; then
382       sed -e "s,^.*\.[a-z]*:,$object:," < "$tmpdepfile" > "$depfile"
383       # That's a tab and a space in the [].
384       sed -e 's,^.*\.[a-z]*:[    ]*,,' -e 's,$,:,' < "$tmpdepfile" >> "$depfile"
385    else
386       echo "#dummy" > "$depfile"
387    fi
388    rm -f "$tmpdepfile"
389    ;;
391 #nosideeffect)
392   # This comment above is used by automake to tell side-effect
393   # dependency tracking mechanisms from slower ones.
395 dashmstdout)
396   # Important note: in order to support this mode, a compiler *must*
397   # always write the preprocessed file to stdout, regardless of -o.
398   "$@" || exit $?
400   # Remove the call to Libtool.
401   if test "$libtool" = yes; then
402     while test $1 != '--mode=compile'; do
403       shift
404     done
405     shift
406   fi
408   # Remove `-o $object'.
409   IFS=" "
410   for arg
411   do
412     case $arg in
413     -o)
414       shift
415       ;;
416     $object)
417       shift
418       ;;
419     *)
420       set fnord "$@" "$arg"
421       shift # fnord
422       shift # $arg
423       ;;
424     esac
425   done
427   test -z "$dashmflag" && dashmflag=-M
428   # Require at least two characters before searching for `:'
429   # in the target name.  This is to cope with DOS-style filenames:
430   # a dependency such as `c:/foo/bar' could be seen as target `c' otherwise.
431   "$@" $dashmflag |
432     sed 's:^[  ]*[^: ][^:][^:]*\:[    ]*:'"$object"'\: :' > "$tmpdepfile"
433   rm -f "$depfile"
434   cat < "$tmpdepfile" > "$depfile"
435   tr ' ' '
436 ' < "$tmpdepfile" | \
437 ## Some versions of the HPUX 10.20 sed can't process this invocation
438 ## correctly.  Breaking it into two sed invocations is a workaround.
439     sed -e 's/^\\$//' -e '/^$/d' -e '/:$/d' | sed -e 's/$/ :/' >> "$depfile"
440   rm -f "$tmpdepfile"
441   ;;
443 dashXmstdout)
444   # This case only exists to satisfy depend.m4.  It is never actually
445   # run, as this mode is specially recognized in the preamble.
446   exit 1
447   ;;
449 makedepend)
450   "$@" || exit $?
451   # Remove any Libtool call
452   if test "$libtool" = yes; then
453     while test $1 != '--mode=compile'; do
454       shift
455     done
456     shift
457   fi
458   # X makedepend
459   shift
460   cleared=no
461   for arg in "$@"; do
462     case $cleared in
463     no)
464       set ""; shift
465       cleared=yes ;;
466     esac
467     case "$arg" in
468     -D*|-I*)
469       set fnord "$@" "$arg"; shift ;;
470     # Strip any option that makedepend may not understand.  Remove
471     # the object too, otherwise makedepend will parse it as a source file.
472     -*|$object)
473       ;;
474     *)
475       set fnord "$@" "$arg"; shift ;;
476     esac
477   done
478   obj_suffix="`echo $object | sed 's/^.*\././'`"
479   touch "$tmpdepfile"
480   ${MAKEDEPEND-makedepend} -o"$obj_suffix" -f"$tmpdepfile" "$@"
481   rm -f "$depfile"
482   cat < "$tmpdepfile" > "$depfile"
483   sed '1,2d' "$tmpdepfile" | tr ' ' '
484 ' | \
485 ## Some versions of the HPUX 10.20 sed can't process this invocation
486 ## correctly.  Breaking it into two sed invocations is a workaround.
487     sed -e 's/^\\$//' -e '/^$/d' -e '/:$/d' | sed -e 's/$/ :/' >> "$depfile"
488   rm -f "$tmpdepfile" "$tmpdepfile".bak
489   ;;
491 cpp)
492   # Important note: in order to support this mode, a compiler *must*
493   # always write the preprocessed file to stdout.
494   "$@" || exit $?
496   # Remove the call to Libtool.
497   if test "$libtool" = yes; then
498     while test $1 != '--mode=compile'; do
499       shift
500     done
501     shift
502   fi
504   # Remove `-o $object'.
505   IFS=" "
506   for arg
507   do
508     case $arg in
509     -o)
510       shift
511       ;;
512     $object)
513       shift
514       ;;
515     *)
516       set fnord "$@" "$arg"
517       shift # fnord
518       shift # $arg
519       ;;
520     esac
521   done
523   "$@" -E |
524     sed -n -e '/^# [0-9][0-9]* "\([^"]*\)".*/ s:: \1 \\:p' \
525        -e '/^#line [0-9][0-9]* "\([^"]*\)".*/ s:: \1 \\:p' |
526     sed '$ s: \\$::' > "$tmpdepfile"
527   rm -f "$depfile"
528   echo "$object : \\" > "$depfile"
529   cat < "$tmpdepfile" >> "$depfile"
530   sed < "$tmpdepfile" '/^$/d;s/^ //;s/ \\$//;s/$/ :/' >> "$depfile"
531   rm -f "$tmpdepfile"
532   ;;
534 msvisualcpp)
535   # Important note: in order to support this mode, a compiler *must*
536   # always write the preprocessed file to stdout, regardless of -o,
537   # because we must use -o when running libtool.
538   "$@" || exit $?
539   IFS=" "
540   for arg
541   do
542     case "$arg" in
543     "-Gm"|"/Gm"|"-Gi"|"/Gi"|"-ZI"|"/ZI")
544         set fnord "$@"
545         shift
546         shift
547         ;;
548     *)
549         set fnord "$@" "$arg"
550         shift
551         shift
552         ;;
553     esac
554   done
555   "$@" -E |
556   sed -n '/^#line [0-9][0-9]* "\([^"]*\)"/ s::echo "`cygpath -u \\"\1\\"`":p' | sort | uniq > "$tmpdepfile"
557   rm -f "$depfile"
558   echo "$object : \\" > "$depfile"
559   . "$tmpdepfile" | sed 's% %\\ %g' | sed -n '/^\(.*\)$/ s::    \1 \\:p' >> "$depfile"
560   echo "        " >> "$depfile"
561   . "$tmpdepfile" | sed 's% %\\ %g' | sed -n '/^\(.*\)$/ s::\1\::p' >> "$depfile"
562   rm -f "$tmpdepfile"
563   ;;
565 none)
566   exec "$@"
567   ;;
569 *)
570   echo "Unknown depmode $depmode" 1>&2
571   exit 1
572   ;;
573 esac
575 exit 0
577 # Local Variables:
578 # mode: shell-script
579 # sh-indentation: 2
580 # eval: (add-hook 'write-file-hooks 'time-stamp)
581 # time-stamp-start: "scriptversion="
582 # time-stamp-format: "%:y-%02m-%02d.%02H"
583 # time-stamp-end: "$"
584 # End: