1 .TH XWIN __filemansuffix__ __vendorversion__
4 .SH NAME
5 XWinrc\- XWin Server Resource Configuration File.
8 .SH DESCRIPTION
9 The X Server for the X Window System on the Cygwin/X environment
10 running on Microsoft Windows, \fIXWin\fP can be optionally configured
11 with the \fIXWinrc\fP file. A system-wide configuration file should
12 be placed in \fI
13 __sysconfdir__/X11/system.XWinrc\fP, a per-user file
14 should be put at \fI$HOME/.XWinrc\fP. The \fIsystem.XWinrc\fP file is
15 read only if no \fI$HOME/.XWinrc\fP exist.
16 .PP
17 With the \fI.XWinrc\fP configuration file it is possible to do the
18 following:
19 .PP
20 1- To include items into the menu associated with the \fIXWin\fP icon
21 which is in the \fIWindows\fP system tray. This feature functions in
22 all XWin modes that have such tray icon.
23 .PP
24 2- To include items into the menu which is associated with the
25 \fIWindows\fP window that \fIXWin -multiwindow\fP produces for each
26 top-level X-window. That can be done both for the generic case and
27 for particular programs.
28 .PP
29 3- To change the icon that is associated to the \fIWindows\fP window
30 that \fIXWin -multiwindow\fP produces for each top-level X-window.
31 Again, that can be done both for the generic case and for particular
32 programs. The new icons associated should be \fIWindows\fP format
33 icons \fI.ico\fP.
34 .PP
35 4- To change the style that is associated to the \fIWindows\fP window
36 that \fI-multiwindow\fP produces for each top-level X window. Again,
37 that can be done both for the generic case and for particular programs.
40 .SH FILE FORMAT
41 .B Keywords
42 are case insensitive, but in this document they will be written
43 completely capitalized.
44 .PP
45 .B Comments
46 are legal pretty much anywhere you can have an end-of-line; they
47 begin with "#" or "//" and go to the end-of-line.
48 .PP
49 Quote marks in strings are optional unless the string has included spaces,
50 or could be parsed, ambiguously, as a misplaced keyword.
51 .PP
52 There are four kinds of instructions: miscellaneous, menu, icon and style.
55 .SH Miscellaneous instruction
56 .TP 8
57 .B DEBUG \fIString\fP
58 The \fIString\fP is printed to the XWin log file.
60 .TP 8
61 .B TRAYICON \fIicon-specifier\fB
62 The \fBTRAYICON\fP keyword changes the icon \fIXWin\fP displays in the
63 system tray area.
65 .TP 8
66 .B SILENTEXIT
67 The \fBSILENTEXIT\fP keyword, which takes no parameters, disables the
68 exit confirmation dialog if no clients are connected.
70 .TP 8
71 .B FORCEEXIT
72 The \fBFORCEEXIT\fP keyword, which takes no parameters, disables the
73 exit confirmation dialog always. Unsaved client work may be lost but
74 this may be useful if you want no dialogs.
76 .SH Menu instructions
77 .TP 8
78 .B MENU \fIMenu_Name\fP {
79 .br
80 .B \fIMenu_Item_Line\fP
81 .br
82 .B \fIMenu_Item_Line\fP
83 .br
84 .B \fI...\fP
85 .br
86 .B }
87 .br
88 This instruction defines a menu and asigns a \fIMenu_Name\fP to it.
89 \fIMenu_Item_Line\fP are lines of any of the following types:
90 .TP 8
91 .B \t SEPARATOR
92 .TP 8
93 .B \t \fIItem_Label\fP EXEC \fICommand\fP
94 .TP 8
95 .B \t \fIItem_Label\fP MENU \fIpreviously-defined-menu-name\fP
96 .TP 8
97 .B \t \fIItem_Label\fP ALWAYSONTOP
98 .TP 8
99 .B \t \fIItem_Label\fP RELOAD
100 .br
101 The \fIItem_Label\fP is the string that is written in the menu item.
102 .br
103 \fICommand\fP is a string with the command that will be executed by /bin/sh.
104 Here paths should be \fICYGWIN\fP style (e.g. /usr/local/bin/myprogram).
105 A string "%display%" appearing in the \fICommand\fP will be replaced
106 with the proper display variable (i.e. 127.0.0.1:<display>.0).
107 .br
108 \fBALWAYSONTOP\fP sets the window to which the menu is associated to
109 display above all others.
110 .br
111 \fBRELOAD\fP causes the XWinrc file to be reloaded and icons and menus
112 regenerated.
113 .TP 8
114 .B ROOTMENU \fIpreviously-defined-menu-name\fP
115 Includes the items in the indicated menu into the menu associated with
116 \fIXWin\fP that appears in the system tray.
117 .TP 8
118 .B DEFAULTSYSMENU \fIpreviously-defined-menu-name\fP ATSTART|ATEND
119 Includes the items in the indicated menu into the menu associated with
120 generic top-level X-Windows in the \fIXWin\fP \fImultiwindow\fP mode. The
121 keywords \fBATSTART\fP and \fBATEND\fP indicate if such items should be
122 included at the start or at the end of the menu.
123 .TP 8
124 .B SYSMENU {
125 \fIclass-or-name-of-window\fP \fIdefined-menu-name\fP \fBATSTART|ATEND\fP
126 .br
127 \fI...\fP
128 .br
129 \fB}\fP
130 .br
131 Associates a specific menu to a specified window class or name
132 in \fI-multiwindow\fP mode. The keywords ATSTART or ATEND indicate if
133 such items should be included at the start or at the end of the menu.
136 .SH Icon Instructions
137 When specifying an \fIicon-file\fP in the following commands several different formats are allowed:
138 .br
139 \fB"NAME.ICO"\fP\fI of an .ico format file\fP
140 .br
141 \t \t ("cygwin.ico", "apple.ico")
142 .br
143 \fB"NAME.DLL,nn"\fP\fI of a .DLL and icon index\fP
144 .br
145 \t \t ("c:\\windows\\system32\\shell32.dll,4" is the default folder icon)
146 .br
147 \fB",nnn"\fP\fI index into XWin.EXE internal ICON resources\fP
148 .br
149 \t \t (",101" is the 1st icon inside \fIXWin.EXE\fP)
150 .TP 8
151 .B ICONDIRECTORY \fIWindows-path-to-icon-directory\fP
152 Defines the default directory to search for \ficon-file\fP files.
153 It should be a \fIWindows\fP style path (e.g. C:\\cygwin\\usr\\local\\icons).
154 .TP 8
155 .B DEFAULTICON \fIicon-file\fP
156 Defines a replacement for the standard X icon for applications without
157 specified icons.
158 .TP 8
159 .B ICONS {
160 .br
161 \fIclass-or-name-of-window\fP \fIicon-file\fP
162 .br
163 \fI...\fP
164 .br
165 \fB}\fP
166 .br
167 Defines icon replacements windows matching the specified window class or names.
168 If multiple name or class matches occur for a window, only the first one
169 will be used.
171 .SH Style Instructions
172 .TP 8
173 .B STYLES {
174 \fIclass-or-name-of-window\fP \fIstyle-keyword-1\fP \fIstyle-keyword-2\fP
175 .br
176 \fI...\fP
177 .br
178 \fB}\fP
180 Associates specific styles to a specified window class or name
181 in \fI-multiwindow\fP mode. If multiple class or name matches occur,
182 for a window, only the first one will be used.
184 The style keywords indicate the following:
186 \fIstyle-keyword-1\fP
188 \fBTOPMOST\fP
189 .br
190 Open the class or name above all NOTOPMOST Microsoft Windows
191 .br
192 \fBMAXIMIZE\fP
193 .br
194 Start the class or name fullscreen.
195 .br
196 \fBMINIMIZE\fP
197 .br
198 Start the class or name iconic.
199 .br
200 \fBBOTTOM\fP
201 .br
202 Open the class or name below all Windows windows.
203 .br
205 \fIstyle-keyword-2\fP
207 \fBNOTITLE\fP
208 .br
209 No Windows title bar, for the class or name.
210 .br
211 \fBOUTLINE\fP
212 .br
213 No Windows title bar and just a thin-line border, for the class or name.
214 .br
215 \fBNOFRAME\fP
216 .br
217 No Windows title bar or border, for the class or name.
219 One keyword in \fIstyle-keyword-1\fP can be used with one keyword in \fIstyle-keyword-2\fP,
220 or any keyword can be used singly.
223 .SH EXAMPLE
224 .TP 8
225 This example adds an Xterm menu item to the system tray icon
226 \fBMENU systray {
227 .br
228 \t xterm EXEC "xterm -display %display% -sb -sl 999"
229 .br
230 \t SEPARATOR
231 .br
232 }
233 .br
234 ROOTMENU systray
235 \fP
237 .TP 8
238 This example makes an oclock window frameless in \fI-multiwindow\fP mode
239 \fBSTYLES {
240 .br
241 \t oclock NOFRAME
242 .br
243 }
247 .SH "SEE ALSO"
248 XWin(1)
251 .SH AUTHOR
252 The XWinrc feature of XWin was written primarily by Earle F. Philhower
253 III. Extended for style configuration by Colin Harrison.