1 /* xorg-server.h.in -*- c -*-
2 *
3 * This file is the template file for the xorg-server.h file which gets
4 * installed as part of the SDK. The #defines in this file overlap
5 * with those from config.h, but only for those options that we want
6 * to export to external modules. Boilerplate autotool #defines such
7 * as HAVE_STUFF and PACKAGE_NAME is kept in config.h
8 *
9 * It is still possible to update config.h.in using autoheader, since
10 * autoheader only creates a .h.in file for the first
11 * AM_CONFIG_HEADER() line, and thus does not overwrite this file.
12 *
13 * However, it should be kept in sync with this file.
14 */
16 #ifndef _XORG_SERVER_H_
17 #define _XORG_SERVER_H_
19 /* Support BigRequests extension */
20 #undef BIGREQS
22 /* Default font path */
23 #undef COMPILEDDEFAULTFONTPATH
25 /* Support Composite Extension */
26 #undef COMPOSITE
28 /* Build DPMS extension */
29 #undef DPMSExtension
31 /* Build GLX extension */
32 #undef GLXEXT
34 /* Support XDM-AUTH*-1 */
35 #undef HASXDMAUTH
37 /* Support SHM */
38 #undef HAS_SHM
40 /* Support IPv6 for TCP connections */
41 #undef IPv6
43 /* Support MIT-SHM Extension */
44 #undef MITSHM
46 /* Internal define for Xinerama */
47 #undef PANORAMIX
49 /* Support RANDR extension */
50 #undef RANDR
52 /* Support RENDER extension */
53 #undef RENDER
55 /* Support X resource extension */
56 #undef RES
58 /* Support MIT-SCREEN-SAVER extension */
59 #undef SCREENSAVER
61 /* Support SHAPE extension */
62 #undef SHAPE
64 /* Define to 1 on systems derived from System V Release 4 */
65 #undef SVR4
67 /* Support TCP socket connections */
68 #undef TCPCONN
70 /* Enable touchscreen support */
71 #undef TOUCHSCREEN
73 /* Support tslib touchscreen abstraction library */
74 #undef TSLIB
76 /* Support UNIX socket connections */
77 #undef UNIXCONN
79 /* unaligned word accesses behave as expected */
80 #undef WORKING_UNALIGNED_INT
82 /* Support XCMisc extension */
83 #undef XCMISC
85 /* Support Xdmcp */
86 #undef XDMCP
88 /* Build XFree86 BigFont extension */
89 #undef XF86BIGFONT
91 /* Support XFree86 Video Mode extension */
92 #undef XF86VIDMODE
94 /* Build XDGA support */
95 #undef XFreeXDGA
97 /* Support Xinerama extension */
98 #undef XINERAMA
100 /* Support X Input extension */
101 #undef XINPUT
103 /* XKB default rules */
104 #undef XKB_DFLT_RULES
106 /* Support loadable input and output drivers */
107 #undef XLOADABLE
109 /* Build DRI extension */
110 #undef XF86DRI
112 /* Build DRI2 extension */
113 #undef DRI2
115 /* Build Xorg server */
116 #undef XORGSERVER
118 /* Vendor release */
119 #undef XORG_RELEASE
121 /* Current Xorg version */
122 #undef XORG_VERSION_CURRENT
124 /* Build Xv Extension */
125 #undef XvExtension
127 /* Build XvMC Extension */
128 #undef XvMCExtension
130 /* Support XSync extension */
131 #undef XSYNC
133 /* Support XTest extension */
134 #undef XTEST
136 /* Support Xv Extension */
137 #undef XV
139 /* Vendor name */
140 #undef XVENDORNAME
142 /* BSD-compliant source */
143 #undef _BSD_SOURCE
145 /* POSIX-compliant source */
146 #undef _POSIX_SOURCE
148 /* X/Open-compliant source */
149 #undef _XOPEN_SOURCE
151 /* Vendor web address for support */
152 #undef __VENDORDWEBSUPPORT__
154 /* Location of configuration file */
155 #undef __XCONFIGFILE__
157 /* Name of X server */
158 #undef __XSERVERNAME__
160 /* Building vgahw module */
161 #undef WITH_VGAHW
163 /* System is BSD-like */
164 #undef CSRG_BASED
166 /* System has PC console */
167 #undef PCCONS_SUPPORT
169 /* System has PCVT console */
170 #undef PCVT_SUPPORT
172 /* System has syscons console */
173 #undef SYSCONS_SUPPORT
175 /* System has wscons console */
176 #undef WSCONS_SUPPORT
178 /* Loadable XFree86 server awesomeness */
179 #undef XFree86LOADER
181 /* Use libpciaccess */
182 #undef XSERVER_LIBPCIACCESS
184 /* X Access Control Extension */
185 #undef XACE
187 #ifdef _LP64
188 #define _XSERVER64 1
189 #endif
191 #endif /* _XORG_SERVER_H_ */