[i3-mote/i3-mote.git] / Basic-Test-Package / CC2650 / Test_CC2650_3wSPI_Master_MSP432_SlaveIRQ / uart_printf.c
1 /**************************************************************************************************\r
2 Filename: uart_printf.c\r
3 \r
4 Description: This file contains the TI-RTOS hooks for printing to UART via\r
5 System_printf(..).\r
6 \r
7 This is a very basic implementation made for the purposes of\r
8 terminal feedback in workshops, trainings and debug.\r
9 \r
10 Copyright 2015 Texas Instruments Incorporated. All rights reserved.\r
11 \r
12 IMPORTANT: Your use of this Software is limited to those specific rights\r
13 granted under the terms of a software license agreement between the user\r
14 who downloaded the software, his/her employer (which must be your employer)\r
15 and Texas Instruments Incorporated (the "License"). You may not use this\r
16 Software unless you agree to abide by the terms of the License. The License\r
17 limits your use, and you acknowledge, that the Software may not be modified,\r
18 copied or distributed unless embedded on a Texas Instruments microcontroller\r
19 or used solely and exclusively in conjunction with a Texas Instruments radio\r
20 frequency transceiver, which is integrated into your product. Other than for\r
21 the foregoing purpose, you may not use, reproduce, copy, prepare derivative\r
22 works of, modify, distribute, perform, display or sell this Software and/or\r
23 its documentation for any purpose.\r
24 \r
25 YOU FURTHER ACKNOWLEDGE AND AGREE THAT THE SOFTWARE AND DOCUMENTATION ARE\r
27 INCLUDING WITHOUT LIMITATION, ANY WARRANTY OF MERCHANTABILITY, TITLE,\r
28 NON-INFRINGEMENT AND FITNESS FOR A PARTICULAR PURPOSE. IN NO EVENT SHALL\r
29 TEXAS INSTRUMENTS OR ITS LICENSORS BE LIABLE OR OBLIGATED UNDER CONTRACT,\r
30 NEGLIGENCE, STRICT LIABILITY, CONTRIBUTION, BREACH OF WARRANTY, OR OTHER\r
31 LEGAL EQUITABLE THEORY ANY DIRECT OR INDIRECT DAMAGES OR EXPENSES\r
32 INCLUDING BUT NOT LIMITED TO ANY INCIDENTAL, SPECIAL, INDIRECT, PUNITIVE\r
33 OR CONSEQUENTIAL DAMAGES, LOST PROFITS OR LOST DATA, COST OF PROCUREMENT\r
34 OF SUBSTITUTE GOODS, TECHNOLOGY, SERVICES, OR ANY CLAIMS BY THIRD PARTIES\r
35 (INCLUDING BUT NOT LIMITED TO ANY DEFENSE THEREOF), OR OTHER SIMILAR COSTS.\r
36 \r
37 Should you have any questions regarding your right to use this Software,\r
38 contact Texas Instruments Incorporated at www.TI.com.\r
39 **************************************************************************************************/\r
40 \r
41 /*********************************************************************\r
42 * INCLUDES\r
43 */\r
44 #include <Board.h>\r
45 #include <ti/drivers/UART.h>\r
46 #include <ti/drivers/uart/UARTCC26XX.h>\r
47 #include <stdint.h>\r
48 \r
49 /*********************************************************************\r
50 * CONSTANTS\r
51 */\r
52 #define UART_PRINTF_BUF_LEN 1024\r
53 \r
54 /*********************************************************************\r
55 * TYPEDEFS\r
56 */\r
57 \r
58 /*********************************************************************\r
59 * LOCAL VARIABLES\r
60 */\r
61 static uint8_t uartPrintf_outArray[UART_PRINTF_BUF_LEN];\r
62 static uint16_t uartPrintf_head = 0;\r
63 static uint16_t uartPrintf_tail = 0;\r
64 static UART_Handle hUart = NULL;\r
65 \r
66 \r
67 /*********************************************************************\r
68 * PUBLIC FUNCTIONS\r
69 */\r
70 \r
71 /*********************************************************************\r
72 * @fn UartPrintf_init\r
73 *\r
74 * @brief Initializes the putchar hooks with the handle to the UART.\r
75 *\r
76 * @param handle - UART driver handle to an initialized and opened UART.\r
77 *\r
78 * @return None.\r
79 */\r
80 void UartPrintf_init(UART_Handle handle)\r
81 {\r
82 hUart = handle;\r
83 }\r
84 \r
85 /*********************************************************************\r
86 * SYSTEM HOOK FUNCTIONS\r
87 */\r
88 \r
89 /*********************************************************************\r
90 * @fn uartPrintf_putch\r
91 *\r
92 * @brief User supplied PutChar function.\r
93 * typedef Void (*SysCallback_PutchFxn)(Char);\r
94 *\r
95 * This function is called whenever the System module needs\r
96 * to output a character.\r
97 *\r
98 * This implementation fills a very basic ring-buffer, and relies\r
99 * on another function to flush this buffer out to UART.\r
100 *\r
101 * Requires SysCallback to be the system provider module.\r
102 * Initialized via SysCallback.putchFxn = "&uartPrintf_putch"; in the\r
103 * TI-RTOS configuration script.\r
104 *\r
105 * @param ch - Character\r
106 *\r
107 * @return None.\r
108 *\r
109 * @post ::uartPrintf_head is incremented by one with wrap at UART_PRINTF_BUF_LEN\r
110 * if there is room.\r
111 */\r
112 void uartPrintf_putch(char ch)\r
113 {\r
114 // uartPrintf_tail should never catch up with uartPrintf_head. Discard in-between bytes.\r
115 if ( (uartPrintf_head + 1) % UART_PRINTF_BUF_LEN == uartPrintf_tail )\r
116 return;\r
117 \r
118 uartPrintf_outArray[uartPrintf_head] = ch;\r
119 uartPrintf_head++;\r
120 \r
121 if (uartPrintf_head >= UART_PRINTF_BUF_LEN)\r
122 uartPrintf_head = 0;\r
123 }\r
124 \r
125 /*********************************************************************\r
126 * @fn uartPrintf_flush\r
127 *\r
128 * @brief Printf-buffer flush function\r
129 *\r
130 * In this implementation it is intended to be called by the\r
131 * Idle task when nothing else is running.\r
132 *\r
133 * This is achieved by setting up the Idle task in the TI-RTOS\r
134 * configuration script like so:\r
135 *\r
136 * var Idle = xdc.useModule('ti.sysbios.knl.Idle');\r
137 * Idle.addFunc('&uartPrintf_flush');\r
138 *\r
139 * @param None. Relies on global state.\r
140 *\r
141 * @return None.\r
142 *\r
143 * @post ::uartPrintf_tail is incremented to where uartPrintf_head\r
144 * was at the time the function was called.\r
145 */\r
146 void uartPrintf_flush()\r
147 {\r
148 // Abort in case UART hasn't been initialized.\r
149 if (NULL == hUart)\r
150 return;\r
151 \r
152 // Lock head position to avoid race conditions\r
153 uint16_t curHead = uartPrintf_head;\r
154 \r
155 // Find out how much data must be output, and how to output it.\r
156 bool needWrap = curHead < uartPrintf_tail;\r
157 uint16_t outLen = needWrap?(UART_PRINTF_BUF_LEN-uartPrintf_tail+curHead):(curHead-uartPrintf_tail);\r
158 \r
159 if (outLen)\r
160 {\r
161 if (needWrap)\r
162 {\r
163 UART_write(hUart, &uartPrintf_outArray[uartPrintf_tail], UART_PRINTF_BUF_LEN - uartPrintf_tail);\r
164 UART_write(hUart, uartPrintf_outArray, curHead);\r
165 }\r
166 else\r
167 {\r
168 UART_write(hUart, &uartPrintf_outArray[uartPrintf_tail], outLen);\r
169 }\r
170 }\r
171 \r
172 uartPrintf_tail = curHead;\r
173 }\r