Created Test MSP432-3wSPI-SlaveIRQ CC2650-Master
authorBorja Martinez <borja.martinez@gmail.com>
Sun, 11 Sep 2016 08:21:51 +0000 (10:21 +0200)
committerBorja Martinez <borja.martinez@gmail.com>
Sun, 11 Sep 2016 08:21:51 +0000 (10:21 +0200)
Basic-Test-Package/MSP432/Test_MSP432_3wSPI_M25P40/i3mote.h
Basic-Test-Package/MSP432/Test_MSP432_3wSPI_SlaveIRQ_CC2650_Master/i3mote.h [new file with mode: 0644]
Basic-Test-Package/MSP432/Test_MSP432_3wSPI_SlaveIRQ_CC2650_Master/main.c [new file with mode: 0644]
Basic-Test-Package/MSP432/Test_MSP432_3wSPI_SlaveIRQ_CC2650_Master/msp432p401r.cmd [new file with mode: 0644]
Basic-Test-Package/MSP432/Test_MSP432_3wSPI_SlaveIRQ_CC2650_Master/startup_msp432p401r_ccs.c [new file with mode: 0644]
Basic-Test-Package/MSP432/Test_MSP432_3wSPI_SlaveIRQ_CC2650_Master/system_msp432p401r.c [new file with mode: 0644]
Basic-Test-Package/MSP432/Test_MSP432_Blink_SysTick/i3mote.h
Basic-Test-Package/MSP432/Test_MSP432_ClockSystem/i3mote.h
Basic-Test-Package/MSP432/Test_MSP432_DebugUART_EchoPC/i3mote.h
Basic-Test-Package/MSP432/Test_MSP432_I2C_M24xx256/i3mote.h
Basic-Test-Package/MSP432/Test_MSP432_I2C_Sensors/i3mote.h

index 92b71fb4122bfba9dfdda9042b5b298dd65640af..6f7dbef77fd2275ef31e882f704e68d066583fd9 100644 (file)
 
 /* Flash SPI */
 #define FLASH_SPI_PORT       GPIO_PORT_P3
-#define FLASH_SPI_NCS_PIN    GPIO_PIN0
+#define FLASH_SPI_CSN_PIN    GPIO_PIN0
 #define FLASH_SPI_CLK_PIN    GPIO_PIN1
 #define FLASH_SPI_MISO_PIN   GPIO_PIN2
 #define FLASH_SPI_MOSI_PIN   GPIO_PIN3
 
 
+/* CC2650 SPI */
+#define CC2650_SPI_PORT      GPIO_PORT_P2
+#define CC2650_SPI_CSN_PIN    GPIO_PIN0
+#define CC2650_SPI_CLK_PIN   GPIO_PIN1
+#define CC2650_SPI_MISO_PIN  GPIO_PIN2
+#define CC2650_SPI_MOSI_PIN  GPIO_PIN3
+
+#define CC2650_INT_PORT      GPIO_PORT_P4
+#define CC2650_IRQ_PIN       GPIO_PIN0
+
 /* On Board EEPROM 25xx256*/
 #define EEPROM_SLAVE_ADDRESS 0x50
 
diff --git a/Basic-Test-Package/MSP432/Test_MSP432_3wSPI_SlaveIRQ_CC2650_Master/i3mote.h b/Basic-Test-Package/MSP432/Test_MSP432_3wSPI_SlaveIRQ_CC2650_Master/i3mote.h
new file mode 100644 (file)
index 0000000..6f7dbef
--- /dev/null
@@ -0,0 +1,63 @@
+/* HID Rev.B */
+#define HID_PORT GPIO_PORT_P6
+#define LEDR     GPIO_PIN2
+#define LEDG     GPIO_PIN3
+#define BUTTON   GPIO_PIN1
+
+/* Rev.A
+#define LED_PORT GPIO_PORT_P8
+#define LEDR    GPIO_PIN5
+#define LEDG    GPIO_PIN6
+#define BUTTON  GPIO_PIN7
+*/
+
+
+/* Power Control */
+#define CTL_PWR_PORT     GPIO_PORT_P2
+#define GPS_PWR_nEN_PIN  GPIO_PIN4
+#define SSM_PWR_nEN_PIN  GPIO_PIN5
+
+
+/* Debg UART */
+#define UART_BAUD_115200
+#define UART_PORT      GPIO_PORT_P1
+#define UART_TX_PIN    GPIO_PIN3
+#define UART_RX_PIN    GPIO_PIN2
+
+/* Flash SPI */
+#define FLASH_SPI_PORT       GPIO_PORT_P3
+#define FLASH_SPI_CSN_PIN    GPIO_PIN0
+#define FLASH_SPI_CLK_PIN    GPIO_PIN1
+#define FLASH_SPI_MISO_PIN   GPIO_PIN2
+#define FLASH_SPI_MOSI_PIN   GPIO_PIN3
+
+
+/* CC2650 SPI */
+#define CC2650_SPI_PORT      GPIO_PORT_P2
+#define CC2650_SPI_CSN_PIN    GPIO_PIN0
+#define CC2650_SPI_CLK_PIN   GPIO_PIN1
+#define CC2650_SPI_MISO_PIN  GPIO_PIN2
+#define CC2650_SPI_MOSI_PIN  GPIO_PIN3
+
+#define CC2650_INT_PORT      GPIO_PORT_P4
+#define CC2650_IRQ_PIN       GPIO_PIN0
+
+/* On Board EEPROM 25xx256*/
+#define EEPROM_SLAVE_ADDRESS 0x50
+
+
+/* On Board Sensors */
+#define IN219
+#define OPT3001
+#define HDC1080
+#define BMP280
+#define MPU9250
+#define TMP007
+
+#define Board_HDC1080_ADDR 0x40
+#define Board_INA219_ADDR  0x41
+#define Board_TMP007_ADDR  0x44
+#define Board_OPT3001_ADDR 0x45
+#define Board_MPU9250_ADDR 0x68
+#define Board_BMP280_ADDR  0x77
+
diff --git a/Basic-Test-Package/MSP432/Test_MSP432_3wSPI_SlaveIRQ_CC2650_Master/main.c b/Basic-Test-Package/MSP432/Test_MSP432_3wSPI_SlaveIRQ_CC2650_Master/main.c
new file mode 100644 (file)
index 0000000..45cc2b0
--- /dev/null
@@ -0,0 +1,250 @@
+/******************************************************************************
+ * MSP432 SPI - 3-wire Master Incremented Data
+ *
+ * This example shows how SPI master talks to SPI slave using 3-wire mode.
+ * Incrementing data is sent by the master starting at 0x01. Received data is
+ * expected to be same as the previous transmission.  eUSCI RX ISR is used to
+ * handle communication with the CPU, normally in LPM0. Because all execution 
+ * after LPM0 is in ISRs, initialization waits for DCO to stabilize against 
+ * ACLK.
+ *
+ * Note that in this example, EUSCIA1 is used for the SPI port. If the user
+ * wants to use EUSCIA for SPI operation, they are able to with the same APIs
+ * with the EUSCI_AX parameters.
+ *
+ * ACLK = ~32.768kHz, MCLK = SMCLK = DCO 3MHz
+ *
+ * Use with SPI Slave Data Echo code example.
+ *
+ *                MSP432P401
+ *              -----------------
+ *             |                 |
+ *             |             P2.3|<- Data In (UCA1SIMO)
+ *             |                 |
+ *             |             P2.2|-> Data Out (UCA1SOMI)
+ *             |                 |
+ *             |             P2.1|<- Serial Clock Out (UCA1CLK)
+ *             |                 |
+ *             |             P2.0|<- CS
+ *             |                 |
+ * Author: Timothy Logan
+*******************************************************************************/
+
+#include "i3mote.h"
+
+/* DriverLib Includes */
+#include "driverlib.h"
+
+/* Standard Includes */
+#include <stdint.h>
+#include <stdbool.h>
+#include <stdio.h>
+
+//#define DEBUG_UART
+#define UART_BAUD_115200
+
+/* Statics */
+static volatile uint8_t RXData = 0;
+static volatile uint8_t RXDataCnt = 0;
+
+static volatile uint8_t TXData = 0;
+
+const eUSCI_SPI_SlaveConfig spiSlaveConfig =
+{
+        EUSCI_B_SPI_MSB_FIRST,                          // MSB First
+        EUSCI_B_SPI_PHASE_DATA_CHANGED_ONFIRST_CAPTURED_ON_NEXT,  // Phase
+        EUSCI_B_SPI_CLOCKPOLARITY_INACTIVITY_HIGH,     // Normal Polarity
+        EUSCI_B_SPI_3PIN                               // 3wire mode
+};
+
+/* UART Configuration Parameter. These are the configuration parameters to
+ * make the eUSCI A UART module to operate with a 9600 baud rate.
+ * These values were calculated using the online calculator that TI provides at:
+ * http://software-dl.ti.com/msp430/msp430_public_sw/mcu/msp430/MSP430BaudRateConverter/index.html
+ */
+#ifdef UART_BAUD_9600
+const eUSCI_UART_Config uartConfig =
+{
+               EUSCI_A_UART_CLOCKSOURCE_SMCLK,          // SMCLK Clock Source
+               78,                                      // BRDIV = 78
+               2,                                       // UCxBRF = 2
+               0,                                       // UCxBRS = 0
+               EUSCI_A_UART_NO_PARITY,                  // No Parity
+               EUSCI_A_UART_LSB_FIRST,                  // LSB First
+               EUSCI_A_UART_ONE_STOP_BIT,               // One stop bit
+               EUSCI_A_UART_MODE,                       // UART mode
+               EUSCI_A_UART_OVERSAMPLING_BAUDRATE_GENERATION  // Oversampling
+};
+#endif
+
+#ifdef UART_BAUD_115200
+const eUSCI_UART_Config uartConfig =
+{
+               EUSCI_A_UART_CLOCKSOURCE_SMCLK,          // SMCLK Clock Source
+               6,                                      // BRDIV = 78
+               8,                                       // UCxBRF = 2
+               0,                                       // UCxBRS = 0
+               EUSCI_A_UART_NO_PARITY,                  // No Parity
+               EUSCI_A_UART_LSB_FIRST,                  // LSB First
+               EUSCI_A_UART_ONE_STOP_BIT,               // One stop bit
+               EUSCI_A_UART_MODE,                       // UART mode
+               EUSCI_A_UART_OVERSAMPLING_BAUDRATE_GENERATION  // Oversampling
+};
+#endif
+
+
+int main(void)
+{
+    volatile uint32_t ii;
+
+    /* Halting WDT  */
+    WDT_A_holdTimer();
+
+       /* LEDS Configuring P8.x as output */
+    /* Set LED Pins as Output */
+    MAP_GPIO_setAsOutputPin(HID_PORT,LEDG|LEDR);
+    MAP_GPIO_setOutputLowOnPin(HID_PORT,LEDG|LEDR);
+
+    /* Setting DCO to 12MHz */
+    CS_setDCOCenteredFrequency(CS_DCO_FREQUENCY_12);
+
+       /******************************************************************************/
+       /******************************************************************************/
+
+    /* Configure INT Pin */
+    MAP_GPIO_setOutputHighOnPin(CC2650_INT_PORT, CC2650_IRQ_PIN);
+    MAP_GPIO_setAsOutputPin(CC2650_INT_PORT, CC2650_IRQ_PIN);
+
+       /* CS Configuring P2.0 as Input */
+       MAP_GPIO_setAsInputPin(CC2650_SPI_PORT, CC2650_SPI_CSN_PIN);
+
+    /* Selecting P2.1, P2.2 and P2.3 in SPI mode */
+    GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P2,
+               CC2650_SPI_CLK_PIN | CC2650_SPI_MOSI_PIN | CC2650_SPI_MISO_PIN, GPIO_PRIMARY_MODULE_FUNCTION);
+
+    /* Configuring SPI in 3wire master mode */
+    //SPI_initMaster(EUSCI_A1_BASE, &spiMasterConfig);
+    SPI_initSlave(EUSCI_A1_BASE, &spiSlaveConfig);
+
+    /* Enable SPI module */
+    SPI_enableModule(EUSCI_A1_BASE);
+
+    /* Enabling interrupts */
+    SPI_enableInterrupt(EUSCI_A1_BASE, EUSCI_A_SPI_RECEIVE_INTERRUPT);
+    Interrupt_enableSleepOnIsrExit();
+    Interrupt_enableInterrupt(INT_EUSCIA1);
+    MAP_Interrupt_enableMaster();
+
+       /******************************************************************************/
+       /******************************************************************************/
+
+    MAP_SysTick_enableModule();
+    MAP_SysTick_setPeriod(12000000);
+    MAP_Interrupt_enableSleepOnIsrExit();
+    MAP_SysTick_enableInterrupt();
+
+       /******************************************************************************/
+       /******************************************************************************/
+
+#ifdef DEBUG_UART
+
+    /* Selecting P1.2 and P1.3 in UART mode */
+    MAP_GPIO_setAsPeripheralModuleFunctionInputPin(UART_PORT,
+               UART_RX_PIN | UART_TX_PIN, GPIO_PRIMARY_MODULE_FUNCTION);
+
+    /* Configuring UART Module */
+    MAP_UART_initModule(EUSCI_A0_BASE, &uartConfig);
+
+    /* Enable UART module */
+    MAP_UART_enableModule(EUSCI_A0_BASE);
+
+    /* Enabling UART interrupts */
+    /*
+     * MAP_UART_enableInterrupt(EUSCI_A0_BASE, EUSCI_A_UART_RECEIVE_INTERRUPT);
+     * MAP_Interrupt_enableInterrupt(INT_EUSCIA0);
+     */
+#endif
+
+       /******************************************************************************/
+       /******************************************************************************/
+
+
+    PCM_gotoLPM0();
+    __no_operation();
+}
+
+//******************************************************************************
+//
+//This is the EUSCI_A1 interrupt vector service routine.
+//
+//******************************************************************************
+void EUSCIA1_IRQHandler(void)
+{
+
+       int i;
+
+    uint32_t status = SPI_getEnabledInterruptStatus(EUSCI_A1_BASE);
+
+    SPI_clearInterruptFlag(EUSCI_A1_BASE, status);
+
+    if(status & EUSCI_A_SPI_RECEIVE_INTERRUPT)
+    {
+
+       MAP_GPIO_setOutputHighOnPin(GPIO_PORT_P6,GPIO_PIN3);
+
+        RXData = SPI_receiveData(EUSCI_A1_BASE);
+        RXDataCnt++;
+
+        printf("Cnt: %d Rx: %02X\n",RXDataCnt,RXData);
+
+        /* Extrenal UART Debug */
+               #ifdef DEBUG_UART
+            MAP_UART_transmitData(EUSCI_A0_BASE, TXData);
+            MAP_UART_transmitData(EUSCI_A0_BASE, RXData);
+               #endif
+
+        /* Send the next data packet */
+
+        /* USCI_A1 TX buffer ready? */
+        while (!(SPI_getInterruptStatus(EUSCI_A1_BASE, EUSCI_A_SPI_TRANSMIT_INTERRUPT)));
+
+               SPI_transmitData(EUSCI_A1_BASE, RXData);
+
+       for(i=0;i<20000;i++);
+               MAP_GPIO_toggleOutputOnPin(GPIO_PORT_P6,GPIO_PIN3);
+
+    }
+}
+
+
+void SysTick_Handler(void)
+{
+    int i;
+       /* Generate Periodic Interrupt */
+       MAP_GPIO_setOutputLowOnPin(CC2650_INT_PORT, CC2650_IRQ_PIN);
+    for(i=0;i<10000;i++);
+    MAP_GPIO_setOutputHighOnPin(CC2650_INT_PORT, CC2650_IRQ_PIN);
+
+    //MAP_GPIO_toggleOutputOnPin(GPIO_PORT_P6, GPIO_PIN2);
+
+}
+
+//******************************************************************************
+/* EUSCI A0 UART ISR - Echoes data back to PC host */
+//******************************************************************************
+/*
+ *
+ * void EUSCIA0_IRQHandler(void)
+ * {
+ *     uint32_t status = MAP_UART_getEnabledInterruptStatus(EUSCI_A0_BASE);
+ *
+ *     MAP_UART_clearInterruptFlag(EUSCI_A0_BASE, status);
+ *
+ *        if(status & EUSCI_A_UART_RECEIVE_INTERRUPT)
+ *     {
+ *        MAP_UART_transmitData(EUSCI_A0_BASE, MAP_UART_receiveData(EUSCI_A0_BASE));
+ *     }
+ *
+ * }
+ *
+ */
diff --git a/Basic-Test-Package/MSP432/Test_MSP432_3wSPI_SlaveIRQ_CC2650_Master/msp432p401r.cmd b/Basic-Test-Package/MSP432/Test_MSP432_3wSPI_SlaveIRQ_CC2650_Master/msp432p401r.cmd
new file mode 100644 (file)
index 0000000..346c191
--- /dev/null
@@ -0,0 +1,84 @@
+/******************************************************************************
+*
+* Copyright (C) 2012 - 2015 Texas Instruments Incorporated - http://www.ti.com/
+*
+* Redistribution and use in source and binary forms, with or without
+* modification, are permitted provided that the following conditions
+* are met:
+*
+*  Redistributions of source code must retain the above copyright
+*  notice, this list of conditions and the following disclaimer.
+*
+*  Redistributions in binary form must reproduce the above copyright
+*  notice, this list of conditions and the following disclaimer in the
+*  documentation and/or other materials provided with the
+*  distribution.
+*
+*  Neither the name of Texas Instruments Incorporated nor the names of
+*  its contributors may be used to endorse or promote products derived
+*  from this software without specific prior written permission.
+*
+* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
+* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
+* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
+* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
+* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
+* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
+* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
+* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
+* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
+* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
+* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
+*
+* Default linker command file for Texas Instruments MSP432P401R
+*
+* File creation date: 2015-09-03
+*
+*****************************************************************************/
+
+--retain=flashMailbox
+
+MEMORY
+{
+    MAIN       (RX) : origin = 0x00000000, length = 0x00040000
+    INFO       (RX) : origin = 0x00200000, length = 0x00004000
+    SRAM_CODE  (RWX): origin = 0x01000000, length = 0x00010000
+    SRAM_DATA  (RW) : origin = 0x20000000, length = 0x00010000
+}
+
+/* The following command line options are set as part of the CCS project.    */
+/* If you are building using the command line, or for some reason want to    */
+/* define them here, you can uncomment and modify these lines as needed.     */
+/* If you are using CCS for building, it is probably better to make any such */
+/* modifications in your CCS project and leave this file alone.              */
+/*                                                                           */
+/* A heap size of 1024 bytes is recommended when you plan to use printf()    */
+/* for debug output to the console window.                                   */
+/*                                                                           */
+/* --heap_size=1024                                                          */
+/* --stack_size=512                                                          */
+/* --library=rtsv7M4_T_le_eabi.lib                                           */
+
+/* Section allocation in memory */
+
+SECTIONS
+{
+    .intvecs:   > 0x00000000
+    .text   :   > MAIN
+    .const  :   > MAIN
+    .cinit  :   > MAIN
+    .pinit  :   > MAIN
+    .init_array  :   > MAIN
+
+    .flashMailbox : > 0x00200000
+
+    .vtable :   > 0x20000000
+    .data   :   > SRAM_DATA
+    .bss    :   > SRAM_DATA
+    .sysmem :   > SRAM_DATA
+    .stack  :   > SRAM_DATA (HIGH)
+}
+
+/* Symbolic definition of the WDTCTL register for RTS */
+WDTCTL_SYM = 0x4000480C;
+
diff --git a/Basic-Test-Package/MSP432/Test_MSP432_3wSPI_SlaveIRQ_CC2650_Master/startup_msp432p401r_ccs.c b/Basic-Test-Package/MSP432/Test_MSP432_3wSPI_SlaveIRQ_CC2650_Master/startup_msp432p401r_ccs.c
new file mode 100644 (file)
index 0000000..47af010
--- /dev/null
@@ -0,0 +1,189 @@
+/*
+ * -------------------------------------------
+ *    MSP432 DriverLib - v3_10_00_09 
+ * -------------------------------------------
+*/
+
+#include <stdint.h>
+
+/* Forward declaration of the default fault handlers. */
+static void resetISR(void);
+static void nmiISR(void);
+static void faultISR(void);
+static void defaultISR(void);
+
+
+/* External declaration for the reset handler that is to be called when the */
+/* processor is started                                                     */
+extern void _c_int00(void);
+
+/* External declaration for system initialization function                  */
+extern void SystemInit(void);
+
+/* Linker variable that marks the top of the stack. */
+extern unsigned long __STACK_END;
+
+
+/* External declarations for the interrupt handlers used by the application. */
+extern void EUSCIA1_IRQHandler (void);
+extern void EUSCIA0_IRQHandler (void);
+extern void SysTick_Handler (void);
+
+/* Interrupt vector table.  Note that the proper constructs must be placed on this to  */
+/* ensure that it ends up at physical address 0x0000.0000 or at the start of          */
+/* the program if located at a start address other than 0.                            */
+#pragma RETAIN(interruptVectors)
+#pragma DATA_SECTION(interruptVectors, ".intvecs")
+void (* const interruptVectors[])(void) =
+{
+    (void (*)(void))((uint32_t)&__STACK_END),
+                                            /* The initial stack pointer */
+    resetISR,                               /* The reset handler         */
+    nmiISR,                                 /* The NMI handler           */
+    faultISR,                               /* The hard fault handler    */
+    defaultISR,                             /* The MPU fault handler     */
+    defaultISR,                             /* The bus fault handler     */
+    defaultISR,                             /* The usage fault handler   */
+    0,                                      /* Reserved                  */
+    0,                                      /* Reserved                  */
+    0,                                      /* Reserved                  */
+    0,                                      /* Reserved                  */
+    defaultISR,                             /* SVCall handler            */
+    defaultISR,                             /* Debug monitor handler     */
+    0,                                      /* Reserved                  */
+    defaultISR,                             /* The PendSV handler        */
+       SysTick_Handler,                        /* The SysTick handler       */
+    defaultISR,                             /* PSS ISR                   */
+    defaultISR,                             /* CS ISR                    */
+    defaultISR,                             /* PCM ISR                   */
+    defaultISR,                             /* WDT ISR                   */
+    defaultISR,                             /* FPU ISR                   */
+    defaultISR,                             /* FLCTL ISR                 */
+    defaultISR,                             /* COMP0 ISR                 */
+    defaultISR,                             /* COMP1 ISR                 */
+    defaultISR,                             /* TA0_0 ISR                 */
+    defaultISR,                             /* TA0_N ISR                 */
+    defaultISR,                             /* TA1_0 ISR                 */
+    defaultISR,                             /* TA1_N ISR                 */
+    defaultISR,                             /* TA2_0 ISR                 */
+    defaultISR,                             /* TA2_N ISR                 */
+    defaultISR,                             /* TA3_0 ISR                 */
+    defaultISR,                             /* TA3_N ISR                 */
+       defaultISR,                             /* EUSCIA0 ISR               */
+       EUSCIA1_IRQHandler,                     /* EUSCIA1 ISR               */
+    defaultISR,                             /* EUSCIA2 ISR               */
+    defaultISR,                             /* EUSCIA3 ISR               */
+    defaultISR,                             /* EUSCIB0 ISR               */
+    defaultISR,                             /* EUSCIB1 ISR               */
+    defaultISR,                             /* EUSCIB2 ISR               */
+    defaultISR,                             /* EUSCIB3 ISR               */
+    defaultISR,                             /* ADC14 ISR                 */
+    defaultISR,                             /* T32_INT1 ISR              */
+    defaultISR,                             /* T32_INT2 ISR              */
+    defaultISR,                             /* T32_INTC ISR              */
+    defaultISR,                             /* AES ISR                   */
+    defaultISR,                             /* RTC ISR                   */
+    defaultISR,                             /* DMA_ERR ISR               */
+    defaultISR,                             /* DMA_INT3 ISR              */
+    defaultISR,                             /* DMA_INT2 ISR              */
+    defaultISR,                             /* DMA_INT1 ISR              */
+    defaultISR,                             /* DMA_INT0 ISR              */
+    defaultISR,                             /* PORT1 ISR                 */
+    defaultISR,                             /* PORT2 ISR                 */
+    defaultISR,                             /* PORT3 ISR                 */
+    defaultISR,                             /* PORT4 ISR                 */
+    defaultISR,                             /* PORT5 ISR                 */
+    defaultISR,                             /* PORT6 ISR                 */
+    defaultISR,                             /* Reserved 41               */
+    defaultISR,                             /* Reserved 42               */
+    defaultISR,                             /* Reserved 43               */
+    defaultISR,                             /* Reserved 44               */
+    defaultISR,                             /* Reserved 45               */
+    defaultISR,                             /* Reserved 46               */
+    defaultISR,                             /* Reserved 47               */
+    defaultISR,                             /* Reserved 48               */
+    defaultISR,                             /* Reserved 49               */
+    defaultISR,                             /* Reserved 50               */
+    defaultISR,                             /* Reserved 51               */
+    defaultISR,                             /* Reserved 52               */
+    defaultISR,                             /* Reserved 53               */
+    defaultISR,                             /* Reserved 54               */
+    defaultISR,                             /* Reserved 55               */
+    defaultISR,                             /* Reserved 56               */
+    defaultISR,                             /* Reserved 57               */
+    defaultISR,                             /* Reserved 58               */
+    defaultISR,                             /* Reserved 59               */
+    defaultISR,                             /* Reserved 60               */
+    defaultISR,                             /* Reserved 61               */
+    defaultISR,                             /* Reserved 62               */
+    defaultISR                              /* Reserved 63               */
+};
+
+
+/* This is the code that gets called when the processor first starts execution */
+/* following a reset event.  Only the absolutely necessary set is performed,   */
+/* after which the application supplied entry() routine is called.  Any fancy  */
+/* actions (such as making decisions based on the reset cause register, and    */
+/* resetting the bits in that register) are left solely in the hands of the    */
+/* application.                                                                */
+void resetISR(void)
+{
+    SystemInit();
+
+    /* Jump to the CCS C Initialization Routine. */
+    __asm("    .global _c_int00\n"
+          "    b.w     _c_int00");
+}
+
+/* This is the code that gets called when the processor receives a NMI.  This  */
+/* simply enters an infinite loop, preserving the system state for examination */
+/* by a debugger.                                                              */
+static void nmiISR(void)
+{
+    /* Fault trap exempt from ULP advisor */
+    #pragma diag_push
+    #pragma CHECK_ULP("-2.1")
+
+    /* Enter an infinite loop. */
+    while(1)
+    {
+    }
+
+    #pragma diag_pop
+}
+
+
+/* This is the code that gets called when the processor receives a fault        */
+/* interrupt.  This simply enters an infinite loop, preserving the system state */
+/* for examination by a debugger.                                               */
+static void faultISR(void)
+{
+    /* Fault trap exempt from ULP advisor */
+    #pragma diag_push
+    #pragma CHECK_ULP("-2.1")
+
+    /* Enter an infinite loop. */
+    while(1)
+    {
+    }
+
+    #pragma diag_pop
+}
+
+
+/* This is the code that gets called when the processor receives an unexpected  */
+/* interrupt.  This simply enters an infinite loop, preserving the system state */
+/* for examination by a debugger.                                               */
+static void defaultISR(void)
+{
+    /* Fault trap exempt from ULP advisor */
+    #pragma diag_push
+    #pragma CHECK_ULP("-2.1")
+
+    /* Enter an infinite loop. */
+    while(1)
+    {
+    }
+
+    #pragma diag_pop
+}
diff --git a/Basic-Test-Package/MSP432/Test_MSP432_3wSPI_SlaveIRQ_CC2650_Master/system_msp432p401r.c b/Basic-Test-Package/MSP432/Test_MSP432_3wSPI_SlaveIRQ_CC2650_Master/system_msp432p401r.c
new file mode 100644 (file)
index 0000000..93b5a72
--- /dev/null
@@ -0,0 +1,435 @@
+/*
+ * -------------------------------------------
+ *    MSP432 DriverLib - v3_10_00_09 
+ * -------------------------------------------
+ *
+ * --COPYRIGHT--,BSD,BSD
+ * Copyright (c) 2014, Texas Instruments Incorporated
+ * All rights reserved.
+ *
+ * Redistribution and use in source and binary forms, with or without
+ * modification, are permitted provided that the following conditions
+ * are met:
+ *
+ * *  Redistributions of source code must retain the above copyright
+ *    notice, this list of conditions and the following disclaimer.
+ *
+ * *  Redistributions in binary form must reproduce the above copyright
+ *    notice, this list of conditions and the following disclaimer in the
+ *    documentation and/or other materials provided with the distribution.
+ *
+ * *  Neither the name of Texas Instruments Incorporated nor the names of
+ *    its contributors may be used to endorse or promote products derived
+ *    from this software without specific prior written permission.
+ *
+ * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
+ * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
+ * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
+ * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
+ * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
+ * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
+ * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
+ * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
+ * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
+ * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
+ * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
+ * --/COPYRIGHT--*/
+/**************************************************************************//**
+* @file     system_msp432p401r.c
+* @brief    CMSIS Cortex-M4F Device Peripheral Access Layer Source File for
+*           MSP432P401R
+* @version  V1.00
+* @date     20-Oct-2015
+*
+* @note     View configuration instructions embedded in comments
+*
+******************************************************************************/
+//*****************************************************************************
+//
+// Copyright (C) 2015 Texas Instruments Incorporated - http://www.ti.com/
+//
+// Redistribution and use in source and binary forms, with or without
+// modification, are permitted provided that the following conditions
+// are met:
+//
+//  Redistributions of source code must retain the above copyright
+//  notice, this list of conditions and the following disclaimer.
+//
+//  Redistributions in binary form must reproduce the above copyright
+//  notice, this list of conditions and the following disclaimer in the
+//  documentation and/or other materials provided with the
+//  distribution.
+//
+//  Neither the name of Texas Instruments Incorporated nor the names of
+//  its contributors may be used to endorse or promote products derived
+//  from this software without specific prior written permission.
+//
+// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
+// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
+// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
+// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
+// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
+// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
+// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
+// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
+// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
+// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
+// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
+//
+//*****************************************************************************
+
+#include <stdint.h>
+
+#include "msp.h"
+
+/*--------------------- Configuration Instructions ----------------------------
+   1. If you prefer to halt the Watchdog Timer, set __HALT_WDT to 1:
+   #define __HALT_WDT       1
+   2. Insert your desired CPU frequency in Hz at:
+   #define __SYSTEM_CLOCK   3000000
+   3. If you prefer the DC-DC power regulator (more efficient at higher
+       frequencies), set the __REGULATOR to 1:
+   #define __REGULATOR      1
+ *---------------------------------------------------------------------------*/
+
+/*--------------------- Watchdog Timer Configuration ------------------------*/
+//  Halt the Watchdog Timer
+//     <0> Do not halt the WDT
+//     <1> Halt the WDT
+#define __HALT_WDT         1
+
+/*--------------------- CPU Frequency Configuration -------------------------*/
+//  CPU Frequency
+//     <1500000> 1.5 MHz
+//     <3000000> 3 MHz
+//     <12000000> 12 MHz
+//     <24000000> 24 MHz
+//     <48000000> 48 MHz
+#define  __SYSTEM_CLOCK    1500000
+
+/*--------------------- Power Regulator Configuration -----------------------*/
+//  Power Regulator Mode
+//     <0> LDO
+//     <1> DC-DC
+#define __REGULATOR        1
+
+/*----------------------------------------------------------------------------
+   Define clocks, used for SystemCoreClockUpdate()
+ *---------------------------------------------------------------------------*/
+#define __VLOCLK           10000
+#define __MODCLK           24000000
+#define __LFXT             32768
+#define __HFXT             48000000
+
+/*----------------------------------------------------------------------------
+   Clock Variable definitions
+ *---------------------------------------------------------------------------*/
+uint32_t SystemCoreClock = __SYSTEM_CLOCK;  /*!< System Clock Frequency (Core Clock)*/
+
+/**
+ * Update SystemCoreClock variable
+ *
+ * @param  none
+ * @return none
+ *
+ * @brief  Updates the SystemCoreClock with current core Clock
+ *         retrieved from cpu registers.
+ */
+void SystemCoreClockUpdate(void)
+{
+    uint32_t source, divider;
+    uint8_t dividerValue;
+
+    float dcoConst;
+    int32_t calVal;
+    uint32_t centeredFreq;
+    int16_t dcoTune;
+
+    divider = (CS->CTL1 & CS_CTL1_DIVM_MASK) >> CS_CTL1_DIVM_OFS;
+    dividerValue = 1 << divider;
+    source = CS->CTL1 & CS_CTL1_SELM_MASK;
+
+    switch(source)
+    {
+    case CS_CTL1_SELM__LFXTCLK:
+        if(BITBAND_PERI(CS->IFG, CS_IFG_LFXTIFG_OFS))
+        {
+            // Clear interrupt flag
+            CS->KEY = CS_KEY_VAL;
+            CS->CLRIFG |= CS_CLRIFG_CLR_LFXTIFG;
+            CS->KEY = 1;
+
+            if(BITBAND_PERI(CS->IFG, CS_IFG_LFXTIFG_OFS))
+            {
+                if(BITBAND_PERI(CS->CLKEN, CS_CLKEN_REFOFSEL_OFS))
+                {
+                    SystemCoreClock = (128000 / dividerValue);
+                }
+                else
+                {
+                    SystemCoreClock = (32000 / dividerValue);
+                }
+            }
+            else
+            {
+                SystemCoreClock = __LFXT / dividerValue;
+            }
+        }
+        else
+        {
+            SystemCoreClock = __LFXT / dividerValue;
+        }
+        break;
+    case CS_CTL1_SELM__VLOCLK:
+        SystemCoreClock = __VLOCLK / dividerValue;
+        break;
+    case CS_CTL1_SELM__REFOCLK:
+        if (BITBAND_PERI(CS->CLKEN, CS_CLKEN_REFOFSEL_OFS))
+        {
+            SystemCoreClock = (128000 / dividerValue);
+        }
+        else
+        {
+            SystemCoreClock = (32000 / dividerValue);
+        }
+        break;
+    case CS_CTL1_SELM__DCOCLK:
+        dcoTune = (CS->CTL0 & CS_CTL0_DCOTUNE_MASK) >> CS_CTL0_DCOTUNE_OFS;
+    
+        switch(CS->CTL0 & CS_CTL0_DCORSEL_MASK)
+        {
+        case CS_CTL0_DCORSEL_0:
+            centeredFreq = 1500000;
+            break;
+        case CS_CTL0_DCORSEL_1:
+            centeredFreq = 3000000;
+            break;
+        case CS_CTL0_DCORSEL_2:
+            centeredFreq = 6000000;
+            break;
+        case CS_CTL0_DCORSEL_3:
+            centeredFreq = 12000000;
+            break;
+        case CS_CTL0_DCORSEL_4:
+            centeredFreq = 24000000;
+            break;
+        case CS_CTL0_DCORSEL_5:
+            centeredFreq = 48000000;
+            break;
+        }
+
+        if(dcoTune == 0)
+        {
+            SystemCoreClock = centeredFreq;
+        }
+        else
+        {
+
+            if(dcoTune & 0x1000)
+            {
+                dcoTune = dcoTune | 0xF000;
+            }
+
+            if (BITBAND_PERI(CS->CTL0, CS_CTL0_DCORES_OFS))
+            {
+                dcoConst = *((float *) &TLV->DCOER_CONSTK_RSEL04);
+                calVal = TLV->DCOER_FCAL_RSEL04;
+            }
+            /* Internal Resistor */
+            else
+            {
+                dcoConst = *((float *) &TLV->DCOIR_CONSTK_RSEL04);
+                calVal = TLV->DCOIR_FCAL_RSEL04;
+            }
+
+            SystemCoreClock = (uint32_t) ((centeredFreq)
+                               / (1
+                                    - ((dcoConst * dcoTune)
+                                            / (8 * (1 + dcoConst * (768 - calVal))))));
+        }
+        break;
+    case CS_CTL1_SELM__MODOSC:
+        SystemCoreClock = __MODCLK / dividerValue;
+        break;
+    case CS_CTL1_SELM__HFXTCLK:
+        if(BITBAND_PERI(CS->IFG, CS_IFG_HFXTIFG_OFS))
+        {
+            // Clear interrupt flag
+            CS->KEY = CS_KEY_VAL;
+            CS->CLRIFG |= CS_CLRIFG_CLR_HFXTIFG;
+            CS->KEY = 1;
+
+            if(BITBAND_PERI(CS->IFG, CS_IFG_HFXTIFG_OFS))
+            {
+                if(BITBAND_PERI(CS->CLKEN, CS_CLKEN_REFOFSEL_OFS))
+                {
+                    SystemCoreClock = (128000 / dividerValue);
+                }
+                else
+                {
+                    SystemCoreClock = (32000 / dividerValue);
+                }
+            }
+            else
+            {
+                SystemCoreClock = __HFXT / dividerValue;
+            }
+        }
+        else
+        {
+            SystemCoreClock = __HFXT / dividerValue;
+        }
+        break;
+    }
+}
+
+/**
+ * Initialize the system
+ *
+ * @param  none
+ * @return none
+ *
+ * @brief  Setup the microcontroller system.
+ *
+ * Performs the following initialization steps:
+ *     1. Enables the FPU
+ *     2. Halts the WDT if requested
+ *     3. Enables all SRAM banks
+ *     4. Sets up power regulator and VCORE
+ *     5. Enable Flash wait states if needed
+ *     6. Change MCLK to desired frequency
+ *     7. Enable Flash read buffering
+ */
+void SystemInit(void)
+{
+    // Enable FPU if used
+    #if (__FPU_USED == 1)                              /* __FPU_USED is defined in core_cm4.h */
+    SCB->CPACR |= ((3UL << 10 * 2) |                   /* Set CP10 Full Access */
+                   (3UL << 11 * 2));                   /* Set CP11 Full Access */
+    #endif
+
+    #if (__HALT_WDT == 1)
+    WDT_A->CTL = WDT_A_CTL_PW | WDT_A_CTL_HOLD;         // Halt the WDT
+    #endif
+
+    SYSCTL->SRAM_BANKEN = SYSCTL_SRAM_BANKEN_BNK7_EN;   // Enable all SRAM banks
+
+    #if (__SYSTEM_CLOCK == 1500000)                                  // 1.5 MHz
+    // Default VCORE is LDO VCORE0 so no change necessary
+
+    // Switches LDO VCORE0 to DCDC VCORE0 if requested
+    #if __REGULATOR
+    while((PCM->CTL1 & PCM_CTL1_PMR_BUSY));
+    PCM->CTL0 = PCM_CTL0_KEY_VAL | PCM_CTL0_AMR_4;
+    while((PCM->CTL1 & PCM_CTL1_PMR_BUSY));
+    #endif
+
+    // No flash wait states necessary
+
+    // DCO = 1.5 MHz; MCLK = source
+    CS->KEY = CS_KEY_VAL;                                 // Unlock CS module for register access
+    CS->CTL0 = CS_CTL0_DCORSEL_0;                                // Set DCO to 1.5MHz
+    CS->CTL1 &= ~(CS_CTL1_SELM_MASK | CS_CTL1_DIVM_MASK) | CS_CTL1_SELM__DCOCLK;  // Select MCLK as DCO source
+    CS->KEY = 0;
+
+    // Set Flash Bank read buffering
+    FLCTL->BANK0_RDCTL &= ~(FLCTL_BANK0_RDCTL_BUFD | FLCTL_BANK0_RDCTL_BUFI);
+    FLCTL->BANK1_RDCTL &= ~(FLCTL_BANK0_RDCTL_BUFD | FLCTL_BANK0_RDCTL_BUFI);
+
+    #elif (__SYSTEM_CLOCK == 3000000)                                  // 3 MHz
+    // Default VCORE is LDO VCORE0 so no change necessary
+
+    // Switches LDO VCORE0 to DCDC VCORE0 if requested
+    #if __REGULATOR
+    while(PCM->CTL1 & PCM_CTL1_PMR_BUSY);
+    PCM->CTL0 = PCM_CTL0_KEY_VAL | PCM_CTL0_AMR_4;
+    while(PCM->CTL1 & PCM_CTL1_PMR_BUSY);
+    #endif
+
+    // No flash wait states necessary
+
+    // DCO = 3 MHz; MCLK = source
+    CS->KEY = CS_KEY_VAL;                                                         // Unlock CS module for register access
+    CS->CTL0 = CS_CTL0_DCORSEL_1;                                                  // Set DCO to 1.5MHz
+    CS->CTL1 &= ~(CS_CTL1_SELM_MASK | CS_CTL1_DIVM_MASK) | CS_CTL1_SELM__DCOCLK;  // Select MCLK as DCO source
+    CS->KEY = 0;
+
+    // Set Flash Bank read buffering
+    FLCTL->BANK0_RDCTL &= ~(FLCTL_BANK0_RDCTL_BUFD | FLCTL_BANK0_RDCTL_BUFI);
+    FLCTL->BANK1_RDCTL &= ~(FLCTL_BANK0_RDCTL_BUFD | FLCTL_BANK0_RDCTL_BUFI);
+
+    #elif (__SYSTEM_CLOCK == 12000000)                                // 12 MHz
+    // Default VCORE is LDO VCORE0 so no change necessary
+
+    // Switches LDO VCORE0 to DCDC VCORE0 if requested
+    #if __REGULATOR
+    while((PCM->CTL1 & PCM_CTL1_PMR_BUSY));
+    PCM->CTL0 = PCM_CTL0_KEY_VAL | PCM_CTL0_AMR_4;
+    while((PCM->CTL1 & PCM_CTL1_PMR_BUSY));
+    #endif
+
+    // No flash wait states necessary
+
+    // DCO = 12 MHz; MCLK = source
+    CS->KEY = CS_KEY_VAL;                                                         // Unlock CS module for register access
+    CS->CTL0 = CS_CTL0_DCORSEL_3;                                                  // Set DCO to 12MHz
+    CS->CTL1 &= ~(CS_CTL1_SELM_MASK | CS_CTL1_DIVM_MASK) | CS_CTL1_SELM__DCOCLK;  // Select MCLK as DCO source
+    CS->KEY = 0;
+
+    // Set Flash Bank read buffering
+    FLCTL->BANK0_RDCTL &= ~(FLCTL_BANK0_RDCTL_BUFD | FLCTL_BANK0_RDCTL_BUFI);
+    FLCTL->BANK1_RDCTL &= ~(FLCTL_BANK0_RDCTL_BUFD | FLCTL_BANK0_RDCTL_BUFI);
+
+    #elif (__SYSTEM_CLOCK == 24000000)                                // 24 MHz
+    // Default VCORE is LDO VCORE0 so no change necessary
+
+    // Switches LDO VCORE0 to DCDC VCORE0 if requested
+    #if __REGULATOR
+    while((PCM->CTL1 & PCM_CTL1_PMR_BUSY));
+    PCM->CTL0 = PCM_CTL0_KEY_VAL | PCM_CTL0_AMR_4;
+    while((PCM->CTL1 & PCM_CTL1_PMR_BUSY));
+    #endif
+
+    // 1 flash wait state (BANK0 VCORE0 max is 12 MHz)
+    FLCTL->BANK0_RDCTL &= ~FLCTL_BANK0_RDCTL_WAIT_MASK | FLCTL_BANK0_RDCTL_WAIT_1;
+    FLCTL->BANK1_RDCTL &= ~FLCTL_BANK0_RDCTL_WAIT_MASK | FLCTL_BANK0_RDCTL_WAIT_1;
+
+    // DCO = 24 MHz; MCLK = source
+    CS->KEY = CS_KEY_VAL;                                                         // Unlock CS module for register access
+    CS->CTL0 = CS_CTL0_DCORSEL_4;                                                  // Set DCO to 24MHz
+    CS->CTL1 &= ~(CS_CTL1_SELM_MASK | CS_CTL1_DIVM_MASK) | CS_CTL1_SELM__DCOCLK;  // Select MCLK as DCO source
+    CS->KEY = 0;
+
+    // Set Flash Bank read buffering
+    FLCTL->BANK0_RDCTL |= (FLCTL_BANK0_RDCTL_BUFD | FLCTL_BANK0_RDCTL_BUFI);
+    FLCTL->BANK1_RDCTL &= ~(FLCTL_BANK0_RDCTL_BUFD | FLCTL_BANK0_RDCTL_BUFI);
+
+    #elif (__SYSTEM_CLOCK == 48000000)                                // 48 MHz
+    // Switches LDO VCORE0 to LDO VCORE1; mandatory for 48 MHz setting
+    while((PCM->CTL1 & PCM_CTL1_PMR_BUSY));
+    PCM->CTL0 = PCM_CTL0_KEY_VAL | PCM_CTL0_AMR_1;
+    while((PCM->CTL1 & PCM_CTL1_PMR_BUSY));
+
+    // Switches LDO VCORE1 to DCDC VCORE1 if requested
+    #if __REGULATOR
+    while((PCM->CTL1 & PCM_CTL1_PMR_BUSY));
+    PCM->CTL0 = PCM_CTL0_KEY_VAL | PCM_CTL0_AMR_5;
+    while((PCM->CTL1 & PCM_CTL1_PMR_BUSY));
+    #endif
+
+    // 2 flash wait states (BANK0 VCORE1 max is 16 MHz, BANK1 VCORE1 max is 32 MHz)
+    FLCTL->BANK0_RDCTL &= ~FLCTL_BANK0_RDCTL_WAIT_MASK | FLCTL_BANK0_RDCTL_WAIT_2;
+    FLCTL->BANK1_RDCTL &= ~FLCTL_BANK1_RDCTL_WAIT_MASK | FLCTL_BANK1_RDCTL_WAIT_2;
+
+    // DCO = 48 MHz; MCLK = source
+    CS->KEY = CS_KEY_VAL;                                                         // Unlock CS module for register access
+    CS->CTL0 = CS_CTL0_DCORSEL_5;                                                  // Set DCO to 48MHz
+    CS->CTL1 &= ~(CS_CTL1_SELM_MASK | CS_CTL1_DIVM_MASK) | CS_CTL1_SELM__DCOCLK;  // Select MCLK as DCO source
+    CS->KEY = 0;
+
+    // Set Flash Bank read buffering
+    FLCTL->BANK0_RDCTL |= (FLCTL_BANK0_RDCTL_BUFD | FLCTL_BANK0_RDCTL_BUFI);
+    FLCTL->BANK1_RDCTL |= (FLCTL_BANK1_RDCTL_BUFD | FLCTL_BANK1_RDCTL_BUFI);
+    #endif
+
+}
index 92b71fb4122bfba9dfdda9042b5b298dd65640af..6f7dbef77fd2275ef31e882f704e68d066583fd9 100644 (file)
 
 /* Flash SPI */
 #define FLASH_SPI_PORT       GPIO_PORT_P3
-#define FLASH_SPI_NCS_PIN    GPIO_PIN0
+#define FLASH_SPI_CSN_PIN    GPIO_PIN0
 #define FLASH_SPI_CLK_PIN    GPIO_PIN1
 #define FLASH_SPI_MISO_PIN   GPIO_PIN2
 #define FLASH_SPI_MOSI_PIN   GPIO_PIN3
 
 
+/* CC2650 SPI */
+#define CC2650_SPI_PORT      GPIO_PORT_P2
+#define CC2650_SPI_CSN_PIN    GPIO_PIN0
+#define CC2650_SPI_CLK_PIN   GPIO_PIN1
+#define CC2650_SPI_MISO_PIN  GPIO_PIN2
+#define CC2650_SPI_MOSI_PIN  GPIO_PIN3
+
+#define CC2650_INT_PORT      GPIO_PORT_P4
+#define CC2650_IRQ_PIN       GPIO_PIN0
+
 /* On Board EEPROM 25xx256*/
 #define EEPROM_SLAVE_ADDRESS 0x50
 
index 92b71fb4122bfba9dfdda9042b5b298dd65640af..6f7dbef77fd2275ef31e882f704e68d066583fd9 100644 (file)
 
 /* Flash SPI */
 #define FLASH_SPI_PORT       GPIO_PORT_P3
-#define FLASH_SPI_NCS_PIN    GPIO_PIN0
+#define FLASH_SPI_CSN_PIN    GPIO_PIN0
 #define FLASH_SPI_CLK_PIN    GPIO_PIN1
 #define FLASH_SPI_MISO_PIN   GPIO_PIN2
 #define FLASH_SPI_MOSI_PIN   GPIO_PIN3
 
 
+/* CC2650 SPI */
+#define CC2650_SPI_PORT      GPIO_PORT_P2
+#define CC2650_SPI_CSN_PIN    GPIO_PIN0
+#define CC2650_SPI_CLK_PIN   GPIO_PIN1
+#define CC2650_SPI_MISO_PIN  GPIO_PIN2
+#define CC2650_SPI_MOSI_PIN  GPIO_PIN3
+
+#define CC2650_INT_PORT      GPIO_PORT_P4
+#define CC2650_IRQ_PIN       GPIO_PIN0
+
 /* On Board EEPROM 25xx256*/
 #define EEPROM_SLAVE_ADDRESS 0x50
 
index 92b71fb4122bfba9dfdda9042b5b298dd65640af..6f7dbef77fd2275ef31e882f704e68d066583fd9 100644 (file)
 
 /* Flash SPI */
 #define FLASH_SPI_PORT       GPIO_PORT_P3
-#define FLASH_SPI_NCS_PIN    GPIO_PIN0
+#define FLASH_SPI_CSN_PIN    GPIO_PIN0
 #define FLASH_SPI_CLK_PIN    GPIO_PIN1
 #define FLASH_SPI_MISO_PIN   GPIO_PIN2
 #define FLASH_SPI_MOSI_PIN   GPIO_PIN3
 
 
+/* CC2650 SPI */
+#define CC2650_SPI_PORT      GPIO_PORT_P2
+#define CC2650_SPI_CSN_PIN    GPIO_PIN0
+#define CC2650_SPI_CLK_PIN   GPIO_PIN1
+#define CC2650_SPI_MISO_PIN  GPIO_PIN2
+#define CC2650_SPI_MOSI_PIN  GPIO_PIN3
+
+#define CC2650_INT_PORT      GPIO_PORT_P4
+#define CC2650_IRQ_PIN       GPIO_PIN0
+
 /* On Board EEPROM 25xx256*/
 #define EEPROM_SLAVE_ADDRESS 0x50
 
index 92b71fb4122bfba9dfdda9042b5b298dd65640af..6f7dbef77fd2275ef31e882f704e68d066583fd9 100644 (file)
 
 /* Flash SPI */
 #define FLASH_SPI_PORT       GPIO_PORT_P3
-#define FLASH_SPI_NCS_PIN    GPIO_PIN0
+#define FLASH_SPI_CSN_PIN    GPIO_PIN0
 #define FLASH_SPI_CLK_PIN    GPIO_PIN1
 #define FLASH_SPI_MISO_PIN   GPIO_PIN2
 #define FLASH_SPI_MOSI_PIN   GPIO_PIN3
 
 
+/* CC2650 SPI */
+#define CC2650_SPI_PORT      GPIO_PORT_P2
+#define CC2650_SPI_CSN_PIN    GPIO_PIN0
+#define CC2650_SPI_CLK_PIN   GPIO_PIN1
+#define CC2650_SPI_MISO_PIN  GPIO_PIN2
+#define CC2650_SPI_MOSI_PIN  GPIO_PIN3
+
+#define CC2650_INT_PORT      GPIO_PORT_P4
+#define CC2650_IRQ_PIN       GPIO_PIN0
+
 /* On Board EEPROM 25xx256*/
 #define EEPROM_SLAVE_ADDRESS 0x50
 
index 92b71fb4122bfba9dfdda9042b5b298dd65640af..6f7dbef77fd2275ef31e882f704e68d066583fd9 100644 (file)
 
 /* Flash SPI */
 #define FLASH_SPI_PORT       GPIO_PORT_P3
-#define FLASH_SPI_NCS_PIN    GPIO_PIN0
+#define FLASH_SPI_CSN_PIN    GPIO_PIN0
 #define FLASH_SPI_CLK_PIN    GPIO_PIN1
 #define FLASH_SPI_MISO_PIN   GPIO_PIN2
 #define FLASH_SPI_MOSI_PIN   GPIO_PIN3
 
 
+/* CC2650 SPI */
+#define CC2650_SPI_PORT      GPIO_PORT_P2
+#define CC2650_SPI_CSN_PIN    GPIO_PIN0
+#define CC2650_SPI_CLK_PIN   GPIO_PIN1
+#define CC2650_SPI_MISO_PIN  GPIO_PIN2
+#define CC2650_SPI_MOSI_PIN  GPIO_PIN3
+
+#define CC2650_INT_PORT      GPIO_PORT_P4
+#define CC2650_IRQ_PIN       GPIO_PIN0
+
 /* On Board EEPROM 25xx256*/
 #define EEPROM_SLAVE_ADDRESS 0x50