diff --git a/aws_iot_src/shadow/aws_iot_shadow_json_data.h b/aws_iot_src/shadow/aws_iot_shadow_json_data.h
+++ /dev/null
@@ -1,132 +0,0 @@
-/*
- * Copyright 2010-2015 Amazon.com, Inc. or its affiliates. All Rights Reserved.
- *
- * Licensed under the Apache License, Version 2.0 (the "License").
- * You may not use this file except in compliance with the License.
- * A copy of the License is located at
- *
- * http://aws.amazon.com/apache2.0
- *
- * or in the "license" file accompanying this file. This file is distributed
- * on an "AS IS" BASIS, WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either
- * express or implied. See the License for the specific language governing
- * permissions and limitations under the License.
- */
-
-#ifndef SRC_SHADOW_AWS_IOT_SHADOW_JSON_DATA_H_
-#define SRC_SHADOW_AWS_IOT_SHADOW_JSON_DATA_H_
-
-#include <stddef.h>
-
-/**
- * @brief This is a static JSON object that could be used in code
- *
- */
-typedef struct jsonStruct jsonStruct_t;
-/**
- * @brief Every JSON name value can have a callback. The callback should follow this signature
- */
-typedef void (*jsonStructCallback_t)(const char *pJsonValueBuffer, uint32_t valueLength, jsonStruct_t *pJsonStruct_t);
-
-/**
- * @brief All the JSON object types enum
- *
- * JSON number types need to be split into proper integer / floating point data types and sizes on embedded platforms.
- */
-typedef enum {
- SHADOW_JSON_INT32,
- SHADOW_JSON_INT16,
- SHADOW_JSON_INT8,
- SHADOW_JSON_UINT32,
- SHADOW_JSON_UINT16,
- SHADOW_JSON_UINT8,
- SHADOW_JSON_FLOAT,
- SHADOW_JSON_DOUBLE,
- SHADOW_JSON_BOOL,
- SHADOW_JSON_STRING,
- SHADOW_JSON_OBJECT
-} JsonPrimitiveType;
-
-struct jsonStruct {
- const char *pKey;
- void *pData;
- JsonPrimitiveType type;
- jsonStructCallback_t cb;
-};
-
-/**
- * @brief Initialize the JSON document with Shadow expected name/value
- *
- * This Function will fill the JSON Buffer with a null terminated string. Internally it uses snprintf
- * This function should always be used First, followed by iot_shadow_add_reported and/or iot_shadow_add_desired.
- * Always finish the call sequence with iot_finalize_json_document
- *
- * @note Ensure the size of the Buffer is enough to hold the entire JSON Document.
- *
- *
- * @param pJsonDocument The JSON Document filled in this char buffer
- * @param maxSizeOfJsonDocument maximum size of the pJsonDocument that can be used to fill the JSON document
- * @return An IoT Error Type defining if the buffer was null or the entire string was not filled up
- */
-IoT_Error_t aws_iot_shadow_init_json_document(char *pJsonDocument, size_t maxSizeOfJsonDocument);
-
-/**
- * @brief Add the reported section of the JSON document of jsonStruct_t
- *
- * This is a variadic function and please be careful with the usage. count is the number of jsonStruct_t types that you would like to add in the reported section
- * This function will add "reported":{<all the values that needs to be added>}
- *
- * @note Ensure the size of the Buffer is enough to hold the reported section + the init section. Always use the same JSON document buffer used in the iot_shadow_init_json_document function. This function will accommodate the size of previous null terminated string, so pass teh max size of the buffer
- *
- *
- * @param pJsonDocument The JSON Document filled in this char buffer
- * @param maxSizeOfJsonDocument maximum size of the pJsonDocument that can be used to fill the JSON document
- * @param count total number of arguments(jsonStruct_t object) passed in the arguments
- * @return An IoT Error Type defining if the buffer was null or the entire string was not filled up
- */
-IoT_Error_t aws_iot_shadow_add_reported(char *pJsonDocument, size_t maxSizeOfJsonDocument, uint8_t count, ...);
-
-/**
- * @brief Add the desired section of the JSON document of jsonStruct_t
- *
- * This is a variadic function and please be careful with the usage. count is the number of jsonStruct_t types that you would like to add in the reported section
- * This function will add "desired":{<all the values that needs to be added>}
- *
- * @note Ensure the size of the Buffer is enough to hold the reported section + the init section. Always use the same JSON document buffer used in the iot_shadow_init_json_document function. This function will accommodate the size of previous null terminated string, so pass the max size of the buffer
- *
- *
- * @param pJsonDocument The JSON Document filled in this char buffer
- * @param maxSizeOfJsonDocument maximum size of the pJsonDocument that can be used to fill the JSON document
- * @param count total number of arguments(jsonStruct_t object) passed in the arguments
- * @return An IoT Error Type defining if the buffer was null or the entire string was not filled up
- */
-IoT_Error_t aws_iot_shadow_add_desired(char *pJsonDocument, size_t maxSizeOfJsonDocument, uint8_t count, ...);
-
-/**
- * @brief Finalize the JSON document with Shadow expected client Token.
- *
- * This function will automatically increment the client token every time this function is called.
- *
- * @note Ensure the size of the Buffer is enough to hold the entire JSON Document. If the finalized section is not invoked then the JSON doucment will not be valid
- *
- *
- * @param pJsonDocument The JSON Document filled in this char buffer
- * @param maxSizeOfJsonDocument maximum size of the pJsonDocument that can be used to fill the JSON document
- * @return An IoT Error Type defining if the buffer was null or the entire string was not filled up
- */
-IoT_Error_t aws_iot_finalize_json_document(char *pJsonDocument, size_t maxSizeOfJsonDocument);
-
-/**
- * @brief Fill the given buffer with client token for tracking the Repsonse.
- *
- * This function will add the AWS_IOT_MQTT_CLIENT_ID with a sequence number. Every time this function is used the sequence number gets incremented
- *
- *
- * @param pBufferToBeUpdatedWithClientToken buffer to be updated with the client token string
- * @param maxSizeOfJsonDocument maximum size of the pBufferToBeUpdatedWithClientToken that can be used
- * @return An IoT Error Type defining if the buffer was null or the entire string was not filled up
- */
-
-IoT_Error_t aws_iot_fill_with_client_token(char *pBufferToBeUpdatedWithClientToken, size_t maxSizeOfJsonDocument);
-
-#endif /* SRC_SHADOW_AWS_IOT_SHADOW_JSON_DATA_H_ */