QNX: Shmemallocator: Fix Compilation Warnings This patch fixes compilation warnings introduced with the newer QNX version. Signed-off-by: Angela Stegmaier <angelabaker@ti.com>
Clean up exported contents in QNX This commit modifies 'make install' to export only tests that we run. It also puts all tests into the 'tests' subdirectory and builds them all in debug and release modes for consistency. Signed-off-by: VW <vwan@ti.com>
Reduce QNX build output verbosity This commit reduces the build output verbosity, and allows it to be configured in the qnx/quiet.mk file. This helps address SDOCM00113501. Signed-off-by: VW <vwan@ti.com>
Remove references to SysLink in QNX code base This commit removes all references to "SysLink" in the QNX IPC code base, with the exception that it preserves the file and directory names. The decision was made to preserve the path names to avoid breaking any existing apps that may be including headers and/or libraries based on the existing directory structure, and to ease git history lookup going forward. Note that this does introduce a break in the naming of internal features such as SYSLINK_DEBUG and SYSLINK_DEBUG_TRACE_LEVEL. This helps address SDOCM00108142. Signed-off-by: VW <vwan@ti.com>
GateMP: Introduce support for GateMP on QNX To enable GateMP,throw the -g option when launching the IPC resource manager. On the BIOS side, DSP1 must be configured as the owner of SR0 and the new GateMP.hostSupport config param must be set to true like this: var GateMP = xdc.useModule('ti.sdo.ipc.GateMP'); GateMP.hostSupport = true; Note that it's initially only been validated on DRA7XX DSP1. Signed-off-by: VW <vwan@ti.com>
Moved files from the ipc3x_dev branch in syslink_qnx repository into direct ory qnx/src/ipc3x_dev Reference point is https://gforge01.dal.design.ti.com/gf/project/syslink_qnx/scmgit/?p=syslink_qnx;a=shortlog;h=refs/heads/ipc3x_dev, commit id 0eafb4c5a0025248a745cf6c42a0e4e80c34d6b4