]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - ipc/ipcdev.git/blob - depcomp
OPBU Merge: Pulled in srvmgr/NameMap into rpmsg/
[ipc/ipcdev.git] / depcomp
1 #! /bin/sh
2 # depcomp - compile a program generating dependencies as side-effects
4 scriptversion=2005-07-09.11
6 # Copyright (C) 1999, 2000, 2003, 2004, 2005 Free Software Foundation, Inc.
8 # This program is free software; you can redistribute it and/or modify
9 # it under the terms of the GNU General Public License as published by
10 # the Free Software Foundation; either version 2, or (at your option)
11 # any later version.
13 # This program is distributed in the hope that it will be useful,
14 # but WITHOUT ANY WARRANTY; without even the implied warranty of
15 # MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
16 # GNU General Public License for more details.
18 # You should have received a copy of the GNU General Public License
19 # along with this program; if not, write to the Free Software
20 # Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA
21 # 02110-1301, USA.
23 # As a special exception to the GNU General Public License, if you
24 # distribute this file as part of a program that contains a
25 # configuration script generated by Autoconf, you may include it under
26 # the same distribution terms that you use for the rest of that program.
28 # Originally written by Alexandre Oliva <oliva@dcc.unicamp.br>.
30 case $1 in
31   '')
32      echo "$0: No command.  Try \`$0 --help' for more information." 1>&2
33      exit 1;
34      ;;
35   -h | --h*)
36     cat <<\EOF
37 Usage: depcomp [--help] [--version] PROGRAM [ARGS]
39 Run PROGRAMS ARGS to compile a file, generating dependencies
40 as side-effects.
42 Environment variables:
43   depmode     Dependency tracking mode.
44   source      Source file read by `PROGRAMS ARGS'.
45   object      Object file output by `PROGRAMS ARGS'.
46   DEPDIR      directory where to store dependencies.
47   depfile     Dependency file to output.
48   tmpdepfile  Temporary file to use when outputing dependencies.
49   libtool     Whether libtool is used (yes/no).
51 Report bugs to <bug-automake@gnu.org>.
52 EOF
53     exit $?
54     ;;
55   -v | --v*)
56     echo "depcomp $scriptversion"
57     exit $?
58     ;;
59 esac
61 if test -z "$depmode" || test -z "$source" || test -z "$object"; then
62   echo "depcomp: Variables source, object and depmode must be set" 1>&2
63   exit 1
64 fi
66 # Dependencies for sub/bar.o or sub/bar.obj go into sub/.deps/bar.Po.
67 depfile=${depfile-`echo "$object" |
68   sed 's|[^\\/]*$|'${DEPDIR-.deps}'/&|;s|\.\([^.]*\)$|.P\1|;s|Pobj$|Po|'`}
69 tmpdepfile=${tmpdepfile-`echo "$depfile" | sed 's/\.\([^.]*\)$/.T\1/'`}
71 rm -f "$tmpdepfile"
73 # Some modes work just like other modes, but use different flags.  We
74 # parameterize here, but still list the modes in the big case below,
75 # to make depend.m4 easier to write.  Note that we *cannot* use a case
76 # here, because this file can only contain one case statement.
77 if test "$depmode" = hp; then
78   # HP compiler uses -M and no extra arg.
79   gccflag=-M
80   depmode=gcc
81 fi
83 if test "$depmode" = dashXmstdout; then
84    # This is just like dashmstdout with a different argument.
85    dashmflag=-xM
86    depmode=dashmstdout
87 fi
89 case "$depmode" in
90 gcc3)
91 ## gcc 3 implements dependency tracking that does exactly what
92 ## we want.  Yay!  Note: for some reason libtool 1.4 doesn't like
93 ## it if -MD -MP comes after the -MF stuff.  Hmm.
94   "$@" -MT "$object" -MD -MP -MF "$tmpdepfile"
95   stat=$?
96   if test $stat -eq 0; then :
97   else
98     rm -f "$tmpdepfile"
99     exit $stat
100   fi
101   mv "$tmpdepfile" "$depfile"
102   ;;
104 gcc)
105 ## There are various ways to get dependency output from gcc.  Here's
106 ## why we pick this rather obscure method:
107 ## - Don't want to use -MD because we'd like the dependencies to end
108 ##   up in a subdir.  Having to rename by hand is ugly.
109 ##   (We might end up doing this anyway to support other compilers.)
110 ## - The DEPENDENCIES_OUTPUT environment variable makes gcc act like
111 ##   -MM, not -M (despite what the docs say).
112 ## - Using -M directly means running the compiler twice (even worse
113 ##   than renaming).
114   if test -z "$gccflag"; then
115     gccflag=-MD,
116   fi
117   "$@" -Wp,"$gccflag$tmpdepfile"
118   stat=$?
119   if test $stat -eq 0; then :
120   else
121     rm -f "$tmpdepfile"
122     exit $stat
123   fi
124   rm -f "$depfile"
125   echo "$object : \\" > "$depfile"
126   alpha=ABCDEFGHIJKLMNOPQRSTUVWXYZabcdefghijklmnopqrstuvwxyz
127 ## The second -e expression handles DOS-style file names with drive letters.
128   sed -e 's/^[^:]*: / /' \
129       -e 's/^['$alpha']:\/[^:]*: / /' < "$tmpdepfile" >> "$depfile"
130 ## This next piece of magic avoids the `deleted header file' problem.
131 ## The problem is that when a header file which appears in a .P file
132 ## is deleted, the dependency causes make to die (because there is
133 ## typically no way to rebuild the header).  We avoid this by adding
134 ## dummy dependencies for each header file.  Too bad gcc doesn't do
135 ## this for us directly.
136   tr ' ' '
137 ' < "$tmpdepfile" |
138 ## Some versions of gcc put a space before the `:'.  On the theory
139 ## that the space means something, we add a space to the output as
140 ## well.
141 ## Some versions of the HPUX 10.20 sed can't process this invocation
142 ## correctly.  Breaking it into two sed invocations is a workaround.
143     sed -e 's/^\\$//' -e '/^$/d' -e '/:$/d' | sed -e 's/$/ :/' >> "$depfile"
144   rm -f "$tmpdepfile"
145   ;;
147 hp)
148   # This case exists only to let depend.m4 do its work.  It works by
149   # looking at the text of this script.  This case will never be run,
150   # since it is checked for above.
151   exit 1
152   ;;
154 sgi)
155   if test "$libtool" = yes; then
156     "$@" "-Wp,-MDupdate,$tmpdepfile"
157   else
158     "$@" -MDupdate "$tmpdepfile"
159   fi
160   stat=$?
161   if test $stat -eq 0; then :
162   else
163     rm -f "$tmpdepfile"
164     exit $stat
165   fi
166   rm -f "$depfile"
168   if test -f "$tmpdepfile"; then  # yes, the sourcefile depend on other files
169     echo "$object : \\" > "$depfile"
171     # Clip off the initial element (the dependent).  Don't try to be
172     # clever and replace this with sed code, as IRIX sed won't handle
173     # lines with more than a fixed number of characters (4096 in
174     # IRIX 6.2 sed, 8192 in IRIX 6.5).  We also remove comment lines;
175     # the IRIX cc adds comments like `#:fec' to the end of the
176     # dependency line.
177     tr ' ' '
178 ' < "$tmpdepfile" \
179     | sed -e 's/^.*\.o://' -e 's/#.*$//' -e '/^$/ d' | \
180     tr '
181 ' ' ' >> $depfile
182     echo >> $depfile
184     # The second pass generates a dummy entry for each header file.
185     tr ' ' '
186 ' < "$tmpdepfile" \
187    | sed -e 's/^.*\.o://' -e 's/#.*$//' -e '/^$/ d' -e 's/$/:/' \
188    >> $depfile
189   else
190     # The sourcefile does not contain any dependencies, so just
191     # store a dummy comment line, to avoid errors with the Makefile
192     # "include basename.Plo" scheme.
193     echo "#dummy" > "$depfile"
194   fi
195   rm -f "$tmpdepfile"
196   ;;
198 aix)
199   # The C for AIX Compiler uses -M and outputs the dependencies
200   # in a .u file.  In older versions, this file always lives in the
201   # current directory.  Also, the AIX compiler puts `$object:' at the
202   # start of each line; $object doesn't have directory information.
203   # Version 6 uses the directory in both cases.
204   stripped=`echo "$object" | sed 's/\(.*\)\..*$/\1/'`
205   tmpdepfile="$stripped.u"
206   if test "$libtool" = yes; then
207     "$@" -Wc,-M
208   else
209     "$@" -M
210   fi
211   stat=$?
213   if test -f "$tmpdepfile"; then :
214   else
215     stripped=`echo "$stripped" | sed 's,^.*/,,'`
216     tmpdepfile="$stripped.u"
217   fi
219   if test $stat -eq 0; then :
220   else
221     rm -f "$tmpdepfile"
222     exit $stat
223   fi
225   if test -f "$tmpdepfile"; then
226     outname="$stripped.o"
227     # Each line is of the form `foo.o: dependent.h'.
228     # Do two passes, one to just change these to
229     # `$object: dependent.h' and one to simply `dependent.h:'.
230     sed -e "s,^$outname:,$object :," < "$tmpdepfile" > "$depfile"
231     sed -e "s,^$outname: \(.*\)$,\1:," < "$tmpdepfile" >> "$depfile"
232   else
233     # The sourcefile does not contain any dependencies, so just
234     # store a dummy comment line, to avoid errors with the Makefile
235     # "include basename.Plo" scheme.
236     echo "#dummy" > "$depfile"
237   fi
238   rm -f "$tmpdepfile"
239   ;;
241 icc)
242   # Intel's C compiler understands `-MD -MF file'.  However on
243   #    icc -MD -MF foo.d -c -o sub/foo.o sub/foo.c
244   # ICC 7.0 will fill foo.d with something like
245   #    foo.o: sub/foo.c
246   #    foo.o: sub/foo.h
247   # which is wrong.  We want:
248   #    sub/foo.o: sub/foo.c
249   #    sub/foo.o: sub/foo.h
250   #    sub/foo.c:
251   #    sub/foo.h:
252   # ICC 7.1 will output
253   #    foo.o: sub/foo.c sub/foo.h
254   # and will wrap long lines using \ :
255   #    foo.o: sub/foo.c ... \
256   #     sub/foo.h ... \
257   #     ...
259   "$@" -MD -MF "$tmpdepfile"
260   stat=$?
261   if test $stat -eq 0; then :
262   else
263     rm -f "$tmpdepfile"
264     exit $stat
265   fi
266   rm -f "$depfile"
267   # Each line is of the form `foo.o: dependent.h',
268   # or `foo.o: dep1.h dep2.h \', or ` dep3.h dep4.h \'.
269   # Do two passes, one to just change these to
270   # `$object: dependent.h' and one to simply `dependent.h:'.
271   sed "s,^[^:]*:,$object :," < "$tmpdepfile" > "$depfile"
272   # Some versions of the HPUX 10.20 sed can't process this invocation
273   # correctly.  Breaking it into two sed invocations is a workaround.
274   sed 's,^[^:]*: \(.*\)$,\1,;s/^\\$//;/^$/d;/:$/d' < "$tmpdepfile" |
275     sed -e 's/$/ :/' >> "$depfile"
276   rm -f "$tmpdepfile"
277   ;;
279 tru64)
280    # The Tru64 compiler uses -MD to generate dependencies as a side
281    # effect.  `cc -MD -o foo.o ...' puts the dependencies into `foo.o.d'.
282    # At least on Alpha/Redhat 6.1, Compaq CCC V6.2-504 seems to put
283    # dependencies in `foo.d' instead, so we check for that too.
284    # Subdirectories are respected.
285    dir=`echo "$object" | sed -e 's|/[^/]*$|/|'`
286    test "x$dir" = "x$object" && dir=
287    base=`echo "$object" | sed -e 's|^.*/||' -e 's/\.o$//' -e 's/\.lo$//'`
289    if test "$libtool" = yes; then
290       # With Tru64 cc, shared objects can also be used to make a
291       # static library.  This mecanism is used in libtool 1.4 series to
292       # handle both shared and static libraries in a single compilation.
293       # With libtool 1.4, dependencies were output in $dir.libs/$base.lo.d.
294       #
295       # With libtool 1.5 this exception was removed, and libtool now
296       # generates 2 separate objects for the 2 libraries.  These two
297       # compilations output dependencies in in $dir.libs/$base.o.d and
298       # in $dir$base.o.d.  We have to check for both files, because
299       # one of the two compilations can be disabled.  We should prefer
300       # $dir$base.o.d over $dir.libs/$base.o.d because the latter is
301       # automatically cleaned when .libs/ is deleted, while ignoring
302       # the former would cause a distcleancheck panic.
303       tmpdepfile1=$dir.libs/$base.lo.d   # libtool 1.4
304       tmpdepfile2=$dir$base.o.d          # libtool 1.5
305       tmpdepfile3=$dir.libs/$base.o.d    # libtool 1.5
306       tmpdepfile4=$dir.libs/$base.d      # Compaq CCC V6.2-504
307       "$@" -Wc,-MD
308    else
309       tmpdepfile1=$dir$base.o.d
310       tmpdepfile2=$dir$base.d
311       tmpdepfile3=$dir$base.d
312       tmpdepfile4=$dir$base.d
313       "$@" -MD
314    fi
316    stat=$?
317    if test $stat -eq 0; then :
318    else
319       rm -f "$tmpdepfile1" "$tmpdepfile2" "$tmpdepfile3" "$tmpdepfile4"
320       exit $stat
321    fi
323    for tmpdepfile in "$tmpdepfile1" "$tmpdepfile2" "$tmpdepfile3" "$tmpdepfile4"
324    do
325      test -f "$tmpdepfile" && break
326    done
327    if test -f "$tmpdepfile"; then
328       sed -e "s,^.*\.[a-z]*:,$object:," < "$tmpdepfile" > "$depfile"
329       # That's a tab and a space in the [].
330       sed -e 's,^.*\.[a-z]*:[    ]*,,' -e 's,$,:,' < "$tmpdepfile" >> "$depfile"
331    else
332       echo "#dummy" > "$depfile"
333    fi
334    rm -f "$tmpdepfile"
335    ;;
337 #nosideeffect)
338   # This comment above is used by automake to tell side-effect
339   # dependency tracking mechanisms from slower ones.
341 dashmstdout)
342   # Important note: in order to support this mode, a compiler *must*
343   # always write the preprocessed file to stdout, regardless of -o.
344   "$@" || exit $?
346   # Remove the call to Libtool.
347   if test "$libtool" = yes; then
348     while test $1 != '--mode=compile'; do
349       shift
350     done
351     shift
352   fi
354   # Remove `-o $object'.
355   IFS=" "
356   for arg
357   do
358     case $arg in
359     -o)
360       shift
361       ;;
362     $object)
363       shift
364       ;;
365     *)
366       set fnord "$@" "$arg"
367       shift # fnord
368       shift # $arg
369       ;;
370     esac
371   done
373   test -z "$dashmflag" && dashmflag=-M
374   # Require at least two characters before searching for `:'
375   # in the target name.  This is to cope with DOS-style filenames:
376   # a dependency such as `c:/foo/bar' could be seen as target `c' otherwise.
377   "$@" $dashmflag |
378     sed 's:^[  ]*[^: ][^:][^:]*\:[    ]*:'"$object"'\: :' > "$tmpdepfile"
379   rm -f "$depfile"
380   cat < "$tmpdepfile" > "$depfile"
381   tr ' ' '
382 ' < "$tmpdepfile" | \
383 ## Some versions of the HPUX 10.20 sed can't process this invocation
384 ## correctly.  Breaking it into two sed invocations is a workaround.
385     sed -e 's/^\\$//' -e '/^$/d' -e '/:$/d' | sed -e 's/$/ :/' >> "$depfile"
386   rm -f "$tmpdepfile"
387   ;;
389 dashXmstdout)
390   # This case only exists to satisfy depend.m4.  It is never actually
391   # run, as this mode is specially recognized in the preamble.
392   exit 1
393   ;;
395 makedepend)
396   "$@" || exit $?
397   # Remove any Libtool call
398   if test "$libtool" = yes; then
399     while test $1 != '--mode=compile'; do
400       shift
401     done
402     shift
403   fi
404   # X makedepend
405   shift
406   cleared=no
407   for arg in "$@"; do
408     case $cleared in
409     no)
410       set ""; shift
411       cleared=yes ;;
412     esac
413     case "$arg" in
414     -D*|-I*)
415       set fnord "$@" "$arg"; shift ;;
416     # Strip any option that makedepend may not understand.  Remove
417     # the object too, otherwise makedepend will parse it as a source file.
418     -*|$object)
419       ;;
420     *)
421       set fnord "$@" "$arg"; shift ;;
422     esac
423   done
424   obj_suffix="`echo $object | sed 's/^.*\././'`"
425   touch "$tmpdepfile"
426   ${MAKEDEPEND-makedepend} -o"$obj_suffix" -f"$tmpdepfile" "$@"
427   rm -f "$depfile"
428   cat < "$tmpdepfile" > "$depfile"
429   sed '1,2d' "$tmpdepfile" | tr ' ' '
430 ' | \
431 ## Some versions of the HPUX 10.20 sed can't process this invocation
432 ## correctly.  Breaking it into two sed invocations is a workaround.
433     sed -e 's/^\\$//' -e '/^$/d' -e '/:$/d' | sed -e 's/$/ :/' >> "$depfile"
434   rm -f "$tmpdepfile" "$tmpdepfile".bak
435   ;;
437 cpp)
438   # Important note: in order to support this mode, a compiler *must*
439   # always write the preprocessed file to stdout.
440   "$@" || exit $?
442   # Remove the call to Libtool.
443   if test "$libtool" = yes; then
444     while test $1 != '--mode=compile'; do
445       shift
446     done
447     shift
448   fi
450   # Remove `-o $object'.
451   IFS=" "
452   for arg
453   do
454     case $arg in
455     -o)
456       shift
457       ;;
458     $object)
459       shift
460       ;;
461     *)
462       set fnord "$@" "$arg"
463       shift # fnord
464       shift # $arg
465       ;;
466     esac
467   done
469   "$@" -E |
470     sed -n -e '/^# [0-9][0-9]* "\([^"]*\)".*/ s:: \1 \\:p' \
471        -e '/^#line [0-9][0-9]* "\([^"]*\)".*/ s:: \1 \\:p' |
472     sed '$ s: \\$::' > "$tmpdepfile"
473   rm -f "$depfile"
474   echo "$object : \\" > "$depfile"
475   cat < "$tmpdepfile" >> "$depfile"
476   sed < "$tmpdepfile" '/^$/d;s/^ //;s/ \\$//;s/$/ :/' >> "$depfile"
477   rm -f "$tmpdepfile"
478   ;;
480 msvisualcpp)
481   # Important note: in order to support this mode, a compiler *must*
482   # always write the preprocessed file to stdout, regardless of -o,
483   # because we must use -o when running libtool.
484   "$@" || exit $?
485   IFS=" "
486   for arg
487   do
488     case "$arg" in
489     "-Gm"|"/Gm"|"-Gi"|"/Gi"|"-ZI"|"/ZI")
490         set fnord "$@"
491         shift
492         shift
493         ;;
494     *)
495         set fnord "$@" "$arg"
496         shift
497         shift
498         ;;
499     esac
500   done
501   "$@" -E |
502   sed -n '/^#line [0-9][0-9]* "\([^"]*\)"/ s::echo "`cygpath -u \\"\1\\"`":p' | sort | uniq > "$tmpdepfile"
503   rm -f "$depfile"
504   echo "$object : \\" > "$depfile"
505   . "$tmpdepfile" | sed 's% %\\ %g' | sed -n '/^\(.*\)$/ s::    \1 \\:p' >> "$depfile"
506   echo "        " >> "$depfile"
507   . "$tmpdepfile" | sed 's% %\\ %g' | sed -n '/^\(.*\)$/ s::\1\::p' >> "$depfile"
508   rm -f "$tmpdepfile"
509   ;;
511 none)
512   exec "$@"
513   ;;
515 *)
516   echo "Unknown depmode $depmode" 1>&2
517   exit 1
518   ;;
519 esac
521 exit 0
523 # Local Variables:
524 # mode: shell-script
525 # sh-indentation: 2
526 # eval: (add-hook 'write-file-hooks 'time-stamp)
527 # time-stamp-start: "scriptversion="
528 # time-stamp-format: "%:y-%02m-%02d.%02H"
529 # time-stamp-end: "$"
530 # End: