]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - ipc/ipcdev.git/blob - packages/ti/ipc/HeapBufMP.h
BIOS: Fixed NameServerRemoteRpmsg MessageQ instanceName and name length
[ipc/ipcdev.git] / packages / ti / ipc / HeapBufMP.h
1 /*
2  * Copyright (c) 2012-2013, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * *  Redistributions of source code must retain the above copyright
10  *    notice, this list of conditions and the following disclaimer.
11  *
12  * *  Redistributions in binary form must reproduce the above copyright
13  *    notice, this list of conditions and the following disclaimer in the
14  *    documentation and/or other materials provided with the distribution.
15  *
16  * *  Neither the name of Texas Instruments Incorporated nor the names of
17  *    its contributors may be used to endorse or promote products derived
18  *    from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 /** ============================================================================
33  *  @file       HeapBufMP.h
34  *
35  *  @brief      Multi-processor fixed-size buffer heap implementation
36  *
37  *  Heap implementation that manages fixed size buffers that can be used
38  *  in a multiprocessor system with shared memory.
39  *
40  *  The HeapBufMP manager provides functions to allocate and free storage from a
41  *  heap of type HeapBufMP which inherits from IHeap. HeapBufMP manages a single
42  *  fixed-size buffer, split into equally sized allocatable blocks.
43  *
44  *  The HeapBufMP manager is intended as a very fast memory
45  *  manager which can only allocate blocks of a single size. It is ideal for
46  *  managing a heap that is only used for allocating a single type of object,
47  *  or for objects that have very similar sizes.
48  *
49  *  The HeapBufMP module uses a NameServer instance to
50  *  store instance information when an instance is created.  The name supplied
51  *  must be unique for all HeapBufMP instances.
52  *
53  *  The #HeapBufMP_create call initializes the shared memory as needed. Once an
54  *  instance is created, a #HeapBufMP_open can be performed. The
55  *  open is used to gain access to the same HeapBufMP instance.
56  *  Generally an instance is created on one processor and opened on the
57  *  other processor(s).
58  *
59  *  The open returns a HeapBufMP instance handle like the create,
60  *  however the open does not modify the shared memory.
61  *
62  *  The HeapBufMP header should be included in an application as follows:
63  *  @code
64  *  #include <ti/ipc/HeapBufMP.h>
65  *  @endcode
66  *
67  *  @version        0.00.01
68  */
71 #ifndef ti_ipc_HeapBufMP__include
72 #define ti_ipc_HeapBufMP__include
74 #if defined (__cplusplus)
75 extern "C" {
76 #endif
78 #include <ti/ipc/GateMP.h>
80 /* =============================================================================
81  *  All success and failure codes for the module
82  * =============================================================================
83  */
85 /*!
86  *  @def    HeapBufMP_S_BUSY
87  *  @brief  The resource is still in use
88  */
89 #define HeapBufMP_S_BUSY               2
91 /*!
92  *  @def    HeapBufMP_S_ALREADYSETUP
93  *  @brief  The module has been already setup
94  */
95 #define HeapBufMP_S_ALREADYSETUP       1
97 /*!
98  *  @def    HeapBufMP_S_SUCCESS
99  *  @brief  Operation is successful.
100  */
101 #define HeapBufMP_S_SUCCESS            0
103 /*!
104  *  @def    HeapBufMP_E_FAIL
105  *  @brief  Generic failure.
106  */
107 #define HeapBufMP_E_FAIL              -1
109 /*!
110  *  @def    HeapBufMP_E_INVALIDARG
111  *  @brief  Argument passed to function is invalid.
112  */
113 #define HeapBufMP_E_INVALIDARG        -2
115 /*!
116  *  @def    HeapBufMP_E_MEMORY
117  *  @brief  Operation resulted in memory failure.
118  */
119 #define HeapBufMP_E_MEMORY            -3
121 /*!
122  *  @def    HeapBufMP_E_ALREADYEXISTS
123  *  @brief  The specified entity already exists.
124  */
125 #define HeapBufMP_E_ALREADYEXISTS     -4
127 /*!
128  *  @def    HeapBufMP_E_NOTFOUND
129  *  @brief  Unable to find the specified entity.
130  */
131 #define HeapBufMP_E_NOTFOUND          -5
133 /*!
134  *  @def    HeapBufMP_E_TIMEOUT
135  *  @brief  Operation timed out.
136  */
137 #define HeapBufMP_E_TIMEOUT           -6
139 /*!
140  *  @def    HeapBufMP_E_INVALIDSTATE
141  *  @brief  Module is not initialized.
142  */
143 #define HeapBufMP_E_INVALIDSTATE      -7
145 /*!
146  *  @def    HeapBufMP_E_OSFAILURE
147  *  @brief  A failure occurred in an OS-specific call  */
148 #define HeapBufMP_E_OSFAILURE         -8
150 /*!
151  *  @def    HeapBufMP_E_RESOURCE
152  *  @brief  Specified resource is not available  */
153 #define HeapBufMP_E_RESOURCE          -9
155 /*!
156  *  @def    HeapBufMP_E_RESTART
157  *  @brief  Operation was interrupted. Please restart the operation  */
158 #define HeapBufMP_E_RESTART           -10
160 /* =============================================================================
161  *  Structures & Enums
162  * =============================================================================
163  */
165 /*!
166  *  @brief  HeapBufMP_Handle type
167  */
168 typedef struct HeapBufMP_Object *HeapBufMP_Handle;
170 /*!
171  *  @brief  Structure defining parameters for the HeapBufMP module.
172  */
173 typedef struct HeapBufMP_Params {
174     String name;
175     /*!< Name of this instance.
176      *
177      *  The name (if not NULL) must be unique among all HeapBufMP
178      *  instances in the entire system.  When creating a new
179      *  heap, it is necessary to supply an instance name.
180      *
181      *  The name does not have to be persistent.  The supplied string is copied
182      *  into persistent memory.
183      */
185     UInt16 regionId;
186     /*!< Shared region ID
187      *
188      *  The index corresponding to the shared region from which shared memory
189      *  will be allocated.
190      */
192     /*! @cond */
193     Ptr sharedAddr;
194     /*!< Physical address of the shared memory
195      *
196      *  This value can be left as 'null' unless it is required to place the
197      *  heap at a specific location in shared memory.  If sharedAddr is null,
198      *  then shared memory for a new instance will be allocated from the
199      *  heap belonging to the region identified by #HeapBufMP_Params::regionId.
200      */
201     /*! @endcond */
203     SizeT blockSize;
204     /*!< Size (in MAUs) of each block.
205      *
206      *  HeapBufMP will round the blockSize up to the nearest multiple of the
207      *  alignment, so the actual blockSize may be larger. When creating a
208      *  HeapBufMP dynamically, this needs to be taken into account to determine
209      *  the proper buffer size to pass in.
210      *
211      *  Required parameter.
212      *
213      *  The default size of the blocks is 0 MAUs.
214      */
216     UInt numBlocks;
217     /*!<Number of fixed-size blocks.
218      *
219      *  This is a required parameter for all new HeapBufMP instances.
220      */
222     SizeT align;
223     /*!< Alignment (in MAUs) of each block.
224      *
225      *  The alignment must be a power of 2. If the value 0 is specified,
226      *  the value will be changed to meet minimum structure alignment
227      *  requirements and the cache alignment size of the region in which the
228      *  heap will be placed.  Therefore, the actual alignment may be larger.
229      *
230      *  The default alignment is 0.
231      */
233     Bool exact;
234     /*!< Use exact matching
235      *
236      *  Setting this flag will allow allocation only if the requested size
237      *  is equal to (rather than less than or equal to) the buffer's block
238      *  size.
239      */
241     GateMP_Handle gate;
242     /*!< GateMP used for critical region management of the shared memory
243      *
244      *  Using the default value of NULL will result in use of the GateMP
245      *  system gate for context protection.
246      */
248 } HeapBufMP_Params;
250 /*!
251  *  @brief  Stats structure for the HeapBufMP_getExtendedStats API.
252  */
253 typedef struct HeapBufMP_ExtendedStats {
254     UInt maxAllocatedBlocks;
255     /*!< The maximum number of blocks allocated from this heap at any point in
256      *  time during the lifetime of this HeapBufMP instance.
257      */
259     UInt numAllocatedBlocks;
260     /*!< The total number of blocks currently allocated in this HeapBufMP
261      *  instance.
262      */
263 } HeapBufMP_ExtendedStats;
265 /* =============================================================================
266  *  HeapBufMP Module-wide Functions
267  * =============================================================================
268  */
270 /*!
271  *  @brief      Close a HeapBufMP instance
272  *
273  *  Closing an instance will free local memory consumed by the opened
274  *  instance. All opened instances should be closed before the instance
275  *  is deleted.
276  *
277  *  @param[in,out]  handlePtr   Pointer to HeapBufMP handle typically returned
278  *                              from #HeapBufMP_open
279  *
280  *  @return     HeapBufMP status:
281  *              - #HeapBufMP_S_SUCCESS: Heap successfully closed
282  *
283  *  @sa         HeapBufMP_open
284  */
285 Int HeapBufMP_close(HeapBufMP_Handle *handlePtr);
287 /*!
288  *  @brief      Create a HeapBufMP instance
289  *
290  *  @param[in]  params      HeapBufMP parameters
291  *
292  *  @return     HeapBufMP Handle
293  */
294 HeapBufMP_Handle HeapBufMP_create(const HeapBufMP_Params *params);
296 /*!
297  *  @brief      Delete a created HeapBufMP instance
298  *
299  *  @param[in,out]  handlePtr   Pointer to handle to delete.
300  *
301  *  @return     HeapBufMP status:
302  *              - #HeapBufMP_S_SUCCESS: Heap successfully deleted
303  */
304 Int HeapBufMP_delete(HeapBufMP_Handle *handlePtr);
306 /*!
307  *  @brief      Open a created HeapBufMP instance
308  *
309  *  Once an instance is created, an open can be performed. The
310  *  open is used to gain access to the same HeapBufMP instance.
311  *  Generally an instance is created on one processor and opened on the
312  *  other processor.
313  *
314  *  The open returns a HeapBufMP instance handle like the create,
315  *  however the open does not initialize the shared memory. The supplied
316  *  name is used to identify the created instance.
317  *
318  *  Call #HeapBufMP_close when the opened instance is not longer needed.
319  *
320  *  @param[in]  name        Name of created HeapBufMP instance
321  *  @param[out] handlePtr   Pointer to HeapBufMP handle to be opened
322  *
323  *  @return     HeapBufMP status:
324  *              - #HeapBufMP_S_SUCCESS: Heap successfully opened
325  *              - #HeapBufMP_E_NOTFOUND: Heap is not yet ready to be opened.
326  *              - #HeapBufMP_E_FAIL: A general failure has occurred
327  *
328  *  @sa         HeapBufMP_close
329  */
330 Int HeapBufMP_open(String name, HeapBufMP_Handle *handlePtr);
332 /*! @cond */
333 Int HeapBufMP_openByAddr(Ptr sharedAddr, HeapBufMP_Handle *handlePtr);
335 /*! @endcond */
337 /*!
338  *  @brief      Initialize a HeapBufMP parameters struct
339  *
340  *  @param[out] params      Pointer to GateMP parameters
341  *
342  */
343 Void HeapBufMP_Params_init(HeapBufMP_Params *params);
345 /*! @cond */
346 /*!
347  *  @brief      Amount of shared memory required for creation of each instance
348  *
349  *  @param[in]  params      Pointer to the parameters that will be used in
350  *                          the create.
351  *
352  *  @return     Number of MAUs needed to create the instance.
353  */
354 SizeT HeapBufMP_sharedMemReq(const HeapBufMP_Params *params);
356 /*! @endcond */
358 /* =============================================================================
359  *  HeapBufMP Per-instance Functions
360  * =============================================================================
361  */
363 /*!
364  *  @brief      Allocate a block of memory of specified size and alignment
365  *
366  *  The actual block returned may be larger than requested to satisfy
367  *  alignment requirements. NULL is returned if alloc fails.
368  *
369  *  HeapBufMP_alloc will lock the heap using the HeapBufMP gate
370  *  while it traverses the list of free blocks to find a large enough block
371  *  for the request.
372  *
373  *  Guidelines for using large heaps and multiple alloc() calls.
374  *      - If possible, allocate larger blocks first. Previous allocations
375  *        of small memory blocks can reduce the size of the blocks
376  *        available for larger memory allocations.
377  *      - Realize that alloc() can fail even if the heap contains a
378  *        sufficient absolute amount of unalloccated space. This is
379  *        because the largest free memory block may be smaller than
380  *        total amount of unallocated memory.
381  *
382  *  @param[in]  handle    Handle to previously created/opened instance.
383  *  @param[in]  size      Size to be allocated (in MADUs)
384  *  @param[in]  align     Alignment for allocation (power of 2)
385  *
386  *  @sa         HeapBufMP_free
387  */
388 Void *HeapBufMP_alloc(HeapBufMP_Handle handle, SizeT size, SizeT align);
390 /*!
391  *  @brief      Frees a block of memory.
392  *
393  *  free() places the memory block specified by addr and size back into the
394  *  free pool of the heap specified. The newly freed block is combined with
395  *  any adjacent free blocks. The space is then available for further
396  *  allocation by alloc().
397  *
398  *  #HeapBufMP_free will lock the heap using the HeapBufMP gate if one is
399  *  specified or the system GateMP if not.
400  *
401  *  @param[in]  handle    Handle to previously created/opened instance.
402  *  @param[in]  block     Block of memory to be freed.
403  *  @param[in]  size      Size to be freed (in MADUs)
404  *
405  *  @sa         HeapBufMP_alloc
406  */
407 Void HeapBufMP_free(HeapBufMP_Handle handle, Ptr block, SizeT size);
409 /*!
410  *  @brief      Get extended memory statistics
411  *
412  *  This function retrieves the extended statistics for a HeapBufMP
413  *  instance.  It does not retrieve the standard Memory_Stats
414  *  information.  Refer to #HeapBufMP_ExtendedStats for more information
415  *  regarding what information is returned.
416  *
417  *  In BIOS, HeapBufMP.trackAllocs needs to be set to 'true' in the
418  *  configuration to get meaningful extended stats.
419  *
420  *  @param[in]  handle    Handle to previously created/opened instance.
421  *  @param[out] stats     ExtendedStats structure
422  *
423  *  @sa     HeapBufMP_getStats
424  */
425 Void HeapBufMP_getExtendedStats(HeapBufMP_Handle handle,
426                                 HeapBufMP_ExtendedStats *stats);
428 /*!
429  *  @brief      Get memory statistics
430  *
431  *  @param[in]  handle    Handle to previously created/opened instance.
432  *  @param[out] stats     Memory statistics structure
433  *
434  *  @sa     HeapBufMP_getExtendedStats
435  */
436 Void HeapBufMP_getStats(HeapBufMP_Handle handle, Ptr stats);
438 #if defined (__cplusplus)
440 #endif /* defined (__cplusplus) */
441 #endif /* ti_ipc_HeapBufMP__include */