1 /*
2 * Copyright (c) 2011-2013, Texas Instruments Incorporated
3 * All rights reserved.
4 *
5 * Redistribution and use in source and binary forms, with or without
6 * modification, are permitted provided that the following conditions
7 * are met:
8 *
9 * * Redistributions of source code must retain the above copyright
10 * notice, this list of conditions and the following disclaimer.
11 *
12 * * Redistributions in binary form must reproduce the above copyright
13 * notice, this list of conditions and the following disclaimer in the
14 * documentation and/or other materials provided with the distribution.
15 *
16 * * Neither the name of Texas Instruments Incorporated nor the names of
17 * its contributors may be used to endorse or promote products derived
18 * from this software without specific prior written permission.
19 *
20 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31 */
32 /** ============================================================================
33 * @file VirtQueue.h
34 *
35 * @brief Virtio Queue interface for BIOS
36 *
37 * Differences between BIOS version and Linux kernel (include/linux/virtio.h):
38 * - Renamed module from virtio.h to VirtQueue.h to match the API prefixes;
39 * - BIOS (XDC) types and CamelCasing used;
40 * - virtio_device concept removed (i.e, assumes no containing device);
41 * - removed scatterlist;
42 * - VirtQueues are created statically here, so just added a VirtQueue_init()
43 * fxn to take the place of the Virtio vring_new_virtqueue() API;
44 * - The notify function is implicit in the implementation, and not provided
45 * by the client, as it is in Linux virtio.
46 * - Broke into APIs to add/get used and avail buffers, as the API is
47 * assymmetric.
48 *
49 * Usage:
50 * This IPC only works between one processor designated as the Host (Linux)
51 * and one or more Slave processors (BIOS).
52 *
53 * For any Host/Slave pair, there are 2 VirtQueues (aka Vrings);
54 * Only the Host adds new buffers to the avail list of a vring;
55 * Available buffers can be empty or full, depending on direction;
56 * Used buffer means "processed" (emptied or filled);
57 *
58 * Host:
59 * - To send buffer to the slave processor:
60 * add_avail_buf(slave_virtqueue);
61 * kick(slave_virtqueue);
62 * get_used_buf(slave_virtqueue);
63 * - To receive buffer from slave processor:
64 * add_avail_buf(host_virtqueue);
65 * kick(host_virtqueue);
66 * get_used_buf(host_virtqueue);
67 *
68 * Slave:
69 * - To send buffer to the host:
70 * get_avail_buf(host_virtqueue);
71 * add_used_buf(host_virtqueue);
72 * kick(host_virtqueue);
73 * - To receive buffer from the host:
74 * get_avail_buf(slave_virtqueue);
75 * add_used_buf(slave_virtqueue);
76 * kick(slave_virtqueue);
77 *
78 * All VirtQueue operations can be called in any context.
79 *
80 * The virtio header should be included in an application as follows:
81 * @code
82 * #include <ti/ipc/rpmsg/VirtQueue.h>
83 * @endcode
84 *
85 * ============================================================================
86 */
88 #ifndef ti_ipc_family_omap54xx_VirtQueue__include
89 #define ti_ipc_family_omap54xx_VirtQueue__include
91 #include <xdc/runtime/Error.h>
93 #if defined (__cplusplus)
94 extern "C" {
95 #endif
97 /*!
98 * @brief a queue to register buffers for sending or receiving.
99 */
100 typedef struct VirtQueue_Object *VirtQueue_Handle;
102 /*!
103 * @var VirtQueue_callback
104 * @brief Signature of any callback function that can be registered with the
105 * VirtQueue
106 *
107 * @param[in] VirtQueue Pointer to the VirtQueue which was signalled.
108 */
109 typedef Void (*VirtQueue_callback)(VirtQueue_Handle);
111 /*!
112 * @brief VirtQueue_params
113 */
114 typedef struct VirtQueue_Params {
115 VirtQueue_callback callback;
116 Int vqId;
117 } VirtQueue_Params;
119 /* Params_init */
120 static inline void VirtQueue_Params_init( VirtQueue_Params *prms )
121 {
122 /* Do nothing: We are emulating an XDC generated fxn, w/o XDC config! */
123 }
125 /*!
126 * @brief Initialize at runtime the VirtQueue
127 *
128 * @param[in] procId Processor ID associated with this VirtQueue.
129 * @param[in] params VirtQueue_Params {callback, vqId}.
130 * @param[in] eb Error_Block (or NULL).
131 *
132 * @Returns Returns a handle to a new initialized VirtQueue.
133 */
134 VirtQueue_Handle VirtQueue_create(UInt16 procId, VirtQueue_Params *params,
135 Error_Block *eb);
137 /*!
138 * @brief Notify other processor of new buffers in the queue.
139 *
140 * After one or more add_buf calls, invoke this to kick the other side.
141 *
142 * @param[in] vq the VirtQueue.
143 *
144 * @sa VirtQueue_addBuf
145 */
146 Void VirtQueue_kick(VirtQueue_Handle vq);
148 /*!
149 * @brief Used at startup-time for initialization
150 *
151 * Should be called before any other VirtQueue APIs
152 */
153 Void VirtQueue_startup();
156 /*
157 * ============================================================================
158 * Host Only Functions:
159 * ============================================================================
160 */
162 /*!
163 * @brief Add available buffer to virtqueue's available buffer list.
164 * Only used by Host.
165 *
166 * @param[in] vq the VirtQueue.
167 * @param[in] buf the buffer to be processed by the slave.
168 *
169 * @return Remaining capacity of queue or a negative error.
170 *
171 * @sa VirtQueue_getUsedBuf
172 */
173 Int VirtQueue_addAvailBuf(VirtQueue_Handle vq, Void *buf);
175 /*!
176 * @brief Get the next used buffer.
177 * Only used by Host.
178 *
179 * @param[in] vq the VirtQueue.
180 *
181 * @return Returns NULL or the processed buffer.
182 *
183 * @sa VirtQueue_addAvailBuf
184 */
185 Void *VirtQueue_getUsedBuf(VirtQueue_Handle vq);
187 /*
188 * ============================================================================
189 * Slave Only Functions:
190 * ============================================================================
191 */
193 /*!
194 * @brief Get the next available buffer.
195 * Only used by Slave.
196 *
197 * @param[in] vq the VirtQueue.
198 * @param[out] buf Pointer to location of available buffer;
199 * @param[out] len Length of the available buffer message.
200 *
201 * @return Returns a token used to identify the available buffer, to be
202 * passed back into VirtQueue_addUsedBuf();
203 * token is negative if failure to find an available buffer.
204 *
205 * @sa VirtQueue_addUsedBuf
206 */
207 Int16 VirtQueue_getAvailBuf(VirtQueue_Handle vq, Void **buf, Int *len);
209 /*!
210 * @brief Add used buffer to virtqueue's used buffer list.
211 * Only used by Slave.
212 *
213 * @param[in] vq the VirtQueue.
214 * @param[in] token token of the buffer to be added to vring used list.
215 * @param[in] len length of the message being added.
216 *
217 * @return Remaining capacity of queue or a negative error.
218 *
219 * @sa VirtQueue_getAvailBuf
220 */
221 Int VirtQueue_addUsedBuf(VirtQueue_Handle vq, Int16 token, Int len);
223 /*!
224 * @brief Post crash message to host mailbox
225 */
226 Void VirtQueue_postCrashToMailbox(Void);
228 #if defined (__cplusplus)
229 }
230 #endif /* defined (__cplusplus) */
232 #endif /* ti_ipc_family_omap54xx_VirtQueue__include */