d4c9cdf86581e8d1d8c48d1dc52a739e0367641f
[ipc/ipcdev.git] / packages / ti / ipc / family / tci6638 / VirtQueue.c
1 /*
2  * Copyright (c) 2011-2018 Texas Instruments Incorporated - http://www.ti.com
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * *  Redistributions of source code must retain the above copyright
10  *    notice, this list of conditions and the following disclaimer.
11  *
12  * *  Redistributions in binary form must reproduce the above copyright
13  *    notice, this list of conditions and the following disclaimer in the
14  *    documentation and/or other materials provided with the distribution.
15  *
16  * *  Neither the name of Texas Instruments Incorporated nor the names of
17  *    its contributors may be used to endorse or promote products derived
18  *    from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
33 /** ============================================================================
34  *  @file       VirtQueue.c
35  *
36  *  @brief      Virtio Queue implementation for BIOS
37  *
38  *  Differences between BIOS version and Linux kernel (include/linux/virtio.h):
39  *  - Renamed module from virtio.h to VirtQueue.h to match the API prefixes
40  *  - XDC Standard Types and CamelCasing used
41  *  - virtio_device concept removed (i.e, assumes no containing device)
42  *  - simplified scatterlist from Linux version
43  *  - VirtQueue objects are created statically, added VirtQueue_Instance_init()
44  *    fxn to take the place of the Virtio vring_new_virtqueue() API
45  *  - The notify function is implicit in the implementation, and not provided
46  *    by the client, as it is in Linux virtio
47  *
48  *  All VirtQueue operations can be called in any context.
49  */
51 #include <xdc/std.h>
52 #include <xdc/runtime/System.h>
53 #include <xdc/runtime/Assert.h>
54 #include <xdc/runtime/Error.h>
55 #include <xdc/runtime/Memory.h>
56 #include <xdc/runtime/Log.h>
57 #include <xdc/runtime/Diags.h>
58 #include <ti/sysbios/gates/GateAll.h>
60 #include <ti/sysbios/knl/Clock.h>
61 #include <ti/sysbios/family/c66/Cache.h>
62 #include <ti/sysbios/knl/Swi.h>
64 #include <ti/ipc/remoteproc/Resource.h>
66 #include <ti/ipc/MultiProc.h>
68 #include "package/internal/VirtQueue.xdc.h"
70 #include <string.h>
72 #include <ti/ipc/rpmsg/_VirtQueue.h>
73 #include <ti/ipc/rpmsg/virtio_ring.h>
75 /* Used for defining the size of the virtqueue registry */
76 #define NUM_QUEUES 2
78 #define DIV_ROUND_UP(n,d)   (((n) + (d) - 1) / (d))
79 #define RP_MSG_BUFS_SPACE   (VirtQueue_RP_MSG_NUM_BUFS * RPMSG_BUF_SIZE * 2)
81 /* With 256 buffers, our vring will occupy 3 pages */
82 #define RP_MSG_RING_SIZE    \
83         ((DIV_ROUND_UP(vring_size(VirtQueue_RP_MSG_NUM_BUFS, \
84         VirtQueue_RP_MSG_VRING_ALIGN), \
85         VirtQueue_PAGE_SIZE)) * VirtQueue_PAGE_SIZE)
87 /* The total IPC space needed to communicate with a remote processor */
88 #define RPMSG_IPC_MEM   (RP_MSG_BUFS_SPACE + 2 * RP_MSG_RING_SIZE)
90 #define ID_SELF_TO_HOST 0
91 #define ID_HOST_TO_SELF 1
93 extern volatile cregister UInt DNUM;
95 static VirtQueue_Object *queueRegistry[NUM_QUEUES] = {NULL};
97 static inline  Void * mapPAtoVA(UInt pa)
98 {
99     return (Void *)(pa | 0x80000000);
102 static inline UInt mapVAtoPA(Void * va)
104     return ((UInt)va & 0x000fffffU) | 0xe1000000U;
107 /*
108  * ======== VirtQueue_init ========
109  */
110 Void VirtQueue_init()
112     extern cregister volatile UInt DNUM;
113     UInt16 clusterId;
114     UInt16 procId;
116     /*  VirtQueue_init() must be called before MultiProcSetup_init().
117      *  Check the xdc_runtime_Startup_firstFxns__A array in the XDC
118      *  generated code. Abort if the procId has already been set; we
119      *  must set it!
120      */
121     if (MultiProc_self() != MultiProc_INVALIDID) {
122         System_abort("VirtQueue_init(): MultiProc_self already set!");
123         return;
124     }
126     /* clusterId is needed to support single image loading */
127     clusterId = MultiProc_getBaseIdOfCluster();
129     /* compute local procId, add one to account for HOST processor */
130     procId = clusterId + DNUM + 1;
132     /* set the local procId */
133     MultiProc_setLocalId(procId);
136 /*
137  * ======== VirtQueue_Instance_init ========
138  */
139 Int VirtQueue_Instance_init(VirtQueue_Object *vq, UInt16 remoteProcId,
140                              const VirtQueue_Params *params, Error_Block *eb)
142     void *vringAddr = NULL;
143 #if !defined(xdc_runtime_Assert_DISABLE_ALL) \
144         || !defined(xdc_runtime_Log_DISABLE_ALL)
145     UInt32 marValue;
146 #endif
148     VirtQueue_module->traceBufPtr = Resource_getTraceBufPtr();
150     /* create the thread protection gate */
151     vq->gateH = GateAll_create(NULL, eb);
152     if (Error_check(eb)) {
153         Log_error0("VirtQueue_create: could not create gate object");
154         Error_raise(NULL, Error_E_generic, 0, 0);
155         return(0);
156     }
158     vq->vringPtr = Memory_calloc(NULL, sizeof(struct vring), 0, eb);
159     Assert_isTrue((vq->vringPtr != NULL), NULL);
161     vq->callback = params->callback;
162     vq->id = params->vqId;
163     vq->procId = remoteProcId;
164     vq->last_avail_idx = 0;
165     vq->last_used_idx = 0;
166     vq->num_free = VirtQueue_RP_MSG_NUM_BUFS;
167     vq->swiHandle = params->swiHandle;
169     switch (vq->id) {
170         case ID_SELF_TO_HOST:
171         case ID_HOST_TO_SELF:
172             vringAddr = (struct vring *)Resource_getVringDA(vq->id);
173             Assert_isTrue(vringAddr != NULL, NULL);
174 #ifdef PER_CORE_VRING_PATCH
175             /* Add per core offset: must match on host side: */
176             vringAddr = (struct vring *)((UInt32)vringAddr +
177                                          (DNUM * VirtQueue_VRING_OFFSET));
178 #endif
179             /* Also, assert that the vring address is non-cached: */
180 #if !defined(xdc_runtime_Assert_DISABLE_ALL) \
181         || !defined(xdc_runtime_Log_DISABLE_ALL)
182             marValue = Cache_getMar((Ptr)vringAddr);
183 #endif
184             Log_print1(Diags_USER1, "Vring cache is %s",
185                  (IArg)(marValue & 0x1 ? "enabled" : "disabled"));
186             Assert_isTrue(!(marValue & 0x1), NULL);
187             break ;
189          default:
190             Log_error1("VirtQueue_create: invalid vq->id: %d", vq->id);
191             GateAll_delete(&vq->gateH);
192             Memory_free(NULL, vq->vringPtr, sizeof(struct vring));
193             Error_raise(NULL, Error_E_generic, 0, 0);
194             return(0);
195     }
197     Log_print3(Diags_USER1, "vring: %d 0x%x (0x%x)", vq->id, (IArg)vringAddr,
198             RP_MSG_RING_SIZE);
200     vring_init(vq->vringPtr, VirtQueue_RP_MSG_NUM_BUFS, vringAddr,
201             VirtQueue_RP_MSG_VRING_ALIGN);
203     queueRegistry[vq->id] = vq;
204     return(0);
207 /*
208  * ======== VirtQueue_kick ========
209  */
210 Void VirtQueue_kick(VirtQueue_Handle vq)
212     struct vring *vring = vq->vringPtr;
214     /* For now, simply interrupt remote processor */
215     if (vring->avail->flags & VRING_AVAIL_F_NO_INTERRUPT) {
216         Log_print0(Diags_USER1, "VirtQueue_kick: no kick because of "
217                 "VRING_AVAIL_F_NO_INTERRUPT");
218         return;
219     }
221     Log_print2(Diags_USER1, "VirtQueue_kick: Sending interrupt to proc %d "
222             "with payload 0x%x", (IArg)vq->procId, (IArg)vq->id);
224     VirtQueue_InterruptProxy_intSend(vq->procId, NULL, 0);
227 /*
228  * ======== VirtQueue_addUsedBuf ========
229  */
230 Int VirtQueue_addUsedBuf(VirtQueue_Handle vq, Int16 head, Int len)
232     struct vring_used_elem *used;
233     struct vring *vring = vq->vringPtr;
234     IArg key;
236     key = GateAll_enter(vq->gateH);
237     if ((head > vring->num) || (head < 0)) {
238         Error_raise(NULL, Error_E_generic, 0, 0);
239     }
240     else {
241         /*
242          * The virtqueue contains a ring of used buffers.  Get a pointer to the
243          * next entry in that used ring.
244          */
245         used = &vring->used->ring[vring->used->idx % vring->num];
246         used->id = head;
247         used->len = len;
249         vring->used->idx++;
250     }
251     GateAll_leave(vq->gateH, key);
253     return (0);
256 /*
257  * ======== VirtQueue_addAvailBuf ========
258  */
259 Int VirtQueue_addAvailBuf(VirtQueue_Object *vq, Void *buf)
261     UInt16 avail;
262     struct vring *vring = vq->vringPtr;
263     IArg key;
265     key = GateAll_enter(vq->gateH);
266     if (vq->num_free == 0) {
267         /* There's no more space */
268         Error_raise(NULL, Error_E_generic, 0, 0);
269     }
270     else {
271         vq->num_free--;
273         avail =  vring->avail->idx++ % vring->num;
275         vring->desc[avail].addr = mapVAtoPA(buf);
276         vring->desc[avail].len = RPMSG_BUF_SIZE;
277     }
278     GateAll_leave(vq->gateH, key);
280     return (vq->num_free);
283 /*
284  * ======== VirtQueue_getUsedBuf ========
285  */
286 Void *VirtQueue_getUsedBuf(VirtQueue_Object *vq)
288     UInt16 head;
289     Void *buf;
290     struct vring *vring = vq->vringPtr;
291     IArg key;
293     key = GateAll_enter(vq->gateH);
294     /* There's nothing available? */
295     if (vq->last_used_idx == vring->used->idx) {
296         buf = NULL;
297     }
298     else {
299         head = vring->used->ring[vq->last_used_idx % vring->num].id;
300         vq->last_used_idx++;
301         vq->num_free++;
303         buf = mapPAtoVA(vring->desc[head].addr);
304     }
305     GateAll_leave(vq->gateH, key);
307     return (buf);
310 /*
311  * ======== VirtQueue_getAvailBuf ========
312  */
313 Int16 VirtQueue_getAvailBuf(VirtQueue_Handle vq, Void **buf, Int *len)
315     Int16 head;
316     struct vring *vring = vq->vringPtr;
317     IArg key;
319     key = GateAll_enter(vq->gateH);
320     Log_print6(Diags_USER1, "getAvailBuf vq: 0x%x %d %d %d 0x%x 0x%x",
321         (IArg)vq, (IArg)vq->last_avail_idx, (IArg)vring->avail->idx,
322         (IArg)vring->num, (IArg)&vring->avail, (IArg)vring->avail);
324     /*  Clear flag here to avoid race condition with remote processor.
325      *  This is a negative flag, clearing it means that we want to
326      *  receive an interrupt when a buffer has been added to the pool.
327      */
328     vring->used->flags &= ~VRING_USED_F_NO_NOTIFY;
330     /* There's nothing available? */
331     if (vq->last_avail_idx == vring->avail->idx) {
332         head = (-1);
333     }
334     else {
335         /* No need to be kicked about added buffers anymore */
336         vring->used->flags |= VRING_USED_F_NO_NOTIFY;
338         /*
339          * Grab the next descriptor number they're advertising, and increment
340          * the index we've seen.
341          */
342         head = vring->avail->ring[vq->last_avail_idx++ % vring->num];
344         *buf = mapPAtoVA(vring->desc[head].addr);
345         *len = vring->desc[head].len;
346     }
347     GateAll_leave(vq->gateH, key);
349     return (head);
352 /*
353  * ======== VirtQueue_isr ========
354  * Note 'msg' is ignored: it is only used where there is a mailbox payload.
355  */
356 static Void VirtQueue_isr(UArg msg)
358     VirtQueue_Object *vq;
360     Log_print1(Diags_USER1, "VirtQueue_isr received msg = 0x%x", msg);
362     vq = queueRegistry[0];
363     if (vq) {
364         vq->callback(vq);
365     }
366     vq = queueRegistry[1];
367     if (vq) {
368         vq->callback(vq);
369     }
372 /*
373  * ======== VirtQueue_startup ========
374  */
375 Void VirtQueue_startup(UInt16 procId, Bool isHost)
378     /* Wait for first kick from host, which happens to coincide with the
379      * priming of host's receive buffers, indicating host is ready to send.
380      * Since interrupt is cleared, we throw away this first kick, which is
381      * OK since we don't process this in the ISR anyway.
382      */
383     Log_print0(Diags_USER1, "VirtQueue_startup: Polling for host int...");
384     while (!VirtQueue_InterruptProxy_intClear(procId, NULL));
386     VirtQueue_InterruptProxy_intRegister(procId, NULL, (Fxn)VirtQueue_isr, 0);
387     Log_print0(Diags_USER1, "Passed VirtQueue_startup");
390 /* By convention, Host VirtQueues host are the even number in the pair */
391 Bool VirtQueue_isSlave(VirtQueue_Handle vq)
393   return (vq->id & 0x1);
396 Bool VirtQueue_isHost(VirtQueue_Handle vq)
398   return (~(vq->id & 0x1));
401 UInt16 VirtQueue_getId(VirtQueue_Handle vq)
403   return (vq->id);
406 Swi_Handle VirtQueue_getSwiHandle(VirtQueue_Handle vq)
408   return (vq->swiHandle);
411 #define CACHE_WB_TICK_PERIOD    5
413 /*
414  * ======== VirtQueue_cacheWb ========
415  *
416  * Used for flushing SysMin trace buffer.
417  */
418 Void VirtQueue_cacheWb()
420     static UInt32 oldticks = 0;
421     UInt32 newticks;
423     newticks = Clock_getTicks();
424     if (newticks - oldticks < (UInt32)CACHE_WB_TICK_PERIOD) {
425         /* Don't keep flushing cache */
426         return;
427     }
429     oldticks = newticks;
431     /* Flush the cache of the SysMin buffer only: */
432     Assert_isTrue((VirtQueue_module->traceBufPtr != NULL), NULL);
433     Cache_wb(VirtQueue_module->traceBufPtr, Resource_getTraceBufSize(), Cache_Type_ALL,
434              FALSE);