b1bccc366f57112934c9e5d7188f57c32687d6bb
[ipc/ipcdev.git] / packages / ti / ipc / family / vayu / VirtQueue.c
1 /*
2  * Copyright (c) 2011-2013, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * *  Redistributions of source code must retain the above copyright
10  *    notice, this list of conditions and the following disclaimer.
11  *
12  * *  Redistributions in binary form must reproduce the above copyright
13  *    notice, this list of conditions and the following disclaimer in the
14  *    documentation and/or other materials provided with the distribution.
15  *
16  * *  Neither the name of Texas Instruments Incorporated nor the names of
17  *    its contributors may be used to endorse or promote products derived
18  *    from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 /** ============================================================================
33  *  @file       VirtQueue.c
34  *
35  *  @brief      Virtio Queue implementation for BIOS
36  *
37  *  Differences between BIOS version and Linux kernel (include/linux/virtio.h):
38  *  - Renamed module from virtio.h to VirtQueue_Object.h to match the API prefixes;
39  *  - BIOS (XDC) types and CamelCasing used;
40  *  - virtio_device concept removed (i.e, assumes no containing device);
41  *  - simplified scatterlist from Linux version;
42  *  - VirtQueue_Objects are created statically here, so just added a VirtQueue_Object_init()
43  *    fxn to take the place of the Virtio vring_new_virtqueue() API;
44  *  - The notify function is implicit in the implementation, and not provided
45  *    by the client, as it is in Linux virtio.
46  *
47  *  All VirtQueue operations can be called in any context.
48  *
49  *  The virtio header should be included in an application as follows:
50  *  @code
51  *  #include <ti/ipc/family/vayu/VirtQueue.h>
52  *  @endcode
53  *
54  */
56 #include <xdc/std.h>
57 #include <xdc/runtime/System.h>
58 #include <xdc/runtime/Error.h>
59 #include <xdc/runtime/Memory.h>
60 #include <xdc/runtime/Log.h>
61 #include <xdc/runtime/Diags.h>
63 #include <ti/sysbios/hal/Hwi.h>
64 #include <ti/sysbios/knl/Clock.h>
65 #include <ti/sysbios/gates/GateHwi.h>
66 #include <ti/sysbios/BIOS.h>
67 #include <ti/sysbios/hal/Cache.h>
69 #include <ti/ipc/MultiProc.h>
71 #include <ti/ipc/rpmsg/virtio_ring.h>
72 #ifndef DSP
73 #include <ti/pm/IpcPower.h>
74 #endif
75 #include <string.h>
77 #include <ti/ipc/rpmsg/_VirtQueue.h>
79 #include <ti/sdo/ipc/notifyDrivers/IInterrupt.h>
80 #include "InterruptProxy.h"
81 #include "VirtQueue.h"
84 /* Used for defining the size of the virtqueue registry */
85 #define NUM_QUEUES              4
87 /* Predefined device addresses */
88 #ifdef DSP
89 #define IPC_MEM_VRING0          0xA0000000
90 #define IPC_MEM_VRING1          0xA0004000
91 #define IPC_MEM_VRING2          0xA0008000
92 #define IPC_MEM_VRING3          0xA000c000
93 #else
94 #define IPC_MEM_VRING0          0x60000000
95 #define IPC_MEM_VRING1          0x60004000
96 #define IPC_MEM_VRING2          0x60008000
97 #define IPC_MEM_VRING3          0x6000c000
98 #endif
100 /*
101  * Sizes of the virtqueues (expressed in number of buffers supported,
102  * and must be power of two)
103  */
104 #define VQ0_SIZE                256
105 #define VQ1_SIZE                256
106 #define VQ2_SIZE                256
107 #define VQ3_SIZE                256
109 /*
110  * enum - Predefined Mailbox Messages
111  *
112  * @RP_MSG_MBOX_READY: informs the M3's that we're up and running. will be
113  * followed by another mailbox message that carries the A9's virtual address
114  * of the shared buffer. This would allow the A9's drivers to send virtual
115  * addresses of the buffers.
116  *
117  * @RP_MSG_MBOX_STATE_CHANGE: informs the receiver that there is an inbound
118  * message waiting in its own receive-side vring. please note that currently
119  * this message is optional: alternatively, one can explicitly send the index
120  * of the triggered virtqueue itself. the preferred approach will be decided
121  * as we progress and experiment with those design ideas.
122  *
123  * @RP_MSG_MBOX_CRASH: this message indicates that the BIOS side is unhappy
124  *
125  * @RP_MBOX_ECHO_REQUEST: this message requests the remote processor to reply
126  * with RP_MBOX_ECHO_REPLY
127  *
128  * @RP_MBOX_ECHO_REPLY: this is a reply that is sent when RP_MBOX_ECHO_REQUEST
129  * is received.
130  *
131  * @RP_MBOX_ABORT_REQUEST:  tells the M3 to crash on demand
132  *
133  * @RP_MBOX_BOOTINIT_DONE: this message indicates the BIOS side has reached a
134  * certain state during the boot process. This message is used to inform the
135  * host that the basic BIOS initialization is done, and lets the host use this
136  * notification to perform certain actions.
137  */
138 enum {
139     RP_MSG_MBOX_READY           = (Int)0xFFFFFF00,
140     RP_MSG_MBOX_STATE_CHANGE    = (Int)0xFFFFFF01,
141     RP_MSG_MBOX_CRASH           = (Int)0xFFFFFF02,
142     RP_MBOX_ECHO_REQUEST        = (Int)0xFFFFFF03,
143     RP_MBOX_ECHO_REPLY          = (Int)0xFFFFFF04,
144     RP_MBOX_ABORT_REQUEST       = (Int)0xFFFFFF05,
145     RP_MSG_FLUSH_CACHE          = (Int)0xFFFFFF06,
146     RP_MSG_BOOTINIT_DONE        = (Int)0xFFFFFF07,
147     RP_MSG_HIBERNATION          = (Int)0xFFFFFF10,
148     RP_MSG_HIBERNATION_FORCE    = (Int)0xFFFFFF11,
149     RP_MSG_HIBERNATION_ACK      = (Int)0xFFFFFF12,
150     RP_MSG_HIBERNATION_CANCEL   = (Int)0xFFFFFF13
151 };
153 #define DIV_ROUND_UP(n,d)   (((n) + (d) - 1) / (d))
154 #define RP_MSG_NUM_BUFS     (VQ0_SIZE) /* must be power of two */
155 #define RP_MSG_BUF_SIZE     (512)
156 #define RP_MSG_BUFS_SPACE   (RP_MSG_NUM_BUFS * RP_MSG_BUF_SIZE * 2)
158 #define PAGE_SIZE           (4096)
159 /*
160  * The alignment to use between consumer and producer parts of vring.
161  * Note: this is part of the "wire" protocol. If you change this, you need
162  * to update your BIOS image as well
163  */
164 #define RP_MSG_VRING_ALIGN  (4096)
166 /* With 256 buffers, our vring will occupy 3 pages */
167 #define RP_MSG_RING_SIZE    ((DIV_ROUND_UP(vring_size(RP_MSG_NUM_BUFS, \
168                             RP_MSG_VRING_ALIGN), PAGE_SIZE)) * PAGE_SIZE)
170 /* The total IPC space needed to communicate with a remote processor */
171 #define RPMSG_IPC_MEM   (RP_MSG_BUFS_SPACE + 2 * RP_MSG_RING_SIZE)
173 #define ID_SYSM3_TO_A9      ID_SELF_TO_A9
174 #define ID_A9_TO_SYSM3      ID_A9_TO_SELF
175 #define ID_DSP_TO_A9        ID_SELF_TO_A9
176 #define ID_A9_TO_DSP        ID_A9_TO_SELF
177 #define ID_APPM3_TO_A9      2
178 #define ID_A9_TO_APPM3      3
180 typedef struct VirtQueue_Object {
181     /* Id for this VirtQueue_Object */
182     UInt16                  id;
184     /* The function to call when buffers are consumed (can be NULL) */
185     VirtQueue_callback      callback;
187     /* Shared state */
188     struct vring            vring;
190     /* Number of free buffers */
191     UInt16                  num_free;
193     /* Last available index; updated by VirtQueue_getAvailBuf */
194     UInt16                  last_avail_idx;
196     /* Last available index; updated by VirtQueue_addUsedBuf */
197     UInt16                  last_used_idx;
199     /* Will eventually be used to kick remote processor */
200     UInt16                  procId;
202     /* Gate to protect from multiple threads */
203     GateHwi_Handle       gateH;
204 } VirtQueue_Object;
206 static struct VirtQueue_Object *queueRegistry[NUM_QUEUES] = {NULL};
208 static UInt16 hostProcId;
209 #ifndef SMP
210 static UInt16 dsp1ProcId;
211 static UInt16 sysm3ProcId;
212 static UInt16 appm3ProcId;
213 #endif
215 #define DSPEVENTID              5
216 IInterrupt_IntInfo intInfo;
218 #if defined(M3_ONLY) && !defined(SMP)
219 extern Void OffloadM3_init();
220 extern Int OffloadM3_processSysM3Tasks(UArg msg);
221 #endif
223 static inline Void * mapPAtoVA(UInt pa)
225     return (Void *)((pa & 0x000fffffU) | IPC_MEM_VRING0);
228 static inline UInt mapVAtoPA(Void * va)
230     return ((UInt)va & 0x000fffffU) | 0x9cf00000U;
233 /*!
234  * ======== VirtQueue_kick ========
235  */
236 Void VirtQueue_kick(VirtQueue_Handle vq)
238     /* For now, simply interrupt remote processor */
239     if (vq->vring.avail->flags & VRING_AVAIL_F_NO_INTERRUPT) {
240         Log_print0(Diags_USER1,
241                 "VirtQueue_kick: no kick because of VRING_AVAIL_F_NO_INTERRUPT\n");
242         return;
243     }
245     Log_print2(Diags_USER1,
246             "VirtQueue_kick: Sending interrupt to proc %d with payload 0x%x\n",
247             (IArg)vq->procId, (IArg)vq->id);
248     InterruptProxy_intSend(vq->procId, NULL, vq->id);
251 /*!
252  * ======== VirtQueue_addUsedBuf ========
253  */
254 Int VirtQueue_addUsedBuf(VirtQueue_Handle vq, Int16 head, Int len)
256     struct vring_used_elem *used;
257     IArg key;
259     key = GateHwi_enter(vq->gateH);
260     if ((head > vq->vring.num) || (head < 0)) {
261         GateHwi_leave(vq->gateH, key);
262         Error_raise(NULL, Error_E_generic, 0, 0);
263     }
265     /*
266     * The virtqueue contains a ring of used buffers.  Get a pointer to the
267     * next entry in that used ring.
268     */
269     used = &vq->vring.used->ring[vq->vring.used->idx % vq->vring.num];
270     used->id = head;
271     used->len = len;
273     vq->vring.used->idx++;
274     GateHwi_leave(vq->gateH, key);
276     return (0);
279 /*!
280  * ======== VirtQueue_addAvailBuf ========
281  */
282 Int VirtQueue_addAvailBuf(VirtQueue_Object *vq, Void *buf)
284     UInt16 avail;
285     IArg key;
287     if (vq->num_free == 0) {
288         /* There's no more space */
289         Error_raise(NULL, Error_E_generic, 0, 0);
290     }
292     vq->num_free--;
294     key = GateHwi_enter(vq->gateH);
295     avail =  vq->vring.avail->idx++ % vq->vring.num;
297     vq->vring.desc[avail].addr = mapVAtoPA(buf);
298     vq->vring.desc[avail].len = RP_MSG_BUF_SIZE;
299     GateHwi_leave(vq->gateH, key);
301     return (vq->num_free);
304 /*!
305  * ======== VirtQueue_getUsedBuf ========
306  */
307 Void *VirtQueue_getUsedBuf(VirtQueue_Object *vq)
309     UInt16 head;
310     Void *buf;
311     IArg key;
313     key = GateHwi_enter(vq->gateH);
314     /* There's nothing available? */
315     if (vq->last_used_idx == vq->vring.used->idx) {
316         buf = NULL;
317     }
318     else {
319         head = vq->vring.used->ring[vq->last_used_idx % vq->vring.num].id;
320         vq->last_used_idx++;
322         buf = mapPAtoVA(vq->vring.desc[head].addr);
323     }
324     GateHwi_leave(vq->gateH, key);
326     return (buf);
329 /*!
330  * ======== VirtQueue_getAvailBuf ========
331  */
332 Int16 VirtQueue_getAvailBuf(VirtQueue_Handle vq, Void **buf, Int *len)
334     Int16 head;
335     IArg key;
337     key = GateHwi_enter(vq->gateH);
338     Log_print6(Diags_USER1, "getAvailBuf vq: 0x%x %d %d %d 0x%x 0x%x\n",
339         (IArg)vq, vq->last_avail_idx, vq->vring.avail->idx, vq->vring.num,
340         (IArg)&vq->vring.avail, (IArg)vq->vring.avail);
342     /* There's nothing available? */
343     if (vq->last_avail_idx == vq->vring.avail->idx) {
344         /* We need to know about added buffers */
345         vq->vring.used->flags &= ~VRING_USED_F_NO_NOTIFY;
346         head = (-1);
347     }
348     else {
349         /*
350          * Grab the next descriptor number they're advertising, and increment
351          * the index we've seen.
352          */
353         head = vq->vring.avail->ring[vq->last_avail_idx++ % vq->vring.num];
355         *buf = mapPAtoVA(vq->vring.desc[head].addr);
356         *len = vq->vring.desc[head].len;
357     }
358     GateHwi_leave(vq->gateH, key);
360     return (head);
363 /*!
364  * ======== VirtQueue_disableCallback ========
365  */
366 Void VirtQueue_disableCallback(VirtQueue_Object *vq)
368     //TODO
369     Log_print0(Diags_USER1, "VirtQueue_disableCallback called.");
372 /*!
373  * ======== VirtQueue_enableCallback ========
374  */
375 Bool VirtQueue_enableCallback(VirtQueue_Object *vq)
377     Log_print0(Diags_USER1, "VirtQueue_enableCallback called.");
379     //TODO
380     return (FALSE);
383 /*!
384  * ======== VirtQueue_isr ========
385  * Note 'arg' is ignored: it is the Hwi argument, not the mailbox argument.
386  */
387 Void VirtQueue_isr(UArg msg)
389     VirtQueue_Object *vq;
391     msg = InterruptProxy_intClear(hostProcId, &intInfo);
393     Log_print1(Diags_USER1, "VirtQueue_isr received msg = 0x%x\n", msg);
395 #ifndef SMP
396     if (MultiProc_self() == sysm3ProcId || MultiProc_self() == dsp1ProcId) {
397 #endif
398         switch(msg) {
399             case (UInt)RP_MSG_MBOX_READY:
400                 return;
402             case (UInt)RP_MBOX_ECHO_REQUEST:
403                 InterruptProxy_intSend(hostProcId, NULL,
404                                        (UInt)(RP_MBOX_ECHO_REPLY));
405                 return;
407             case (UInt)RP_MBOX_ABORT_REQUEST:
408                 {
409                     /* Suppress Coverity Error: FORWARD_NULL: */
410                     // coverity[assign_zero]
411                     Fxn f = (Fxn)0x0;
412                     Log_print0(Diags_USER1, "Crash on demand ...\n");
413                     // coverity[var_deref_op]
414                     f();
415                 }
416                 return;
418             case (UInt)RP_MSG_FLUSH_CACHE:
419                 Cache_wbAll();
420                 return;
422 #ifndef DSP
423             case (UInt)RP_MSG_HIBERNATION:
424                 if (IpcPower_canHibernate() == FALSE) {
425                     InterruptProxy_intSend(hostProcId, NULL,
426                                            (UInt)RP_MSG_HIBERNATION_CANCEL);
427                     return;
428                 }
430             /* Fall through */
431             case (UInt)RP_MSG_HIBERNATION_FORCE:
432 #ifndef SMP
433                 /* Core0 should notify Core1 */
434                 if (MultiProc_self() == sysm3ProcId) {
435                     InterruptProxy_intSend(appm3ProcId, NULL,
436                                            (UInt)(RP_MSG_HIBERNATION));
437                 }
438 #endif
439                 /* Ack request */
440                 InterruptProxy_intSend(hostProcId, NULL,
441                                        (UInt)RP_MSG_HIBERNATION_ACK);
442                 IpcPower_suspend();
443                 return;
444 #endif
445             default:
446 #if defined(M3_ONLY) && !defined(SMP)
447                 /* Check and process any Inter-M3 Offload messages */
448                 if (OffloadM3_processSysM3Tasks(msg))
449                     return;
450 #endif
452                 /*
453                  *  If the message isn't one of the above, it's either part of the
454                  *  2-message synchronization sequence or it a virtqueue message
455                  */
456                 break;
457         }
458 #ifndef SMP
459     }
460     else if (msg & 0xFFFF0000) {
461 #ifndef DSP
462         if (msg == (UInt)RP_MSG_HIBERNATION) {
463             IpcPower_suspend();
464         }
465 #endif
466         return;
467     }
469     if (MultiProc_self() == sysm3ProcId && (msg == ID_A9_TO_APPM3 || msg == ID_APPM3_TO_A9)) {
470         InterruptProxy_intSend(appm3ProcId, NULL, (UInt)msg);
471     }
472     else {
473 #endif
474         /* Don't let unknown messages to pass as a virtqueue index */
475         if (msg >= NUM_QUEUES) {
476             /* Adding print here deliberately, we should never see this */
477             System_printf("VirtQueue_isr: Invalid mailbox message 0x%x "
478                           "received\n", msg);
479             return;
480         }
482         vq = queueRegistry[msg];
483         if (vq) {
484             vq->callback(vq);
485         }
486 #ifndef SMP
487     }
488 #endif
492 /*!
493  * ======== VirtQueue_create ========
494  */
495 VirtQueue_Handle VirtQueue_create(UInt16 remoteProcId, VirtQueue_Params *params,
496                                   Error_Block *eb)
498     VirtQueue_Object *vq;
499     Void *vringAddr;
501     vq = Memory_alloc(NULL, sizeof(VirtQueue_Object), 0, eb);
502     if (NULL == vq) {
503         return (NULL);
504     }
506     /* Create the thread protection gate */
507     vq->gateH = GateHwi_create(NULL, eb);
508     if (Error_check(eb)) {
509         Log_error0("VirtQueue_create: could not create gate object");
510         Memory_free(NULL, vq, sizeof(VirtQueue_Object));
511         return (NULL);
512     }
514     vq->callback = params->callback;
515     vq->id = params->vqId;
516     vq->procId = remoteProcId;
517     vq->last_avail_idx = 0;
519 #ifndef SMP
520     if (MultiProc_self() == appm3ProcId) {
521         /* vqindices that belong to AppM3 should be big so they don't
522          * collide with SysM3's virtqueues */
523          vq->id += 2;
524     }
525 #endif
527     switch (vq->id) {
528         /* IPC transport vrings */
529         case ID_SELF_TO_A9:
530             /* IPU/DSP -> A9 */
531             vringAddr = (struct vring *) IPC_MEM_VRING0;
532             break;
533         case ID_A9_TO_SELF:
534             /* A9 -> IPU/DSP */
535             vringAddr = (struct vring *) IPC_MEM_VRING1;
536             break;
537 #ifndef SMP
538         case ID_APPM3_TO_A9:
539             /* APPM3 -> A9 */
540             vringAddr = (struct vring *) IPC_MEM_VRING2;
541             break;
542         case ID_A9_TO_APPM3:
543             /* A9 -> APPM3 */
544             vringAddr = (struct vring *) IPC_MEM_VRING3;
545             break;
546 #endif
547         default:
548             GateHwi_delete(&vq->gateH);
549             Memory_free(NULL, vq, sizeof(VirtQueue_Object));
550             return (NULL);
551     }
553     Log_print3(Diags_USER1,
554             "vring: %d 0x%x (0x%x)\n", vq->id, (IArg)vringAddr,
555             RP_MSG_RING_SIZE);
557     /* See coverity related comment in vring_init() */
558     // coverity[overrun-call]
559     vring_init(&(vq->vring), RP_MSG_NUM_BUFS, vringAddr, RP_MSG_VRING_ALIGN);
561     /*
562      *  Don't trigger a mailbox message every time MPU makes another buffer
563      *  available
564      */
565     if (vq->procId == hostProcId) {
566         vq->vring.used->flags |= VRING_USED_F_NO_NOTIFY;
567     }
569     queueRegistry[vq->id] = vq;
571     return (vq);
574 /*!
575  * ======== VirtQueue_startup ========
576  */
577 Void VirtQueue_startup()
579     hostProcId      = MultiProc_getId("HOST");
580 #ifndef SMP
581     dsp1ProcId       = MultiProc_getId("DSP1");
582     sysm3ProcId     = MultiProc_getId("CORE0");
583     appm3ProcId     = MultiProc_getId("CORE1");
584 #endif
586 #ifdef DSP
587     intInfo.intVectorId = DSPEVENTID;
588 #else
589     /* Initilize the IpcPower module */
590     IpcPower_init();
591 #endif
593     InterruptProxy_intRegister(hostProcId, &intInfo, (Fxn)VirtQueue_isr, NULL);
596 /*!
597  * ======== VirtQueue_postCrashToMailbox ========
598  */
599 Void VirtQueue_postCrashToMailbox(Void)
601     InterruptProxy_intSend(0, NULL, (UInt)RP_MSG_MBOX_CRASH);
604 #define CACHE_WB_TICK_PERIOD    5
606 /*!
607  * ======== VirtQueue_cacheWb ========
608  *
609  * Used for flushing SysMin trace buffer.
610  */
611 Void VirtQueue_cacheWb()
613     static UInt32 oldticks = 0;
614     UInt32 newticks;
616     newticks = Clock_getTicks();
617     if (newticks - oldticks < (UInt32)CACHE_WB_TICK_PERIOD) {
618         /* Don't keep flushing cache */
619         return;
620     }
622     oldticks = newticks;
624     /* Flush the cache */
625     Cache_wbAll();