Merge remote-tracking branch 'vincent-ext/3.00.00.14_eng' into 14_eng
[ipc/ipcdev.git] / packages / ti / srvmgr / omaprpc / OmapRpc.h
1 /*
2  * Copyright (c) 2012-2013, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * *  Redistributions of source code must retain the above copyright
10  *    notice, this list of conditions and the following disclaimer.
11  *
12  * *  Redistributions in binary form must reproduce the above copyright
13  *    notice, this list of conditions and the following disclaimer in the
14  *    documentation and/or other materials provided with the distribution.
15  *
16  * *  Neither the name of Texas Instruments Incorporated nor the names of
17  *    its contributors may be used to endorse or promote products derived
18  *    from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
33 /*
34  *  ======== OmapRpc.h ========
35  *  OMAP Remote Procedure Call Driver.
36  *
37  */
39 #ifndef ti_srvmgr_OmapRpc__include
40 #define ti_srvmgr_OmapRpc__include
42 #include <ti/grcm/RcmServer.h>
43 #include <ti/ipc/mm/MmType.h>
46 #if defined (__cplusplus)
47 extern "C" {
48 #endif
51 /*!
52  *  @def    OmapRpc_S_SUCCESS
53  *  @brief  Operation is successful.
54  */
55 #define OmapRpc_S_SUCCESS              0
57 /*!
58  *  @def    OmapRpc_E_FAIL
59  *  @brief  Operation is not successful.
60  */
61 #define OmapRpc_E_FAIL                 -1
63 #define OmapRpc_NUM_PARAMETERS(size) \
64     (size/sizeof(struct OmapRpc_Parameter))
66 #define OmapRpc_PAYLOAD(ptr, type) \
67     ((struct type *)&(ptr)[sizeof(struct OmapRpc_MsgHeader)])
69 #define OmapRpc_PARAM(param, type) (param.size == sizeof(type) ? (type)param.data : 0)
71 #define OmapRpc_Stringerize(func)   #func
73 #define OmapRpc_dimof(x)    (sizeof(x)/sizeof(x[0]))
75 #define OmapRpc_DESC_EXEC_SYNC  (0x0100)
76 #define OmapRpc_DESC_EXEC_ASYNC (0x0200)
77 #define OmapRpc_DESC_SYM_ADD    (0x0300)
78 #define OmapRpc_DESC_SYM_IDX    (0x0400)
79 #define OmapRpc_DESC_CMD        (0x0500)
80 #define OmapRpc_DESC_TYPE_MASK  (0x0F00)
81 #define OmapRpc_JOBID_DISCRETE  (0)
82 #define OmapRpc_POOLID_DEFAULT  (0x8000)
84 #define OmapRpc_SET_FXN_IDX(idx)    (idx | 0x80000000)
85 #define OmapRpc_FXN_MASK(idx)       (idx & 0x7FFFFFFF)
87 #define OMAPRPC_MAX_CHANNEL_NAMELEN (64)
88 #define OMAPRPC_MAX_FUNC_NAMELEN    (64)
89 #define OMAPRPC_MAX_NUM_PARAMS      (10)
90 #define OMAPRPC_MAX_INST_NAMELEN    (48)
92 typedef enum OmapRpc_InfoType {
93     /** The function signature */
94     OmapRpc_InfoType_FUNC_SIGNATURE = 1,
95     /** The number of times a function has been called */
96     OmapRpc_InfoType_NUM_CALLS,
97     /** The performance information releated to the function */
98     OmapRpc_InfoType_FUNC_PERFORMANCE,
100     /** @hidden used to define the maximum info type */
101     OmapRpc_InfoType_MAX
102 } OmapRpc_InfoType;
104 /** The applicable types of messages that the HOST may send the SERVICE.
105  */
106 typedef enum OmapRpc_MsgType {
107     /** Ask Service for channel information, uses \ref OmapRpc_ChannelInfo */
108     OmapRpc_MsgType_QUERY_CHAN_INFO = 0,
109     /** The return message from OMAPRPC_MSG_QUERY_CHAN_INFO*/
110     OmapRpc_MsgType_CHAN_INFO = 1,
111     /** Ask the Service Instance to send information about the Service.
112      * Uses \ref OmapRpc_QueryFunction */
113     OmapRpc_MsgType_QUERY_FUNCTION = 2,
114     /** The return message from OMAPRPC_QUERY_INSTANCE,
115      * which contains the information about the instance.
116      * Uses \ref OmapRpc_Instance_Info */
117     OmapRpc_MsgType_FUNCTION_INFO = 3,
118     /** Ask the ServiceMgr to create a new instance of the service.
119      * No secondary data is needed. */
120     OmapRpc_MsgType_CREATE_INSTANCE = 6,
121     /** The return message from OMAPRPC_CREATE_INSTANCE,
122      * contains the new endpoint address in the OmapRpc_InstanceHandle */
123     OmapRpc_MsgType_INSTANCE_CREATED = 8,
124     /** Ask the Service Mgr to destroy an instance */
125     OmapRpc_MsgType_DESTROY_INSTANCE = 4,
126     /** The return message from OMAPRPC_DESTROY_INSTANCE.
127      * contains the old endpoint address in the OmapRpc_InstanceHandle */
128     OmapRpc_MsgType_INSTANCE_DESTROYED = 7,
129     /** Ask the Service Instance to call a particular function */
130     OmapRpc_MsgType_CALL_FUNCTION = 5,
131     /** The return values from a function call */
132     OmapRpc_MsgType_FUNCTION_RETURN = 9,
133     /** Returned from either the ServiceMgr or Service Instance
134      * when an error occurs */
135     OmapRpc_MsgType_ERROR = 10,
136     /** \hidden used to define the max msg enum, not an actual message */
137     OmapRpc_MsgType_MAX
138 } OmapRpc_MsgType;
140 typedef enum OmapRpc_ErrorType {
141     /**< No errors to report */
142     OmapRpc_ErrorType_NONE = 0,
143     /**< Not enough memory exist to process request */
144     OmapRpc_ErrorType_NOT_ENOUGH_MEMORY,
145     /**< The instance died */
146     OmapRpc_ErrorType_INSTANCE_DIED,
147     /**< Some resource was unavailable. */
148     OmapRpc_ErrorType_RESOURCE_UNAVAILABLE,
149     /**< A provided parameter was either out of range, incorrect or NULL */
150     OmapRpc_ErrorType_BAD_PARAMETER,
151     /**< The requested item is not supported */
152     OmapRpc_ErrorType_NOT_SUPPORTED,
154     /** @hidden used to define the max error value */
155     OmapRpc_ErrorType_MAX_VALUE
156 } OmapRpc_ErrorType;
158 typedef struct OmapRpc_CreateInstance {
159     Char name[OMAPRPC_MAX_INST_NAMELEN];
160 } OmapRpc_CreateInstance;
162 typedef struct OmapRpc_ChannelInfo {
163     UInt32 numFuncs;        /**< The number of functions supported on this endpoint */
164 } OmapRpc_ChannelInfo;
166 typedef struct OmapRpc_FuncPerf {
167     UInt32 clocksPerSec;
168     UInt32 clockCycles;
169 } OmapRpc_FuncPerf;
171 /** The parameter direction as relative to the function it describes */
172 typedef enum OmapRpc_Direction {
173     OmapRpc_Direction_In = 0,
174     OmapRpc_Direction_Out,
175     OmapRpc_Direction_Bi,
176     OmapRpc_Direction_MAX
177 } OmapRpc_Direction;
179 typedef enum OmapRpc_Param_Type {
180     OmapRpc_Param_VOID = 0,
181     OmapRpc_Param_S08,
182     OmapRpc_Param_U08,
183     OmapRpc_Param_S16,
184     OmapRpc_Param_U16,
185     OmapRpc_Param_S32,
186     OmapRpc_Param_U32,
187     OmapRpc_Param_S64,
188     OmapRpc_Param_U64,
190     OmapRpc_Param_PTR = 0x80,   /**< Logically OR'd with lower type to make a
191                                      pointer to the correct type */
192     OmapRpc_Param_MAX
193 } OmapRpc_Param_Type;
195 #define OmapRpc_PtrType(type)   (type | OmapRpc_Param_PTR)
197 typedef struct OmapRpc_ParamSignature {
198     UInt32 direction;   /**< @see OmapRpc_Direction */
199     UInt32 type;        /**< @see OmapRpc_Param_Type */
200     UInt32 count;       /**< Used to do some basic sanity checking on array bounds */
201 } OmapRpc_ParamSignature;
203 /**
204  * This is the data structure that represents the function signature.
205  * @note The first parameter (params[0]) is the return value.
206  */
207 typedef struct OmapRpc_FuncSignature {
208     Char name[OMAPRPC_MAX_FUNC_NAMELEN];
209     UInt32 numParam;
210     OmapRpc_ParamSignature params[OMAPRPC_MAX_NUM_PARAMS+1];
211 } OmapRpc_FuncSignature;
213 /**
214  * \brief Function Query Structure.
215  * \details This is used by the host first to ask the remote side for details
216  * about it's published functions
217  */
218 typedef struct OmapRpc_QueryFunction {
219     UInt32 infoType;        /**< @see OmapRpc_InfoType */
220     UInt32 funcIndex;       /**< The function index to query */
221     union info {
222         UInt32 numCalls;
223         OmapRpc_FuncPerf performance;
224         OmapRpc_FuncSignature signature;
225     } info;
226 } OmapRpc_QueryFunction;
228 /** @brief The generic OMAPRPC message header.
229  * (actually a copy of omx_msg_hdr which is a copy of an RCM header)
230  */
231 typedef struct OmapRpc_MsgHeader {
232     UInt32 msgType;    /**< @see OmapRpc_MsgType */
233     UInt32 msgLen;     /**< The length of the message data in bytes */
234 } OmapRpc_MsgHeader;
236 typedef struct OmapRpc_InstanceHandle {
237     UInt32 endpointAddress;
238     UInt32 status;
239 } OmapRpc_InstanceHandle;
241 typedef struct OmapRpc_Error {
242     UInt32 endpointAddress;
243     UInt32 status;
244 } OmapRpc_Error;
246 typedef struct OmapRpc_Parameter {
247     SizeT size;
248     SizeT data;
249 } OmapRpc_Parameter;
251 /** This is actually a frankensteined structure of RCM */
252 typedef struct OmapRpc_Packet{
253     UInt16  desc;       /**< @see RcmClient_Packet.desc */
254     UInt16  msgId;      /**< @see RcmClient_Packet.msgId */
255     UInt16  poolId;     /**< @see RcmClient_Message.poolId */
256     UInt16  jobId;      /**< @see RcmClient_Message.jobId */
257     UInt32  fxnIdx;     /**< @see RcmClient_Message.fxnIdx */
258     Int32   result;     /**< @see RcmClient_Message.result */
259     UInt32  dataSize;   /**< @see RcmClient_Message.data_size */
260 } OmapRpc_Packet;
262 /** An OmapRpc Function is really an RCM function */
263 typedef RcmServer_MsgFxn OmapRpc_Function;
265 /**
266  * \brief The Function Declaration Structure.
267  * \details This structure is used to declare the function signature and their
268  * associated functions
269  */
270 typedef struct OmapRpc_FuncDeclaration {
271     OmapRpc_Function      function;  /**< \brief The function pointer */
272     OmapRpc_FuncSignature signature; /**< \brief The signature of the function */
273 } OmapRpc_FuncDeclaration;
275 typedef struct OmapRpc_Object *OmapRpc_Handle;
276 typedef Void (*OmapRpc_SrvDelNotifyFxn)(Void);
278 #if 0
279 OmapRpc_Handle OmapRpc_createChannel(String channelName, UInt16 dstProc,
280         UInt32 port, UInt32 numFuncs, OmapRpc_FuncDeclaration* fxns,
281         OmapRpc_SrvDelNotifyFxn func);
282 #else
283 OmapRpc_Handle OmapRpc_createChannel(String channelName, UInt16 dstProc,
284         UInt32 port, RcmServer_Params *rcmParams, MmType_FxnSigTab *fxnSigTab,
285         OmapRpc_SrvDelNotifyFxn srvDelCBFunc);
286 #endif
288 Int OmapRpc_deleteChannel(OmapRpc_Handle handle);
291 #if defined (__cplusplus)
293 #endif /* defined (__cplusplus) */
295 /*@}*/
296 #endif /* ti_srvmgr_OmapRpc__include */