]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - ipc/ipcdev.git/blob - qnx/include/_MessageQ.h
acf006d735d3cc47e3e1d27e3fa885de65725302
[ipc/ipcdev.git] / qnx / include / _MessageQ.h
1 /*
2  *  Copyright (c) 2008-2013, Texas Instruments Incorporated
3  *  All rights reserved.
4  *
5  *  Redistribution and use in source and binary forms, with or without
6  *  modification, are permitted provided that the following conditions
7  *  are met:
8  *
9  *  *  Redistributions of source code must retain the above copyright
10  *     notice, this list of conditions and the following disclaimer.
11  *
12  *  *  Redistributions in binary form must reproduce the above copyright
13  *     notice, this list of conditions and the following disclaimer in the
14  *     documentation and/or other materials provided with the distribution.
15  *
16  *  *  Neither the name of Texas Instruments Incorporated nor the names of
17  *     its contributors may be used to endorse or promote products derived
18  *     from this software without specific prior written permission.
19  *
20  *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  *  AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  *  THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  *  PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  *  CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  *  EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  *  PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  *  OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  *  WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  *  OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  *  EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 /** ============================================================================
33  *  @file   _MessageQ.h
34  *
35  *  @brief  Defines MessageQ module.
36  *  ============================================================================
37  */
40 #ifndef MESSAGEQ_H_0xded2
41 #define MESSAGEQ_H_0xded2
43 /* Utilities headers */
44 #include <ti/ipc/NameServer.h>
47 #if defined (__cplusplus)
48 extern "C" {
49 #endif
52 /*!
53  *  @def    MessageQ_MODULEID
54  *  @brief  Unique module ID.
55  */
56 #define MessageQ_MODULEID               (0xded2)
58 /*!
59  *  @def    MessageQ_ALLOWGROWTH
60  *  @brief  Allow runtime growth
61  */
62 #define MessageQ_ALLOWGROWTH             NameServer_ALLOWGROWTH
64 /*! @brief Number of queues */
65 #define MessageQ_NUM_PRIORITY_QUEUES  2
67 /*
68  *  Used to denote a message that was initialized
69  *  with the #MessageQ_staticMsgInit function.
70  */
71 #define MessageQ_STATICMSG              0xFFFF
73 /*! Version setting */
74 #define MessageQ_HEADERVERSION   (UInt) 0x2000
76 /*! Mask to extract Trace setting */
77 #define MessageQ_TRACEMASK       (UInt) 0x1000
79 /*! Shift for Trace setting */
80 #define MessageQ_TRACESHIFT      (UInt) 12
83 /*!
84  *  @brief  Structure defining config parameters for the MessageQ Buf module.
85  */
86 typedef struct MessageQ_Config_tag {
87     Bool   traceFlag;
88     /*!< Trace flag
89      *  This flag allows the configuration of the default module trace
90      *  settings.
91      */
92     UInt maxRuntimeEntries;
93     /*!< Maximum number of MessageQs that can be dynamically created */
94     UInt maxNameLen;
95     /*!< Maximum length for Message queue names */
96 } MessageQ_Config;
98 /* =============================================================================
99  *  APIs
100  * =============================================================================
101  */
102 /*!
103  *  @brief      Function to get the default configuration for the MessageQ
104  *              module.
105  *
106  *              This function can be called by the application to get their
107  *              configuration parameter to MessageQ_setup filled in by the
108  *              MessageQ module with the default parameters. If the user does
109  *              not wish to make any change in the default parameters, this API
110  *              is not required to be called.
111  *
112  *  @param      cfg     Pointer to the MessageQ module configuration structure
113  *                      in which the default config is to be returned.
114  *
115  *  @sa         MessageQ_setup
116  */
117 Void MessageQ_getConfig (MessageQ_Config * cfg);
119 /*!
120  *  @brief      Function to setup the MessageQ module.
121  *
122  *              This function sets up the MessageQ module. This function must
123  *              be called before any other instance-level APIs can be invoked.
124  *              Module-level configuration needs to be provided to this
125  *              function. If the user wishes to change some specific config
126  *              parameters, then MessageQ_getConfig can be called to get the
127  *              configuration filled with the default values. After this, only
128  *              the required configuration values can be changed. If the user
129  *              does not wish to make any change in the default parameters, the
130  *              application can simply call MessageQ with NULL parameters.
131  *              The default parameters would get automatically used.
132  *
133  *  @param      cfg   Optional MessageQ module configuration. If provided as
134  *                    NULL, default configuration is used.
135  *
136  *  @sa         MessageQ_destroy
137  *              NameServer_create
138  *              GateSpinlock_create
139  *              Memory_alloc
140  */
141 Int MessageQ_setup (const MessageQ_Config * cfg);
143 /* Function to destroy the MessageQ module. */
144 Int MessageQ_destroy (void);
146 /* Returns the amount of shared memory used by one transport instance.
147  *
148  *  The MessageQ module itself does not use any shared memory but the
149  *  underlying transport may use some shared memory.
150  */
151 SizeT MessageQ_sharedMemReq (Ptr sharedAddr);
153 /* Calls the SetupProxy function to setup the MessageQ transports. */
154 Int MessageQ_attach (UInt16 remoteProcId, Ptr sharedAddr);
156 /* Calls the SetupProxy function to detach the MessageQ transports. */
157 Int MessageQ_detach (UInt16 remoteProcId);
159 NameServer_Handle MessageQ_getNameServerHandle(void);
161 Void MessageQ_setQueueOwner(MessageQ_Handle handle, Int pid);
163 Void MessageQ_cleanupOwner(Int pid);
165 Void MessageQ_msgInit(MessageQ_Msg msg);
167 #if defined (__cplusplus)
169 #endif /* defined (__cplusplus) */
172 #endif /* MESSAGEQ_H_0xded2 */