1 /*
2 * Copyright (c) 2012-2013, Texas Instruments Incorporated
3 * All rights reserved.
4 *
5 * Redistribution and use in source and binary forms, with or without
6 * modification, are permitted provided that the following conditions
7 * are met:
8 *
9 * * Redistributions of source code must retain the above copyright
10 * notice, this list of conditions and the following disclaimer.
11 *
12 * * Redistributions in binary form must reproduce the above copyright
13 * notice, this list of conditions and the following disclaimer in the
14 * documentation and/or other materials provided with the distribution.
15 *
16 * * Neither the name of Texas Instruments Incorporated nor the names of
17 * its contributors may be used to endorse or promote products derived
18 * from this software without specific prior written permission.
19 *
20 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31 */
32 /*============================================================================
33 * @file MessageQ.c
34 *
35 * @brief MessageQ module "client" implementation
36 *
37 * This implementation is geared for use in a "client/server" model, whereby
38 * system-wide data is maintained in a "server" component and process-
39 * specific data is handled here. At the moment, this implementation
40 * connects and communicates with LAD for the server connection.
41 *
42 * The MessageQ module supports the structured sending and receiving of
43 * variable length messages. This module can be used for homogeneous or
44 * heterogeneous multi-processor messaging.
45 *
46 * MessageQ provides more sophisticated messaging than other modules. It is
47 * typically used for complex situations such as multi-processor messaging.
48 *
49 * The following are key features of the MessageQ module:
50 * -Writers and readers can be relocated to another processor with no
51 * runtime code changes.
52 * -Timeouts are allowed when receiving messages.
53 * -Readers can determine the writer and reply back.
54 * -Receiving a message is deterministic when the timeout is zero.
55 * -Messages can reside on any message queue.
56 * -Supports zero-copy transfers.
57 * -Can send and receive from any type of thread.
58 * -Notification mechanism is specified by application.
59 * -Allows QoS (quality of service) on message buffer pools. For example,
60 * using specific buffer pools for specific message queues.
61 *
62 * Messages are sent and received via a message queue. A reader is a thread
63 * that gets (reads) messages from a message queue. A writer is a thread that
64 * puts (writes) a message to a message queue. Each message queue has one
65 * reader and can have many writers. A thread may read from or write to multiple
66 * message queues.
67 *
68 * Conceptually, the reader thread owns a message queue. The reader thread
69 * creates a message queue. Writer threads a created message queues to
70 * get access to them.
71 *
72 * Message queues are identified by a system-wide unique name. Internally,
73 * MessageQ uses the NameServermodule for managing
74 * these names. The names are used for opening a message queue. Using
75 * names is not required.
76 *
77 * Messages must be allocated from the MessageQ module. Once a message is
78 * allocated, it can be sent on any message queue. Once a message is sent, the
79 * writer loses ownership of the message and should not attempt to modify the
80 * message. Once the reader receives the message, it owns the message. It
81 * may either free the message or re-use the message.
82 *
83 * Messages in a message queue can be of variable length. The only
84 * requirement is that the first field in the definition of a message must be a
85 * MsgHeader structure. For example:
86 * typedef struct MyMsg {
87 * MessageQ_MsgHeader header;
88 * ...
89 * } MyMsg;
90 *
91 * The MessageQ API uses the MessageQ_MsgHeader internally. Your application
92 * should not modify or directly access the fields in the MessageQ_MsgHeader.
93 *
94 * All messages sent via the MessageQ module must be allocated from a
95 * Heap implementation. The heap can be used for
96 * other memory allocation not related to MessageQ.
97 *
98 * An application can use multiple heaps. The purpose of having multiple
99 * heaps is to allow an application to regulate its message usage. For
100 * example, an application can allocate critical messages from one heap of fast
101 * on-chip memory and non-critical messages from another heap of slower
102 * external memory
103 *
104 * MessageQ does support the usage of messages that allocated via the
105 * alloc function. Please refer to the staticMsgInit
106 * function description for more details.
107 *
108 * In a multiple processor system, MessageQ communications to other
109 * processors via MessageQTransport instances. There must be one and
110 * only one MessageQTransport instance for each processor where communication
111 * is desired.
112 * So on a four processor system, each processor must have three
113 * MessageQTransport instance.
114 *
115 * The user only needs to create the MessageQTransport instances. The instances
116 * are responsible for registering themselves with MessageQ.
117 * This is accomplished via the registerTransport function.
118 *
119 * ============================================================================
120 */
123 /* Standard headers */
124 #include <ti/ipc/Std.h>
126 /* Linux specific header files, replacing OSAL: */
127 #include <pthread.h>
129 /* Module level headers */
130 #include <ti/ipc/NameServer.h>
131 #include <ti/ipc/MultiProc.h>
132 #include <ti/syslink/inc/_MultiProc.h>
133 #include <ti/ipc/MessageQ.h>
134 #include <_MessageQ.h>
135 #include <_IpcLog.h>
136 #include <ti/syslink/inc/MessageQDrvDefs.h>
138 #include <sys/select.h>
139 #include <sys/time.h>
140 #include <sys/types.h>
141 #include <sys/param.h>
143 #include <errno.h>
144 #include <stdio.h>
145 #include <string.h>
146 #include <stdlib.h>
147 #include <unistd.h>
148 #include <assert.h>
149 #include <fcntl.h>
151 #include <ti/syslink/inc/usr/Qnx/MessageQDrv.h>
153 /* TI IPC utils: */
154 #include <TiIpcFxns.h>
156 #include <ti/syslink/inc/ti/ipc/ti_ipc.h>
158 /* =============================================================================
159 * Macros/Constants
160 * =============================================================================
161 */
163 /*!
164 * @brief Name of the reserved NameServer used for MessageQ.
165 */
166 #define MessageQ_NAMESERVER "MessageQ"
168 /* More magic rpmsg port numbers: */
169 #define MESSAGEQ_RPMSG_PORT 61
170 #define MESSAGEQ_RPMSG_MAXSIZE 512
171 #define RPMSG_RESERVED_ADDRESSES (1024)
173 /* Trace flag settings: */
174 #define TRACESHIFT 12
175 #define TRACEMASK 0x1000
177 /* =============================================================================
178 * Structures & Enums
179 * =============================================================================
180 */
182 /* structure for MessageQ module state */
183 typedef struct MessageQ_ModuleObject {
184 Int refCount;
185 /*!< Reference count */
186 NameServer_Handle nameServer;
187 /*!< Handle to the local NameServer used for storing GP objects */
188 pthread_mutex_t gate;
189 /*!< Handle of gate to be used for local thread safety */
190 MessageQ_Params defaultInstParams;
191 /*!< Default instance creation parameters */
192 int ipcFd[MultiProc_MAXPROCESSORS];
193 /*!< File Descriptors for sending to each remote processor */
194 int seqNum;
195 /*!< Process-specific sequence number */
196 } MessageQ_ModuleObject;
198 /*!
199 * @brief Structure for the Handle for the MessageQ.
200 */
201 typedef struct MessageQ_Object_tag {
202 MessageQ_Params params;
203 /*! Instance specific creation parameters */
204 MessageQ_QueueId queue;
205 /* Unique id */
206 int ipcFd;
207 /* File Descriptors to receive from a message queue. */
208 int unblockFdW;
209 /* Write this fd to unblock the select() call in MessageQ _get() */
210 int unblockFdR;
211 /* File Descriptor to block on to listen to unblockFdW. */
212 void *serverHandle;
213 } MessageQ_Object;
215 static Bool verbose = FALSE;
217 /* =============================================================================
218 * Globals
219 * =============================================================================
220 */
221 static MessageQ_ModuleObject MessageQ_state =
222 {
223 .refCount = 0,
224 .nameServer = NULL,
225 };
227 /*!
228 * @var MessageQ_module
229 *
230 * @brief Pointer to the MessageQ module state.
231 */
232 MessageQ_ModuleObject * MessageQ_module = &MessageQ_state;
235 /* =============================================================================
236 * Forward declarations of internal functions
237 * =============================================================================
238 */
240 /* This is a helper function to initialize a message. */
241 static Int transportCreateEndpoint(int * fd, UInt16 queueIndex);
242 static Int transportCloseEndpoint(int fd);
243 static Int transportGet(int fd, MessageQ_Msg * retMsg);
244 static Int transportPut(MessageQ_Msg msg, UInt16 dstId, UInt16 dstProcId);
246 /* =============================================================================
247 * APIS
248 * =============================================================================
249 */
250 /* Function to get default configuration for the MessageQ module.
251 *
252 */
253 Void MessageQ_getConfig (MessageQ_Config * cfg)
254 {
255 Int status;
256 MessageQDrv_CmdArgs cmdArgs;
258 assert (cfg != NULL);
260 cmdArgs.args.getConfig.config = cfg;
261 status = MessageQDrv_ioctl (CMD_MESSAGEQ_GETCONFIG, &cmdArgs);
263 if (status < 0) {
264 PRINTVERBOSE1("MessageQ_getConfig: API (through IOCTL) failed, \
265 status=%d\n", status)
266 }
268 return;
269 }
271 /* Function to setup the MessageQ module. */
272 Int MessageQ_setup (const MessageQ_Config * cfg)
273 {
274 Int status;
275 MessageQDrv_CmdArgs cmdArgs;
277 Int i;
279 cmdArgs.args.setup.config = (MessageQ_Config *) cfg;
280 status = MessageQDrv_ioctl(CMD_MESSAGEQ_SETUP, &cmdArgs);
281 if (status < 0) {
282 PRINTVERBOSE1("MessageQ_setup: API (through IOCTL) failed, \
283 status=%d\n", status)
284 return status;
285 }
287 MessageQ_module->nameServer = cmdArgs.args.setup.nameServerHandle;
288 MessageQ_module->seqNum = 0;
290 /* Create a default local gate. */
291 pthread_mutex_init (&(MessageQ_module->gate), NULL);
293 /* Clear ipcFd array. */
294 for (i = 0; i < MultiProc_MAXPROCESSORS; i++) {
295 MessageQ_module->ipcFd[i] = -1;
296 }
298 return status;
299 }
301 /*
302 * Function to destroy the MessageQ module.
303 */
304 Int MessageQ_destroy (void)
305 {
306 Int status;
307 MessageQDrv_CmdArgs cmdArgs;
309 status = MessageQDrv_ioctl (CMD_MESSAGEQ_DESTROY, &cmdArgs);
310 if (status < 0) {
311 PRINTVERBOSE1("MessageQ_destroy: API (through IOCTL) failed, \
312 status=%d\n", status)
313 }
315 return status;
316 }
318 /* Function to initialize the parameters for the MessageQ instance. */
319 Void MessageQ_Params_init (MessageQ_Params * params)
320 {
321 memcpy (params, &(MessageQ_module->defaultInstParams),
322 sizeof (MessageQ_Params));
324 return;
325 }
327 /*
328 * Function to create a MessageQ object for receiving.
329 *
330 * Create a file descriptor and bind the source address
331 * (local ProcId/MessageQ ID) in
332 * order to get messages dispatched to this messageQ.
333 */
334 MessageQ_Handle MessageQ_create (String name, const MessageQ_Params * params)
335 {
336 Int status = MessageQ_S_SUCCESS;
337 MessageQ_Object * obj = NULL;
338 UInt16 queueIndex = 0u;
339 UInt16 procId;
340 MessageQDrv_CmdArgs cmdArgs;
341 int fildes[2];
343 cmdArgs.args.create.params = (MessageQ_Params *) params;
344 cmdArgs.args.create.name = name;
345 if (name != NULL) {
346 cmdArgs.args.create.nameLen = (strlen (name) + 1);
347 }
348 else {
349 cmdArgs.args.create.nameLen = 0;
350 }
352 status = MessageQDrv_ioctl (CMD_MESSAGEQ_CREATE, &cmdArgs);
353 if (status < 0) {
354 PRINTVERBOSE1("MessageQ_create: API (through IOCTL) failed, \
355 status=%d\n", status)
356 return NULL;
357 }
359 /* Create the generic obj */
360 obj = (MessageQ_Object *)calloc(1, sizeof (MessageQ_Object));
362 if (params != NULL) {
363 /* Populate the params member */
364 memcpy((Ptr) &obj->params, (Ptr)params, sizeof (MessageQ_Params));
365 }
367 procId = MultiProc_self();
368 queueIndex = (MessageQ_QueueIndex)cmdArgs.args.create.queueId;
369 obj->queue = cmdArgs.args.create.queueId;
370 obj->serverHandle = cmdArgs.args.create.handle;
372 PRINTVERBOSE2("MessageQ_create: creating endpoint for: %s, \
373 queueIndex: %d\n", name, queueIndex)
374 status = transportCreateEndpoint(&obj->ipcFd, queueIndex);
375 if (status < 0) {
376 goto cleanup;
377 }
379 /*
380 * Now, to support MessageQ_unblock() functionality, create an event object.
381 * Writing to this event will unblock the select() call in MessageQ_get().
382 */
383 if (pipe(fildes) == -1) {
384 printf ("MessageQ_create: pipe creation failed: %d, %s\n",
385 errno, strerror(errno));
386 status = MessageQ_E_FAIL;
387 }
388 obj->unblockFdW = fildes[1];
389 obj->unblockFdR = fildes[0];
391 cleanup:
392 /* Cleanup if fail: */
393 if (status < 0) {
394 MessageQ_delete((MessageQ_Handle *)&obj);
395 }
397 return ((MessageQ_Handle) obj);
398 }
400 /*
401 * Function to delete a MessageQ object for a specific slave processor.
402 *
403 * Deletes the file descriptors associated with this MessageQ object.
404 */
405 Int MessageQ_delete (MessageQ_Handle * handlePtr)
406 {
407 Int status = MessageQ_S_SUCCESS;
408 MessageQ_Object * obj = NULL;
409 MessageQDrv_CmdArgs cmdArgs;
411 obj = (MessageQ_Object *) (*handlePtr);
413 cmdArgs.args.deleteMessageQ.handle = obj->serverHandle;
414 status = MessageQDrv_ioctl (CMD_MESSAGEQ_DELETE, &cmdArgs);
415 if (status < 0) {
416 PRINTVERBOSE1("MessageQ_delete: API (through IOCTL) failed, \
417 status=%d\n", status)
418 }
420 /* Close the fds used for MessageQ_unblock(): */
421 close(obj->unblockFdW);
422 close(obj->unblockFdR);
424 /* Close the communication endpoint: */
425 status = transportCloseEndpoint(obj->ipcFd);
427 /* Now free the obj */
428 free (obj);
429 *handlePtr = NULL;
431 return (status);
432 }
434 /*
435 * Opens an instance of MessageQ for sending.
436 *
437 * We need not create a tiipc file descriptor here; the file descriptors for
438 * all remote processors were created during MessageQ_attach(), and will be
439 * retrieved during MessageQ_put().
440 */
441 Int MessageQ_open (String name, MessageQ_QueueId * queueId)
442 {
443 Int status = MessageQ_S_SUCCESS;
445 status = NameServer_getUInt32 (MessageQ_module->nameServer,
446 name, queueId, NULL);
448 if (status == NameServer_E_NOTFOUND) {
449 /* Set return queue ID to invalid. */
450 *queueId = MessageQ_INVALIDMESSAGEQ;
451 status = MessageQ_E_NOTFOUND;
452 }
453 else if (status >= 0) {
454 /* Override with a MessageQ status code. */
455 status = MessageQ_S_SUCCESS;
456 }
457 else {
458 /* Set return queue ID to invalid. */
459 *queueId = MessageQ_INVALIDMESSAGEQ;
460 /* Override with a MessageQ status code. */
461 if (status == NameServer_E_TIMEOUT) {
462 status = MessageQ_E_TIMEOUT;
463 }
464 else {
465 status = MessageQ_E_FAIL;
466 }
467 }
469 return (status);
470 }
472 /* Closes previously opened instance of MessageQ module. */
473 Int MessageQ_close (MessageQ_QueueId * queueId)
474 {
475 Int32 status = MessageQ_S_SUCCESS;
477 /* Nothing more to be done for closing the MessageQ. */
478 *queueId = MessageQ_INVALIDMESSAGEQ;
480 return (status);
481 }
483 /*
484 * Place a message onto a message queue.
485 *
486 * Calls TransportShm_put(), which handles the sending of the message using the
487 * appropriate kernel interface (socket, device ioctl) call for the remote
488 * procId encoded in the queueId argument.
489 *
490 */
491 Int MessageQ_put (MessageQ_QueueId queueId, MessageQ_Msg msg)
492 {
493 Int status;
494 UInt16 dstProcId = (UInt16)(queueId >> 16);
495 UInt16 queueIndex = (MessageQ_QueueIndex)(queueId & 0x0000ffff);
497 msg->dstId = queueIndex;
498 msg->dstProc = dstProcId;
500 status = transportPut(msg, queueIndex, dstProcId);
502 return (status);
503 }
505 /*
506 * Gets a message for a message queue and blocks if the queue is empty.
507 * If a message is present, it returns it. Otherwise it blocks
508 * waiting for a message to arrive.
509 * When a message is returned, it is owned by the caller.
510 *
511 * We block using select() on the receiving tiipc file descriptor, then
512 * get the waiting message via a read.
513 * We use the file descriptors stored in the messageQ object via a previous
514 * call to MessageQ_create().
515 *
516 * Note: We currently do not support messages to be sent between threads on the
517 * lcoal processor.
518 *
519 */
520 Int MessageQ_get (MessageQ_Handle handle, MessageQ_Msg * msg ,UInt timeout)
521 {
522 Int status = MessageQ_S_SUCCESS;
523 Int tmpStatus;
524 MessageQ_Object * obj = (MessageQ_Object *) handle;
525 int retval;
526 int nfds;
527 fd_set rfds;
528 struct timeval tv;
529 void *timevalPtr;
530 int maxfd = 0;
532 /* Wait (with timeout) and retreive message */
533 FD_ZERO(&rfds);
534 FD_SET(obj->ipcFd, &rfds);
535 maxfd = obj->ipcFd;
537 /* Wait also on the event fd, which may be written by MessageQ_unblock(): */
538 FD_SET(obj->unblockFdR, &rfds);
540 if (timeout == MessageQ_FOREVER) {
541 timevalPtr = NULL;
542 }
543 else {
544 /* Timeout given in msec: convert: */
545 tv.tv_sec = timeout / 1000;
546 tv.tv_usec = (timeout % 1000) * 1000;
547 timevalPtr = &tv;
548 }
549 /* Add one to last fd created: */
550 nfds = ((maxfd > obj->unblockFdR) ? maxfd : obj->unblockFdR) + 1;
552 retval = select(nfds, &rfds, NULL, NULL, timevalPtr);
553 if (retval) {
554 if (FD_ISSET(obj->unblockFdR, &rfds)) {
555 /*
556 * Our event was signalled by MessageQ_unblock().
557 *
558 * This is typically done during a shutdown sequence, where
559 * the intention of the client would be to ignore (i.e. not fetch)
560 * any pending messages in the transport's queue.
561 * Thus, we shall not check for nor return any messages.
562 */
563 *msg = NULL;
564 status = MessageQ_E_UNBLOCKED;
565 }
566 else {
567 if (FD_ISSET(obj->ipcFd, &rfds)) {
568 /* Our transport's fd was signalled: Get the message: */
569 tmpStatus = transportGet(obj->ipcFd, msg);
570 if (tmpStatus < 0) {
571 printf ("MessageQ_get: tranposrtshm_get failed.");
572 status = MessageQ_E_FAIL;
573 }
574 }
575 }
576 }
577 else if (retval == 0) {
578 *msg = NULL;
579 status = MessageQ_E_TIMEOUT;
580 }
582 return (status);
583 }
585 /*
586 * Return a count of the number of messages in the queue
587 *
588 * TBD: To be implemented. Return -1 for now.
589 */
590 Int MessageQ_count (MessageQ_Handle handle)
591 {
592 Int count = -1;
593 return (count);
594 }
596 /* Initializes a message not obtained from MessageQ_alloc. */
597 Void MessageQ_staticMsgInit (MessageQ_Msg msg, UInt32 size)
598 {
599 /* Fill in the fields of the message */
600 MessageQ_msgInit (msg);
601 msg->heapId = MessageQ_STATICMSG;
602 msg->msgSize = size;
603 }
605 /*
606 * Allocate a message and initialize the needed fields (note some
607 * of the fields in the header are set via other APIs or in the
608 * MessageQ_put function,
609 */
610 MessageQ_Msg MessageQ_alloc (UInt16 heapId, UInt32 size)
611 {
612 MessageQ_Msg msg = NULL;
614 /*
615 * heapId not used for local alloc (as this is over a copy transport), but
616 * we need to send to other side as heapId is used in BIOS transport:
617 */
618 msg = (MessageQ_Msg)calloc (1, size);
619 MessageQ_msgInit (msg);
620 msg->msgSize = size;
621 msg->heapId = heapId;
623 return msg;
624 }
626 /* Frees the message back to the heap that was used to allocate it. */
627 Int MessageQ_free (MessageQ_Msg msg)
628 {
629 UInt32 status = MessageQ_S_SUCCESS;
631 /* Check to ensure this was not allocated by user: */
632 if (msg->heapId == MessageQ_STATICMSG) {
633 status = MessageQ_E_CANNOTFREESTATICMSG;
634 }
635 else {
636 free (msg);
637 }
639 return status;
640 }
642 /* Register a heap with MessageQ. */
643 Int MessageQ_registerHeap (Ptr heap, UInt16 heapId)
644 {
645 Int status = MessageQ_S_SUCCESS;
647 /* Do nothing, as this uses a copy transport: */
649 return status;
650 }
652 /* Unregister a heap with MessageQ. */
653 Int MessageQ_unregisterHeap (UInt16 heapId)
654 {
655 Int status = MessageQ_S_SUCCESS;
657 /* Do nothing, as this uses a copy transport: */
659 return status;
660 }
662 /* Unblocks a MessageQ */
663 Void MessageQ_unblock (MessageQ_Handle handle)
664 {
665 MessageQ_Object * obj = (MessageQ_Object *) handle;
666 char buf = 'n';
667 int numBytes;
669 /* Write to pipe to awaken any threads blocked on this messageQ: */
670 numBytes = write(obj->unblockFdW, &buf, 1);
671 }
673 /* Embeds a source message queue into a message. */
674 Void MessageQ_setReplyQueue (MessageQ_Handle handle, MessageQ_Msg msg)
675 {
676 MessageQ_Object * obj = (MessageQ_Object *) handle;
678 msg->replyId = (UInt16)(obj->queue);
679 msg->replyProc = (UInt16)(obj->queue >> 16);
680 }
682 /* Returns the QueueId associated with the handle. */
683 MessageQ_QueueId MessageQ_getQueueId (MessageQ_Handle handle)
684 {
685 MessageQ_Object * obj = (MessageQ_Object *) handle;
686 UInt32 queueId;
688 queueId = (obj->queue);
690 return queueId;
691 }
693 /* Sets the tracing of a message */
694 Void MessageQ_setMsgTrace (MessageQ_Msg msg, Bool traceFlag)
695 {
696 msg->flags = (msg->flags & ~TRACEMASK) | (traceFlag << TRACESHIFT);
697 }
699 /*
700 * Returns the amount of shared memory used by one transport instance.
701 *
702 * The MessageQ module itself does not use any shared memory but the
703 * underlying transport may use some shared memory.
704 */
705 SizeT MessageQ_sharedMemReq (Ptr sharedAddr)
706 {
707 SizeT memReq = 0u;
709 /* Do nothing, as this is a copy transport. */
711 return (memReq);
712 }
714 /*
715 * Opens a file descriptor for this remote proc.
716 *
717 * Only opens it if one does not already exist for this procId.
718 *
719 * Note: remoteProcId may be MultiProc_Self() for loopback case.
720 */
721 Int MessageQ_attach (UInt16 remoteProcId, Ptr sharedAddr)
722 {
723 Int status = MessageQ_S_SUCCESS;
724 int ipcFd;
725 int err;
727 PRINTVERBOSE1("MessageQ_attach: remoteProcId: %d\n", remoteProcId)
729 if (remoteProcId >= MultiProc_MAXPROCESSORS) {
730 status = MessageQ_E_INVALIDPROCID;
731 goto exit;
732 }
734 pthread_mutex_lock (&(MessageQ_module->gate));
736 /* Only open a fd if one doesn't exist: */
737 if (MessageQ_module->ipcFd[remoteProcId] == -1) {
738 /* Create a fd for sending messages to the remote proc: */
739 ipcFd = open("/dev/tiipc", O_RDWR);
740 if (ipcFd < 0) {
741 status = MessageQ_E_FAIL;
742 printf ("MessageQ_attach: open of tiipc device failed: %d, %s\n",
743 errno, strerror(errno));
744 }
745 else {
746 PRINTVERBOSE1("MessageQ_attach: opened tiipc fd for sending: %d\n",
747 ipcFd)
748 MessageQ_module->ipcFd[remoteProcId] = ipcFd;
749 /*
750 * Connect to the remote endpoint and bind any reserved address as
751 * local endpoint
752 */
753 Connect(ipcFd, remoteProcId, MESSAGEQ_RPMSG_PORT);
754 err = BindAddr(ipcFd, TIIPC_ADDRANY);
755 if (err < 0) {
756 status = MessageQ_E_FAIL;
757 printf ("MessageQ_attach: bind failed: %d, %s\n",
758 errno, strerror(errno));
759 }
760 }
761 }
762 else {
763 status = MessageQ_E_ALREADYEXISTS;
764 }
766 pthread_mutex_unlock (&(MessageQ_module->gate));
768 exit:
769 return (status);
770 }
772 /*
773 * Close the fd for this remote proc.
774 *
775 */
776 Int MessageQ_detach (UInt16 remoteProcId)
777 {
778 Int status = MessageQ_S_SUCCESS;
779 int ipcFd;
781 if (remoteProcId >= MultiProc_MAXPROCESSORS) {
782 status = MessageQ_E_INVALIDPROCID;
783 goto exit;
784 }
786 pthread_mutex_lock (&(MessageQ_module->gate));
788 ipcFd = MessageQ_module->ipcFd[remoteProcId];
789 if (close (ipcFd)) {
790 status = MessageQ_E_OSFAILURE;
791 printf("MessageQ_detach: close failed: %d, %s\n",
792 errno, strerror(errno));
793 }
794 else {
795 PRINTVERBOSE1("MessageQ_detach: closed fd: %d\n", ipcFd)
796 MessageQ_module->ipcFd[remoteProcId] = -1;
797 }
799 pthread_mutex_unlock (&(MessageQ_module->gate));
801 exit:
802 return (status);
803 }
805 /*
806 * This is a helper function to initialize a message.
807 */
808 Void MessageQ_msgInit (MessageQ_Msg msg)
809 {
810 msg->reserved0 = 0; /* We set this to distinguish from NameServerMsg */
811 msg->replyId = (UInt16)MessageQ_INVALIDMESSAGEQ;
812 msg->msgId = MessageQ_INVALIDMSGID;
813 msg->dstId = (UInt16)MessageQ_INVALIDMESSAGEQ;
814 msg->flags = MessageQ_HEADERVERSION | MessageQ_NORMALPRI;
815 msg->srcProc = MultiProc_self();
817 pthread_mutex_lock(&(MessageQ_module->gate));
818 msg->seqNum = MessageQ_module->seqNum++;
819 pthread_mutex_unlock(&(MessageQ_module->gate));
820 }
822 /*
823 * =============================================================================
824 * Transport: Fxns kept here until need for a transport layer is realized.
825 * =============================================================================
826 */
827 /*
828 * ======== transportCreateEndpoint ========
829 *
830 * Create a communication endpoint to receive messages.
831 */
832 static Int transportCreateEndpoint(int * fd, UInt16 queueIndex)
833 {
834 Int status = MessageQ_S_SUCCESS;
835 int err;
837 /* Create a fd to the ti-ipc to receive messages for this messageQ */
838 *fd= open("/dev/tiipc", O_RDWR);
839 if (*fd < 0) {
840 status = MessageQ_E_FAIL;
841 printf ("transportCreateEndpoint: Couldn't open tiipc device: %d, %s\n",
842 errno, strerror(errno));
844 goto exit;
845 }
847 PRINTVERBOSE1("transportCreateEndpoint: opened fd: %d\n", *fd)
849 err = BindAddr(*fd, (UInt32)queueIndex);
850 if (err < 0) {
851 status = MessageQ_E_FAIL;
852 printf ("transportCreateEndpoint: bind failed: %d, %s\n",
853 errno, strerror(errno));
854 }
856 exit:
857 return (status);
858 }
860 /*
861 * ======== transportCloseEndpoint ========
862 *
863 * Close the communication endpoint.
864 */
865 static Int transportCloseEndpoint(int fd)
866 {
867 Int status = MessageQ_S_SUCCESS;
869 PRINTVERBOSE1("transportCloseEndpoint: closing fd: %d\n", fd)
871 /* Stop communication to this endpoint */
872 close(fd);
874 return (status);
875 }
877 /*
878 * ======== transportGet ========
879 * Retrieve a message waiting in the queue.
880 */
881 static Int transportGet(int fd, MessageQ_Msg * retMsg)
882 {
883 Int status = MessageQ_S_SUCCESS;
884 MessageQ_Msg msg;
885 int ret;
886 int byteCount;
887 tiipc_remote_params remote;
889 /*
890 * We have no way of peeking to see what message size we'll get, so we
891 * allocate a message of max size to receive contents from tiipc
892 * (currently, a copy transport)
893 */
894 msg = MessageQ_alloc (0, MESSAGEQ_RPMSG_MAXSIZE);
895 if (!msg) {
896 status = MessageQ_E_MEMORY;
897 goto exit;
898 }
900 /* Get message */
901 byteCount = read(fd, msg, MESSAGEQ_RPMSG_MAXSIZE);
902 if (byteCount < 0) {
903 printf("read failed: %s (%d)\n", strerror(errno), errno);
904 status = MessageQ_E_FAIL;
905 goto exit;
906 }
907 else {
908 /* Update the allocated message size (even though this may waste space
909 * when the actual message is smaller than the maximum rpmsg size,
910 * the message will be freed soon anyway, and it avoids an extra copy).
911 */
912 msg->msgSize = byteCount;
914 /*
915 * If the message received was statically allocated, reset the
916 * heapId, so the app can free it.
917 */
918 if (msg->heapId == MessageQ_STATICMSG) {
919 msg->heapId = 0; /* for a copy transport, heap id is 0. */
920 }
921 }
923 PRINTVERBOSE1("transportGet: read from fd: %d\n", fd)
924 ret = ioctl(fd, TIIPC_IOCGETREMOTE, &remote);
925 PRINTVERBOSE3("\tReceived a msg: byteCount: %d, rpmsg addr: %d, rpmsg \
926 proc: %d\n", byteCount, remote.remote_addr, remote.remote_proc)
927 PRINTVERBOSE2("\tMessage Id: %d, Message size: %d\n", msg->msgId, msg->msgSize)
929 *retMsg = msg;
931 exit:
932 return (status);
933 }
935 /*
936 * ======== transportPut ========
937 *
938 * Write to tiipc file descriptor associated with
939 * with this destination procID.
940 */
941 static Int transportPut(MessageQ_Msg msg, UInt16 dstId, UInt16 dstProcId)
942 {
943 Int status = MessageQ_S_SUCCESS;
944 int ipcFd;
945 int err;
947 /*
948 * Retrieve the tiipc file descriptor associated with this
949 * transport for the destination processor.
950 */
951 ipcFd = MessageQ_module->ipcFd[dstProcId];
953 PRINTVERBOSE2("Sending msgId: %d via fd: %d\n", msg->msgId, ipcFd)
955 /* send response message to remote processor */
956 err = write(ipcFd, msg, msg->msgSize);
957 if (err < 0) {
958 printf ("transportPut: write failed: %d, %s\n",
959 errno, strerror(errno));
960 status = MessageQ_E_FAIL;
961 }
963 /*
964 * Free the message, as this is a copy transport, we maintain MessageQ
965 * semantics.
966 */
967 MessageQ_free (msg);
969 return (status);
970 }