Re-work MessageQ_put to eliminate transport recursion
[ipc/ipcdev.git] / qnx / src / api / MessageQ.c
1 /*
2  * Copyright (c) 2012-2015, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * *  Redistributions of source code must retain the above copyright
10  *    notice, this list of conditions and the following disclaimer.
11  *
12  * *  Redistributions in binary form must reproduce the above copyright
13  *    notice, this list of conditions and the following disclaimer in the
14  *    documentation and/or other materials provided with the distribution.
15  *
16  * *  Neither the name of Texas Instruments Incorporated nor the names of
17  *    its contributors may be used to endorse or promote products derived
18  *    from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 /*============================================================================
33  *  @file   MessageQ.c
34  *
35  *  @brief  MessageQ module "client" implementation
36  *
37  *  This implementation is geared for use in a "client/server" model, whereby
38  *  system-wide data is maintained in a "server" component and process-
39  *  specific data is handled here.  At the moment, this implementation
40  *  connects and communicates with LAD for the server connection.
41  *
42  *  The MessageQ module supports the structured sending and receiving of
43  *  variable length messages. This module can be used for homogeneous or
44  *  heterogeneous multi-processor messaging.
45  *
46  *  MessageQ provides more sophisticated messaging than other modules. It is
47  *  typically used for complex situations such as multi-processor messaging.
48  *
49  *  The following are key features of the MessageQ module:
50  *  -Writers and readers can be relocated to another processor with no
51  *   runtime code changes.
52  *  -Timeouts are allowed when receiving messages.
53  *  -Readers can determine the writer and reply back.
54  *  -Receiving a message is deterministic when the timeout is zero.
55  *  -Messages can reside on any message queue.
56  *  -Supports zero-copy transfers.
57  *  -Can send and receive from any type of thread.
58  *  -Notification mechanism is specified by application.
59  *  -Allows QoS (quality of service) on message buffer pools. For example,
60  *   using specific buffer pools for specific message queues.
61  *
62  *  Messages are sent and received via a message queue. A reader is a thread
63  *  that gets (reads) messages from a message queue. A writer is a thread that
64  *  puts (writes) a message to a message queue. Each message queue has one
65  *  reader and can have many writers. A thread may read from or write to multiple
66  *  message queues.
67  *
68  *  Conceptually, the reader thread owns a message queue. The reader thread
69  *  creates a message queue. Writer threads  a created message queues to
70  *  get access to them.
71  *
72  *  Message queues are identified by a system-wide unique name. Internally,
73  *  MessageQ uses the NameServermodule for managing
74  *  these names. The names are used for opening a message queue. Using
75  *  names is not required.
76  *
77  *  Messages must be allocated from the MessageQ module. Once a message is
78  *  allocated, it can be sent on any message queue. Once a message is sent, the
79  *  writer loses ownership of the message and should not attempt to modify the
80  *  message. Once the reader receives the message, it owns the message. It
81  *  may either free the message or re-use the message.
82  *
83  *  Messages in a message queue can be of variable length. The only
84  *  requirement is that the first field in the definition of a message must be a
85  *  MsgHeader structure. For example:
86  *  typedef struct MyMsg {
87  *      MessageQ_MsgHeader header;
88  *      ...
89  *  } MyMsg;
90  *
91  *  The MessageQ API uses the MessageQ_MsgHeader internally. Your application
92  *  should not modify or directly access the fields in the MessageQ_MsgHeader.
93  *
94  *  All messages sent via the MessageQ module must be allocated from a
95  *  Heap implementation. The heap can be used for
96  *  other memory allocation not related to MessageQ.
97  *
98  *  An application can use multiple heaps. The purpose of having multiple
99  *  heaps is to allow an application to regulate its message usage. For
100  *  example, an application can allocate critical messages from one heap of fast
101  *  on-chip memory and non-critical messages from another heap of slower
102  *  external memory
103  *
104  *  MessageQ does support the usage of messages that allocated via the
105  *  alloc function. Please refer to the staticMsgInit
106  *  function description for more details.
107  *
108  *  In a multiple processor system, MessageQ communications to other
109  *  processors via MessageQTransport instances. There must be one and
110  *  only one MessageQTransport instance for each processor where communication
111  *  is desired.
112  *  So on a four processor system, each processor must have three
113  *  MessageQTransport instance.
114  *
115  *  The user only needs to create the MessageQTransport instances. The instances
116  *  are responsible for registering themselves with MessageQ.
117  *  This is accomplished via the registerTransport function.
118  *
119  *  ============================================================================
120  */
123 /* Standard headers */
124 #include <ti/ipc/Std.h>
126 /* Linux specific header files, replacing OSAL: */
127 #include <pthread.h>
129 /* Module level headers */
130 #include <ti/ipc/NameServer.h>
131 #include <ti/ipc/MultiProc.h>
132 #include <ti/syslink/inc/_MultiProc.h>
133 #define MessageQ_internal 1     /* must be defined before include file */
134 #include <ti/ipc/MessageQ.h>
135 #include <_MessageQ.h>
136 #include <_IpcLog.h>
137 #include <ti/syslink/inc/MessageQDrvDefs.h>
139 #include <sys/select.h>
140 #include <sys/time.h>
141 #include <sys/types.h>
142 #include <sys/param.h>
144 #include <errno.h>
145 #include <stdio.h>
146 #include <string.h>
147 #include <stdlib.h>
148 #include <unistd.h>
149 #include <assert.h>
150 #include <fcntl.h>
152 #include <ti/syslink/inc/usr/Qnx/MessageQDrv.h>
154 /* TI IPC utils: */
155 #include <TiIpcFxns.h>
157 #include <ti/syslink/inc/ti/ipc/ti_ipc.h>
159 /* =============================================================================
160  * Macros/Constants
161  * =============================================================================
162  */
164 /*!
165  *  @brief  Name of the reserved NameServer used for MessageQ.
166  */
167 #define MessageQ_NAMESERVER  "MessageQ"
169 /* More magic rpmsg port numbers: */
170 #define MESSAGEQ_RPMSG_PORT       61
171 #define MESSAGEQ_RPMSG_MAXSIZE    512
172 #define RPMSG_RESERVED_ADDRESSES  (1024)
174 /* MessageQ needs local address bound to be a 16-bit value */
175 #define MAX_LOCAL_ADDR            0x10000
177 /* Trace flag settings: */
178 #define TRACESHIFT    12
179 #define TRACEMASK     0x1000
181 /* =============================================================================
182  * Structures & Enums
183  * =============================================================================
184  */
186 /* params structure evolution */
187 typedef struct {
188     Void *synchronizer;
189 } MessageQ_Params_Legacy;
191 typedef struct {
192     Int __version;
193     Void *synchronizer;
194     MessageQ_QueueIndex queueIndex;
195 } MessageQ_Params_Version2;
197 /* structure for MessageQ module state */
198 typedef struct MessageQ_ModuleObject {
199     Int                 refCount;
200     /*!< Reference count */
201     NameServer_Handle   nameServer;
202     /*!< Handle to the local NameServer used for storing GP objects */
203     pthread_mutex_t     gate;
204     /*!< Handle of gate to be used for local thread safety */
205     int                 ipcFd[MultiProc_MAXPROCESSORS];
206     /*!< File Descriptors for sending to each remote processor */
207     int                 seqNum;
208     /*!< Process-specific sequence number */
209     MessageQ_PutHookFxn putHookFxn;
210     /*!< hook function for MessageQ_put method */
211 } MessageQ_ModuleObject;
213 /*!
214  *  @brief  Structure for the Handle for the MessageQ.
215  */
216 typedef struct MessageQ_Object_tag {
217     MessageQ_Params         params;
218     /*! Instance specific creation parameters */
219     MessageQ_QueueId        queue;
220     /* Unique id */
221     int                     ipcFd;
222     /* File Descriptors to receive from a message queue. */
223     int                     unblockFdW;
224     /* Write this fd to unblock the select() call in MessageQ _get() */
225     int                     unblockFdR;
226      /* File Descriptor to block on to listen to unblockFdW. */
227     void                    *serverHandle;
228 } MessageQ_Object;
230 static Bool verbose = FALSE;
232 /* =============================================================================
233  *  Globals
234  * =============================================================================
235  */
236 static MessageQ_ModuleObject MessageQ_state =
238     .refCount   = 0,
239     .nameServer = NULL,
240     .putHookFxn = NULL
241 };
243 /*!
244  *  @var    MessageQ_module
245  *
246  *  @brief  Pointer to the MessageQ module state.
247  */
248 MessageQ_ModuleObject * MessageQ_module = &MessageQ_state;
251 /* =============================================================================
252  * Forward declarations of internal functions
253  * =============================================================================
254  */
256 /* This is a helper function to initialize a message. */
257 static Int transportCreateEndpoint(int * fd, UInt16 * queueIndex);
258 static Int transportCloseEndpoint(int fd);
259 static Int transportGet(int fd, MessageQ_Msg * retMsg);
260 static Int transportPut(MessageQ_Msg msg, UInt16 dstId, UInt16 dstProcId);
262 /* =============================================================================
263  * APIS
264  * =============================================================================
265  */
266 /* Function to get default configuration for the MessageQ module.
267  *
268  */
269 Void MessageQ_getConfig (MessageQ_Config * cfg)
271     Int status;
272     MessageQDrv_CmdArgs cmdArgs;
274     assert (cfg != NULL);
276     cmdArgs.args.getConfig.config = cfg;
277     status = MessageQDrv_ioctl (CMD_MESSAGEQ_GETCONFIG, &cmdArgs);
279     if (status < 0) {
280         PRINTVERBOSE1("MessageQ_getConfig: API (through IOCTL) failed, \
281             status=%d\n", status)
282     }
284     return;
287 /* Function to setup the MessageQ module. */
288 Int MessageQ_setup (const MessageQ_Config * cfg)
290     Int status;
291     MessageQDrv_CmdArgs cmdArgs;
293     Int i;
295     cmdArgs.args.setup.config = (MessageQ_Config *) cfg;
296     status = MessageQDrv_ioctl(CMD_MESSAGEQ_SETUP, &cmdArgs);
297     if (status < 0) {
298         PRINTVERBOSE1("MessageQ_setup: API (through IOCTL) failed, \
299             status=%d\n", status)
300         return status;
301     }
303     MessageQ_module->nameServer = cmdArgs.args.setup.nameServerHandle;
304     MessageQ_module->seqNum = 0;
306     /* Create a default local gate. */
307     pthread_mutex_init (&(MessageQ_module->gate), NULL);
309     /* Clear ipcFd array. */
310     for (i = 0; i < MultiProc_MAXPROCESSORS; i++) {
311        MessageQ_module->ipcFd[i]      = -1;
312     }
314     return status;
317 /*
318  * Function to destroy the MessageQ module.
319  */
320 Int MessageQ_destroy (void)
322     Int status;
323     MessageQDrv_CmdArgs    cmdArgs;
325     status = MessageQDrv_ioctl (CMD_MESSAGEQ_DESTROY, &cmdArgs);
326     if (status < 0) {
327         PRINTVERBOSE1("MessageQ_destroy: API (through IOCTL) failed, \
328             status=%d\n", status)
329     }
331     return status;
334 /*
335  *  ======== MessageQ_Params_init ========
336  *  Legacy implementation.
337  */
338 Void MessageQ_Params_init(MessageQ_Params *params)
340     ((MessageQ_Params_Legacy *)params)->synchronizer = NULL;
343 /*
344  *  ======== MessageQ_Params_init__S ========
345  *  New implementation which is version aware.
346  */
347 Void MessageQ_Params_init__S(MessageQ_Params *params, Int version)
349     MessageQ_Params_Version2 *params2;
351     switch (version) {
353         case MessageQ_Params_VERSION_2:
354             params2 = (MessageQ_Params_Version2 *)params;
355             params2->__version = MessageQ_Params_VERSION_2;
356             params2->synchronizer = NULL;
357             params2->queueIndex = MessageQ_ANY;
358             break;
360         default:
361             assert(FALSE);
362             break;
363     }
366 /*
367  *   Function to create a MessageQ object for receiving.
368  *
369  *   Create a file descriptor and bind the source address
370  *   (local ProcId/MessageQ ID) in
371  *   order to get messages dispatched to this messageQ.
372  */
373 MessageQ_Handle MessageQ_create (String name, const MessageQ_Params * pp)
375     Int                   status    = MessageQ_S_SUCCESS;
376     MessageQ_Object *     obj    = NULL;
377     UInt16                queueIndex = 0u;
378     MessageQDrv_CmdArgs   cmdArgs;
379     int                   fildes[2];
380     MessageQ_Params       ps;
382     MessageQ_Params_init__S(&ps, MessageQ_Params_VERSION);
384     /* copy the given params into the current params structure */
385     if (pp != NULL) {
387         /* snoop the params pointer to see if it's a legacy structure */
388         if ((pp->__version == 0) || (pp->__version > 100)) {
389             ps.synchronizer = ((MessageQ_Params_Legacy *)pp)->synchronizer;
390         }
392         /* not legacy structure, use params version field */
393         else if (pp->__version == MessageQ_Params_VERSION_2) {
394             ps.__version = ((MessageQ_Params_Version2 *)pp)->__version;
395             ps.synchronizer = ((MessageQ_Params_Version2 *)pp)->synchronizer;
396             ps.queueIndex = ((MessageQ_Params_Version2 *)pp)->queueIndex;
397         }
398         else {
399             assert(FALSE);
400         }
401     }
403     cmdArgs.args.create.params = &ps;
404     cmdArgs.args.create.name = name;
406     if (name != NULL) {
407         cmdArgs.args.create.nameLen = (strlen (name) + 1);
408     }
409     else {
410         cmdArgs.args.create.nameLen = 0;
411     }
413     /* Create the generic obj */
414     obj = (MessageQ_Object *)calloc(1, sizeof (MessageQ_Object));
415     if (obj == NULL) {
416         PRINTVERBOSE0("MessageQ_create: memory allocation failed\n")
417         return NULL;
418     }
420     PRINTVERBOSE2("MessageQ_create: creating endpoint for: %s, \
421        queueIndex: %d\n", name, queueIndex)
422     status = transportCreateEndpoint(&obj->ipcFd, &queueIndex);
423     if (status < 0) {
424         goto cleanup;
425     }
427     /*
428      * We expect the endpoint creation to return a port number from
429      * the MessageQCopy layer. This port number will be greater than
430      * 1024 and less than 0x10000. Use this number as the queueIndex.
431      */
432     cmdArgs.args.create.queueId = queueIndex;
434     status = MessageQDrv_ioctl (CMD_MESSAGEQ_CREATE, &cmdArgs);
435     if (status < 0) {
436         PRINTVERBOSE1("MessageQ_create: API (through IOCTL) failed, \
437             status=%d\n", status)
438         goto cleanup;
439     }
441    /* Populate the params member */
442     memcpy(&obj->params, &ps, sizeof(ps));
444     obj->queue = cmdArgs.args.create.queueId;
445     obj->serverHandle = cmdArgs.args.create.handle;
447     /*
448      * Now, to support MessageQ_unblock() functionality, create an event object.
449      * Writing to this event will unblock the select() call in MessageQ_get().
450      */
451     if (pipe(fildes) == -1) {
452         printf ("MessageQ_create: pipe creation failed: %d, %s\n",
453                    errno, strerror(errno));
454         status = MessageQ_E_FAIL;
455         obj->unblockFdW = obj->unblockFdR = -1;
456     }
457     else {
458         obj->unblockFdW = fildes[1];
459         obj->unblockFdR = fildes[0];
460     }
462 cleanup:
463     /* Cleanup if fail: */
464     if (status < 0) {
465         MessageQ_delete((MessageQ_Handle *)&obj);
466     }
468     return ((MessageQ_Handle) obj);
471 /*
472  * Function to delete a MessageQ object for a specific slave processor.
473  *
474  * Deletes the file descriptors associated with this MessageQ object.
475  */
476 Int MessageQ_delete (MessageQ_Handle * handlePtr)
478     Int               status    = MessageQ_S_SUCCESS;
479     MessageQ_Object * obj       = NULL;
480     MessageQDrv_CmdArgs cmdArgs;
482     assert(handlePtr != NULL);
483     obj = (MessageQ_Object *) (*handlePtr);
484     assert(obj != NULL);
486     if (obj->serverHandle != NULL) {
487         cmdArgs.args.deleteMessageQ.handle = obj->serverHandle;
488         status = MessageQDrv_ioctl (CMD_MESSAGEQ_DELETE, &cmdArgs);
489         if (status < 0) {
490             PRINTVERBOSE1("MessageQ_delete: API (through IOCTL) failed, \
491                 status=%d\n", status)
492         }
493     }
495     /* Close the fds used for MessageQ_unblock(): */
496     if (obj->unblockFdW >= 0) {
497         close(obj->unblockFdW);
498     }
499     if (obj->unblockFdR >= 0) {
500         close(obj->unblockFdR);
501     }
503     /* Close the communication endpoint: */
504     if (obj->ipcFd >= 0) {
505         transportCloseEndpoint(obj->ipcFd);
506     }
508     /* Now free the obj */
509     free (obj);
510     *handlePtr = NULL;
512     return (status);
515 /*
516  *  Opens an instance of MessageQ for sending.
517  *
518  *  We need not create a tiipc file descriptor here; the file descriptors for
519  *  all remote processors were created during MessageQ_attach(), and will be
520  *  retrieved during MessageQ_put().
521  */
522 Int MessageQ_open (String name, MessageQ_QueueId * queueId)
524     Int status = MessageQ_S_SUCCESS;
526     status = NameServer_getUInt32 (MessageQ_module->nameServer,
527                                      name, queueId, NULL);
529     if (status == NameServer_E_NOTFOUND) {
530         /* Set return queue ID to invalid. */
531         *queueId = MessageQ_INVALIDMESSAGEQ;
532         status = MessageQ_E_NOTFOUND;
533     }
534     else if (status >= 0) {
535         /* Override with a MessageQ status code. */
536         status = MessageQ_S_SUCCESS;
537     }
538     else {
539         /* Set return queue ID to invalid. */
540         *queueId = MessageQ_INVALIDMESSAGEQ;
541         /* Override with a MessageQ status code. */
542         if (status == NameServer_E_TIMEOUT) {
543             status = MessageQ_E_TIMEOUT;
544         }
545         else {
546             status = MessageQ_E_FAIL;
547         }
548     }
550     return (status);
553 /* Closes previously opened instance of MessageQ module. */
554 Int MessageQ_close (MessageQ_QueueId * queueId)
556     Int32 status = MessageQ_S_SUCCESS;
558     /* Nothing more to be done for closing the MessageQ. */
559     *queueId = MessageQ_INVALIDMESSAGEQ;
561     return (status);
564 /*
565  * Place a message onto a message queue.
566  *
567  * Calls TransportShm_put(), which handles the sending of the message using the
568  * appropriate kernel interface (socket, device ioctl) call for the remote
569  * procId encoded in the queueId argument.
570  *
571  */
572 Int MessageQ_put (MessageQ_QueueId queueId, MessageQ_Msg msg)
574     Int      status;
575     UInt16   dstProcId  = (UInt16)(queueId >> 16);
576     UInt16   queueIndex = (MessageQ_QueueIndex)(queueId & 0x0000ffff);
578     msg->dstId     = queueIndex;
579     msg->dstProc   = dstProcId;
581     /* invoke put hook function after addressing the message */
582     if (MessageQ_module->putHookFxn != NULL) {
583         MessageQ_module->putHookFxn(queueId, msg);
584     }
586     status = transportPut(msg, queueIndex, dstProcId);
588     return (status);
591 /*
592  * Gets a message for a message queue and blocks if the queue is empty.
593  * If a message is present, it returns it.  Otherwise it blocks
594  * waiting for a message to arrive.
595  * When a message is returned, it is owned by the caller.
596  *
597  * We block using select() on the receiving tiipc file descriptor, then
598  * get the waiting message via a read.
599  * We use the file descriptors stored in the messageQ object via a previous
600  * call to MessageQ_create().
601  *
602  * Note: We currently do not support messages to be sent between threads on the
603  * lcoal processor.
604  *
605  */
606 Int MessageQ_get (MessageQ_Handle handle, MessageQ_Msg * msg ,UInt timeout)
608     Int     status = MessageQ_S_SUCCESS;
609     Int     tmpStatus;
610     MessageQ_Object * obj = (MessageQ_Object *) handle;
611     int     retval;
612     int     nfds;
613     fd_set  rfds;
614     struct  timeval tv;
615     void    *timevalPtr;
616     int     maxfd = 0;
618     /* Wait (with timeout) and retreive message */
619     FD_ZERO(&rfds);
620     FD_SET(obj->ipcFd, &rfds);
621     maxfd = obj->ipcFd;
623     /* Wait also on the event fd, which may be written by MessageQ_unblock(): */
624     FD_SET(obj->unblockFdR, &rfds);
626     if (timeout == MessageQ_FOREVER) {
627         timevalPtr = NULL;
628     }
629     else {
630         /* Timeout given in msec: convert:  */
631         tv.tv_sec = timeout / 1000;
632         tv.tv_usec = (timeout % 1000) * 1000;
633         timevalPtr = &tv;
634     }
635     /* Add one to last fd created: */
636     nfds = ((maxfd > obj->unblockFdR) ? maxfd : obj->unblockFdR) + 1;
638     retval = select(nfds, &rfds, NULL, NULL, timevalPtr);
639     if (retval)  {
640         if (FD_ISSET(obj->unblockFdR, &rfds))  {
641             /*
642              * Our event was signalled by MessageQ_unblock().
643              *
644              * This is typically done during a shutdown sequence, where
645              * the intention of the client would be to ignore (i.e. not fetch)
646              * any pending messages in the transport's queue.
647              * Thus, we shall not check for nor return any messages.
648              */
649             *msg = NULL;
650             status = MessageQ_E_UNBLOCKED;
651         }
652         else {
653             if (FD_ISSET(obj->ipcFd, &rfds)) {
654                 /* Our transport's fd was signalled: Get the message: */
655                 tmpStatus = transportGet(obj->ipcFd, msg);
656                 if (tmpStatus < 0) {
657                     printf ("MessageQ_get: tranposrtshm_get failed.");
658                     status = MessageQ_E_FAIL;
659                 }
660             }
661         }
662     }
663     else if (retval == 0) {
664         *msg = NULL;
665         status = MessageQ_E_TIMEOUT;
666     }
668     return (status);
671 /*
672  * Return a count of the number of messages in the queue
673  *
674  * TBD: To be implemented. Return -1 for now.
675  */
676 Int MessageQ_count (MessageQ_Handle handle)
678     Int               count = -1;
679     return (count);
682 /* Initializes a message not obtained from MessageQ_alloc. */
683 Void MessageQ_staticMsgInit (MessageQ_Msg msg, UInt32 size)
685     /* Fill in the fields of the message */
686     MessageQ_msgInit (msg);
687     msg->heapId  = MessageQ_STATICMSG;
688     msg->msgSize = size;
691 /*
692  * Allocate a message and initialize the needed fields (note some
693  * of the fields in the header are set via other APIs or in the
694  * MessageQ_put function,
695  */
696 MessageQ_Msg MessageQ_alloc (UInt16 heapId, UInt32 size)
698     MessageQ_Msg msg       = NULL;
700     /*
701      * heapId not used for local alloc (as this is over a copy transport), but
702      * we need to send to other side as heapId is used in BIOS transport:
703      */
704     msg = (MessageQ_Msg)calloc (1, size);
705     MessageQ_msgInit (msg);
706     msg->msgSize = size;
707     msg->heapId  = heapId;
709     return msg;
712 /* Frees the message back to the heap that was used to allocate it. */
713 Int MessageQ_free (MessageQ_Msg msg)
715     UInt32         status = MessageQ_S_SUCCESS;
717     /* Check to ensure this was not allocated by user: */
718     if (msg->heapId == MessageQ_STATICMSG)  {
719         status =  MessageQ_E_CANNOTFREESTATICMSG;
720     }
721     else {
722         free (msg);
723     }
725     return status;
728 /* Register a heap with MessageQ. */
729 Int MessageQ_registerHeap (Ptr heap, UInt16 heapId)
731     Int  status = MessageQ_S_SUCCESS;
733     /* Do nothing, as this uses a copy transport: */
735     return status;
738 /* Unregister a heap with MessageQ. */
739 Int MessageQ_unregisterHeap (UInt16 heapId)
741     Int  status = MessageQ_S_SUCCESS;
743     /* Do nothing, as this uses a copy transport: */
745     return status;
748 /* Unblocks a MessageQ */
749 Void MessageQ_unblock (MessageQ_Handle handle)
751     MessageQ_Object * obj   = (MessageQ_Object *) handle;
752     char         buf = 'n';
754     /* Write to pipe to awaken any threads blocked on this messageQ: */
755     write(obj->unblockFdW, &buf, 1);
758 /* Embeds a source message queue into a message. */
759 Void MessageQ_setReplyQueue (MessageQ_Handle handle, MessageQ_Msg msg)
761     MessageQ_Object * obj   = (MessageQ_Object *) handle;
763     msg->replyId   = (UInt16)(obj->queue);
764     msg->replyProc = (UInt16)(obj->queue >> 16);
767 /* Returns the QueueId associated with the handle. */
768 MessageQ_QueueId MessageQ_getQueueId (MessageQ_Handle handle)
770     MessageQ_Object * obj = (MessageQ_Object *) handle;
771     UInt32            queueId;
773     queueId = (obj->queue);
775     return queueId;
778 /* Sets the tracing of a message */
779 Void MessageQ_setMsgTrace (MessageQ_Msg msg, Bool traceFlag)
781     msg->flags = (msg->flags & ~TRACEMASK) |   (traceFlag << TRACESHIFT);
784 /*
785  *  Returns the amount of shared memory used by one transport instance.
786  *
787  *  The MessageQ module itself does not use any shared memory but the
788  *  underlying transport may use some shared memory.
789  */
790 SizeT MessageQ_sharedMemReq (Ptr sharedAddr)
792     SizeT memReq = 0u;
794     /* Do nothing, as this is a copy transport. */
796     return (memReq);
799 /*
800  *  Opens a file descriptor for this remote proc.
801  *
802  *  Only opens it if one does not already exist for this procId.
803  *
804  *  Note: remoteProcId may be MultiProc_Self() for loopback case.
805  */
806 Int MessageQ_attach (UInt16 remoteProcId, Ptr sharedAddr)
808     Int     status = MessageQ_S_SUCCESS;
809     UInt32  localAddr;
810     int     ipcFd;
811     int     err;
813     PRINTVERBOSE1("MessageQ_attach: remoteProcId: %d\n", remoteProcId)
815     if (remoteProcId >= MultiProc_MAXPROCESSORS) {
816         status = MessageQ_E_INVALIDPROCID;
817         goto exit;
818     }
820     pthread_mutex_lock (&(MessageQ_module->gate));
822     /* Only open a fd if one doesn't exist: */
823     if (MessageQ_module->ipcFd[remoteProcId] == -1)  {
824         /* Create a fd for sending messages to the remote proc: */
825         ipcFd = open("/dev/tiipc", O_RDWR);
826         if (ipcFd < 0) {
827             status = MessageQ_E_FAIL;
828             printf ("MessageQ_attach: open of tiipc device failed: %d, %s\n",
829                        errno, strerror(errno));
830         }
831         else  {
832             PRINTVERBOSE1("MessageQ_attach: opened tiipc fd for sending: %d\n",
833                 ipcFd)
834             MessageQ_module->ipcFd[remoteProcId] = ipcFd;
835             /*
836              * Connect to the remote endpoint and bind any reserved address as
837              * local endpoint
838              */
839             Connect(ipcFd, remoteProcId, MESSAGEQ_RPMSG_PORT);
840             err = BindAddr(ipcFd, &localAddr);
841             if (err < 0) {
842                 status = MessageQ_E_FAIL;
843                 printf ("MessageQ_attach: bind failed: %d, %s\n",
844                     errno, strerror(errno));
845             }
846         }
847     }
848     else {
849         status = MessageQ_E_ALREADYEXISTS;
850     }
852     pthread_mutex_unlock (&(MessageQ_module->gate));
854 exit:
855     return (status);
858 /*
859  *  Close the fd for this remote proc.
860  *
861  */
862 Int MessageQ_detach (UInt16 remoteProcId)
864     Int status = MessageQ_S_SUCCESS;
865     int ipcFd;
867     if (remoteProcId >= MultiProc_MAXPROCESSORS) {
868         status = MessageQ_E_INVALIDPROCID;
869         goto exit;
870     }
872     pthread_mutex_lock (&(MessageQ_module->gate));
874     ipcFd = MessageQ_module->ipcFd[remoteProcId];
875     if (close (ipcFd)) {
876         status = MessageQ_E_OSFAILURE;
877         printf("MessageQ_detach: close failed: %d, %s\n",
878                        errno, strerror(errno));
879     }
880     else {
881         PRINTVERBOSE1("MessageQ_detach: closed fd: %d\n", ipcFd)
882         MessageQ_module->ipcFd[remoteProcId] = -1;
883     }
885     pthread_mutex_unlock (&(MessageQ_module->gate));
887 exit:
888     return (status);
891 /*
892  * This is a helper function to initialize a message.
893  */
894 Void MessageQ_msgInit (MessageQ_Msg msg)
896     msg->reserved0 = 0;  /* We set this to distinguish from NameServerMsg */
897     msg->replyId   = (UInt16)MessageQ_INVALIDMESSAGEQ;
898     msg->msgId     = MessageQ_INVALIDMSGID;
899     msg->dstId     = (UInt16)MessageQ_INVALIDMESSAGEQ;
900     msg->flags     = MessageQ_HEADERVERSION | MessageQ_NORMALPRI;
901     msg->srcProc   = MultiProc_self();
903     pthread_mutex_lock(&(MessageQ_module->gate));
904     msg->seqNum  = MessageQ_module->seqNum++;
905     pthread_mutex_unlock(&(MessageQ_module->gate));
908 /*
909  * =============================================================================
910  * Transport: Fxns kept here until need for a transport layer is realized.
911  * =============================================================================
912  */
913 /*
914  * ======== transportCreateEndpoint ========
915  *
916  * Create a communication endpoint to receive messages.
917  */
918 static Int transportCreateEndpoint(int * fd, UInt16 * queueIndex)
920     Int          status    = MessageQ_S_SUCCESS;
921     int          err;
922     UInt32       localAddr;
924     /* Create a fd to the ti-ipc to receive messages for this messageQ */
925     *fd= open("/dev/tiipc", O_RDWR);
926     if (*fd < 0) {
927         status = MessageQ_E_FAIL;
928         printf ("transportCreateEndpoint: Couldn't open tiipc device: %d, %s\n",
929                   errno, strerror(errno));
931         goto exit;
932     }
934     PRINTVERBOSE1("transportCreateEndpoint: opened fd: %d\n", *fd)
936     err = BindAddr(*fd, &localAddr);
937     if (err < 0) {
938         status = MessageQ_E_FAIL;
939         printf("transportCreateEndpoint: bind failed: %d, %s\n",
940                   errno, strerror(errno));
942         close(*fd);
943         goto exit;
944     }
946     if (localAddr >= MAX_LOCAL_ADDR) {
947         status = MessageQ_E_FAIL;
948         printf("transportCreateEndpoint: local address returned is"
949             "by BindAddr is greater than max supported\n");
951         close(*fd);
952         goto exit;
953     }
955     *queueIndex = localAddr;
957 exit:
958     return (status);
961 /*
962  * ======== transportCloseEndpoint ========
963  *
964  *  Close the communication endpoint.
965  */
966 static Int transportCloseEndpoint(int fd)
968     Int status = MessageQ_S_SUCCESS;
970     PRINTVERBOSE1("transportCloseEndpoint: closing fd: %d\n", fd)
972     /* Stop communication to this endpoint */
973     close(fd);
975     return (status);
978 /*
979  * ======== transportGet ========
980  *  Retrieve a message waiting in the queue.
981 */
982 static Int transportGet(int fd, MessageQ_Msg * retMsg)
984     Int           status    = MessageQ_S_SUCCESS;
985     MessageQ_Msg  msg;
986     int           ret;
987     int           byteCount;
988     tiipc_remote_params remote;
990     /*
991      * We have no way of peeking to see what message size we'll get, so we
992      * allocate a message of max size to receive contents from tiipc
993      * (currently, a copy transport)
994      */
995     msg = MessageQ_alloc (0, MESSAGEQ_RPMSG_MAXSIZE);
996     if (!msg)  {
997         status = MessageQ_E_MEMORY;
998         goto exit;
999     }
1001     /* Get message */
1002     byteCount = read(fd, msg, MESSAGEQ_RPMSG_MAXSIZE);
1003     if (byteCount < 0) {
1004         printf("read failed: %s (%d)\n", strerror(errno), errno);
1005         status = MessageQ_E_FAIL;
1006         goto exit;
1007     }
1008     else {
1009          /* Update the allocated message size (even though this may waste space
1010           * when the actual message is smaller than the maximum rpmsg size,
1011           * the message will be freed soon anyway, and it avoids an extra copy).
1012           */
1013          msg->msgSize = byteCount;
1015          /*
1016           * If the message received was statically allocated, reset the
1017           * heapId, so the app can free it.
1018           */
1019          if (msg->heapId == MessageQ_STATICMSG)  {
1020              msg->heapId = 0;  /* for a copy transport, heap id is 0. */
1021          }
1022     }
1024     PRINTVERBOSE1("transportGet: read from fd: %d\n", fd)
1025     ret = ioctl(fd, TIIPC_IOCGETREMOTE, &remote);
1026     if (ret == -1) {
1027         printf("ioctl failed: %s (%d)\n", strerror(errno), errno);
1028         status = MessageQ_E_FAIL;
1029         goto exit;
1030     }
1031     PRINTVERBOSE3("\tReceived a msg: byteCount: %d, rpmsg addr: %d, rpmsg \
1032         proc: %d\n", byteCount, remote.remote_addr, remote.remote_proc)
1033     PRINTVERBOSE2("\tMessage Id: %d, Message size: %d\n", msg->msgId,
1034         msg->msgSize)
1036     *retMsg = msg;
1038 exit:
1039     return (status);
1042 /*
1043  * ======== transportPut ========
1044  *
1045  * Write to tiipc file descriptor associated with
1046  * with this destination procID.
1047  */
1048 static Int transportPut(MessageQ_Msg msg, UInt16 dstId, UInt16 dstProcId)
1050     Int     status    = MessageQ_S_SUCCESS;
1051     int     ipcFd;
1052     int     err;
1054     /*
1055      * Retrieve the tiipc file descriptor associated with this
1056      * transport for the destination processor.
1057      */
1058     ipcFd = MessageQ_module->ipcFd[dstProcId];
1060     PRINTVERBOSE2("Sending msgId: %d via fd: %d\n", msg->msgId, ipcFd)
1062     /* send response message to remote processor */
1063     err = write(ipcFd, msg, msg->msgSize);
1064     if (err < 0) {
1065         printf ("transportPut: write failed: %d, %s\n",
1066                   errno, strerror(errno));
1067         status = MessageQ_E_FAIL;
1068         goto exit;
1069     }
1071     /*
1072      * Free the message, as this is a copy transport, we maintain MessageQ
1073      * semantics.
1074      */
1075     MessageQ_free (msg);
1077 exit:
1078     return (status);