76f1263cd207c2990c3f56b3333901f0f10b44ba
[ipc/ipcdev.git] / qnx / src / ipc3x_dev / ti / syslink / build / Qnx / resmgr / ipc.use
1 ipc - IPC Resource Manager
3 ipc: [-HTgdca] <core_id1> <executable1> [<core_id2> <executable2> ...]
5   <core_id#> should be set to a core name
6       followed by the path to the executable to load on that core.
7       Supported core ids are
8           OMAP54xx: IPU, DSP
9           DRA7xx: IPU2, DSP1, IPU1
11 Options:
12  -H <option>    Enable/Disable Ducati hibernation.  Default: 1
13                 where <option> is:
14                     0: OFF
15                     1: ON
16                 Supported on: OMAP54xx
17  -T <timeout>   Set the timeout value of the Ducati hibernation in ms.
18                 Default: 5000 ms
19                 Supported on: OMAP54xx
20  -g             Enable GateMP support on host
21                 Supported on: DRA7xx
22  -d             Disable automatic crash recovery
23  -c <dump_file> Generate dump of slave trace during crashes. Use
24                 absolute path for filename.
25  -a<n>          Specify that the first 'n' cores have been pre-loaded and
26                 started. Perform late-attach to these cores.