/* * Copyright (c) 2008-2013, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /** ============================================================================ * @file _MessageQ.h * * @brief Defines MessageQ module. * ============================================================================ */ #ifndef MESSAGEQ_H_0xded2 #define MESSAGEQ_H_0xded2 /* Utilities headers */ #include #if defined (__cplusplus) extern "C" { #endif /*! * @def MessageQ_MODULEID * @brief Unique module ID. */ #define MessageQ_MODULEID (0xded2) /*! * @def MessageQ_ALLOWGROWTH * @brief Allow runtime growth */ #define MessageQ_ALLOWGROWTH NameServer_ALLOWGROWTH /*! @brief Number of queues */ #define MessageQ_NUM_PRIORITY_QUEUES 2 /* * Used to denote a message that was initialized * with the #MessageQ_staticMsgInit function. */ #define MessageQ_STATICMSG 0xFFFF /*! Version setting */ #define MessageQ_HEADERVERSION (UInt) 0x2000 /*! Mask to extract Trace setting */ #define MessageQ_TRACEMASK (UInt) 0x1000 /*! Shift for Trace setting */ #define MessageQ_TRACESHIFT (UInt) 12 /*! * @brief Structure defining config parameters for the MessageQ Buf module. */ typedef struct MessageQ_Config_tag { Bool traceFlag; /*!< Trace flag * This flag allows the configuration of the default module trace * settings. */ UInt maxRuntimeEntries; /*!< Maximum number of MessageQs that can be dynamically created */ UInt maxNameLen; /*!< Maximum length for Message queue names */ } MessageQ_Config; /* ============================================================================= * APIs * ============================================================================= */ /*! * @brief Function to get the default configuration for the MessageQ * module. * * This function can be called by the application to get their * configuration parameter to MessageQ_setup filled in by the * MessageQ module with the default parameters. If the user does * not wish to make any change in the default parameters, this API * is not required to be called. * * @param cfg Pointer to the MessageQ module configuration structure * in which the default config is to be returned. * * @sa MessageQ_setup */ Void MessageQ_getConfig (MessageQ_Config * cfg); /*! * @brief Function to setup the MessageQ module. * * This function sets up the MessageQ module. This function must * be called before any other instance-level APIs can be invoked. * Module-level configuration needs to be provided to this * function. If the user wishes to change some specific config * parameters, then MessageQ_getConfig can be called to get the * configuration filled with the default values. After this, only * the required configuration values can be changed. If the user * does not wish to make any change in the default parameters, the * application can simply call MessageQ with NULL parameters. * The default parameters would get automatically used. * * @param cfg Optional MessageQ module configuration. If provided as * NULL, default configuration is used. * * @sa MessageQ_destroy * NameServer_create * GateSpinlock_create * Memory_alloc */ Int MessageQ_setup (const MessageQ_Config * cfg); /* Function to destroy the MessageQ module. */ Int MessageQ_destroy (void); /* Returns the amount of shared memory used by one transport instance. * * The MessageQ module itself does not use any shared memory but the * underlying transport may use some shared memory. */ SizeT MessageQ_sharedMemReq (Ptr sharedAddr); /* Calls the SetupProxy function to setup the MessageQ transports. */ Int MessageQ_attach (UInt16 remoteProcId, Ptr sharedAddr); /* Calls the SetupProxy function to detach the MessageQ transports. */ Int MessageQ_detach (UInt16 remoteProcId); NameServer_Handle MessageQ_getNameServerHandle(void); Void MessageQ_setQueueOwner(MessageQ_Handle handle, Int pid); Void MessageQ_cleanupOwner(Int pid); Void MessageQ_msgInit(MessageQ_Msg msg); #if defined (__cplusplus) } #endif /* defined (__cplusplus) */ #endif /* MESSAGEQ_H_0xded2 */