/* * Copyright (c) 2008-2014, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /* * ======== GateHWSpinlock.h ======== */ #ifndef GATEHWSPINLOCK_H_0xF416 #define GATEHWSPINLOCK_H_0xF416 /* Utilities & Osal headers */ #include #include #if defined (__cplusplus) extern "C" { #endif /*! * @def GateHWSpinlock_MODULEID * @brief Unique module ID. */ #define GateHWSpinlock_MODULEID (0xc43d) /* ============================================================================= * Module Success and Failure codes * ============================================================================= */ /*! * @def GateHWSpinlock_E_INVALIDARG * @brief Argument passed to a function is invalid. */ #define GateHWSpinlock_E_INVALIDARG -1 /*! * @def GateHWSpinlock_E_MEMORY * @brief Memory allocation failed. */ #define GateHWSpinlock_E_MEMORY -2 /*! * @def GateHWSpinlock_E_BUSY * @brief the name is already registered or not. */ #define GateHWSpinlock_E_BUSY -3 /*! * @def GateHWSpinlock_E_FAIL * @brief Generic failure. */ #define GateHWSpinlock_E_FAIL -4 /*! * @def GateHWSpinlock_E_NOTFOUND * @brief name not found in the nameserver. */ #define GateHWSpinlock_E_NOTFOUND -5 /*! * @def GateHWSpinlock_E_INVALIDSTATE * @brief Module is not initialized. */ #define GateHWSpinlock_E_INVALIDSTATE -6 /*! * @def GateHWSpinlock_E_NOTONWER * @brief Instance is not created on this processor. */ #define GateHWSpinlock_E_NOTONWER -7 /*! * @def GateHWSpinlock_E_REMOTEACTIVE * @brief Remote opener of the instance has not closed the instance. */ #define GateHWSpinlock_E_REMOTEACTIVE -8 /*! * @def GateHWSpinlock_E_INUSE * @brief Indicates that the instance is in use.. */ #define GateHWSpinlock_E_INUSE -9 /*! * @def GateHWSpinlock_E_OSFAILURE * @brief Failure in OS call. */ #define GateHWSpinlock_E_OSFAILURE -10 /*! * @def GateHWSpinlock_E_VERSION * @brief Version mismatch error. */ #define GateHWSpinlock_E_VERSION -11 /*! * @def GateHWSpinlock_S_SUCCESS * @brief Operation successful. */ #define GateHWSpinlock_S_SUCCESS 0 /*! * @def GateHWSpinlock_S_ALREADYSETUP * @brief The GATEHWSPINLOCK module has already been setup in this process. */ #define GateHWSpinlock_S_ALREADYSETUP 1 /* ============================================================================= * Macros * ============================================================================= */ /*! @brief Forward declaration of structure defining object for the * GateHWSpinlock. */ typedef struct GateHWSpinlock_Object GateHWSpinlock_Object; /*! * @brief Handle for the GateHWSpinlock. */ typedef struct GateHWSpinlock_Object * GateHWSpinlock_Handle; /* Q_BLOCKING */ #define GateHWSem_Q_BLOCKING (1) /* Q_PREEMPTING */ #define GateHWSem_Q_PREEMPTING (2) /* ============================================================================= * Structures & Enums * ============================================================================= */ /*! * @brief Structure defining config parameters for the GateHWSpinlock module. */ typedef struct GateHWSpinlock_Config { UInt32 baseAddr; /* Device-specific base address for HW Semaphore subsystem in HOST OS * address space, this is updated in Ipc module */ UInt32 size; /* Device-specific size for HW Semaphore subsystem */ UInt32 offset; /* Device-specific size for HW Semaphore subsystem */ } GateHWSpinlock_Config; /*! * @brief Structure defining config parameters for the GateHWSpinlock * instances. */ typedef struct GateHWSpinlock_Params { Bits32 resourceId; Bool openFlag; UInt16 regionId; Ptr sharedAddr; } GateHWSpinlock_Params; typedef enum GateHWSpinlock_LocalProtect { GateHWSpinlock_LocalProtect_NONE = 0, GateHWSpinlock_LocalProtect_INTERRUPT = 1, GateHWSpinlock_LocalProtect_TASKLET = 2, GateHWSpinlock_LocalProtect_THREAD = 3, GateHWSpinlock_LocalProtect_PROCESS = 4 } GateHWSpinlock_LocalProtect; /* ============================================================================= * APIs * ============================================================================= */ /* Function to get the default configuration for the GateHWSpinlock module. */ Void GateHWSpinlock_getConfig (GateHWSpinlock_Config * cfgParams); /* Function to setup the GateHWSpinlock module. */ Int GateHWSpinlock_setup (const GateHWSpinlock_Config * config); /* Function to destroy the GateHWSpinlock module */ Int GateHWSpinlock_destroy (Void); /* Initialize parameter structure */ Void GateHWSpinlock_Params_init(GateHWSpinlock_Params *params); /* Function to start GateHWSpinlock module */ Int32 GateHWSpinlock_start(Void); /* Funciton to stop GateHWSpinlock module */ Int GateHWSpinlock_stop(Void); /* Function to create an instance of GateHWSpinlock */ GateHWSpinlock_Handle GateHWSpinlock_create ( GateMP_LocalProtect localProtect, const GateHWSpinlock_Params * params); /* Function to delete an instance of GateHWSpinlock */ Int GateHWSpinlock_delete (GateHWSpinlock_Handle * handlePtr); /* Function to delete all instances of GateHWSpinlock */ Int GateHWSpinlock_deleteAll (Void); /* Function to enter the GateHWSpinlock instance */ IArg GateHWSpinlock_enter (GateHWSpinlock_Handle handle); /* Function to leave the GateHWSpinlock instance */ Int GateHWSpinlock_leave (GateHWSpinlock_Handle handle, IArg key); /*! * @brief Function to return the number of instances configured in the * module. * * @return Number of instances configured. */ UInt32 GateHWSpinlock_getNumInstances (Void); /*! * @brief Function to initialize the locks * module. * */ Void GateHWSpinlock_locksinit(Void); /* This is exported from daemon/GateHWSpinlockCfg_.c */ extern GateHWSpinlock_Config _GateHWSpinlock_cfgParams; /* Internal variable to enable/disable tracing throughout GateHWSpinlock */ extern Bool _GateHWSpinlock_verbose; #if defined (__cplusplus) } #endif /* defined (__cplusplus) */ #endif /* GATEHWSPINLOCK_H_0xF416 */