/* * Copyright (c) 2012-2013, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /** * @file ti/ipc/MessageQ.h * * @brief MessageQ Manager * * The MessageQ module supports the structured sending and receiving of * variable length messages. This module can be used for homogeneous * (e.g. DSP to DSP) or heterogeneous (e.g. ARM to DSP) multi-processor * messaging. * * MessageQ provides more sophisticated messaging than other modules. It is * typically used for complex situations such as multi-processor messaging. * * The following are key features of the MessageQ module: * - Writers and readers can be relocated to another processor with no * runtime code changes. * - Timeouts are allowed when receiving messages. * - Readers can determine the writer and reply back. * - Receiving a message is deterministic when the timeout is zero. * - Messages can reside on any message queue. * - Supports zero-copy transfers. * - Can send and receive from any type of thread. * - Notification mechanism is specified by application. * - Allows QoS (quality of service) on message buffer pools. For example, * using specific buffer pools for specific message queues. * * Messages are sent and received by being placed on and removed from a * message queue. A reader is a thread that gets (reads) messages from a * message queue. A writer is a thread that puts (writes) a message to a * message queue. Each message queue has one reader and can have many writers. * A thread may read from or write to multiple message queues. * * Conceptually, the reader thread owns a message queue. The reader thread * creates a message queue. The writer threads open a created message queue * to get access to them. * * Message queues are identified by a system-wide unique name. Internally, * MessageQ uses the NameServer module for managing * these names. The names are used for opening a message queue. * * Messages must be allocated from the MessageQ module. Once a message is * allocated, it can be sent to any message queue. Once a message is sent, the * writer loses ownership of the message and should not attempt to modify the * message. Once the reader receives the message, it owns the message. It * may either free the message or re-use the message. * * Messages in a message queue can be of variable length. The only * requirement is that the first field in the definition of a message must be a * #MessageQ_MsgHeader structure. For example: * @code * typedef struct MyMsg { * MessageQ_MsgHeader header; * ... * } MyMsg; * @endcode * * The MessageQ API uses the MessageQ_MsgHeader internally. Your application * should not modify or directly access the fields in the MessageQ_MsgHeader. * * All messages sent via the MessageQ module must be allocated from a * heap. The heap can also be used for other memory allocation not related to * MessageQ. * * An application can use multiple heaps. The purpose of having multiple * heaps is to allow an application to regulate its message usage. For * example, an application can allocate critical messages from one heap of fast * on-chip memory and non-critical messages from another heap of slower * external memory. * * The MessageQ_registerHeap() API is used to * assign a MessageQ heapId to a heap. When allocating a message, the heapId * is used, not the heap handle. This heapId is actually placed into the * message (part of the #MessageQ_MsgHeader). Care must be taken when * assigning heapIds. Refer to the MessageQ_registerHeap() API description for * more details. * * MessageQ also supports the usage of messages that are not allocated via the * MessageQ_alloc() function. Please refer to the MessageQ_staticMsgInit() * function description for more details. * * MessageQ supports reads/writes of different thread models. This is * accomplished by having the creator of the message queue specify a * synchronizer via the #MessageQ_Params.synchronizer * configuration parameter. The synchronizer is signaled whenever the * MessageQ_put() is called. The synchronizer waits if MessageQ_get() is called * and there are no messages. * * Since ISyncs are binary, the reader must drain the message queue of all * messages before waiting for another signal. For example, if the reader * was a SYS/BIOS Swi, the synchronizer instance could be a SyncSwi. * If a MessageQ_put() was called, the Swi_post() would * be called. The Swi would run and it must call MessageQ_get() until no * messages are returned. * * The MessageQ header should be included in an application as follows: * @code * #include * @endcode */ #ifndef ti_ipc_MessageQ__include #define ti_ipc_MessageQ__include #include #if defined (__cplusplus) extern "C" { #endif /* ============================================================================= * All success and failure codes for the module * ============================================================================= */ /*! * @brief The resource is still in use */ #define MessageQ_S_BUSY 2 /*! * @brief The module has been already setup */ #define MessageQ_S_ALREADYSETUP 1 /*! * @brief Operation is successful. */ #define MessageQ_S_SUCCESS 0 /*! * @brief Operation is not successful. */ #define MessageQ_E_FAIL -1 /*! * @brief There is an invalid argument. */ #define MessageQ_E_INVALIDARG -2 /*! * @brief Operation resulted in memory failure. */ #define MessageQ_E_MEMORY -3 /*! * @brief The specified entity already exists. */ #define MessageQ_E_ALREADYEXISTS -4 /*! * @brief Unable to find the specified entity. */ #define MessageQ_E_NOTFOUND -5 /*! * @brief Operation timed out. */ #define MessageQ_E_TIMEOUT -6 /*! * @brief Module is not initialized. */ #define MessageQ_E_INVALIDSTATE -7 /*! * @brief A failure occurred in an OS-specific call */ #define MessageQ_E_OSFAILURE -8 /*! * @brief Specified resource is not available */ #define MessageQ_E_RESOURCE -9 /*! * @brief Operation was interrupted. Please restart the operation */ #define MessageQ_E_RESTART -10 /*! * @brief An invalid message was encountered */ #define MessageQ_E_INVALIDMSG -11 /*! * @brief Not the owner */ #define MessageQ_E_NOTOWNER -12 /*! * @brief Operation resulted in error */ #define MessageQ_E_REMOTEACTIVE -13 /*! * @brief An invalid heap id was encountered */ #define MessageQ_E_INVALIDHEAPID -14 /*! * @brief An invalid MultiProc id was encountered */ #define MessageQ_E_INVALIDPROCID -15 /*! * @brief The max has been reached. */ #define MessageQ_E_MAXREACHED -16 /*! * @brief Attempting to use an unregistered heap id. */ #define MessageQ_E_UNREGISTEREDHEAPID -17 /*! * @brief Trying to free a statically initialized message */ #define MessageQ_E_CANNOTFREESTATICMSG -18 /*! * @brief MessageQ was unblocked */ #define MessageQ_E_UNBLOCKED -19 /* ============================================================================= * Macros * ============================================================================= */ /*! * @brief Used as the timeout value to specify wait forever */ #define MessageQ_FOREVER ~(0) /*! * @brief Invalid message id */ #define MessageQ_INVALIDMSGID 0xffff /*! * @brief Invalid message queue */ #define MessageQ_INVALIDMESSAGEQ 0xffff /*! * @brief Mask to extract priority setting */ #define MessageQ_PRIORITYMASK 0x3 /*! * @brief Extract the destination queue ID from a message. * * Can only be used on the same processor where the destination queue resides. * This function should only be used by Message Queue Transport writers. * * @param[in] msg Message of type #MessageQ_Msg * * @retval queueId Destination message queue ID of type #MessageQ_QueueId */ #define MessageQ_getDstQueue(msg) \ ((msg)->dstId == (MessageQ_QueueIndex)MessageQ_INVALIDMESSAGEQ) ? \ (MessageQ_QueueId)MessageQ_INVALIDMESSAGEQ : \ (MessageQ_QueueId)(((MessageQ_QueueId)MultiProc_self() << 16u) \ | (((MessageQ_Msg)(msg))->dstId)) /*! * @brief Retrieves the message ID of a message. * * This function retrieves the message ID from the message. The * MessageQ_setMsgId() function is used to insert the message ID. * * The message id is part of the #MessageQ_MsgHeader header and is in every * MessageQ message. All message ids are initialized to #MessageQ_INVALIDMSGID * in the MessageQ_alloc() and MessageQ_staticMsgInit() calls. * * @param[in] msg Message of type #MessageQ_Msg * * @retval msgId 16-bit message ID from the message */ #define MessageQ_getMsgId(msg) (((MessageQ_Msg) (msg))->msgId) /*! * @brief Returns the size of the specified message. This function is helpful * when re-using a message. * * @param[in] msg Message of type #MessageQ_Msg * * @retval size Size of the message */ #define MessageQ_getMsgSize(msg) (((MessageQ_Msg) (msg))->msgSize) /*! * @brief Gets the message priority of a message * * @param[in] msg Message of type #MessageQ_Msg * * @retval priority Priority of the message */ #define MessageQ_getMsgPri(msg) \ ((((MessageQ_Msg) (msg))->flags & MessageQ_PRIORITYMASK)) /*! * @brief Returns the MultiProc processor id on which the queue resides * * Message queues reside on the processor that created them. This function * allows the caller to determined on which processor the queue resides. * * @param[in] queueId Unique #MessageQ_QueueId that identifies the queue * * @retval procId The MultiProc id on which the queue resides */ #define MessageQ_getProcId(queueId) \ ((UInt16)((queueId) >> 16)) /*! * @brief Retrieves the message queue ID from a message. * * This function along with the MessageQ_setReplyQueue() function can be used * instead of the open function. The sender of a message can embed a messageQ * into the message with the MessageQ_setReplyQueue() function. The receiver of * the message can extract the message queue ID with this function. * * This method is particularly useful in a client/server relationship where * the server does not want to know who the clients are. The clients can embed * their message queue into the message to the server and the server extracts * it and uses it to reply. * * @param[in] msg Message of type #MessageQ_Msg * * @retval queueId Message queue ID of type #MessageQ_QueueId */ #define MessageQ_getReplyQueue(msg) \ (MessageQ_QueueId)((((MessageQ_Msg) (msg))->replyProc << 16u) \ | ((MessageQ_Msg)(msg))->replyId) /*! * @brief Sets the message id in a message. * * This function sets the message ID in the message. The MessageQ_getMsgId() * function is used to retrieve the message ID. The message id is part of the * #MessageQ_MsgHeader header and is in every MessageQ message. All message ids * are initialized to #MessageQ_INVALIDMSGID in the MessageQ_alloc() and * MessageQ_staticMsgInit() calls. * * @param[in] msg Message of type #MessageQ_Msg * @param[in] id 16-bit value */ #define MessageQ_setMsgId(msg, id) ((MessageQ_Msg) (msg))->msgId = (id) /*! * @brief Sets the message priority of a message * * @param[in] msg Message of type #MessageQ_Msg * @param[in] priority Priority of message to be set. */ #define MessageQ_setMsgPri(msg, priority) \ (((MessageQ_Msg) (msg))->flags = ((priority) & MessageQ_PRIORITYMASK)) /* ============================================================================= * Structures & Enums * ============================================================================= */ /*! * @brief A 32-bit value that uniquely identifies a message queue */ typedef UInt32 MessageQ_QueueId; /*! * @brief Local queue index */ typedef UInt16 MessageQ_QueueIndex; /*! * @brief MessageQ_Handle type */ typedef struct MessageQ_Object *MessageQ_Handle; /*! * @brief Structure defining parameters for the MessageQ module. */ typedef struct { Void *synchronizer; /*!< Synchronizer instance used to signal IO completion * * The synchronizer is used in MessageQ_put() and MessageQ_get(). * The synchronizer signal is called as part of MessageQ_put(). * The synchronizer waits in MessageQ_get() if there are no messages * present. */ } MessageQ_Params; /*! * @brief Required first field in every message */ typedef struct { Bits32 reserved0; /*!< reserved for List.elem->next */ Bits32 reserved1; /*!< reserved for List.elem->prev */ Bits32 msgSize; /*!< message size */ Bits16 flags; /*!< bitmask of different flags */ Bits16 msgId; /*!< message id */ Bits16 dstId; /*!< destination queue id */ Bits16 dstProc; /*!< destination processor id */ Bits16 replyId; /*!< reply id */ Bits16 replyProc; /*!< reply processor */ Bits16 srcProc; /*!< source processor */ Bits16 heapId; /*!< heap id */ Bits16 seqNum; /*!< sequence number */ Bits16 reserved; /*!< reserved */ } MessageQ_MsgHeader; /*! * @brief Typedef for ease of use */ typedef MessageQ_MsgHeader *MessageQ_Msg; /*! * @brief Message priority */ typedef enum { MessageQ_NORMALPRI = 0, /*!< Normal Priority */ MessageQ_HIGHPRI = 1, /*!< High Priority */ MessageQ_RESERVEDPRI = 2, /*!< Reserved Priority */ MessageQ_URGENTPRI = 3 /*!< Urgent Priority */ } MessageQ_Priority; /* ============================================================================= * MessageQ Module-wide Functions * ============================================================================= */ /*! * @brief Initialize MessageQ_Params * * @param[in] params Parameters required to create a MessageQ */ Void MessageQ_Params_init(MessageQ_Params *params); /*! * @brief Create a MessageQ instance * * The name supplied here does not have to be in persistent memory. The * maximum length of the string supplied here, including the '\\0' terminator * is '32' by default. * * There are no verifications to ensure that the name supplied in * MessageQ_create() is unique across all processors. Caution must be exercised * to ensure that each processor uses a unique name. * * @param[in] name Name of the queue * @param[in] params Initialized MessageQ parameters * * @return MessageQ Handle */ MessageQ_Handle MessageQ_create(String name, const MessageQ_Params *params); /*! * @brief Delete a created MessageQ instance * * This function deletes a created message queue instance. If the * message queue is non-empty, any messages remaining in the queue * will not be freed and will be lost. * * @param[in,out] handlePtr Pointer to handle to delete. * * @return MessageQ status: * - #MessageQ_E_FAIL: delete failed * - #MessageQ_S_SUCCESS: delete successful */ Int MessageQ_delete(MessageQ_Handle *handlePtr); /*! * @brief Open a message queue * * MessageQ_open() is used to retrieve the queue id for a queue that has been * created either locally or remotely. Note that the queueId is simply a * 32 bit value that uniquely identifies a queue. Therefore, it is also * possible to put a message on a queue whose queueId has been retrieved using * any other method. * * @param[in] name Name of queue to open * @param[out] queueId QueueId that can be used in MessageQ_put() * * @return MessageQ status: * - #MessageQ_E_NOTFOUND: open failed (name not found on any * processor) * - #MessageQ_S_SUCCESS: open successful */ Int MessageQ_open(String name, MessageQ_QueueId *queueId); /*! * @brief Close the opened handle * * Only close a queueId that was returned from MessageQ_open(). * * @param[in] queueId Pointer to queueId to close * * @return MessageQ status: * - #MessageQ_E_FAIL: close failed * - #MessageQ_S_SUCCESS: close successful */ Int MessageQ_close(MessageQ_QueueId *queueId); /*! * @brief Allocates a message from the heap * * This function allocates a message from the heap associated with the heapId. * The first field of the message must be a #MessageQ_MsgHeader structure. * For example: * @code * typedef struct MyMsg { * MessageQ_MsgHeader header; * ... * } MyMsg; * @endcode * * @param[in] heapId heapId * @param[in] size size of requested message (including the * #MessageQ_MsgHeader). * * @pre @c size must be at least large enough to hold a * MessageQ_MsgHeader * * @return Allocated message or NULL if no memory. */ MessageQ_Msg MessageQ_alloc(UInt16 heapId, UInt32 size); /*! * @brief Frees a message back to the heap * * Frees the message back to the heap that was used to allocate it. * * @param[in] msg Message to free. * * @return MessageQ status: * - #MessageQ_E_FAIL: failed to free message * - #MessageQ_S_SUCCESS: successfully freed the message */ Int MessageQ_free(MessageQ_Msg msg); /*! * @brief Register a heap with MessageQ * * This function registers a heap with MessageQ. The user selects a unique * heapId associated with this heap. When a message is allocated via * MessageQ_alloc(), the heapId is specified. Internally, MessageQ * uses the heapId to access the heap. * * Care must be taken when assigning heapIds. Internally MessageQ stores * the heapId into the message. When the message is freed * (via MessageQ_free()), the heapId is used to determine which heap to use. * On systems with shared memory the heapIds must match on corresponding * processors. For example, assume there is a heap called myHeap which * acts on shared memory and processors 0 and 1 both use this heap. * When you register the heap with MessageQ, the same heapId must be used * on both processor 0 and 1. * * If a heap is already registered for the specified heapId, no action is * taken and #MessageQ_E_ALREADYEXISTS is returned. * * @param[in] heap Heap to register * @param[in] heapId heapId associated with the heap * * @return MessageQ status: * - #MessageQ_S_SUCCESS: heap successfully registered * - #MessageQ_E_ALREADYEXISTS: heap already exists with heapId */ Int MessageQ_registerHeap(Ptr heap, UInt16 heapId); /*! * @brief Unregister a heap with MessageQ * * This function unregisters the heap associated with the heapId. * Care must be taken to ensure that there are no outstanding messages * allocated from this heap. If there are outstanding messages, an attempt * to free the message will result in non-deterministic results. * * @param[in] heapId Heap to unregister * * @return MessageQ status: * - #MessageQ_S_SUCCESS: heap successfully unregistered */ Int MessageQ_unregisterHeap(UInt16 heapId); /*! * @brief Sets the message tracing flag on a given message * * This function enables message tracing for a message. Tracing is offered * in the form of Log messages that are output during operations on the * message (i.e. MessageQ_free(), MessageQ_put(), etc). * * @param msg Message * @param traceFlag Message trace flag (TRUE = tracing enabled) */ Void MessageQ_setMsgTrace(MessageQ_Msg msg, Bool traceFlag); /*! * @brief Initializes a message not obtained from MessageQ_alloc() * * There are several fields in the #MessageQ_MsgHeader that * are initialized by the MessageQ_alloc() function. MessageQ_staticMsgInit() * can be used to initialize these fields for messages that are * not allocated from MessageQ. * * There is one strict constraint with using messages not allocated * from MessageQ. The message cannot be freed via MessageQ_free(). * This includes * - The application calling MessageQ_free() on the same processor * - The application calling MessageQ_free() on a different processor * - The application cannot send the message to another processor * where the transport might call MessageQ_free() on the message. * For example, copy based transport call MessageQ_free() after sending * the message. * If a staticMsgInit'd msg is passed to MessageQ_free() an assert will occur * * @param msg Message to initialize * @param[in] size Size of the message in MAUs * * @pre @c size must be at least large enough to hold a #MessageQ_MsgHeader */ Void MessageQ_staticMsgInit(MessageQ_Msg msg, UInt32 size); /* ============================================================================= * MessageQ Per-instance Functions * ============================================================================= */ /*! * @brief Gets a message from the message queue * * This function returns a status. It also returns a message in msg. * If no message is available, it blocks on the synchronizer object * until the synchronizer is signaled or a timeout occurs. * The synchronizer is signaled, when Message_put is called on the MessageQ * handle. If a timeout occurs, the msg is set to NULL and the status is * #MessageQ_E_TIMEOUT. If a timeout of zero is specified, the function * returns immediately and if no message is available, the msg * is set to NULL and the status is #MessageQ_E_TIMEOUT. The * #MessageQ_E_UNBLOCKED status is return, if MessageQ_unblock is called * on the MessageQ handle. If a message is successfully retrieved, the msg * is set to the message and a #MessageQ_S_SUCCESS status is returned. * * @param[in] handle MessageQ handle * @param[out] msg Pointer to the message * @param[in] timeout Maximum duration to wait for a message in * microseconds. * * @return MessageQ status: * - #MessageQ_S_SUCCESS: Message successfully returned * - #MessageQ_E_TIMEOUT: MessageQ_get() timed out * - #MessageQ_E_UNBLOCKED: MessageQ_get() was unblocked * - #MessageQ_E_FAIL: A general failure has occurred * * @sa MessageQ_put() * @sa MessageQ_unblock() */ Int MessageQ_get(MessageQ_Handle handle, MessageQ_Msg *msg, UInt timeout); /*! * @brief Place a message onto a message queue * * This call places the message onto the specified message queue. The * message queue could be local or remote. The MessageQ module manages * the delivery. * * In the case where the queue is remote, MessageQ does not guarantee that * the message is actually delivered before the MessageQ_put() call returns * * The queue id must have been returned from one of the following functions: * - MessageQ_open() * - MessageQ_getReplyQueue() * - MessageQ_getDstQueue() * * After the message is placed onto the final destination, the queue's * #MessageQ_Params.synchronizer signal function is called. * * The application loses ownership of the message once MessageQ_put() is called. * * @param[in] queueId Destination MessageQ * @param[in] msg Message to be sent. * * @return Status of the call. * - #MessageQ_S_SUCCESS denotes success. * - #MessageQ_E_FAIL denotes failure. The put was not successful. * The caller still owns the message. */ Int MessageQ_put(MessageQ_QueueId queueId, MessageQ_Msg msg); /*! * @brief Returns the number of messages in a message queue * * This function returns the number of messages in a message queue. * * @param[in] handle MessageQ handle * * @return Number of messages in the message queue. */ Int MessageQ_count(MessageQ_Handle handle); /*! * @brief Returns the QueueId associated with the handle * * Since the MessageQ_put() function takes a QueueId, the creator * of a message queue cannot send a message to itself without * retrieving the QueueId. This function extracts the QueueId * from the object. * * @param[in] handle MessageQ handle * * @return QueueId associated to the object */ UInt32 MessageQ_getQueueId(MessageQ_Handle handle); /*! * @brief Embeds a source message queue into a message * * This function along with MessageQ_getReplyQueue() * can be used instead of MessageQ_open(). The sender * of a message can embed a messageQ into the message with this * function. The receiver of the message can extract the message queue * id with the MessageQ_getReplyQueue() function. * * This method is particularly useful in a client/server relationship * where the server does not want to know who the clients are. The * clients can embed their message queue into the message to the server * and the server extracts it and uses it to reply. * * @param handle MessageQ handle * @param msg Message to embed queue into */ Void MessageQ_setReplyQueue(MessageQ_Handle handle, MessageQ_Msg msg); /*! * @brief Unblocks a MessageQ * * Unblocks a reader thread that is blocked on a MessageQ_get(). The * MessageQ_get() call will return with status #MessageQ_E_UNBLOCKED indicating * that it returned due to a MessageQ_unblock() rather than a timeout or a * received message. This call should only be used during a shutdown sequence * in order to ensure that there is no blocked reader on a queue before * deleting the queue. A queue may not be used after it has been unblocked. * * MessageQ_unblock() works by raising a flag in the queue indicating that it * is unblocked and then signaling the synchronizer that is configured with * the target queue. If MessageQ_unblock() is called upon a queue that has * no blocked listeners, then any subsequent MessageQ_get will not block and * will immediately return #MessageQ_E_UNBLOCKED regardless of whether there * is a message on the queue. * * Restrictions: * - A queue may not be used after it has been unblocked. * - MessageQ_unblock() may only be called on a local queue. * - May only be used with a queue configured with a blocking synchronizer. * * @param[in] handle MessageQ handle * * @sa MessageQ_get */ Void MessageQ_unblock(MessageQ_Handle handle); #if defined (__cplusplus) } #endif /* defined (__cplusplus) */ #endif /* ti_ipc_MessageQ__include */