/* * Copyright (c) 2012-2015 Texas Instruments Incorporated - http://www.ti.com * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /** * @file ti/ipc/MessageQ.h * * @brief MessageQ Manager * * The MessageQ module supports the structured sending and receiving of * variable length messages. This module can be used for homogeneous * (e.g. DSP to DSP) or heterogeneous (e.g. ARM to DSP) multi-processor * messaging. * * MessageQ provides more sophisticated messaging than other modules. It is * typically used for complex situations such as multi-processor messaging. * * The following are key features of the MessageQ module: * - Writers and readers can be relocated to another processor with no * runtime code changes. * - Timeouts are allowed when receiving messages. * - Readers can determine the writer and reply back. * - Receiving a message is deterministic when the timeout is zero. * - Messages can reside on any message queue. * - Supports zero-copy transfers. * - Can send and receive from any type of thread. * - Notification mechanism is specified by application. * - Allows QoS (quality of service) on message buffer pools. For example, * using specific buffer pools for specific message queues. * * Messages are sent and received by being placed on and removed from a * message queue. A reader is a thread that gets (reads) messages from a * message queue. A writer is a thread that puts (writes) a message to a * message queue. Each message queue has one reader and can have many writers. * A thread may read from or write to multiple message queues. * * Conceptually, the reader thread owns a message queue. The reader thread * creates a message queue. The writer threads open a created message queue * to get access to them. * * Message queues are identified by a system-wide unique name. Internally, * MessageQ uses the NameServer module for managing * these names. The names are used for opening a message queue. * * Messages must be allocated from the MessageQ module. Once a message is * allocated, it can be sent to any message queue. Once a message is sent, the * writer loses ownership of the message and should not attempt to modify the * message. Once the reader receives the message, it owns the message. It * may either free the message or re-use the message. * * Messages in a message queue can be of variable length. The only * requirement is that the first field in the definition of a message must be a * #MessageQ_MsgHeader structure. For example: * @code * typedef struct MyMsg { * MessageQ_MsgHeader header; * ... * } MyMsg; * @endcode * * The MessageQ API uses the MessageQ_MsgHeader internally. Your application * should not modify or directly access the fields in the MessageQ_MsgHeader. * * All messages sent via the MessageQ module must be allocated from a * heap. The heap can also be used for other memory allocation not related to * MessageQ. * * An application can use multiple heaps. The purpose of having multiple * heaps is to allow an application to regulate its message usage. For * example, an application can allocate critical messages from one heap of fast * on-chip memory and non-critical messages from another heap of slower * external memory. * * The MessageQ_registerHeap() API is used to * assign a MessageQ heapId to a heap. When allocating a message, the heapId * is used, not the heap handle. This heapId is actually placed into the * message (part of the #MessageQ_MsgHeader). Care must be taken when * assigning heapIds. Refer to the MessageQ_registerHeap() API description for * more details. * * MessageQ also supports the usage of messages that are not allocated via the * MessageQ_alloc() function. Please refer to the MessageQ_staticMsgInit() * function description for more details. * * MessageQ supports reads/writes of different thread models. This is * accomplished by having the creator of the message queue specify a * synchronizer via the #MessageQ_Params.synchronizer * configuration parameter. The synchronizer is signaled whenever the * MessageQ_put() is called. The synchronizer waits if MessageQ_get() is called * and there are no messages. * * Since ISyncs are binary, the reader must drain the message queue of all * messages before waiting for another signal. For example, if the reader * was a SYS/BIOS Swi, the synchronizer instance could be a SyncSwi. * If a MessageQ_put() was called, the Swi_post() would * be called. The Swi would run and it must call MessageQ_get() until no * messages are returned. * * The MessageQ header should be included in an application as follows: * @code * #include * @endcode */ #ifndef ti_ipc_MessageQ__include #define ti_ipc_MessageQ__include #include #if defined (__cplusplus) extern "C" { #endif /* ============================================================================= * All success and failure codes for the module * ============================================================================= */ /*! * @brief The resource is still in use */ #define MessageQ_S_BUSY (2) /*! * @brief The module has been already setup */ #define MessageQ_S_ALREADYSETUP (1) /*! * @brief Operation is successful. */ #define MessageQ_S_SUCCESS (0) /*! * @brief Operation is not successful. */ #define MessageQ_E_FAIL (-1) /*! * @brief There is an invalid argument. */ #define MessageQ_E_INVALIDARG (-2) /*! * @brief Operation resulted in memory failure. */ #define MessageQ_E_MEMORY (-3) /*! * @brief The specified entity already exists. */ #define MessageQ_E_ALREADYEXISTS (-4) /*! * @brief Unable to find the specified entity. */ #define MessageQ_E_NOTFOUND (-5) /*! * @brief Operation timed out. */ #define MessageQ_E_TIMEOUT (-6) /*! * @brief Module is not initialized. */ #define MessageQ_E_INVALIDSTATE (-7) /*! * @brief A failure occurred in an OS-specific call */ #define MessageQ_E_OSFAILURE (-8) /*! * @brief Specified resource is not available */ #define MessageQ_E_RESOURCE (-9) /*! * @brief Operation was interrupted. Please restart the operation */ #define MessageQ_E_RESTART (-10) /*! * @brief An invalid message was encountered */ #define MessageQ_E_INVALIDMSG (-11) /*! * @brief Not the owner */ #define MessageQ_E_NOTOWNER (-12) /*! * @brief Operation resulted in error */ #define MessageQ_E_REMOTEACTIVE (-13) /*! * @brief An invalid heap id was encountered */ #define MessageQ_E_INVALIDHEAPID (-14) /*! * @brief An invalid MultiProc id was encountered */ #define MessageQ_E_INVALIDPROCID (-15) /*! * @brief The max has been reached. */ #define MessageQ_E_MAXREACHED (-16) /*! * @brief Attempting to use an unregistered heap id. */ #define MessageQ_E_UNREGISTEREDHEAPID (-17) /*! * @brief Trying to free a statically initialized message */ #define MessageQ_E_CANNOTFREESTATICMSG (-18) /*! * @brief MessageQ was unblocked */ #define MessageQ_E_UNBLOCKED (-19) /*! * @brief MessageQ was shutdown */ #define MessageQ_E_SHUTDOWN (-20) /* ============================================================================= * Macros * ============================================================================= */ /*! * @brief Used as the timeout value to specify wait forever */ #define MessageQ_FOREVER (~(0)) /*! * @brief Invalid message id */ #define MessageQ_INVALIDMSGID (0xffff) /*! * @brief Invalid message queue */ #define MessageQ_INVALIDMESSAGEQ (0xffff) /*! * @brief Mask to extract priority setting */ #define MessageQ_PRIORITYMASK (0x3) /** @cond INTERNAL */ /*! * @brief Offset to avoid collision with reserved ports * * A queue's port number is computed by adding this offset to the * queue index. Use the port number to address the message or when * binding a socket. Computing a port number with this offset avoids * collisions with reserved port numbers which are typically in the * same range as the queue indexes. */ #define MessageQ_PORTOFFSET (0x80) /** @endcond INTERNAL */ /*! * @brief Extract the destination queue ID from a message. * * This function is typically used be a transport. * * The destination address is written into the message header when * calling MessageQ_put(). Therefore, you can only use this function * to extract the destination queue ID after MessageQ_put() has been * called on the given message. However, ownership rules dictate that * you cannot dereference a message after calling MessageQ_put() (because * you have transfered ownership to the transport). * * After receiving a message by calling MessageQ_get(), you may safely * use this function. Although there is little benefit from doing so. * * When the message is given to the transport, the destination address * has been written into the message header. In addition, the transport * now has ownership of the message. So, it is appropriate for the transport * to use this macro. * * @param[in] msg Message of type #MessageQ_Msg * * @retval queueId Destination message queue ID of type #MessageQ_QueueId */ #define MessageQ_getDstQueue(msg) \ (((MessageQ_Msg)(msg))->dstId == \ (MessageQ_QueueIndex)MessageQ_INVALIDMESSAGEQ) ? \ (MessageQ_QueueId)MessageQ_INVALIDMESSAGEQ : \ (((MessageQ_QueueId)((MessageQ_Msg)(msg))->dstProc << 16u) \ | (((MessageQ_Msg)(msg))->dstId)) /*! * @brief Retrieves the message ID of a message. * * This function retrieves the message ID from the message. The * MessageQ_setMsgId() function is used to insert the message ID. * * The message id is part of the #MessageQ_MsgHeader header and is in every * MessageQ message. All message ids are initialized to #MessageQ_INVALIDMSGID * in the MessageQ_alloc() and MessageQ_staticMsgInit() calls. * * @param[in] msg Message of type #MessageQ_Msg * * @retval msgId 16-bit message ID from the message */ #define MessageQ_getMsgId(msg) (((MessageQ_Msg) (msg))->msgId) /*! * @brief Returns the size of the specified message. This function is helpful * when re-using a message. * * @param[in] msg Message of type #MessageQ_Msg * * @retval size Size of the message */ #define MessageQ_getMsgSize(msg) (((MessageQ_Msg) (msg))->msgSize) /*! * @brief Gets the message priority of a message * * @param[in] msg Message of type #MessageQ_Msg * * @retval priority Priority of the message */ #define MessageQ_getMsgPri(msg) \ ((((MessageQ_Msg) (msg))->flags & MessageQ_PRIORITYMASK)) /*! * @brief Returns the MultiProc processor id on which the queue resides * * Message queues reside on the processor that created them. This function * allows the caller to determined on which processor the queue resides. * * @param[in] queueId Unique #MessageQ_QueueId that identifies the queue * * @retval procId The MultiProc id on which the queue resides */ #define MessageQ_getProcId(queueId) \ ((UInt16)((queueId) >> 16)) /*! * @brief Extract the queue index from the given queue ID * * When creating and opening queues, the queue index is embedded * into the queue ID using an implementation dependent format. This * function extracts the queue index from the queue ID. * * For example, in the MessageQ_put() hook function, you might extract * the queue index in order to set the transport ID. * * @code * Void msgqPutHook(MessageQ_QueueId queueId, MessageQ_Msg msg) * { * MessageQ_QueueIndex queueIndex; * UInt tid; * * queueIndex = MessageQ_getQueueIndex(queueId); * ... * MessageQ_setTransportId(msg, tid); * } * @endcode * * This function performs no error checking. Using an invalid queue ID * will result in undefined behavior. * * @param[in] queueId Message queue ID of type #MessageQ_QueueId * * @retval queueIndex The queue index of type #MessageQ_QueueIndex */ #define MessageQ_getQueueIndex(queueId) \ (((MessageQ_QueueIndex)((MessageQ_QueueId)0xFFFF & (queueId))) \ - MessageQ_PORTOFFSET) /*! * @brief Retrieves the message queue ID from a message. * * This function along with the MessageQ_setReplyQueue() function can be used * instead of the open function. The sender of a message can embed a messageQ * into the message with the MessageQ_setReplyQueue() function. The receiver of * the message can extract the message queue ID with this function. * * This method is particularly useful in a client/server relationship where * the server does not want to know who the clients are. The clients can embed * their message queue into the message to the server and the server extracts * it and uses it to reply. * * @param[in] msg Message of type #MessageQ_Msg * * @retval queueId Message queue ID of type #MessageQ_QueueId */ #define MessageQ_getReplyQueue(msg) \ (MessageQ_QueueId)((((MessageQ_Msg) (msg))->replyProc << 16u) \ | ((MessageQ_Msg)(msg))->replyId) /*! * @brief Return the transport Id for the given message * * Extract the transport Id from the message header. * * @param[in] msg message of type #MessageQ_Msg * @retval tid transport Id */ #define MessageQ_getTransportId(msg) \ ((((MessageQ_Msg)(msg))->flags & (0x7 << 2)) >> 2) /*! * @brief Sets the message id in a message. * * This function sets the message ID in the message. The MessageQ_getMsgId() * function is used to retrieve the message ID. The message id is part of the * #MessageQ_MsgHeader header and is in every MessageQ message. All message ids * are initialized to #MessageQ_INVALIDMSGID in the MessageQ_alloc() and * MessageQ_staticMsgInit() calls. * * @param[in] msg Message of type #MessageQ_Msg * @param[in] id 16-bit value */ #define MessageQ_setMsgId(msg, id) ((MessageQ_Msg) (msg))->msgId = (id) /*! * @brief Sets the message priority of a message * * @param[in] msg Message of type #MessageQ_Msg * @param[in] priority Priority of message to be set. */ #define MessageQ_setMsgPri(msg, priority) \ ((MessageQ_Msg)(msg))->flags = \ (((MessageQ_Msg)(msg))->flags & ~(MessageQ_PRIORITYMASK)) \ | ((priority) & MessageQ_PRIORITYMASK) /*! * @brief Set the transport Id for the given message * * Set the transport Id in the flags field of the message header. When * set to a non-zero value, the message will be given to the specified * transport for delivery. The transport must be registered with MessageQ * with the given Id. * * There is no error checking on the transport Id. * * @param[in] msg message of type #MessageQ_Msg * @param[in] tid transport ID (1-7) */ #define MessageQ_setTransportId(msg, tid) \ ((MessageQ_Msg)(msg))->flags = \ ((((MessageQ_Msg)(msg))->flags & ~(0x7 << 2)) | ((tid) << 2)) /* ============================================================================= * Structures & Enums * ============================================================================= */ /*! * @brief A 32-bit value that uniquely identifies a message queue */ typedef UInt32 MessageQ_QueueId; /*! * @brief Local queue index */ typedef UInt16 MessageQ_QueueIndex; /*! * @brief MessageQ_Handle type */ typedef struct MessageQ_Object *MessageQ_Handle; /*! * @brief Structure defining parameters for MessageQ_create(). */ typedef struct { /** @cond INTERNAL */ Int __version; /* Used internally for tracking implementation evolution. * For internal use only. */ /** @endcond INTERNAL */ Void *synchronizer; /*!< Synchronizer instance used to signal IO completion * * The synchronizer is used in MessageQ_put() and MessageQ_get(). * The synchronizer signal is called as part of MessageQ_put(). * The synchronizer waits in MessageQ_get() if there are no messages * present. */ MessageQ_QueueIndex queueIndex; /*!< Value used to specify the index in the MessageQ array * * This parameter allows an application to specify a queueIndex to * be used for a message queue. To use this functionality, the * MessageQ.numReservedEntries static configuration parameter must be * set to one more than the highest requested queueIndex. The * MessageQ.numReservedEntries parameter reserves that number of * message queue slots starting at 0 and proceeding to * (MessageQ.numReservedEntries - 1). * * The default is MessageQ_ANY, which means it is not taken from the * reserved slots. */ } MessageQ_Params; /** @cond INTERNAL */ /* Date: 02 Dec 2014 * * Initial implementation of params structure which contains * a version field. This allows for binary compatibility as * the params structure is modified in the future. */ #define MessageQ_Params_VERSION_2 2 /** @endcond INTERNAL */ /** @cond INTERNAL */ /*! * @brief Defines the current params structure version */ #define MessageQ_Params_VERSION MessageQ_Params_VERSION_2 /** @endcond INTERNAL */ /*! * @brief Structure defining parameters for MessageQ_create2(). * * MessageQ_Params2 is a superset of MessageQ_Params. It is used * with MessageQ_create2(). * * @deprecated This type has been deprecated. It will be removed * in a future release. Please use MessageQ_Params instead. */ typedef struct { Void *synchronizer; /*!< Synchronizer instance used to signal IO completion * * The synchronizer is used in MessageQ_put() and MessageQ_get(). * The synchronizer signal is called as part of MessageQ_put(). * The synchronizer waits in MessageQ_get() if there are no messages * present. */ MessageQ_QueueIndex queueIndex; /*!< Value used to specify the index in the MessageQ array * * This parameter allows an application to specify a queueIndex to * be used for a message queue. To use this functionality, the * MessageQ.numReservedEntries static configuration parameter must be * set to one more than the highest requested queueIndex. The * MessageQ.numReservedEntries parameter reserves that number of * message queue slots starting at 0 and proceeding to * (MessageQ.numReservedEntries - 1). * * The default is MessageQ_ANY, which means it is not taken from the * reserved slots. */ } MessageQ_Params2; /*! * @brief Required first field in every message */ typedef struct { Bits32 reserved0; /*!< reserved for List.elem->next */ Bits32 reserved1; /*!< reserved for List.elem->prev */ Bits32 msgSize; /*!< message size */ Bits16 flags; /*!< bitmask of different flags */ Bits16 msgId; /*!< message id */ Bits16 dstId; /*!< destination queue id */ Bits16 dstProc; /*!< destination processor id */ Bits16 replyId; /*!< reply id */ Bits16 replyProc; /*!< reply processor */ Bits16 srcProc; /*!< source processor */ Bits16 heapId; /*!< heap id */ Bits16 seqNum; /*!< sequence number */ Bits16 reserved; /*!< reserved */ } MessageQ_MsgHeader; /*! * @brief Typedef for ease of use */ typedef MessageQ_MsgHeader *MessageQ_Msg; /*! * @brief Message priority */ typedef enum { MessageQ_NORMALPRI = 0, /*!< Normal Priority */ MessageQ_HIGHPRI = 1, /*!< High Priority */ MessageQ_RESERVEDPRI = 2, /*!< Reserved Priority */ MessageQ_URGENTPRI = 3 /*!< Urgent Priority */ } MessageQ_Priority; /*! * @brief Denotes any queueId is acceptable. * * This constant is the default for the queueId in the MessageQ_Params * structure. */ #define MessageQ_ANY (Bits16)~(0) /*! * @brief Free hook prototype * * @param[in] heapId heapId of message that was freed * @param[in] msgId msgId of message that was freed */ typedef Void (*MessageQ_FreeHookFxn)(Bits16 heapId, Bits16 msgId); /*! * @brief Put hook function definition * * This function is invoked near the beginning of the MessageQ_put() * function. It allows client code to augment the addressing of the * given message before it is delivered. * * @param[in] queueId destination message queue * @param[in] msg message to be sent */ typedef Void (*MessageQ_PutHookFxn)(MessageQ_QueueId queueId, MessageQ_Msg msg); #ifdef STD_H #include #include #else #include #include #endif Bool MessageQ_registerTransport(IMessageQTransport_Handle handle, UInt16 rprocId, UInt priority); Void MessageQ_unregisterTransport(UInt16 rprocId, UInt priority); /* ============================================================================= * MessageQ Module-wide Functions * ============================================================================= */ /** @cond INTERNAL */ /* Returns the local handle associated with queueId. */ MessageQ_Handle MessageQ_getLocalHandle(MessageQ_QueueId queueId); /** @endcond INTERNAL */ /** @cond INTERNAL */ Void MessageQ_Params_init__S(MessageQ_Params *params, Int version); /** @endcond INTERNAL */ /*! * @brief Initialize MessageQ_Params * * Initialized the given structure to its default values. * * @param[in] params Parameters required to create a MessageQ */ #ifndef MessageQ_internal static inline Void MessageQ_Params_init(MessageQ_Params *params) { if (params != NULL) { MessageQ_Params_init__S(params, MessageQ_Params_VERSION); } } #endif /*! * @brief Initialize MessageQ_Params2 * * Initialized the given structure to its default values. * * @deprecated This function has been deprecated. It will be removed * in a future release. Please use MessageQ_Params_init() instead. * * @param[in] params Parameters required to create a MessageQ */ Void MessageQ_Params2_init(MessageQ_Params2 *params); /*! * @brief Create a MessageQ instance * * The name supplied here does not have to be in persistent memory. The * maximum length of the string supplied here, including the '\\0' terminator, * is '32' by default. * * There are no verifications to ensure that the name supplied in * MessageQ_create() is unique across all processors. Caution must be exercised * to ensure that each processor uses a unique name. * * @param[in] name Name of the queue * @param[in] params Initialized MessageQ parameters * * @return MessageQ Handle */ MessageQ_Handle MessageQ_create(String name, const MessageQ_Params *params); /*! * @brief Create a MessageQ instance using the type MessageQ_Params2 * * The name supplied here does not have to be in persistent memory. The * maximum length of the string supplied here, including the '\\0' terminator, * is '32' by default. * * There are no verifications to ensure that the name supplied in * MessageQ_create2() is unique across all processors. Caution must * be exercised to ensure that each processor uses a unique name. * * @deprecated This function has been deprecated. It will be removed * in a future release. Please use MessageQ_create() instead. * * @param[in] name Name of the queue * @param[in] params Initialized MessageQ_Params2 * * @return MessageQ Handle */ MessageQ_Handle MessageQ_create2(String name, const MessageQ_Params2 *params); /*! * @brief Delete a created MessageQ instance * * This function deletes a created message queue instance. If the * message queue is non-empty, any messages remaining in the queue * will not be freed and will be lost. * * @param[in,out] handlePtr Pointer to handle to delete. * * @return MessageQ status: * - #MessageQ_E_FAIL: delete failed * - #MessageQ_S_SUCCESS: delete successful */ Int MessageQ_delete(MessageQ_Handle *handlePtr); /*! * @brief Open a message queue * * MessageQ_open() is used to retrieve the queue id for a queue that has been * created either locally or remotely. Note that the queueId is simply a * 32 bit value that uniquely identifies a queue. Therefore, it is also * possible to put a message on a queue whose queueId has been retrieved using * any other method. * * @param[in] name Name of queue to open * @param[out] queueId QueueId that can be used in MessageQ_put() * * @return MessageQ status: * - #MessageQ_E_NOTFOUND: open failed (name not found on any * processor) * - #MessageQ_S_SUCCESS: open successful */ Int MessageQ_open(String name, MessageQ_QueueId *queueId); /*! * @brief Open a MessageQ given the queue index and processor ID * * This function can be used instead of MessageQ_open() if the queue * was created with a reserved queue index. In the example below, the * serverFxn function must be running on the processor with PROCID 2. * * @code * #define SERVER_QUEIDX 1 * #define SERVER_PROCID 2 * * serverFxn() * { * MessageQ_Params params; * * MessageQ_Params_init(¶ms); * params.queueIndex = SERVER_QUEIDX; * messageQ = MessageQ_create(NULL, ¶ms); * ... * } * * clientFxn() * { * MessageQ_QueueId serverQueue; * serverQueue = MessageQ_openQueueId(SERVER_QUEIDX, SERVER_PROCID); * } * @endcode * * It is up to the application to guarantee that the queue which is being * opened has already been created. MessageQ_openQueueId() does not validate * that the queue has been created (unlike the MessageQ_open() function). * * @param[in] queueIndex QueueIndex specified in MessageQ_Params when * the message queue was created. * @param[in] procId Multiproc_Id of where the created queue resides. * * @return The MessageQ_QueueId associated with the queueIndex * and remoteProcId */ MessageQ_QueueId MessageQ_openQueueId(UInt16 queueIndex, UInt16 procId); /*! * @brief Close the opened handle * * Only close a queueId that was returned from MessageQ_open(). * * @param[in] queueId Pointer to queueId to close * * @return MessageQ status: * - #MessageQ_E_FAIL: close failed * - #MessageQ_S_SUCCESS: close successful */ Int MessageQ_close(MessageQ_QueueId *queueId); /*! * @brief Allocates a message from the heap * * This function allocates a message from the heap associated with the heapId. * The first field of the message must be a #MessageQ_MsgHeader structure. * For example: * @code * typedef struct MyMsg { * MessageQ_MsgHeader header; * ... * } MyMsg; * @endcode * * @param[in] heapId heapId * @param[in] size size of requested message (including the * #MessageQ_MsgHeader). * * @pre @c size must be at least large enough to hold a * MessageQ_MsgHeader * * @return Allocated message or NULL if no memory. */ MessageQ_Msg MessageQ_alloc(UInt16 heapId, UInt32 size); /*! * @brief Frees a message back to the heap * * Frees the message back to the heap that was used to allocate it. * * @param[in] msg Message to free. * * @return MessageQ status: * - #MessageQ_E_FAIL: failed to free message * - #MessageQ_S_SUCCESS: successfully freed the message */ Int MessageQ_free(MessageQ_Msg msg); /*! * @brief Register a heap with MessageQ * * This function registers a heap with MessageQ. The user selects a unique * heapId associated with this heap. When a message is allocated via * MessageQ_alloc(), the heapId is specified. Internally, MessageQ * uses the heapId to access the heap. * * Care must be taken when assigning heapIds. Internally MessageQ stores * the heapId into the message. When the message is freed * (via MessageQ_free()), the heapId is used to determine which heap to use. * On systems with shared memory the heapIds must match on corresponding * processors. For example, assume there is a heap called myHeap which * acts on shared memory and processors 0 and 1 both use this heap. * When you register the heap with MessageQ, the same heapId must be used * on both processor 0 and 1. * * If a heap is already registered for the specified heapId, no action is * taken and #MessageQ_E_ALREADYEXISTS is returned. * * @param[in] heap Heap to register * @param[in] heapId heapId associated with the heap * * @return MessageQ status: * - #MessageQ_S_SUCCESS: heap successfully registered * - #MessageQ_E_ALREADYEXISTS: heap already exists with heapId */ Int MessageQ_registerHeap(Ptr heap, UInt16 heapId); /*! * @brief Register a transport instance for the given ID * * Additional transport instances can be registered with the MessageQ * module. This allows for message delivery over selected transports. * * To arrange for a message to be delivered using a registered transport, * the corresponding transport ID must be set in the message header by * calling MessageQ_setTransportId(). * * @param[in] tid Transport ID, must be 1-7 inclusive * @param[in] inst Transport instance handle * * @return Status result * - TRUE: transport handle successfully registered * - FALSE: failure, most likely transport ID already in use * * @sa MessageQ_setTransportId() * @sa MessageQ_unregisterTransportId() */ Bool MessageQ_registerTransportId(UInt tid, ITransport_Handle inst); /*! * @brief Unregister a heap with MessageQ * * This function unregisters the heap associated with the heapId. * Care must be taken to ensure that there are no outstanding messages * allocated from this heap. If there are outstanding messages, an attempt * to free the message will result in non-deterministic results. * * @param[in] heapId Heap to unregister * * @return MessageQ status: * - #MessageQ_S_SUCCESS: heap successfully unregistered */ Int MessageQ_unregisterHeap(UInt16 heapId); /*! * @brief Unregister the transport instance for the given ID * * Remove the registered transport instance for the give transport ID. * * @param[in] tid Transport ID, must be 1-7 inclusive * * @sa MessageQ_registerTransportId() */ Void MessageQ_unregisterTransportId(UInt tid); /*! * @brief Sets the message tracing flag on a given message * * This function enables message tracing for a message. Tracing is offered * in the form of Log messages that are output during operations on the * message (i.e. MessageQ_free(), MessageQ_put(), etc). * * @param msg Message * @param traceFlag Message trace flag (TRUE = tracing enabled) */ Void MessageQ_setMsgTrace(MessageQ_Msg msg, Bool traceFlag); /*! * @brief Initializes a message not obtained from MessageQ_alloc() * * There are several fields in the #MessageQ_MsgHeader that * are initialized by the MessageQ_alloc() function. MessageQ_staticMsgInit() * can be used to initialize these fields for messages that are * not allocated from MessageQ. * * There is one strict constraint with using messages not allocated * from MessageQ. The message cannot be freed via MessageQ_free(). * This includes * - The application calling MessageQ_free() on the same processor * - The application calling MessageQ_free() on a different processor * - The application cannot send the message to another processor * where the transport might call MessageQ_free() on the message. * For example, copy based transport call MessageQ_free() after sending * the message. * If a staticMsgInit'd msg is passed to MessageQ_free() an assert will occur * * @param msg Message to initialize * @param[in] size Size of the message in MAUs * * @pre @c size must be at least large enough to hold a #MessageQ_MsgHeader */ Void MessageQ_staticMsgInit(MessageQ_Msg msg, UInt32 size); /*! * @brief Sets MessageQ's free hook function. * * This API allows a user to specify a hook function which is called within * MessageQ_free(). The hook is called after a message is freed back to the * associated heap. The two parameters to the hook function are the heapId * and the msgId of the freed message. * * The function is called within MessageQ_free(), so care must be taken to * minimize any performance or calling context impact. * * MessageQ_setFreeHookFxn() is not thread safe. It should only * be called when no MessageQ_free()'s are happening. * * To disable the hook function, call MessageQ_setFreeHookFxn() with NULL. * * @param[in] freeHookFxn function to be called within MessageQ_free() */ Void MessageQ_setFreeHookFxn(MessageQ_FreeHookFxn freeHookFxn); /*! * @brief Set the function hook for the MessageQ_put() method * * Register a hook function which is called from the beginning of the * MessageQ_put() function. Only one hook may be registered at a time. * Subsequent calls to register a put function will overwrite the * previously registered function. * * To disable the hook function, call MessageQ_setPutHookFxn() with NULL. * * @param[in] putHookFxn function to be called within MessageQ_put() */ Void MessageQ_setPutHookFxn(MessageQ_PutHookFxn putHookFxn); /* ============================================================================= * MessageQ Per-instance Functions * ============================================================================= */ /*! * @brief Gets a message from the message queue * * This function returns a status. It also returns a message in msg. * If no message is available, it blocks on the synchronizer object * until the synchronizer is signaled or a timeout occurs. * The synchronizer is signaled, when Message_put is called on the MessageQ * handle. If a timeout occurs, the msg is set to NULL and the status is * #MessageQ_E_TIMEOUT. If a timeout of zero is specified, the function * returns immediately and if no message is available, the msg * is set to NULL and the status is #MessageQ_E_TIMEOUT. The * #MessageQ_E_UNBLOCKED status is return, if MessageQ_unblock is called * on the MessageQ handle. The #MessageQ_E_SHUTDOWN status is returned if * MessageQ_shutdown is called on the MessageQ handle. If a message is * successfully retrieved, the msg is set to the message and a * #MessageQ_S_SUCCESS status is returned. * * @param[in] handle MessageQ handle * @param[out] msg Pointer to the message * @param[in] timeout Maximum duration to wait for a message in * microseconds. * * @return MessageQ status: * - #MessageQ_S_SUCCESS: Message successfully returned * - #MessageQ_E_TIMEOUT: MessageQ_get() timed out * - #MessageQ_E_UNBLOCKED: MessageQ_get() was unblocked * - #MessageQ_E_FAIL: A general failure has occurred * * @sa MessageQ_put() * @sa MessageQ_unblock() * @sa MessageQ_shutdown() */ Int MessageQ_get(MessageQ_Handle handle, MessageQ_Msg *msg, UInt timeout); /*! * @brief Place a message onto a message queue * * This call places the message onto the specified message queue. The * message queue could be local or remote. The MessageQ module manages * the delivery. * * In the case where the queue is remote, MessageQ does not guarantee that * the message is actually delivered before the MessageQ_put() call returns * * The queue id must have been returned from one of the following functions: * - MessageQ_open() * - MessageQ_getReplyQueue() * - MessageQ_getDstQueue() * * After the message is placed onto the final destination, the queue's * #MessageQ_Params.synchronizer signal function is called. * * The application loses ownership of the message once MessageQ_put() is called. * * @param[in] queueId Destination MessageQ * @param[in] msg Message to be sent. * * @return Status of the call. * - #MessageQ_S_SUCCESS denotes success. * - #MessageQ_E_FAIL denotes failure. The put was not successful. * The caller still owns the message. */ Int MessageQ_put(MessageQ_QueueId queueId, MessageQ_Msg msg); /*! * @brief Returns the number of messages in a message queue * * This function returns the number of messages in a message queue. * * @param[in] handle MessageQ handle * * @return Number of messages in the message queue. */ Int MessageQ_count(MessageQ_Handle handle); /*! * @brief Returns the QueueId associated with the handle * * Since the MessageQ_put() function takes a QueueId, the creator * of a message queue cannot send a message to itself without * retrieving the QueueId. This function extracts the QueueId * from the object. * * @param[in] handle MessageQ handle * * @return QueueId associated to the object */ UInt32 MessageQ_getQueueId(MessageQ_Handle handle); /*! * @brief Embeds a source message queue into a message * * This function along with MessageQ_getReplyQueue() * can be used instead of MessageQ_open(). The sender * of a message can embed a messageQ into the message with this * function. The receiver of the message can extract the message queue * id with the MessageQ_getReplyQueue() function. * * This method is particularly useful in a client/server relationship * where the server does not want to know who the clients are. The * clients can embed their message queue into the message to the server * and the server extracts it and uses it to reply. * * @param handle MessageQ handle * @param msg Message to embed queue into */ Void MessageQ_setReplyQueue(MessageQ_Handle handle, MessageQ_Msg msg); /*! * @brief Unblocks a MessageQ * * Unblocks a reader thread that is blocked on a MessageQ_get(). The * MessageQ_get() call will return with status #MessageQ_E_UNBLOCKED indicating * that it returned due to a MessageQ_unblock() rather than a timeout or a * received message. This call should only be used during a shutdown sequence * in order to ensure that there is no blocked reader on a queue before * deleting the queue. A queue may not be used after it has been unblocked. * * MessageQ_unblock() works by raising a flag in the queue indicating that it * is unblocked and then signaling the synchronizer that is configured with * the target queue. If MessageQ_unblock() is called upon a queue that has * no blocked listeners, then any subsequent MessageQ_get will not block and * will immediately return #MessageQ_E_UNBLOCKED regardless of whether there * is a message on the queue. * * Restrictions: * - A queue may not be used after it has been unblocked. * - MessageQ_unblock() may only be called on a local queue. * - May only be used with a queue configured with a blocking synchronizer. * * @param[in] handle MessageQ handle * * @sa MessageQ_get * @sa MessageQ_shutdown() */ Void MessageQ_unblock(MessageQ_Handle handle); /*! * @brief Shuts down a MessageQ * * Similar to MessageQ_unblock(), MessageQ_shutdown() unblocks a reader thread * that is blocked on a MessageQ_get(), but causes a different return code * to be returned from MessageQ_get(). The MessageQ_get() call will return * with status #MessageQ_E_SHUTDOWN indicating that it returned due to a * MessageQ_shutdown() rather than MessageQ_unblock(), a timeout or a * received message. This call is intended to be used by MessageQ transports * when the transport detects that the transport framework corresponding to * the MessageQ has become unusable. This call should only be used during a * shutdown sequence in order to ensure that there is no blocked reader on a * queue before deleting the queue. A queue may not be used after it has been * shut down. * * MessageQ_shutdown() works by raising a flag in the queue indicating that it * is shut down and then signaling the synchronizer that is configured with * the target queue. If MessageQ_shutdown() is called upon a queue that has * no blocked listeners, then any subsequent MessageQ_get will not block and * will immediately return #MessageQ_E_SHUTDOWN regardless of whether there * is a message on the queue. * * Restrictions: * - A queue may not be used after it has been shut down. * - MessageQ_shutdown() may only be called on a local queue. * - May only be used with a queue configured with a blocking synchronizer. * * @param[in] handle MessageQ handle * * @sa MessageQ_get * @sa MessageQ_unblock */ Void MessageQ_shutdown(MessageQ_Handle handle); #if defined (__cplusplus) } #endif /* defined (__cplusplus) */ #endif /* ti_ipc_MessageQ__include */