/*
* Copyright (c) 2012-2015 Texas Instruments Incorporated - http://www.ti.com
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
/**
* @file ti/ipc/NameServer.h
*
* @brief NameServer Manager
*
* The NameServer module manages local name/value pairs that
* enables an application and other modules to store and
* retrieve values based on a name. The module supports different
* lengths of values. The NameServer_add() and NameServer_get()
* functions are for variable length values. The NameServer_addUInt32() and
* NameServer_getUInt32() functions are optimized for UInt32 variables
* and constants.
*
* The NameServer module maintains thread-safety for the APIs. However,
* the NameServer APIs cannot be called from an interrupt (i.e. Hwi) context.
* However, it is safe to use the APIs in Swi's and Tasks.
*
* Each NameServer instance manages a different name/value table.
* This allows each table to be customized to meet the requirements
* of user:
* @li Size differences: one table could allow long values
* (e.g. > 32 bits) while another table could be used to store integers.
* This customization enables better memory usage.
* @li Performance: improves search time when retrieving
* a name/value pair.
* @li Relax name uniqueness: names in a specific table must
* be unique, but the same name can be used in different tables.
*
* When adding a name/value pair, the name and value are copied into
* internal buffers in NameServer. To minimize runtime memory allocation
* these buffers can be allocated at creation time.
*
* NameServer maintains the name/values table in local memory (e.g.
* not shared memory). However the NameServer module can be
* used in a multiprocessor system.
*
* The NameServer module uses the MultiProc module for
* identifying the different processors. Which remote processors and
* the order they are queried is determined by the procId array in the
* NameServer_get() function.
*
* Currently there is no endian or wordsize conversion performed by the
* NameServer module. Also there is no asynchronous support at this time.
*
* The NameServer header should be included in an application as follows:
* @code
* #include
* @endcode
*/
#ifndef ti_ipc_NameServer__include
#define ti_ipc_NameServer__include
#if defined (__cplusplus)
extern "C" {
#endif
/* =============================================================================
* All success and failure codes for the module
* =============================================================================
*/
/*!
* @brief The resource is still in use
*/
#define NameServer_S_BUSY (2)
/*!
* @brief The module has been already setup
*/
#define NameServer_S_ALREADYSETUP (1)
/*!
* @brief Operation is successful.
*/
#define NameServer_S_SUCCESS (0)
/*!
* @brief Generic failure.
*/
#define NameServer_E_FAIL (-1)
/*!
* @brief Argument passed to function is invalid.
*/
#define NameServer_E_INVALIDARG (-2)
/*!
* @brief Operation resulted in memory failure.
*/
#define NameServer_E_MEMORY (-3)
/*!
* @brief The specified entity already exists.
*/
#define NameServer_E_ALREADYEXISTS (-4)
/*!
* @brief Unable to find the specified entity.
*/
#define NameServer_E_NOTFOUND (-5)
/*!
* @brief Operation timed out.
*/
#define NameServer_E_TIMEOUT (-6)
/*!
* @brief Module is not initialized.
*/
#define NameServer_E_INVALIDSTATE (-7)
/*!
* @brief A failure occurred in an OS-specific call
*/
#define NameServer_E_OSFAILURE (-8)
/*!
* @brief Specified resource is not available
*/
#define NameServer_E_RESOURCE (-9)
/*!
* @brief Operation was interrupted. Please restart the operation
*/
#define NameServer_E_RESTART (-10)
/*!
* @brief Name is too long.
*
* The underlying remote implementation was unable to handle such a long
* instance or entry name.
* See these files for the maximum number of characters that can be specified
* in a name for common NameServer remote implementations:
*
* - NameServerRemoteRpmsg:
* packages/ti/ipc/namesrv/_NameServerRemoteRpmsg.h
*
*/
#define NameServer_E_NAMETOOLONG (-11)
/* =============================================================================
* Macros
* =============================================================================
*/
/*!
* @brief Allow dynamic growth of the NameServer instance table
*/
#define NameServer_ALLOWGROWTH (~0)
/*!
* @brief The default maximum length of the name for the name/value pair
*/
#define NameServer_Params_MAXNAMELEN (16)
/* =============================================================================
* Structures & Enums
* =============================================================================
*/
/*!
* @brief NameServer handle type
*/
typedef struct NameServer_Object *NameServer_Handle;
/*!
* @brief NameServer_Handle type
*/
typedef struct NameServer_Params {
UInt maxRuntimeEntries;
/*!< @brief Maximum name/value pairs that can be dynamically created.
*
* This parameter allows NameServer to pre-allocate memory.
* When NameServer_add() or NameServer_addUInt32() is
* called, no memory allocation occurs.
*
* If the number of pairs is not known at configuration time, set this
* value to #NameServer_ALLOWGROWTH. This instructs NameServer
* to grow the table as needed. NameServer will allocate memory from the
* #NameServer_Params.tableHeap when a name/value pair is added.
*
* The default is #NameServer_ALLOWGROWTH.
*/
Ptr tableHeap;
/*!< @brief Name/value table is allocated from this heap.
*
* The instance table and related buffers are allocated out of this heap
* during the dynamic create. This heap is also used to allocate new
* name/value pairs when #NameServer_ALLOWGROWTH for
* #NameServer_Params.maxRuntimeEntries
*
* The default is to use the same heap that instances are allocated
* from which can be configured via the
* NameServer.common$.instanceHeap configuration parameter.
*/
Bool checkExisting;
/*!< @brief Check if a name already exists in the name/value table.
*
* When a name/value pair is added during runtime, if this boolean is
* true, the table is searched to see if the name already exists. If
* it does, the name is not added and the
* #NameServer_E_ALREADYEXISTS error is returned.
*
* If this flag is false, the table will not be checked to see if the
* name already exists. It will simply be added. This mode has better
* performance at the expense of potentially having non-unique names
* in the table.
*
* This flag is used for runtime adds only. Adding non-unique names during
* configuration results in a build error.
*/
UInt maxValueLen;
/*!< @brief Length, in MAUs, of the value field in the table.
*
* Any value less than sizeof(UInt32) will be rounded up to sizeof(UInt32)
*/
UInt maxNameLen;
/*!< @brief Length, in MAUs, of the name field in the table.
*
* The maximum length of the name portion of the name/value
* pair. The length includes the null terminator ('\\0').
*/
} NameServer_Params;
/* =============================================================================
* NameServer Module-wide Functions
* =============================================================================
*/
/*!
* @brief Initializes parameter structure
*
* @param params Instance param structure
*
* @sa NameServer_create()
*/
Void NameServer_Params_init(NameServer_Params *params);
/*!
* @brief Creates a NameServer instance
*
* If NameServer_create() was previously called to create an instance with the
* same name, subsequent calls to NameServer_create() on the same name will
* simply return a valid handle to the existing NameServer instance, similar
* to what is done by NameServer_getHandle().
*
* @param name Instance name
* @param params Instance param structure
*
* @return NameServer handle
*
* @sa NameServer_delete()
*/
NameServer_Handle NameServer_create(String name,
const NameServer_Params *params);
/*!
* @brief Deletes a NameServer instance
*
* If the instance is not empty, the contents is freed back to the
* heap it was allocated from.
*
* If NameServer_create() was called multiple times on the same name,
* a matching number of calls to NameServer_delete() is necessary in
* order to fully deallocate the instance.
*
* @param handlePtr Pointer to a NameServer handle
*
* @return Status
* - #NameServer_S_SUCCESS: Instance successfully deleted
* - #NameServer_E_FAIL: Instance delete failed
*
* @sa NameServer_create()
*/
Int NameServer_delete(NameServer_Handle *handlePtr);
/*!
* @brief Gets the NameServer handle given the name
*
* Each NameServer instance has a name. The name and this function can be
* used by the remote driver module to aid in queries to remote
* processors. This function allows the caller to get the local handle
* based on the instance name.
*
* For example, when a remote driver sends a request to the remote
* processor, it probably contains the name of the instance to query.
* The receiving remote driver uses that name to obtain the handle for
* the local NameServer instance in question. Then that instance
* can be queried for the name/value pair.
*
* This function does not query remote processors.
*
* @param name Name of instance
*
* @return NameServer handle
*/
NameServer_Handle NameServer_getHandle(String name);
/* =============================================================================
* NameServer Per-instance Functions
* =============================================================================
*/
/*!
* @brief Adds a variable length value into the local NameServer table
*
* This function adds a variable length value into the local table.
* If the #NameServer_Params.checkExisting flag was true on
* creation, this function searches the table to make sure the name
* does not already exist. If it does, the name/value pair is not
* added and the #NameServer_E_ALREADYEXISTS error is returned.
*
* There is memory allocation during this function if
* #NameServer_Params.maxRuntimeEntries is set to
* #NameServer_ALLOWGROWTH.
*
* This function copies the name and buffer into the name/value table,
* so they do not need to be persistent after the call.
*
* The function does not query remote processors to make sure the
* name is unique.
*
* @param handle Instance handle
* @param name Name for the name/value pair
* @param buf Pointer to value for the name/value pair
* @param len length of the value
*
* @return Unique entry identifier, or NULL if unsuccessful
*
* @sa NameServer_addUInt32()
* @sa NameServer_get()
*/
Ptr NameServer_add(NameServer_Handle handle, String name, Ptr buf, UInt32 len);
/*!
* @brief Adds a 32-bit value into the local NameServer table
*
* This function adds a 32-bit value into the local table. This
* function is simply a specialized NameServer_add() function
* that allows a convenient way to add UInt32 bit values without needing
* to specify the address of a UInt32 local variable.
*
* If the #NameServer_Params.checkExisting flag was true on
* creation, this function searches the table to make sure the name does
* not already exist. If it does, the name/value pair is not added and the
* #NameServer_E_ALREADYEXISTS error is returned.
*
* This function copies the name into the name/value table.
*
* There is memory allocation during this function if
* #NameServer_Params.maxRuntimeEntries is set to
* #NameServer_ALLOWGROWTH.
*
* The function does not query remote processors to make sure the
* name is unique.
*
* @param handle Instance handle
* @param name Name for the name/value pair
* @param value Value for the name/value pair
*
* @return Unique entry identifier, or NULL if unsuccessful
*
* @sa NameServer_add()
* @sa NameServer_getUInt32()
*/
Ptr NameServer_addUInt32(NameServer_Handle handle, String name, UInt32 value);
/*!
* @brief Gets the variable value length by name
*
* If the name is found, the value is copied into the value
* argument, the number of MAUs copied is returned in len, and
* a success status is returned.
*
* If the name is not found, zero is returned in len, the contents
* of value are not modified. Not finding a name is not considered
* an error.
*
* For NameServer to work across processors, each processor must
* must be assigned a unique id. Because remote NameServer requests
* usually employ the use of notifications, it is good practice to
* sleep/wait between successive NameServer_get[UInt32] operations if polling
* on the success of this call. This helps ensure that remote cores
* are not inundated by a flood of incoming notifications and helps
* reduce the possibility of deadlocks.
*
* The processors to query is determined by the procId array.
* The array is used to specify which processors to query and the order.
* The processor ids are determined via the MultiProc module.
* The following are the valid settings for the procId array:
* @li NULL: denotes that the local table is searched first, then
* all remote processors in ascending order by MultiProc id.
* @li Filled in array: The NameServer will search the processors
* in the order given in the array. The end of the list must be denoted
* by the #MultiProc_INVALIDID value.
*
* @code
* UInt16 queryList[4] = {3, 2, 4, MultiProc_INVALIDID};
* count = NameServer_get(handle, "foo", &value, &len, queryList);
* @endcode
*
* This API should be called only from task context. It cannot be called
* from Hwi or Swi context because it blocks waiting for a response from
* the remote processor.
*
* The NameServer_getLocal() call can be used for searching
* the local table only.
*
* @param handle Instance handle
* @param name Name to query
* @param buf Pointer where the value is returned
* @param len Pointer for input/output length.
* @param procId Array of processor(s) to query
*
* @return NameServer status:
* - #NameServer_S_SUCCESS: Successfully found entry
* - #NameServer_E_NOTFOUND: Entry was not found, len unchanged
* - #NameServer_E_FAIL: Error searching for entry
* - #NameServer_E_NAMETOOLONG: Instance name or query name is
* too long for NameServer remote to process
*
* @sa NameServer_add()
* @sa NameServer_getLocal()
*/
Int NameServer_get(NameServer_Handle handle,
String name,
Ptr buf,
UInt32 *len,
UInt16 procId[]);
/*!
* @brief Gets a 32-bit value by name
*
* If the name is found, the value is copied into the value
* argument, and a success status is returned.
*
* If the name is not found, the contents of value are not modified.
* Not finding a name is not considered an error.
*
* For NameServer to work across processors, each processor must
* must be assigned a unique id. Because remote NameServer requests
* usually employ the use of notifications, it is good practice to
* sleep/wait between successive NameServer_get[UInt32] operations if polling
* on the success of this call. This helps ensure that remote cores
* are not inundated by a flood of incoming notifications and helps
* reduce the possibility of deadlocks.
*
* The processors to query is determined by the procId array.
* The array is used to specify which processors to query and the order.
* The processor ids are determined via the MultiProc module.
* The following are the valid settings for the procId array:
* @li NULL: denotes that the local table is searched first, then
* all remote processors in ascending order by MultiProc id.
* @li Filled in array: The NameServer will search the processors
* in the order given in the array. The end of the list must be denoted
* by the #MultiProc_INVALIDID value.
*
* @code
* UInt16 queryList[4] = {3, 2, 4, MultiProc_INVALIDID};
* count = NameServer_getUInt32(handle, "foo", &value, queryList);
* @endcode
*
* The NameServer_getLocal() call can be used for searching
* the local table only.
* @param handle Instance handle
* @param name Name to query
* @param buf Pointer where the value is returned
* @param procId Array of processor(s) to query
*
* @return Status
* - #NameServer_S_SUCCESS: Successfully found entry
* - #NameServer_E_NOTFOUND: Entry was not found
* - #NameServer_E_FAIL: Error searching for entry
*
* @sa NameServer_addUInt32()
* @sa NameServer_getLocalUInt32()
*/
Int NameServer_getUInt32(NameServer_Handle handle,
String name,
Ptr buf,
UInt16 procId[]);
/*!
* @brief Gets the variable value length by name from the local table
*
* If the name is found, the value is copied into the value
* argument, the number of MAUs copied is returned in len, and
* a success status is returned.
*
* If the name is not found, zero is returned in len, a fail status is
* returned and the contents of value are not modified.
* Not finding a name is not considered an error.
*
* This function only searches the local name/value table.
*
* @param handle Instance handle
* @param name Name to query
* @param buf Pointer where the value is returned
* @param len Length of the value
*
* @return Status
* - #NameServer_S_SUCCESS: Successfully found entry, len
* holds amount of data retrieved.
* - #NameServer_E_NOTFOUND: Entry was not found, len remains
* unchanged.
*
* @sa NameServer_add()
* @sa NameServer_get()
*/
Int NameServer_getLocal(NameServer_Handle handle,
String name,
Ptr buf,
UInt32 *len);
/*!
* @brief Gets a 32-bit value by name from the local table
*
* If the name is found, the 32-bit value is copied into buf
* and NameServer_S_SUCCESS is returned.
*
* If the name is not found, zero is copied into buf and
* NameServer_E_NOTFOUND is returned.
*
* This function only searches the local name/value table.
*
* @param handle Instance handle
* @param name Name to query
* @param buf Pointer where the value is returned
*
* @return Status
* - #NameServer_S_SUCCESS: Successfully found entry
* - #NameServer_E_NOTFOUND: Entry was not found
*
* @sa NameServer_addUInt32()
* @sa NameServer_getUInt32()
*/
Int NameServer_getLocalUInt32(NameServer_Handle handle,
String name,
Ptr buf);
/*! @cond
* @brief Match the name with the longest entry
*
* Returns the number of characters that matched with an entry.
* So if "abc" and "ab" was an entry and you called match with "abcd",
* this function will match the "abc" entry. The return would be 3 since
* three characters matched.
*
* Currently only 32-bit values are supported.
*
* @param handle Instance handle
* @param name Name in question
* @param value Pointer in which the value is returned
*
* @return Number of matching characters
*/
Int NameServer_match(NameServer_Handle handle, String name, UInt32 *value);
/*! @endcond */
/*!
* @brief Remove a name/value pair from the table
*
* This function removes a name/value pair from the table.
*
* If #NameServer_Params.maxRuntimeEntries is set to
* #NameServer_ALLOWGROWTH,
* memory will be freed which was allocated in NameServer_add().
* Otherwise, no memory is freed during this call.
* The entry in the table is simply emptied.
* When another NameServer_add() occurs, it will reuse the empty
* entry.
*
* @param handle Instance handle
* @param name Name to remove
*
* @return Status
* - #NameServer_S_SUCCESS: Successfully removed entry or
* entry does not exists
* - #NameServer_E_FAIL: Operation failed
*
* @sa NameServer_add
*/
Int NameServer_remove(NameServer_Handle handle, String name);
/*!
* @brief Remove a name/value pair from the table
*
* This function removes an entry from the table based on the
* unique identifier returned from NameServer_add() or
* NameServer_addUInt32().
*
* If #NameServer_Params#maxRuntimeEntries is set to
* #NameServer_ALLOWGROWTH,
* memory will be freed which was allocated in NameServer_add().
* Otherwise, no memory is freed during this call.
* The entry in the table is simply emptied.
* When another NameServer_add() occurs, it will reuse the
* empty entry.
*
* Once an entry is removed from the NameServer table, it cannot be
* removed again (just like you cannot free the same block of memory
* twice).
*
* @param handle Instance handle
* @param entry Pointer to entry to be removed
*
* @return Status
* - #NameServer_S_SUCCESS: Successfully removed entry or
* entry does not exists
* - #NameServer_E_FAIL: Operation failed
*
* @sa NameServer_add()
*/
Int NameServer_removeEntry(NameServer_Handle handle, Ptr entry);
#if defined (__cplusplus)
}
#endif /* defined (__cplusplus) */
#endif /* ti_ipc_NameServer__include */