/* * Copyright (c) 2012-2013, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /** * @file ti/ipc/Notify.h * * @brief Notification manager for IPC * * @note Notify is currently only available for SYS/BIOS. * * The Notify module manages the multiplexing/demultiplexing of software * interrupts over hardware interrupts. In order to receive notifications, * a processor registers one or more callback functions to an eventId * using Notify_registerEvent(). The Notify_registerEvent() * call (like most other Notify APIs) uses a MultiProc id and * line id to target a specific interrupt line to/from a specific processor * on a device. The Notify_eventAvailable() API may be used to query whether * an event id is available for use before registration. * * Once an event has been registered, a remote processor may send an event * using the Notify_sendEvent() call. If the event and the interrupt line * are both enabled, all callback functions registered to the event will * be called sequentially. * * A specific event may be disabled or enabled using the Notify_disableEvent() * and Notify_enableEvent() calls. An entire interrupt line may be disabled * or restored using the Notify_disable() or Notify_restore() calls. * Notify_disable() does not alter the state of individual events. * Instead, it just disables the ability of the Notify module to receive * events on the interrupt line. * * Notify APIs should never be called within an Hwi context. All API calls * should be made within main(), a Task or a Swi with the exception of * Notify_sendEvent() which may also be called within a Hwi. * * "Loopback" functionality allows Notifications to be registered * and sent locally. This is accomplished by supplying our own MultiProc id * to Notify APIs. Line id #0 is always used for local notifications. It is * important to be aware of some subtle (but important) differences between * remote and local notifications: * - Loopback callback functions will execute in the same thread in which * Notify_sendEvent() is called. This is in contrast to callback * functions that are called due to another processor's sent * notification- these 'remote' callback functions will execute in an * ISR context. * - Loopback callback functions will execute with interrupts disabled * - Disabling the local interrupt line will cause all notifications that * are sent to the local processor to be lost. By contrast, a * notification sent to an enabled event on a remote processor that has * called Notify_disable() results in a pending notifications until the * disabled processor has called Notify_restore(). * - Local notifications do not support events of different priorities. * By contrast, Notify driver implementations may correlate event ids * with varying priorities. * * In order to use any Notify APIs all necessary Notify drivers, shared memory * and interprocessor interrupts must be initialized. This is typically done * by Ipc_start(), which internally call Notify_attach(). * It is possible for a user application to call Notify_attach() directly * (before Ipc_attach() or Ipc_start()) if notifications must be set up prior * to runtime SharedRegion initialization. Refer to the documentation for * Notify_attach() for more information. * * The Notify header should be included in an application as follows: * @code * #include * @endcode */ #ifndef ti_ipc_Notify__include #define ti_ipc_Notify__include #if defined (__cplusplus) extern "C" { #endif /* ============================================================================= * All success and failure codes for the module * ============================================================================= */ /*! * @brief The resource is still in use */ #define Notify_S_BUSY (2) /*! * @brief Module already set up */ #define Notify_S_ALREADYSETUP (1) /*! * @brief Operation is successful. */ #define Notify_S_SUCCESS (0) /*! * @brief Generic failure. */ #define Notify_E_FAIL (-1) /*! * @brief Argument passed to function is invalid. */ #define Notify_E_INVALIDARG (-2) /*! * @brief Operation resulted in memory failure. */ #define Notify_E_MEMORY (-3) /*! * @brief The specified entity already exists. */ #define Notify_E_ALREADYEXISTS (-4) /*! * @brief Unable to find the specified entity. */ #define Notify_E_NOTFOUND (-5) /*! * @brief Operation timed out. */ #define Notify_E_TIMEOUT (-6) /*! * @brief Module is not initialized. */ #define Notify_E_INVALIDSTATE (-7) /*! * @brief A failure occurred in an OS-specific call */ #define Notify_E_OSFAILURE (-8) /*! * @brief The module has been already setup */ #define Notify_E_ALREADYSETUP (-9) /*! * @brief Specified resource is not available */ #define Notify_E_RESOURCE (-10) /*! * @brief Operation was interrupted. Please restart the operation */ #define Notify_E_RESTART (-11) /*! * @brief The resource is still in use */ #define Notify_E_BUSY (-12) /*! * @brief Driver corresponding to the specified eventId is not registered */ #define Notify_E_DRIVERNOTREGISTERED (-13) /*! * @brief Event not registered */ #define Notify_E_EVTNOTREGISTERED (-14) /*! * @brief Event is disabled */ #define Notify_E_EVTDISABLED (-15) /*! * @brief Remote notification is not initialized */ #define Notify_E_NOTINITIALIZED (-16) /*! * @brief Trying to illegally use a reserved event */ #define Notify_E_EVTRESERVED (-17) /* ============================================================================= * Macros * ============================================================================= */ /*! * @brief Maximum number of events supported by the Notify module */ #define Notify_MAXEVENTS (UInt16)32 /*! * @brief Maximum number of IPC interrupt lines for any pair of processors */ #define Notify_MAX_INTLINES 4u /*! * @brief This key must be provided as the upper 16 bits of the eventId when * registering for an event, if any reserved event numbers are to be * used. */ #define Notify_SYSTEMKEY ((UInt16)0xC1D2) /* ============================================================================= * Structures & Enums * ============================================================================= */ /*! * @var Notify_FnNotifyCbck * @brief Signature of any callback function that can be registered with the * Notify component. * * @param[in] procId Remote processor id * @param[in] lineId Line id * @param[in] eventId Event id (minus system key if reserved event) * @param[in] arg Argument specified in the registerEvent * @param[in] payload Payload specified in the sendEvent */ typedef Void (*Notify_FnNotifyCbck)(UInt16 , UInt16, UInt32, UArg, UInt32); /* ============================================================================= * Notify Module-wide Functions * ============================================================================= */ /*! * @brief Creates notify drivers and registers them with Notify * * This function must be called before other Notify API calls are * invoked. Performing a attach invokes a device-specific Notify * initialization routine that creates required drivers and * registers those drivers with the Notify module. If the drivers * require shared memory, a shared address must be supplied. * * Notify_attach() is typically called internally as part of the IPC * initialization sequence. Any memory required for Notify drivers * is reserved by SharedRegion and passed to Notify_attach(). However, if it * is necessary to pass a specific base address to Notify_attach() (i.e. if * the shared region is not valid yet), then Notify_attach() should be called * before Ipc_start() with this address. When Ipc_start() is eventually * called, Notify_attach() will be internally bypassed since it was directly * called by the user. * * @param[in] remoteProcId Remote processor id * @param[in] sharedAddr Shared address to use if any driver requires * shared memory * @return Notify status: * - #Notify_E_FAIL: failed to attach to remote processor * - #Notify_S_SUCCESS: successfully attach to remote processor */ Int Notify_attach(UInt16 remoteProcId, Ptr sharedAddr); /*! * @brief Disable ability to receive interrupts on an interrupt line * * This function disables a NotifyDriver from processing received * events. The key that is returned from this call must be used * in the Notify_restore() function. * * Notify supports nested disable/restore calls. The value of the returned * key is the nesting depth. * * If Notify_disable() is called upon an interrupt line that is already * disabled, then the corresponding Notify_restore() will not re-enable * notifications. Only the restore call that corresponds to the * Notify_disable() that actually disabled notifications will re-enable * notifications on the interrupt line. * * @param[in] procId Remote processor id * @param[in] lineId Line id * * @return Key that must be used in Notify_restore() * * @sa Notify_restore() */ UInt Notify_disable(UInt16 procId, UInt16 lineId); /*! * @brief Disable an event * * This function allows the disabling of a single event number * from the specified source processor. Sending to a disabled event * will return #Notify_E_EVTDISABLED on the sender if waitClear is false. * Notify_disableEvent() and Notify_enableEvent() may not be supported by all * Notify drivers. Consult the documentation for the Notify driver to determine * whether it supports this API call. * * An event is, by default, enabled upon driver initialization. * Calling Notify_disableEvent() upon an event that is already disabled * results in no change in state. * * Note that callbacks may be registered to an event or removed * from the event even while the event has been disabled. * * @param[in] procId Remote processor id * @param[in] lineId Line id * @param[in] eventId Event id * * @sa Notify_enableEvent() */ Void Notify_disableEvent(UInt16 procId, UInt16 lineId, UInt32 eventId); /*! * @brief Enable an event * * This function re-enables an event that has been previously disabled * using disableEvent(). Calling Notify_enableEvent() upon an event that is * already enabled results in no change in state. An event is, * by default, enabled upon driver initialization. * * Notify_disableEvent() and Notify_enableEvent() may not be supported by all * Notify drivers. Consult the documentation for the Notify driver to determine * whether it supports this API call. * * @param[in] procId Remote processor id * @param[in] lineId Line id * @param[in] eventId Event id * * @sa Notify_disableEvent() */ Void Notify_enableEvent(UInt16 procId, UInt16 lineId, UInt32 eventId); /*! * @brief Whether an unused event is available on an interrupt line * * This function can be used to determine whether an unused eventId for a * specific interrupt line is available for use in Notify_registerEvent() * or Notify_registerEventSingle(). This function will return TRUE if and only * if the following conditions are simultaneously TRUE: * - The corresponding interrupt line is available. Notifications over an * interrupt line to a remote processor are typically made available by * calling Notify_attach() or Ipc_attach(). * - The event is not a reserved event * - The event is a reserved event and #Notify_SYSTEMKEY has been passed * as the upper 16 bits of the 32-bit eventId argument * - No callback functions have been registered to the event * If any of the above conditions is false, this function will return FALSE. * Note that an event may still be registered using Notify_registerEvent() * while the last condition is false if the existing callback function(s) * were registered using Notify_registerEvent() (not * Notify_registerEventSingle()). * * @param[in] procId Remote processor id * @param[in] lineId Line id * @param[in] eventId Event id * * @return TRUE if an unused event is available, FALSE otherwise */ Bool Notify_eventAvailable(UInt16 procId, UInt16 lineId, UInt32 eventId); /*! * @brief Whether notification via interrupt line has been registered. * * This function will return TRUE if and only if a notify driver has been * registered for the interrupt line identified by the supplied procId and * lineId. The interrupt line corresponding to loopback functionality is * always registered. A value of FALSE indicates that either * Notify_attach() has not yet been called or that notification to the * remote processor is unsupported. * * @param[in] procId Remote processor id * @param[in] lineId Line id * * @return TRUE if registered, FALSE otherwise */ Bool Notify_intLineRegistered(UInt16 procId, UInt16 lineId); /*! * @brief Returns number of interrupt lines to remote processor * * This function returns the number of available interrupt lines to a remote * processor. * * @param[in] procId Remote processor id * * @return Number of interrupt lines */ UInt16 Notify_numIntLines(UInt16 procId); /*! @cond */ /*! * @brief Returns the amount of shared memory used by one Notify instance. * * This will typically be used internally by other IPC modules during system * initialization. The return value depends upon the base address because * of cache alignment settings. * * @param[in] sharedAddr Base address that will be passed to * Notify_attach() * * @return Shared memory required (in MAUs) */ SizeT Notify_sharedMemReq(UInt16 procId, Ptr sharedAddr); /*! @endcond */ /*! * @brief Register a callback for an event (supports multiple callbacks) * * This function registers a callback to a specific event number, * processor id and interrupt line. When the event is received by the * specified processor, the callback is called. * * The callback function prototype is of type #Notify_FnNotifyCbck. * This function must be non-blocking. * * It is important to note that multiple callbacks may be registered with * a single event. This is accomplished by simply calling * Notify_registerEvent() for each combination of callback functions and * callback arguments as needed. * * It is important to note that interrupts are disabled during the entire * duration of this function's execution. * * @param[in] procId Remote processor id * @param[in] lineId Line id (0 for most systems) * @param[in] eventId Event id * @param[in] fnNotifyCbck Pointer to callback function * @param[in] cbckArg Callback function argument * * @return Notify status: * - #Notify_S_SUCCESS: Event successfully registered * - #Notify_E_MEMORY: Failed to register due to memory error * * @sa Notify_unregisterEvent() */ Int Notify_registerEvent(UInt16 procId, UInt16 lineId, UInt32 eventId, Notify_FnNotifyCbck fnNotifyCbck, UArg cbckArg); /*! * @brief Register a single callback for an event * * This function registers a callback to a specific event number, * processor id and interrupt line. When the event is received by the * specified processor, the callback is called. * * The callback function prototype is of type #Notify_FnNotifyCbck. * The callback function must be non-blocking. * * Only one callback may be registered with this API. * * Use Notify_registerEvent() to register multiple callbacks for a single event. * * @param[in] procId Remote processor id * @param[in] lineId Line id (0 for most systems) * @param[in] eventId Event id * @param[in] fnNotifyCbck Pointer to callback function * @param[in] cbckArg Callback function argument * * @return Notify status: * - #Notify_E_ALREADYEXISTS: Event already registered * - #Notify_S_SUCCESS: Event successfully registered * * @sa Notify_unregisterEventSingle() */ Int Notify_registerEventSingle(UInt16 procId, UInt16 lineId, UInt32 eventId, Notify_FnNotifyCbck fnNotifyCbck, UArg cbckArg); /*! * @brief Restore ability to receive interrupts on an interrupt line * * This function re-enables receiving notifications on a specific interrupt * line. * * Notify supports nested disable/restore calls. The last restore call * will re-enable Notifications. * * @param[in] procId Remote processor id * @param[in] lineId Line id * @param[in] key Key returned by Notify_disable() * * @sa Notify_disable() */ Void Notify_restore(UInt16 procId, UInt16 lineId, UInt key); /*! * @brief Send an event on an interrupt line * * This function sends an event to a processor via an interrupt line * identified by a processor id and line id. A payload may be optionally * sent to the the remote processor if supported by the device. * * On the destination processor, the callback functions registered * with Notify with the associated eventId and source * processor id are called. * * For example, when using 'NotifyDriverShm', a @c waitClear value of 'TRUE' * indicates that, if an event was previously sent to the same eventId, * sendEvent should spin until the previous event has been acknowledged by the * remote processor. If @c waitClear is FALSE, a pending event with the same * eventId will be overwritten by the event currently being sent. When in * doubt, a value of TRUE should be used because notifications may be * potentially dropped when FALSE is used. When using NotifyDriverShm, a * payload should never be sent with 'waitClear = FALSE.' * * On the other hand, other notify drivers that use a FIFO to transmit events * will spin if @c waitClear is TRUE until the FIFO has enough room to accept * the event being sent. If @c waitClear is FALSE, Notify_sendEvent() will * return #Notify_E_FAIL if the FIFO does not have room for the event. * * Refer to the documentation for the Notify drivers for more information * about the effect of the @c waitClear flag in Notify_sendEvent(). * * Notify_sendEvent can be called from a Hwi context unlike other Notify APIs. * * @param[in] procId Remote processor id * @param[in] lineId Line id * @param[in] eventId Event id * @param[in] payload Payload to be sent along with the event. * @param[in] waitClear Indicates whether to spin waiting for the remote * core to process previous events * * @return Notify status: * - #Notify_E_EVTNOTREGISTERED: event has no registered callback * functions * - #Notify_E_NOTINITIALIZED: remote driver has not yet been * initialized * - #Notify_E_EVTDISABLED: remote event is disabled * - #Notify_E_TIMEOUT: timeout occurred (when waitClear is TRUE) * - #Notify_S_SUCCESS: event successfully sent */ Int Notify_sendEvent(UInt16 procId, UInt16 lineId, UInt32 eventId, UInt32 payload, Bool waitClear); /*! * @brief Remove an event listener from an event * * This function unregisters a single callback that was registered to an event * using Notify_registerEvent(). The @c procId, @c lineId, @c eventId, * @c fnNotifyCbck and @c cbckArg must exactly match with the registered one. * * This API is used to unregister events that were registered with * Notify_registerEvent(). If this is the last event, then * Notify_unregisterEventSingle() is called to completely remove the event. * * @param[in] procId Remote processor id * @param[in] lineId Line id * @param[in] eventId Event id * @param[in] fnNotifyCbck Pointer to callback function * @param[in] cbckArg Callback function argument * * @return Notify status: * - #Notify_E_NOTFOUND: event listener not found * - #Notify_S_SUCCESS: event listener unregistered * * @sa Notify_registerEvent() */ Int Notify_unregisterEvent(UInt16 procId, UInt16 lineId, UInt32 eventId, Notify_FnNotifyCbck fnNotifyCbck, UArg cbckArg); /*! * @brief Remove an event listener from an event * * This function removes a previously registered callback registered with * Notify_registerEventSingle(). The @c procId, @c lineId, and @c eventId * must exactly match the registered one. * * @param[in] procId Remote processor id * @param[in] lineId Line id * @param[in] eventId Event id that is being unregistered * * @return Notify status: * - #Notify_S_SUCCESS: event unregistered * - #Notify_E_FAIL: fail to unregister event * * @sa Notify_registerEventSingle() */ Int Notify_unregisterEventSingle(UInt16 procId, UInt16 lineId, UInt32 eventId); #if defined (__cplusplus) } #endif /* defined (__cplusplus) */ #endif /* ti_ipc_Notify__include */