/* * Copyright (c) 2011-2013, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /* * ======== Interrupt.c ======== * OMAP4430/Ducati Interrupt Manger */ #include #include #include #include #include #include "InterruptDsp.h" /* Register access method. */ #define REG16(A) (*(volatile UInt16 *) (A)) #define REG32(A) (*(volatile UInt32 *) (A)) #define HOSTINT 26 #define DSPINT 55 #define M3INT_MBX 50 #define M3INT 19 #define DSPEVENTID 5 /* Assigned mailboxes */ #define HOST_TO_SYSM3_MBX 0 /* Rx on SysM3 from Host */ #define M3_TO_HOST_MBX 1 /* Tx to Host from M3 */ #define DSP_TO_HOST_MBX 2 /* Tx to Host from DSP */ #define HOST_TO_DSP_MBX 3 /* Rx on DSP from Host */ #define SYSM3_TO_APPM3_MBX 4 /* Rx on AppM3 from Host/SysM3 */ #define MAILBOX_BASEADDR (0x4A0F4000) #define MAILBOX_MESSAGE(M) (MAILBOX_BASEADDR + 0x040 + (0x4 * M)) #define MAILBOX_STATUS(M) (MAILBOX_BASEADDR + 0x0C0 + (0x4 * M)) #define MAILBOX_REG_VAL(M) (0x1 << (2 * M)) #define MAILBOX_IRQSTATUS_CLR_DSP (MAILBOX_BASEADDR + 0x114) #define MAILBOX_IRQENABLE_SET_DSP (MAILBOX_BASEADDR + 0x118) #define MAILBOX_IRQENABLE_CLR_DSP (MAILBOX_BASEADDR + 0x11C) Hwi_FuncPtr userFxn = NULL; Void InterruptDsp_isr(UArg arg); /* ************************************************************************* * Module functions ************************************************************************* */ /*! * ======== InterruptDsp_intEnable ======== * Enable remote processor interrupt */ Void InterruptDsp_intEnable() { REG32(MAILBOX_IRQENABLE_SET_DSP) = MAILBOX_REG_VAL(HOST_TO_DSP_MBX); } /*! * ======== InterruptDsp_intDisable ======== * Disables remote processor interrupt */ Void InterruptDsp_intDisable() { REG32(MAILBOX_IRQENABLE_CLR_DSP) = MAILBOX_REG_VAL(HOST_TO_DSP_MBX); } /*! * ======== InterruptDsp_intRegister ======== */ Void InterruptDsp_intRegister(Hwi_FuncPtr fxn) { Hwi_Params hwiAttrs; UInt key; userFxn = fxn; /* Disable global interrupts */ key = Hwi_disable(); /* * DSP interrupts are edge-triggered, so clear the interrupt status to * regenerate an interrupt if there are some messages sent prior to * booting the DSP. */ REG32(MAILBOX_IRQSTATUS_CLR_DSP) = MAILBOX_REG_VAL(HOST_TO_DSP_MBX); Hwi_Params_init(&hwiAttrs); hwiAttrs.eventId = DSPINT; Hwi_create(DSPEVENTID, (Hwi_FuncPtr)InterruptDsp_isr, &hwiAttrs, NULL); /* Enable the interrupt */ Wugen_enableEvent(DSPINT); Hwi_enableInterrupt(DSPEVENTID); /* Enable the mailbox interrupt to the M3 core */ InterruptDsp_intEnable(); /* Restore global interrupts */ Hwi_restore(key); } /*! * ======== InterruptDsp_intSend ======== * Send interrupt to the remote processor */ Void InterruptDsp_intSend(UInt16 remoteProcId, UArg arg) { static Bool configured = FALSE; static UInt16 sysm3ProcId = MultiProc_INVALIDID; static UInt16 appm3ProcId = MultiProc_INVALIDID; static UInt16 hostProcId = MultiProc_INVALIDID; static UInt16 dspProcId = MultiProc_INVALIDID; if (!configured) { hostProcId = MultiProc_getId("HOST"); dspProcId = MultiProc_getId("DSP"); sysm3ProcId = MultiProc_getId("CORE0"); appm3ProcId = MultiProc_getId("CORE1"); configured = TRUE; } if (remoteProcId == sysm3ProcId) { REG32(MAILBOX_MESSAGE(HOST_TO_SYSM3_MBX)) = arg; } else if (remoteProcId == appm3ProcId) { REG32(MAILBOX_MESSAGE(SYSM3_TO_APPM3_MBX)) = arg; } else if (remoteProcId == hostProcId) { REG32(MAILBOX_MESSAGE(DSP_TO_HOST_MBX)) = arg; } else if (remoteProcId == dspProcId) { REG32(MAILBOX_MESSAGE(HOST_TO_DSP_MBX)) = arg; } else { /* Should never get here */ Assert_isTrue(FALSE, NULL); } } /*! * ======== InterruptDsp_intClear ======== * Clear interrupt and return payload */ UInt InterruptDsp_intClear() { UInt arg = INVALIDPAYLOAD; if (REG32(MAILBOX_STATUS(HOST_TO_DSP_MBX)) != 0) { /* If there is a message, return the argument to the caller */ arg = REG32(MAILBOX_MESSAGE(HOST_TO_DSP_MBX)); REG32(MAILBOX_IRQSTATUS_CLR_DSP) = MAILBOX_REG_VAL(HOST_TO_DSP_MBX); } return (arg); } /*! * ======== InterruptDsp_isr ======== */ Void InterruptDsp_isr(UArg arg) { UArg payload; payload = InterruptDsp_intClear(); if (payload != (UInt)INVALIDPAYLOAD) { userFxn(payload); } }