/* * Copyright (c) 2011-2019 Texas Instruments Incorporated - http://www.ti.com * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /** ============================================================================ * @file VirtQueue.c * * @brief Virtio Queue implementation for BIOS * * Differences between BIOS version and Linux kernel (include/linux/virtio.h): * - Renamed module from virtio.h to VirtQueue_Object.h to match the API prefixes; * - BIOS (XDC) types and CamelCasing used; * - virtio_device concept removed (i.e, assumes no containing device); * - simplified scatterlist from Linux version; * - VirtQueue_Objects are created statically here, so just added a VirtQueue_Object_init() * fxn to take the place of the Virtio vring_new_virtqueue() API; * - The notify function is implicit in the implementation, and not provided * by the client, as it is in Linux virtio. * * All VirtQueue operations can be called in any context. * * The virtio header should be included in an application as follows: * @code * #include * @endcode * */ #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include "package/internal/VirtQueue.xdc.h" #include #include #include /* Used for defining the size of the virtqueue registry */ #define NUM_QUEUES 2 #define DIV_ROUND_UP(n,d) (((n) + (d) - 1) / (d)) #define RP_MSG_BUFS_SPACE (VirtQueue_RP_MSG_NUM_BUFS * RPMSG_BUF_SIZE * 2) /* With 256 buffers, our vring will occupy 3 pages */ #define RP_MSG_RING_SIZE ((DIV_ROUND_UP(vring_size(VirtQueue_RP_MSG_NUM_BUFS, \ VirtQueue_RP_MSG_VRING_ALIGN), VirtQueue_PAGE_SIZE)) * VirtQueue_PAGE_SIZE) /* The total IPC space needed to communicate with a remote processor */ #define RPMSG_IPC_MEM (RP_MSG_BUFS_SPACE + 2 * RP_MSG_RING_SIZE) #define ID_DSP_TO_A9 0 #define ID_A9_TO_DSP 1 extern volatile cregister UInt DNUM; static VirtQueue_Object *queueRegistry[NUM_QUEUES] = {NULL}; /* static inline */ Void * mapPAtoVA(UInt pa) { Void *va; UInt offset; offset = (DNUM * VirtQueue_VRING_OFFSET); va = (Void *)((pa & 0x000fffffU) | offset | 0xa0000000U); return va; } static inline UInt mapVAtoPA(Void * va) { return ((UInt)va & 0x000fffffU) | 0xe1000000U; } /* * ======== VirtQueue_init ======== */ Void VirtQueue_init() { extern cregister volatile UInt DNUM; UInt16 procId; /* * VirtQueue_init() must be called before MultiProcSetup_init(). * (Check the xdc_runtime_Startup_firstFxns__A in the XDC generated code) * Abort if the procId has already been set. We must set it! */ if (MultiProc_self() != MultiProc_INVALIDID) { System_abort("VirtQueue_init(): MultiProc_self already set!"); return; } procId = DNUM + 1; /* Set the local ID */ MultiProc_setLocalId(procId); } /* * ======== VirtQueue_Instance_init ======== */ Int VirtQueue_Instance_init(VirtQueue_Object *vq, UInt16 remoteProcId, const VirtQueue_Params *params, Error_Block *eb) { void *vringAddr = NULL; VirtQueue_module->traceBufPtr = Resource_getTraceBufPtr(); /* Create the thread protection gate */ vq->gateH = GateAll_create(NULL, eb); if (Error_check(eb)) { Log_error0("VirtQueue_create: could not create gate object"); Error_raise(NULL, Error_E_generic, 0, 0); return(0); } vq->vringPtr = Memory_calloc(NULL, sizeof(struct vring), 0, eb); Assert_isTrue((vq->vringPtr != NULL), NULL); vq->callback = params->callback; vq->id = params->vqId; vq->procId = remoteProcId; vq->last_avail_idx = 0; vq->last_used_idx = 0; vq->num_free = VirtQueue_RP_MSG_NUM_BUFS; vq->swiHandle = params->swiHandle; switch (vq->id) { case ID_DSP_TO_A9: vringAddr = (struct vring *) (VirtQueue_CORE0_MEM_VRING0 + (DNUM * VirtQueue_VRING_OFFSET)); break; case ID_A9_TO_DSP: vringAddr = (struct vring *) (VirtQueue_CORE0_MEM_VRING1 + (DNUM * VirtQueue_VRING_OFFSET)); break; default: Log_error1("VirtQueue_create: invalid vq->id: %d", vq->id); GateAll_delete(&vq->gateH); Memory_free(NULL, vq->vringPtr, sizeof(struct vring)); Error_raise(NULL, Error_E_generic, 0, 0); return(0); } Log_print3(Diags_USER1, "vring: %d 0x%x (0x%x)\n", vq->id, (IArg)vringAddr, RP_MSG_RING_SIZE); vring_init(vq->vringPtr, VirtQueue_RP_MSG_NUM_BUFS, vringAddr, VirtQueue_RP_MSG_VRING_ALIGN); queueRegistry[vq->id] = vq; return(0); } /* * ======== VirtQueue_kick ======== */ Void VirtQueue_kick(VirtQueue_Handle vq) { struct vring *vring = vq->vringPtr; IInterrupt_IntInfo intInfo; /* For now, simply interrupt remote processor */ if (vring->avail->flags & VRING_AVAIL_F_NO_INTERRUPT) { Log_print0(Diags_USER1, "VirtQueue_kick: no kick because of VRING_AVAIL_F_NO_INTERRUPT\n"); return; } Log_print2(Diags_USER1, "VirtQueue_kick: Sending interrupt to proc %d with payload 0x%x\n", (IArg)vq->procId, (IArg)vq->id); intInfo.localIntId = Interrupt_SRCS_BITPOS_CORE0; Interrupt_intSend(vq->procId, &intInfo, vq->id); } /* * ======== VirtQueue_addUsedBuf ======== */ Int VirtQueue_addUsedBuf(VirtQueue_Handle vq, Int16 head, Int len) { struct vring_used_elem *used; struct vring *vring = vq->vringPtr; IArg key; key = GateAll_enter(vq->gateH); if (((unsigned int)head > vring->num) || (head < 0)) { Error_raise(NULL, Error_E_generic, 0, 0); } else { /* * The virtqueue contains a ring of used buffers. Get a pointer to the * next entry in that used ring. */ used = &vring->used->ring[vring->used->idx % vring->num]; used->id = head; used->len = len; vring->used->idx++; } GateAll_leave(vq->gateH, key); return (0); } /* * ======== VirtQueue_addAvailBuf ======== */ Int VirtQueue_addAvailBuf(VirtQueue_Object *vq, Void *buf) { UInt16 avail; struct vring *vring = vq->vringPtr; IArg key; key = GateAll_enter(vq->gateH); if (vq->num_free == 0) { /* There's no more space */ Error_raise(NULL, Error_E_generic, 0, 0); } else { vq->num_free--; avail = vring->avail->idx++ % vring->num; vring->desc[avail].addr = mapVAtoPA(buf); vring->desc[avail].len = RPMSG_BUF_SIZE; } GateAll_leave(vq->gateH, key); return (vq->num_free); } /* * ======== VirtQueue_getUsedBuf ======== */ Void *VirtQueue_getUsedBuf(VirtQueue_Object *vq) { UInt16 head; Void *buf; struct vring *vring = vq->vringPtr; IArg key; key = GateAll_enter(vq->gateH); /* There's nothing available? */ if (vq->last_used_idx == vring->used->idx) { buf = NULL; } else { head = vring->used->ring[vq->last_used_idx % vring->num].id; vq->last_used_idx++; vq->num_free++; buf = mapPAtoVA(vring->desc[head].addr); } GateAll_leave(vq->gateH, key); return (buf); } /* * ======== VirtQueue_getAvailBuf ======== */ Int16 VirtQueue_getAvailBuf(VirtQueue_Handle vq, Void **buf, Int *len) { Int16 head; struct vring *vring = vq->vringPtr; IArg key; key = GateAll_enter(vq->gateH); Log_print6(Diags_USER1, "getAvailBuf vq: 0x%x %d %d %d 0x%x 0x%x\n", (IArg)vq, vq->last_avail_idx, vring->avail->idx, vring->num, (IArg)&vring->avail, (IArg)vring->avail); /* Clear flag here to avoid race condition with remote processor. * This is a negative flag, clearing it means that we want to * receive an interrupt when a buffer has been added to the pool. */ vring->used->flags &= ~VRING_USED_F_NO_NOTIFY; /* There's nothing available? */ if (vq->last_avail_idx == vring->avail->idx) { head = (-1); } else { /* No need to be kicked about added buffers anymore */ vring->used->flags |= VRING_USED_F_NO_NOTIFY; /* * Grab the next descriptor number they're advertising, and increment * the index we've seen. */ head = vring->avail->ring[vq->last_avail_idx++ % vring->num]; *buf = mapPAtoVA(vring->desc[head].addr); *len = vring->desc[head].len; } GateAll_leave(vq->gateH, key); return (head); } /* * ======== VirtQueue_isr ======== * Note 'msg' is ignored: it is only used where there is a mailbox payload. */ static Void VirtQueue_isr(UArg msg) { VirtQueue_Object *vq; Log_print1(Diags_USER1, "VirtQueue_isr received msg = 0x%x\n", msg); vq = queueRegistry[0]; if (vq) { vq->callback(vq); } vq = queueRegistry[1]; if (vq) { vq->callback(vq); } } /* * ======== VirtQueue_startup ======== */ Void VirtQueue_startup(UInt16 remoteProcId, Bool isHost) { IInterrupt_IntInfo intInfo; intInfo.intVectorId = Interrupt_DSPINT; intInfo.localIntId = Interrupt_SRCS_BITPOS_HOST; /* * Wait for first kick from host, which happens to coincide with the * priming of host's receive buffers, indicating host is ready to send. * Since interrupt is cleared, we throw away this first kick, which is * OK since we don't process this in the ISR anyway. */ Log_print0(Diags_USER1, "VirtQueue_startup: Polling for host int...\n"); while (!Interrupt_checkAndClear(remoteProcId, &intInfo)); Interrupt_intRegister(remoteProcId, &intInfo, (Fxn)VirtQueue_isr, 0); Log_print0(Diags_USER1, "Passed VirtQueue_startup\n"); } /* By convention, Host VirtQueues host are the even number in the pair */ Bool VirtQueue_isSlave(VirtQueue_Handle vq) { return (vq->id & 0x1); } Bool VirtQueue_isHost(VirtQueue_Handle vq) { return (~(vq->id & 0x1)); } UInt16 VirtQueue_getId(VirtQueue_Handle vq) { return (vq->id); } Swi_Handle VirtQueue_getSwiHandle(VirtQueue_Handle vq) { return (vq->swiHandle); } #define CACHE_WB_TICK_PERIOD 5 /* * ======== VirtQueue_cacheWb ======== * * Used for flushing SysMin trace buffer. */ Void VirtQueue_cacheWb() { static UInt32 oldticks = 0; UInt32 newticks; newticks = Clock_getTicks(); if (newticks - oldticks < (UInt32)CACHE_WB_TICK_PERIOD) { /* Don't keep flushing cache */ return; } oldticks = newticks; /* Flush the cache of the SysMin buffer only: */ Assert_isTrue((VirtQueue_module->traceBufPtr != NULL), NULL); Cache_wb(VirtQueue_module->traceBufPtr, SysMin_bufSize, Cache_Type_ALL, FALSE); }