/* * Copyright (c) 2011-2015, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /** ============================================================================ * @file VirtQueue.c * * @brief Virtio Queue implementation for BIOS * * Differences between BIOS version and Linux kernel (include/linux/virtio.h): * - Renamed module from virtio.h to VirtQueue_Object.h to match the API prefixes; * - BIOS (XDC) types and CamelCasing used; * - virtio_device concept removed (i.e, assumes no containing device); * - simplified scatterlist from Linux version; * - VirtQueue_Objects are created statically here, so just added a VirtQueue_Object_init() * fxn to take the place of the Virtio vring_new_virtqueue() API; * - The notify function is implicit in the implementation, and not provided * by the client, as it is in Linux virtio. * * All VirtQueue operations can be called in any context. * * The virtio header should be included in an application as follows: * @code * #include * @endcode * */ /* this define must precede inclusion of any xdc header file */ #define Registry_CURDESC ti_ipc_family_vayu__Desc #define MODULE_NAME "ti.ipc.family.vayu.VirtQueue" #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include "InterruptProxy.h" #include "VirtQueue.h" /* * The following three VIRTIO_* defines must match those in * /include/uapi/linux/virtio_config.h */ #define VIRTIO_CONFIG_S_ACKNOWLEDGE 1 #define VIRTIO_CONFIG_S_DRIVER 2 #define VIRTIO_CONFIG_S_DRIVER_OK 4 #define VRING_BUFS_PRIMED (VIRTIO_CONFIG_S_ACKNOWLEDGE | \ VIRTIO_CONFIG_S_DRIVER | VIRTIO_CONFIG_S_DRIVER_OK) /* Used for defining the size of the virtqueue registry */ #define NUM_QUEUES 2 /* * Size of the virtqueues (expressed in number of buffers supported, * and must be power of two) */ #define VQ_SIZE 256 /* * enum - Predefined Mailbox Messages * * @RP_MSG_MBOX_READY: informs the slave that we're up and running. will be * followed by another mailbox message that carries the HOST's virtual address * of the shared buffer. This would allow the HOST's drivers to send virtual * addresses of the buffers. * * @RP_MSG_MBOX_STATE_CHANGE: informs the receiver that there is an inbound * message waiting in its own receive-side vring. please note that currently * this message is optional: alternatively, one can explicitly send the index * of the triggered virtqueue itself. the preferred approach will be decided * as we progress and experiment with those design ideas. * * @RP_MSG_MBOX_CRASH: this message indicates that the BIOS side is unhappy * * @RP_MBOX_ECHO_REQUEST: this message requests the remote processor to reply * with RP_MBOX_ECHO_REPLY * * @RP_MBOX_ECHO_REPLY: this is a reply that is sent when RP_MBOX_ECHO_REQUEST * is received. * * @RP_MBOX_ABORT_REQUEST: tells the M3 to crash on demand * * @RP_MBOX_BOOTINIT_DONE: this message indicates the BIOS side has reached a * certain state during the boot process. This message is used to inform the * host that the basic BIOS initialization is done, and lets the host use this * notification to perform certain actions. */ enum { RP_MSG_MBOX_READY = (Int)0xFFFFFF00, RP_MSG_MBOX_STATE_CHANGE = (Int)0xFFFFFF01, RP_MSG_MBOX_CRASH = (Int)0xFFFFFF02, RP_MBOX_ECHO_REQUEST = (Int)0xFFFFFF03, RP_MBOX_ECHO_REPLY = (Int)0xFFFFFF04, RP_MBOX_ABORT_REQUEST = (Int)0xFFFFFF05, RP_MSG_FLUSH_CACHE = (Int)0xFFFFFF06, RP_MSG_BOOTINIT_DONE = (Int)0xFFFFFF07, RP_MSG_HIBERNATION = (Int)0xFFFFFF10, RP_MSG_HIBERNATION_FORCE = (Int)0xFFFFFF11, RP_MSG_HIBERNATION_ACK = (Int)0xFFFFFF12, RP_MSG_HIBERNATION_CANCEL = (Int)0xFFFFFF13 }; #define DIV_ROUND_UP(n,d) (((n) + (d) - 1) / (d)) #define RP_MSG_NUM_BUFS (VQ_SIZE) /* must be power of two */ #define RP_MSG_BUF_SIZE (512) #define RP_MSG_BUFS_SPACE (RP_MSG_NUM_BUFS * RP_MSG_BUF_SIZE * 2) #define PAGE_SIZE (4096) /* * The alignment to use between consumer and producer parts of vring. * Note: this is part of the "wire" protocol. If you change this, you need * to update your BIOS image as well */ #define RP_MSG_VRING_ALIGN (4096) /* With 256 buffers, our vring will occupy 3 pages */ #define RP_MSG_RING_SIZE ((DIV_ROUND_UP(vring_size(RP_MSG_NUM_BUFS, \ RP_MSG_VRING_ALIGN), PAGE_SIZE)) * PAGE_SIZE) /* The total IPC space needed to communicate with a remote processor */ #define RPMSG_IPC_MEM (RP_MSG_BUFS_SPACE + 2 * RP_MSG_RING_SIZE) typedef struct VirtQueue_Object { /* Id for this VirtQueue_Object */ UInt16 id; /* The function to call when buffers are consumed (can be NULL) */ VirtQueue_callback callback; /* Shared state */ struct vring vring; /* Number of free buffers */ UInt16 num_free; /* Last available index; updated by VirtQueue_getAvailBuf */ UInt16 last_avail_idx; /* Will eventually be used to kick remote processor */ UInt16 procId; /* Gate to protect from multiple threads */ GateHwi_Handle gateH; /* Base phys addr - used for quick pa/va translations */ UInt32 basePa; /* Base virt addr - used for quick pa/va translations */ UInt32 baseVa; } VirtQueue_Object; /* module diags mask */ Registry_Desc Registry_CURDESC; static struct VirtQueue_Object *queueRegistry[NUM_QUEUES] = {NULL}; static UInt16 hostProcId; #define DSPEVENTID 5 IInterrupt_IntInfo intInfo; /*! * ======== _VirtQueue_init ======== * * This function adds the VirtQueue "module" to the Registry so that * DIAGS will work with this non-XDC module. * Since VirtQueue_init is not called by XDC-VirtQueue module clients, this * function is called in the first VirtQueue fxn called: VirtQueue_create. */ static Void _VirtQueue_init() { static int initialized = 0; if (!initialized) { Registry_Result result; /* register with xdc.runtime to get a diags mask */ result = Registry_addModule(&Registry_CURDESC, MODULE_NAME); Assert_isTrue(result == Registry_SUCCESS, (Assert_Id)NULL); initialized = 1; } } static inline Void * _VirtQueue_getVA(VirtQueue_Handle vq, UInt32 pa) { return (Void *)(pa - vq->basePa + vq->baseVa); } /*! * ======== VirtQueue_kick ======== */ Void VirtQueue_kick(VirtQueue_Handle vq) { /* For now, simply interrupt remote processor */ if (vq->vring.avail->flags & VRING_AVAIL_F_NO_INTERRUPT) { Log_print0(Diags_USER1, "VirtQueue_kick: no kick because of VRING_AVAIL_F_NO_INTERRUPT\n"); return; } Log_print2(Diags_USER1, "VirtQueue_kick: Sending interrupt to proc %d with payload 0x%x\n", (IArg)vq->procId, (IArg)vq->id); InterruptProxy_intSend(vq->procId, NULL, vq->id); } /*! * ======== VirtQueue_addUsedBuf ======== */ Int VirtQueue_addUsedBuf(VirtQueue_Handle vq, Int16 head, Int len) { struct vring_used_elem *used; IArg key; key = GateHwi_enter(vq->gateH); if ((head > vq->vring.num) || (head < 0)) { GateHwi_leave(vq->gateH, key); Error_raise(NULL, Error_E_generic, 0, 0); } /* * The virtqueue contains a ring of used buffers. Get a pointer to the * next entry in that used ring. */ used = &vq->vring.used->ring[vq->vring.used->idx % vq->vring.num]; used->id = head; used->len = len; vq->vring.used->idx++; GateHwi_leave(vq->gateH, key); return (0); } /*! * ======== VirtQueue_getAvailBuf ======== */ Int16 VirtQueue_getAvailBuf(VirtQueue_Handle vq, Void **buf, Int *len) { Int16 head; IArg key; key = GateHwi_enter(vq->gateH); Log_print6(Diags_USER1, "getAvailBuf vq: 0x%x %d %d %d 0x%x 0x%x\n", (IArg)vq, vq->last_avail_idx, vq->vring.avail->idx, vq->vring.num, (IArg)&vq->vring.avail, (IArg)vq->vring.avail); /* Clear flag here to avoid race condition with remote processor. * This is a negative flag, clearing it means that we want to * receive an interrupt when a buffer has been added to the pool. */ vq->vring.used->flags &= ~VRING_USED_F_NO_NOTIFY; /* There's nothing available? */ if (vq->last_avail_idx == vq->vring.avail->idx) { head = (-1); } else { /* No need to be kicked about added buffers anymore */ vq->vring.used->flags |= VRING_USED_F_NO_NOTIFY; /* * Grab the next descriptor number they're advertising, and increment * the index we've seen. */ head = vq->vring.avail->ring[vq->last_avail_idx++ % vq->vring.num]; *buf = _VirtQueue_getVA(vq, vq->vring.desc[head].addr); *len = vq->vring.desc[head].len; } GateHwi_leave(vq->gateH, key); return (head); } /*! * ======== VirtQueue_disableCallback ======== */ Void VirtQueue_disableCallback(VirtQueue_Object *vq) { /* TODO */ Log_print0(Diags_USER1, "VirtQueue_disableCallback called."); } /*! * ======== VirtQueue_enableCallback ======== */ Bool VirtQueue_enableCallback(VirtQueue_Object *vq) { Log_print0(Diags_USER1, "VirtQueue_enableCallback called."); /* TODO */ return (FALSE); } /*! * ======== VirtQueue_isr ======== * Note 'arg' is ignored: it is the Hwi argument, not the mailbox argument. */ Void VirtQueue_isr(UArg msg) { VirtQueue_Object *vq; msg = InterruptProxy_intClear(hostProcId, &intInfo); Log_print1(Diags_USER1, "VirtQueue_isr received msg = 0x%x\n", msg); switch(msg) { case (UInt)RP_MSG_MBOX_READY: return; case (UInt)RP_MBOX_ECHO_REQUEST: InterruptProxy_intSend(hostProcId, NULL, (UInt)(RP_MBOX_ECHO_REPLY)); return; case (UInt)RP_MBOX_ABORT_REQUEST: { /* Suppress Coverity Error: FORWARD_NULL: */ /* coverity[assign_zero] */ Fxn f = (Fxn)0x0; Log_print0(Diags_USER1, "Crash on demand ...\n"); /* coverity[var_deref_op] */ f(); } return; case (UInt)RP_MSG_FLUSH_CACHE: Cache_wbAll(); return; case (UInt)RP_MSG_HIBERNATION: if (IpcPower_canHibernate() == FALSE) { InterruptProxy_intSend(hostProcId, NULL, (UInt)RP_MSG_HIBERNATION_CANCEL); return; } /* Fall through */ case (UInt)RP_MSG_HIBERNATION_FORCE: /* Ack request */ InterruptProxy_intSend(hostProcId, NULL, (UInt)RP_MSG_HIBERNATION_ACK); IpcPower_suspend(); return; default: /* * If the message isn't one of the above, it's either part of the * 2-message synchronization sequence or it a virtqueue message */ break; } /* Don't let unknown messages to pass as a virtqueue index */ if (msg >= NUM_QUEUES) { /* Adding print here deliberately, we should never see this */ System_printf("VirtQueue_isr: Invalid mailbox message 0x%x " "received\n", msg); return; } vq = queueRegistry[msg]; if (vq) { vq->callback(vq); } } /*! * ======== VirtQueue_create ======== */ VirtQueue_Handle VirtQueue_create(UInt16 remoteProcId, VirtQueue_Params *params, Error_Block *eb) { VirtQueue_Object *vq; Void *vringAddr; Int result; /* Perform initialization we can't do in Instance_init (being non-XDC): */ _VirtQueue_init(); vq = Memory_alloc(NULL, sizeof(VirtQueue_Object), 0, eb); if (NULL == vq) { return (NULL); } /* Create the thread protection gate */ vq->gateH = GateHwi_create(NULL, eb); if (Error_check(eb)) { Log_error0("VirtQueue_create: could not create gate object"); Memory_free(NULL, vq, sizeof(VirtQueue_Object)); return (NULL); } vq->callback = params->callback; vq->id = params->vqId; vq->procId = remoteProcId; vq->last_avail_idx = 0; switch (vq->id) { /* IPC transport vrings */ case ID_SELF_TO_HOST: case ID_HOST_TO_SELF: vq->basePa = (UInt32)Resource_getVringDA(vq->id); Assert_isTrue(vq->basePa != NULL, NULL); result = Resource_physToVirt(vq->basePa, &(vq->baseVa)); Assert_isTrue(result == Resource_S_SUCCESS, (Assert_Id)NULL); vringAddr = (Void *)vq->baseVa; break; default: GateHwi_delete(&vq->gateH); Memory_free(NULL, vq, sizeof(VirtQueue_Object)); return (NULL); } Log_print3(Diags_USER1, "vring: %d 0x%x (0x%x)\n", vq->id, (IArg)vringAddr, RP_MSG_RING_SIZE); /* See coverity related comment in vring_init() */ /* coverity[overrun-call] */ vring_init(&(vq->vring), RP_MSG_NUM_BUFS, vringAddr, RP_MSG_VRING_ALIGN); /* * Don't trigger a mailbox message every time MPU makes another buffer * available */ if (vq->procId == hostProcId) { vq->vring.used->flags &= ~VRING_USED_F_NO_NOTIFY; } queueRegistry[vq->id] = vq; return (vq); } /*! * ======== VirtQueue_startup ======== */ Void VirtQueue_startup() { hostProcId = MultiProc_getId("HOST"); #ifdef DSP intInfo.intVectorId = DSPEVENTID; #endif /* Initilize the IpcPower module */ IpcPower_init(); /* * Wait for HLOS (Virtio device) to indicate that priming of host's receive * buffers is complete, indicating that host is ready to send. * * Though this is a Linux Virtio configuration status, it must be * implemented by each non-Linux HLOS as well. */ Log_print1(Diags_USER1, "VirtQueue_startup: VDEV status: 0x%x\n", Resource_getVdevStatus(VIRTIO_ID_RPMSG)); Log_print0(Diags_USER1, "VirtQueue_startup: Polling VDEV status...\n"); while (Resource_getVdevStatus(VIRTIO_ID_RPMSG) != VRING_BUFS_PRIMED); Log_print1(Diags_USER1, "VirtQueue_startup: VDEV status: 0x%x\n", Resource_getVdevStatus(VIRTIO_ID_RPMSG)); InterruptProxy_intRegister(hostProcId, &intInfo, (Fxn)VirtQueue_isr, NULL); Log_print0(Diags_USER1, "Passed VirtQueue_startup\n"); } /*! * ======== VirtQueue_postCrashToMailbox ======== */ Void VirtQueue_postCrashToMailbox(Void) { InterruptProxy_intSend(0, NULL, (UInt)RP_MSG_MBOX_CRASH); } #define CACHE_WB_TICK_PERIOD 5 /*! * ======== VirtQueue_cacheWb ======== * * Used for flushing SysMin trace buffer. */ Void VirtQueue_cacheWb() { static UInt32 oldticks = 0; UInt32 newticks; newticks = Clock_getTicks(); if (newticks - oldticks < (UInt32)CACHE_WB_TICK_PERIOD) { /* Don't keep flushing cache */ return; } oldticks = newticks; /* Flush the cache */ Cache_wbAll(); }