/* * Copyright (c) 2012-2013, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /** * @file ti/ipc/mm/MmRpc.h * * @brief Multi-Media derived Remote Procedure Call * * @note MmRpc is currently only available for Linux and QNX. * * */ #ifndef ti_ipc_mm_MmRpc__include #define ti_ipc_mm_MmRpc__include /* add includes here */ #include #include #if defined(__cplusplus) extern "C" { #endif /*! * @brief Operation is successful */ #define MmRpc_S_SUCCESS (0) /*! * @brief Operation failed */ #define MmRpc_E_FAIL (-1) /*! * @brief Invalid parameter type */ #define MmRpc_E_INVALIDPARAM (-2) /*! * @brief Size of parameter array in function context structure */ #define MmRpc_MAX_PARAMS (10) /*! * @brief Maximum size of translation array in function context structure */ #define MmRpc_MAX_TRANSLATIONS (1024) /*! * @brief Macro for computing offset to a field of a structure. * * @code * struct foobar { * int a; * int *p; * }; * * struct foobar *sp = ...; * offset = MmRpc_OFFSET(sp, &sp->p); * struct foobar st = ...; * offset = MmRpc_OFFSET(&st, &st.p); * @endcode */ #define MmRpc_OFFSET(base, field) ((unsigned int)(field)-(unsigned int)(base)) /*! * @brief MmRpc_Handle type */ typedef struct MmRpc_Object *MmRpc_Handle; /*! * @brief MmRpc_ParamType enum */ typedef enum { MmRpc_ParamType_Scalar = 1, /*!< pass by value */ MmRpc_ParamType_Ptr, /*!< data pointer */ MmRpc_ParamType_Elem /*!< array element */ } MmRpc_ParamType; /*! * @brief MmRpc_Param type */ typedef struct { MmRpc_ParamType type; /*!< parameter type */ union { struct { size_t size; /*!< size of the data */ size_t data; /*!< data (pass by value)*/ } scalar; struct { size_t size; /*!< size of the data referenced */ size_t addr; /*!< pointer value */ size_t handle; /*!< memory allocator handle */ } ptr; #if 0 /* TBD */ struct { size_t size; /*!< size of the array element */ size_t offset; /*!< offset to current array element */ size_t base; /*!< base address of array */ size_t handle; /*!< memory allocator handle */ } elem; #endif } param; } MmRpc_Param; typedef struct { uint32_t index; /*!< parameter index to base pointer */ ptrdiff_t offset; /*!< offset from the base address to pointer */ size_t base; /*!< user virtual address */ size_t handle; /*!< memory allocator handle */ } MmRpc_Xlt; /*! * @brief Function call context structure */ typedef struct { uint32_t fxn_id; /*!< function id to call */ uint32_t num_params; /*!< number of parameters in params array */ MmRpc_Param params[MmRpc_MAX_PARAMS]; /*!< the array of parameters */ uint32_t num_xlts; /*!< number of translations in xltAry */ MmRpc_Xlt * xltAry; /*!< array of translations */ } MmRpc_FxnCtx; /*! * @brief Instance create parameters */ typedef struct { int reserved; } MmRpc_Params; /*! * @brief Invoke a remote procedure call * */ int MmRpc_call(MmRpc_Handle handle, MmRpc_FxnCtx *ctx, int32_t *ret); /*! * @brief Create an MmRpc instance * */ int MmRpc_create(const char *service, const MmRpc_Params *params, MmRpc_Handle *handlPtr); /*! * @brief Delete an MmRpc instance * */ int MmRpc_delete(MmRpc_Handle *handlePtr); /*! * @brief Initialize the instance create parameter structure * */ void MmRpc_Params_init(MmRpc_Params *params); #if defined(__cplusplus) } #endif #endif /* ti_ipc_mm_MmRpc__include */