/* * Copyright (c) 2011-2013, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /** ============================================================================ * @file RPMessage.c * * @brief A simple copy-based MessageQ, to work with Linux virtio_rp_msg. * * Notes: * - The logic in the functions for sending (_put()) and receiving _swiFxn() * depend on the role (host or slave) the processor is playing in the * asymmetric virtio I/O. * - The host always adds *available* buffers to send/receive, while the slave * always adds *used* buffers to send/receive. * - The logic is summarized below: * * Host: * - Prime vq_host with avail bufs, and kick vq_host so slave can send. * - To send a buffer to the slave processor: * allocate a tx buffer, or get_used_buf(vq_slave); * >> copy data into buf << * add_avail_buf(vq_slave); * kick(vq_slave); * - To receive buffer from slave processor: * get_used_buf(vq_host); * >> empty data from buf << * add_avail_buf(vq_host); * kick(vq_host); * * Slave: * - To receive buffer from the host: * get_avail_buf(vq_slave); * >> empty data from buf << * add_used_buf(vq_slave); * kick(vq_slave); * - To send buffer to the host: * get_avail_buf(vq_host); * >> copy data into buf << * add_used_buf(vq_host); * kick(vq_host); * * ============================================================================ */ /* this define must precede inclusion of any xdc header file */ #define Registry_CURDESC ti_ipc_rpmsg_RPMessage__Desc #define MODULE_NAME "ti.ipc.rpmsg.RPMessage" #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include "_VirtQueue.h" /* TBD: VirtQueue.h needs to somehow get factored out of family directory .*/ #if defined(OMAPL138) #include #elif defined(TCI6614) #include #elif defined(TCI6638) #include #elif defined(OMAP5) #include #elif defined(VAYU) #include #else #error unknown processor! #endif /* ============================================================================= * Structures & Enums * ============================================================================= */ /* Various arbitrary limits: */ #define MAXMESSAGEQOBJECTS 256 #define MAXMESSAGEBUFFERS 512 #define MSGBUFFERSIZE 512 // Max payload + sizeof(ListElem) #define MAXHEAPSIZE (MAXMESSAGEBUFFERS * MSGBUFFERSIZE) #define HEAPALIGNMENT 8 /* The RPMessage Object */ typedef struct RPMessage_Object { UInt32 queueId; /* Unique id (procId | queueIndex) */ Semaphore_Handle semHandle; /* I/O Completion */ RPMessage_callback cb; /* RPMessage Callback */ UArg arg; /* Callback argument */ List_Handle queue; /* Queue of pending messages */ Bool unblocked; /* Use with signal to unblock _receive() */ } RPMessage_Object; /* Module_State */ typedef struct RPMessage_Module { /* Instance gate: */ GateAll_Handle gateH; /* Array of messageQObjects in the system: */ struct RPMessage_Object *msgqObjects[MAXMESSAGEQOBJECTS]; /* Heap from which to allocate free messages for copying: */ HeapBuf_Handle heap; } RPMessage_Module; /* Message Header: Must match mp_msg_hdr in virtio_rp_msg.h on Linux side. */ typedef struct RPMessage_MsgHeader { Bits32 srcAddr; /* source endpoint addr */ Bits32 dstAddr; /* destination endpoint addr */ Bits32 reserved; /* reserved */ Bits16 dataLen; /* data length */ Bits16 flags; /* bitmask of different flags */ UInt8 payload[]; /* Data payload */ } RPMessage_MsgHeader; typedef RPMessage_MsgHeader *RPMessage_Msg; /* Element to hold payload copied onto receiver's queue. */ typedef struct Queue_elem { List_Elem elem; /* Allow list linking. */ UInt len; /* Length of data */ UInt32 src; /* Src address/endpt of the msg */ Char data[]; /* payload begins here */ } Queue_elem; /* Combine transport related objects into a struct for future migration: */ typedef struct RPMessage_Transport { Swi_Handle swiHandle; VirtQueue_Handle virtQueue_toHost; VirtQueue_Handle virtQueue_fromHost; Semaphore_Handle semHandle_toHost; } RPMessage_Transport; /* module diags mask */ Registry_Desc Registry_CURDESC; static RPMessage_Module module; static RPMessage_Transport transport; /* We create a fixed size heap over this memory for copying received msgs */ #pragma DATA_ALIGN (recv_buffers, HEAPALIGNMENT) static UInt8 recv_buffers[MAXHEAPSIZE]; /* Module ref count: */ static Int curInit = 0; /* * ======== RPMessage_swiFxn ======== */ #define FXNN "RPMessage_swiFxn" static Void RPMessage_swiFxn(UArg arg0, UArg arg1) { Int16 token; RPMessage_Msg msg; UInt16 dstProc = MultiProc_self(); Bool usedBufAdded = FALSE; int len; Log_print0(Diags_ENTRY, "--> "FXNN); /* Process all available buffers: */ while ((token = VirtQueue_getAvailBuf(transport.virtQueue_fromHost, (Void **)&msg, &len)) >= 0) { Log_print3(Diags_INFO, FXNN": \n\tReceived msg: from: 0x%x, " "to: 0x%x, dataLen: %d", (IArg)msg->srcAddr, (IArg)msg->dstAddr, (IArg)msg->dataLen); /* Pass to destination queue (on this proc), or callback: */ RPMessage_send(dstProc, msg->dstAddr, msg->srcAddr, (Ptr)msg->payload, msg->dataLen); VirtQueue_addUsedBuf(transport.virtQueue_fromHost, token, RPMSG_BUF_SIZE); usedBufAdded = TRUE; } if (usedBufAdded) { /* Tell host we've processed the buffers: */ VirtQueue_kick(transport.virtQueue_fromHost); } Log_print0(Diags_EXIT, "<-- "FXNN); } #undef FXNN #define FXNN "callback_availBufReady" static Void callback_availBufReady(VirtQueue_Handle vq) { if (vq == transport.virtQueue_fromHost) { /* Post a SWI to process all incoming messages */ Log_print0(Diags_INFO, FXNN": virtQueue_fromHost kicked"); Swi_post(transport.swiHandle); } else if (vq == transport.virtQueue_toHost) { /* Note: We normally post nothing for transport.virtQueue_toHost, * unless we were starved for buffers, and we turned on notifications. */ Semaphore_post(transport.semHandle_toHost); Log_print0(Diags_INFO, FXNN": virtQueue_toHost kicked"); } } #undef FXNN /* ============================================================================= * RPMessage Functions: * ============================================================================= */ /* * ======== MessasgeQCopy_init ======== * * */ #define FXNN "RPMessage_init" Void RPMessage_init(UInt16 remoteProcId) { GateAll_Params gatePrms; HeapBuf_Params prms; int i; Registry_Result result; Bool isHost; VirtQueue_Params vqParams; if (curInit++) { Log_print1(Diags_ENTRY, "--> "FXNN": (remoteProcId=%d)", (IArg)remoteProcId); goto exit; /* module already initialized */ } /* register with xdc.runtime to get a diags mask */ result = Registry_addModule(&Registry_CURDESC, MODULE_NAME); Assert_isTrue(result == Registry_SUCCESS, (Assert_Id)NULL); /* Log should be after the Registry_CURDESC is initialized */ Log_print1(Diags_ENTRY, "--> "FXNN": (remoteProcId=%d)", (IArg)remoteProcId); /* Gate to protect module object and lists: */ GateAll_Params_init(&gatePrms); module.gateH = GateAll_create(&gatePrms, NULL); /* Initialize Module State: */ for (i = 0; i < MAXMESSAGEQOBJECTS; i++) { module.msgqObjects[i] = NULL; } HeapBuf_Params_init(&prms); prms.blockSize = MSGBUFFERSIZE; prms.numBlocks = MAXMESSAGEBUFFERS; prms.buf = recv_buffers; prms.bufSize = MAXHEAPSIZE; prms.align = HEAPALIGNMENT; module.heap = HeapBuf_create(&prms, NULL); if (module.heap == 0) { System_abort("RPMessage_init: HeapBuf_create returned 0\n"); } transport.semHandle_toHost = Semaphore_create(0, NULL, NULL); isHost = (MultiProc_self() == MultiProc_getId("HOST")); /* Initialize Transport related objects: */ VirtQueue_Params_init(&vqParams); if (isHost) { /* We don't handle this case currently! Host would need to prime vq. */ Assert_isTrue(FALSE, NULL); } else { vqParams.callback = callback_availBufReady; } /* * Create a pair VirtQueues (one for sending, one for receiving). * Note: First one gets an even, second gets odd vq ID. */ vqParams.vqId = ID_SELF_TO_A9; transport.virtQueue_toHost = (Ptr)VirtQueue_create(remoteProcId, &vqParams, NULL); vqParams.vqId = ID_A9_TO_SELF; transport.virtQueue_fromHost = (Ptr)VirtQueue_create(remoteProcId, &vqParams, NULL); /* Plug Vring Interrupts, and wait for host ready to recv kick: */ VirtQueue_startup(remoteProcId, isHost); /* construct the Swi to process incoming messages: */ transport.swiHandle = Swi_create(RPMessage_swiFxn, NULL, NULL); exit: Log_print0(Diags_EXIT, "<-- "FXNN); } #undef FXNN /* * ======== MessasgeQCopy_finalize ======== */ #define FXNN "RPMessage_finalize" Void RPMessage_finalize() { Log_print0(Diags_ENTRY, "--> "FXNN); if (!curInit || --curInit) { goto exit; /* module still in use, or uninitialized */ } /* Tear down Module */ HeapBuf_delete(&(module.heap)); Swi_delete(&(transport.swiHandle)); GateAll_delete(&module.gateH); exit: Log_print0(Diags_EXIT, "<-- "FXNN); } #undef FXNN /* * ======== RPMessage_create ======== */ #define FXNN "RPMessage_create" RPMessage_Handle RPMessage_create(UInt32 reserved, RPMessage_callback cb, UArg arg, UInt32 * endpoint) { RPMessage_Object *obj = NULL; Bool found = FALSE; Int i; UInt16 queueIndex = 0; IArg key; Log_print4(Diags_ENTRY, "--> "FXNN": " "(reserved=%d, cb=0x%x, arg=0x%x, endpoint=0x%x)", (IArg)reserved, (IArg)cb, (IArg)arg, (IArg)endpoint); Assert_isTrue((curInit > 0) , NULL); key = GateAll_enter(module.gateH); if (reserved == RPMessage_ASSIGN_ANY) { /* Search the array for a free slot above reserved: */ for (i = RPMessage_MAX_RESERVED_ENDPOINT + 1; (i < MAXMESSAGEQOBJECTS) && (found == FALSE) ; i++) { if (module.msgqObjects[i] == NULL) { queueIndex = i; found = TRUE; break; } } } else if ((queueIndex = reserved) <= RPMessage_MAX_RESERVED_ENDPOINT) { if (module.msgqObjects[queueIndex] == NULL) { found = TRUE; } } if (found) { obj = Memory_alloc(NULL, sizeof(RPMessage_Object), 0, NULL); if (obj != NULL) { if (cb) { /* Store callback and it's arg instead of semaphore: */ obj->cb = cb; obj->arg= arg; } else { obj->cb = NULL; /* Allocate a semaphore to signal when messages received: */ obj->semHandle = Semaphore_create(0, NULL, NULL); /* Create our queue of to be received messages: */ obj->queue = List_create(NULL, NULL); } /* Store our endpoint, and object: */ obj->queueId = queueIndex; module.msgqObjects[queueIndex] = obj; /* See RPMessage_unblock() */ obj->unblocked = FALSE; *endpoint = queueIndex; Log_print1(Diags_LIFECYCLE, FXNN": endPt created: %d", (IArg)queueIndex); } } GateAll_leave(module.gateH, key); Log_print1(Diags_EXIT, "<-- "FXNN": 0x%x", (IArg)obj); return (obj); } #undef FXNN /* * ======== RPMessage_delete ======== */ #define FXNN "RPMessage_delete" Int RPMessage_delete(RPMessage_Handle *handlePtr) { Int status = RPMessage_S_SUCCESS; RPMessage_Object *obj; Queue_elem *payload; IArg key; Log_print1(Diags_ENTRY, "--> "FXNN": (handlePtr=0x%x)", (IArg)handlePtr); Assert_isTrue((curInit > 0) , NULL); if (handlePtr && (obj = (RPMessage_Object *)(*handlePtr))) { if (obj->cb) { obj->cb = NULL; obj->arg= NULL; } else { Semaphore_delete(&(obj->semHandle)); /* Free/discard all queued message buffers: */ while ((payload = (Queue_elem *)List_get(obj->queue)) != NULL) { HeapBuf_free(module.heap, (Ptr)payload, MSGBUFFERSIZE); } List_delete(&(obj->queue)); } /* Null out our slot: */ key = GateAll_enter(module.gateH); module.msgqObjects[obj->queueId] = NULL; GateAll_leave(module.gateH, key); Log_print1(Diags_LIFECYCLE, FXNN": endPt deleted: %d", (IArg)obj->queueId); /* Now free the obj */ Memory_free(NULL, obj, sizeof(RPMessage_Object)); *handlePtr = NULL; } Log_print1(Diags_EXIT, "<-- "FXNN": %d", (IArg)status); return(status); } #undef FXNN /* * ======== RPMessage_recv ======== */ #define FXNN "RPMessage_recv" Int RPMessage_recv(RPMessage_Handle handle, Ptr data, UInt16 *len, UInt32 *rplyEndpt, UInt timeout) { Int status = RPMessage_S_SUCCESS; RPMessage_Object *obj = (RPMessage_Object *)handle; Bool semStatus; Queue_elem *payload; Log_print5(Diags_ENTRY, "--> "FXNN": (handle=0x%x, data=0x%x, len=0x%x," "rplyEndpt=0x%x, timeout=%d)", (IArg)handle, (IArg)data, (IArg)len, (IArg)rplyEndpt, (IArg)timeout); Assert_isTrue((curInit > 0) , NULL); /* A callback was set: client should not be calling this fxn! */ Assert_isTrue((!obj->cb), NULL); /* Check vring for pending messages before we block: */ Swi_post(transport.swiHandle); /* Block until notified. */ semStatus = Semaphore_pend(obj->semHandle, timeout); if (semStatus == FALSE) { status = RPMessage_E_TIMEOUT; Log_print0(Diags_STATUS, FXNN": Sem pend timeout!"); } else if (obj->unblocked) { status = RPMessage_E_UNBLOCKED; } else { payload = (Queue_elem *)List_get(obj->queue); Assert_isTrue((!payload), NULL); } if (status == RPMessage_S_SUCCESS) { /* Now, copy payload to client and free our internal msg */ memcpy(data, payload->data, payload->len); *len = payload->len; *rplyEndpt = payload->src; HeapBuf_free(module.heap, (Ptr)payload, (payload->len + sizeof(Queue_elem))); } Log_print1(Diags_EXIT, "<-- "FXNN": %d", (IArg)status); return (status); } #undef FXNN /* * ======== RPMessage_send ======== */ #define FXNN "RPMessage_send" Int RPMessage_send(UInt16 dstProc, UInt32 dstEndpt, UInt32 srcEndpt, Ptr data, UInt16 len) { Int status = RPMessage_S_SUCCESS; RPMessage_Object *obj; Int16 token = 0; RPMessage_Msg msg; Queue_elem *payload; UInt size; IArg key; int length; Log_print5(Diags_ENTRY, "--> "FXNN": (dstProc=%d, dstEndpt=%d, " "srcEndpt=%d, data=0x%x, len=%d", (IArg)dstProc, (IArg)dstEndpt, (IArg)srcEndpt, (IArg)data, (IArg)len); Assert_isTrue((curInit > 0) , NULL); if (dstProc != MultiProc_self()) { /* Send to remote processor: */ do { token = VirtQueue_getAvailBuf(transport.virtQueue_toHost, (Void **)&msg, &length); } while (token < 0 && Semaphore_pend(transport.semHandle_toHost, BIOS_WAIT_FOREVER)); if (token >= 0) { /* Copy the payload and set message header: */ memcpy(msg->payload, data, len); msg->dataLen = len; msg->dstAddr = dstEndpt; msg->srcAddr = srcEndpt; msg->flags = 0; msg->reserved = 0; VirtQueue_addUsedBuf(transport.virtQueue_toHost, token, RPMSG_BUF_SIZE); VirtQueue_kick(transport.virtQueue_toHost); } else { status = RPMessage_E_FAIL; Log_print0(Diags_STATUS, FXNN": getAvailBuf failed!"); } } else { /* Put on a Message queue on this processor: */ /* Protect from RPMessage_delete */ key = GateAll_enter(module.gateH); obj = module.msgqObjects[dstEndpt]; GateAll_leave(module.gateH, key); if (obj == NULL) { Log_print1(Diags_STATUS, FXNN": no object for endpoint: %d", (IArg)dstEndpt); status = RPMessage_E_NOENDPT; return status; } /* If callback registered, call it: */ if (obj->cb) { Log_print2(Diags_INFO, FXNN": calling callback with data len: " "%d, from: %d\n", len, srcEndpt); obj->cb(obj, obj->arg, data, len, srcEndpt); } else { /* else, put on a Message queue on this processor: */ /* Allocate a buffer to copy the payload: */ size = len + sizeof(Queue_elem); /* HeapBuf_alloc() is non-blocking, so needs protection: */ key = GateAll_enter(module.gateH); payload = (Queue_elem *)HeapBuf_alloc(module.heap, size, 0, NULL); GateAll_leave(module.gateH, key); if (payload != NULL) { memcpy(payload->data, data, len); payload->len = len; payload->src = srcEndpt; /* Put on the endpoint's queue and signal: */ List_put(obj->queue, (List_Elem *)payload); Semaphore_post(obj->semHandle); } else { status = RPMessage_E_MEMORY; Log_print0(Diags_STATUS, FXNN": HeapBuf_alloc failed!"); } } } Log_print1(Diags_EXIT, "<-- "FXNN": %d", (IArg)status); return (status); } #undef FXNN /* * ======== RPMessage_unblock ======== */ #define FXNN "RPMessage_unblock" Void RPMessage_unblock(RPMessage_Handle handle) { RPMessage_Object *obj = (RPMessage_Object *)handle; Log_print1(Diags_ENTRY, "--> "FXNN": (handle=0x%x)", (IArg)handle); Assert_isTrue((!obj->cb), NULL); /* Set instance to 'unblocked' state, and post */ obj->unblocked = TRUE; Semaphore_post(obj->semHandle); Log_print0(Diags_EXIT, "<-- "FXNN); } #undef FXNN