/* * Copyright (c) 2013, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ /* * ======== message_multicore.c ======== * Multiprocessor MessageQ example * * This is an example program that uses MessageQ to pass a message * from one processor to another. * * Each processor creates its own MessageQ first and then will try to open * a remote processor's MessageQ. * * See message_multicore.k file for expected output. */ #include #include /* -----------------------------------XDC.RUNTIME module Headers */ #include #include /* ----------------------------------- IPC module Headers */ #include #include #include #include /* ----------------------------------- BIOS6 module Headers */ #include #include #include #include /* ----------------------------------- To get globals from .cfg Header */ #include /* Define this to eliminate VIRTIO DEV and VRINGS from rsc_table: */ #define TRACE_RESOURCE_ONLY 1 extern char * xdc_runtime_SysMin_Module_State_0_outbuf__A; #if defined(TCI6614) #include #elif defined(TCI6614_v33) #include #elif defined(TCI6638) #include #endif #define HEAP_NAME "myHeapBuf" #define HEAPID 0 #define NUMLOOPS 10 Char localQueueName[10]; Char nextQueueName[10]; UInt16 nextProcId; /* * ======== tsk0_func ======== * Allocates a message and ping-pongs the message around the processors. * A local message queue is created and a remote message queue is opened. * Messages are sent to the remote message queue and retrieved from the * local MessageQ. */ Void tsk0_func(UArg arg0, UArg arg1) { MessageQ_Msg msg; MessageQ_Handle messageQ; MessageQ_QueueId remoteQueueId; Int status; UInt16 msgId = 0; HeapBufMP_Handle heapHandle; HeapBufMP_Params heapBufParams; if (MultiProc_self() == 0) { /* * Create the heap that will be used to allocate messages. */ HeapBufMP_Params_init(&heapBufParams); heapBufParams.regionId = 0; heapBufParams.name = HEAP_NAME; heapBufParams.numBlocks = 1; heapBufParams.blockSize = sizeof(MessageQ_MsgHeader); heapHandle = HeapBufMP_create(&heapBufParams); if (heapHandle == NULL) { System_abort("HeapBufMP_create failed\n" ); } } else { /* Open the heap created by the other processor. Loop until opened. */ do { status = HeapBufMP_open(HEAP_NAME, &heapHandle); /* * Sleep for 1 clock tick to avoid inundating remote processor * with interrupts if open failed */ if (status < 0) { Task_sleep(1); } } while (status < 0); } /* Register this heap with MessageQ */ MessageQ_registerHeap((IHeap_Handle)heapHandle, HEAPID); /* Create the local message queue */ messageQ = MessageQ_create(localQueueName, NULL); if (messageQ == NULL) { System_abort("MessageQ_create failed\n" ); } /* Open the remote message queue. Spin until it is ready. */ do { status = MessageQ_open(nextQueueName, &remoteQueueId); /* * Sleep for 1 clock tick to avoid inundating remote processor * with interrupts if open failed */ if (status < 0) { Task_sleep(1); } } while (status < 0); if (MultiProc_self() == 0) { /* Allocate a message to be ping-ponged around the processors */ msg = MessageQ_alloc(HEAPID, sizeof(MessageQ_MsgHeader)); if (msg == NULL) { System_abort("MessageQ_alloc failed\n" ); } /* * Send the message to the next processor and wait for a message * from the previous processor. */ System_printf("Start the main loop\n"); while (msgId < NUMLOOPS) { /* Increment...the remote side will check this */ msgId++; MessageQ_setMsgId(msg, msgId); System_printf("Sending a message #%d to %s\n", msgId, nextQueueName); /* send the message to the remote processor */ status = MessageQ_put(remoteQueueId, msg); if (status < 0) { System_abort("MessageQ_put had a failure/error\n"); } /* Get a message */ status = MessageQ_get(messageQ, &msg, MessageQ_FOREVER); if (status < 0) { System_abort("This should not happen since timeout is forever\n"); } } } else { /* * Wait for a message from the previous processor and * send it to the next processor */ System_printf("Start the main loop\n"); while (TRUE) { /* Get a message */ status = MessageQ_get(messageQ, &msg, MessageQ_FOREVER); if (status < 0) { System_abort("This should not happen since timeout is forever\n"); } System_printf("Sending a message #%d to %s\n", MessageQ_getMsgId(msg), nextQueueName); /* Get the message id */ msgId = MessageQ_getMsgId(msg); /* send the message to the remote processor */ status = MessageQ_put(remoteQueueId, msg); if (status < 0) { System_abort("MessageQ_put had a failure/error\n"); } /* test done */ if (msgId >= NUMLOOPS) { break; } } } System_printf("The test is complete\n"); BIOS_exit(0); } #define CACHE_WB_TICK_PERIOD 5 /* * ======== VirtQueue_cacheWb ======== * * Used for flushing SysMin trace buffer. */ Void traceBuf_cacheWb() { static UInt32 oldticks = 0; UInt32 newticks; newticks = Clock_getTicks(); if (newticks - oldticks < (UInt32)CACHE_WB_TICK_PERIOD) { /* Don't keep flushing cache */ return; } oldticks = newticks; Cache_wbAll(); } /* * ======== main ======== * Synchronizes all processors (in Ipc_start) and calls BIOS_start */ Int main(Int argc, Char* argv[]) { Int status; #if defined(TCI6614_v33) /* Reference resource table, until IpcMemory.xdt is enabled for TCI66xx */ System_printf("Resource Table: 0x%lx\n", resources); #elif defined (TCI6614) || defined(TCI6638) System_printf("%d Resource Table entries at 0x%x\n", ti_ipc_remoteproc_ResourceTable.num, &ti_ipc_remoteproc_ResourceTable); #endif nextProcId = (MultiProc_self() + 1) % MultiProc_getNumProcessors(); /* Generate queue names based on own proc ID and total number of procs */ System_sprintf(localQueueName, "%s", MultiProc_getName(MultiProc_self())); System_sprintf(nextQueueName, "%s", MultiProc_getName(nextProcId)); /* * Ipc_start() calls Ipc_attach() to synchronize all remote processors * because 'Ipc.procSync' is set to 'Ipc.ProcSync_ALL' in *.cfg */ status = Ipc_start(); if (status < 0) { System_abort("Ipc_start failed\n"); } BIOS_start(); return (0); } /* * @(#) ti.sdo.ipc.examples.multicore.evm667x; 1, 0, 0, 0,2; 10-19-2011 10:53:19; /db/vtree/library/trees/ipc/ipc.git/src/ null */