/* * Copyright (c) 2011-2013, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /** ============================================================================ * @file IpcPower.c * * @brief A simple Power Managment which responses to the host commands. * * TODO: * - Add suspend/resume notifications * ============================================================================ */ #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #ifndef SMP #include #include #else #include #include #endif #include #include #include "_IpcPower.h" #define MASTERCORE (1) #define NO_MASTERCORE (0) #define CPU_COPY (-1) #define REG32(A) (*(volatile UInt32 *) (A)) #define SET_DEEPSLEEP (REG32(M3_SCR_REG) | (1 << DEEPSLEEP_BIT)) #define CLR_DEEPSLEEP (REG32(M3_SCR_REG) & (~(1 << DEEPSLEEP_BIT))) #ifndef SMP #pragma DATA_SECTION(IpcPower_hibLocks, ".ipcpower_data") UInt32 IpcPower_hibLocks[2]; /* One lock for each of the IPU cores */ #else static UInt32 IpcPower_hibLocks; /* Only one lock in SMP mode */ #endif /* PM transition debug counters */ #ifndef SMP UInt32 IpcPower_idleCount = 0; #else UInt32 IpcPower_idleCount[2] = { 0, 0 }; #endif UInt32 IpcPower_suspendCount = 0; UInt32 IpcPower_resumeCount = 0; /* Clock function pointer to handle custom clock functions */ Void *IpcPower_clockFxn = NULL; /* Handle to store BIOS Tick Timer */ static Timer_Handle tickTimerHandle = NULL; static Power_SuspendArgs PowerSuspArgs; static Swi_Handle suspendResumeSwi; #ifndef SMP static Semaphore_Handle IpcPower_semSuspend = NULL; static Semaphore_Handle IpcPower_semExit = NULL; static Task_Handle IpcPower_tskSuspend = NULL; static UInt16 sysm3ProcId; static UInt16 appm3ProcId; #endif static Int32 refWakeLockCnt; /* List for storing all registered callback functions */ static IpcPower_CallbackElem *IpcPower_callbackList = NULL; /* Module ref count: */ static Int curInit = 0; typedef enum IpcPower_SleepMode { IpcPower_SLEEP_MODE_DEEPSLEEP, IpcPower_SLEEP_MODE_WAKELOCK, IpcPower_SLEEP_MODE_WAKEUNLOCK } IpcPower_SleepMode; /* Deep sleep state variable for IpcPower module */ static Bool IpcPower_deepSleep = TRUE; static IpcPower_WugenEvtMask wugenEvtMask; /* * ======== IpcPower_callUserFxns ======== */ static Void IpcPower_callUserFxns(IpcPower_Event event) { IpcPower_CallbackElem *node = IpcPower_callbackList; /* Call the registered functions matching the event */ while (node != NULL) { if (node->event == event) { (*(node->callback))(event, node->data); } node = node->next; } } static inline Void IpcPower_sleepMode(IpcPower_SleepMode opt) { IArg hwiKey; /* Set/Restore the DeepSleep bit if no timer already in use */ hwiKey = Hwi_disable(); switch (opt) { case IpcPower_SLEEP_MODE_WAKEUNLOCK: if (refWakeLockCnt) { refWakeLockCnt--; } /* Fall through: */ case IpcPower_SLEEP_MODE_DEEPSLEEP: if (!refWakeLockCnt) { IpcPower_deepSleep = TRUE; } break; case IpcPower_SLEEP_MODE_WAKELOCK: refWakeLockCnt++; IpcPower_deepSleep = FALSE; break; } Hwi_restore(hwiKey); } Void IpcPower_getWugenEvtMask(IpcPower_WugenEvtMask *mask) { mask->mevt0 = wugenEvtMask.mevt0; mask->mevt1 = wugenEvtMask.mevt1; } Void IpcPower_setWugenEvtMask(IpcPower_WugenEvtMask *mask) { wugenEvtMask.mevt0 = mask->mevt0; wugenEvtMask.mevt1 = mask->mevt1; } static inline Void IpcPower_getWugen(IpcPower_WugenEvtMask *mask) { mask->mevt0 = REG32(WUGEN_MEVT0); mask->mevt1 = REG32(WUGEN_MEVT1); } static inline Void IpcPower_setWugen(IpcPower_WugenEvtMask *mask) { REG32(WUGEN_MEVT0) = mask->mevt0; REG32(WUGEN_MEVT1) = mask->mevt1; } /* * ======== IpcPower_suspendSwi ======== */ #define FXNN "IpcPower_suspendSwi" static Void IpcPower_suspendSwi(UArg arg0, UArg arg1) { #ifndef SMP if (MultiProc_self() == sysm3ProcId) { #endif Log_print0(Diags_INFO, FXNN":Core0 Hibernation Swi"); #ifndef SMP PowerSuspArgs.pmMasterCore = MASTERCORE; } else if (MultiProc_self() == appm3ProcId) { Log_print0(Diags_INFO, FXNN":Core1 Hibernation Swi"); PowerSuspArgs.pmMasterCore = NO_MASTERCORE; } #endif if (refWakeLockCnt) { System_printf("Warning: Wake locks in use\n"); } Power_suspend(&PowerSuspArgs); #ifndef SMP IpcPower_sleepMode(IpcPower_SLEEP_MODE_DEEPSLEEP); IpcPower_setWugen(&wugenEvtMask); Log_print0(Diags_INFO, FXNN":Resume"); #endif } #undef FXNN /* ============================================================================= * IpcPower Functions: * ============================================================================= */ #ifndef SMP /* * ======== IpcPower_suspendTaskFxn ======== */ Void IpcPower_suspendTaskFxn(UArg arg0, UArg arg1) { while (curInit) { /* Wait for suspend notification from host-side */ Semaphore_pend(IpcPower_semSuspend, BIOS_WAIT_FOREVER); if (curInit) { /* Call pre-suspend preparation function */ IpcPower_preSuspend(); Swi_post(suspendResumeSwi); /* Call post-resume preparation function */ IpcPower_postResume(); } } /* Signal the task end */ Semaphore_post(IpcPower_semExit); } #endif /* * ======== IpcPower_init ======== */ Void IpcPower_init() { Swi_Params swiParams; #ifndef SMP Task_Params taskParams; UInt coreIdx = Core_getId(); #endif Int i; UArg arg; UInt func; Timer_Handle tHandle = NULL; if (curInit++) { return; } #ifndef SMP IpcPower_hibLocks[coreIdx] = 0; sysm3ProcId = MultiProc_getId("CORE0"); appm3ProcId = MultiProc_getId("CORE1"); #else IpcPower_hibLocks = 0; #endif refWakeLockCnt = 0; for (i = 0; i < Timer_Object_count(); i++) { tHandle = Timer_Object_get(NULL, i); func = (UInt) Timer_getFunc(tHandle, &arg); if (func && ((func == (UInt) ti_sysbios_knl_Clock_doTick__I) || (func == (UInt) Clock_tick) || (func == (UInt) IpcPower_clockFxn))) { tickTimerHandle = tHandle; break; } } if (tickTimerHandle == NULL) { System_abort("IpcPower_init: Cannot find tickTimer Handle. Custom" " clock timer functions currently not supported.\n"); } #ifndef SMP IpcPower_semSuspend = Semaphore_create(0, NULL, NULL); IpcPower_semExit = Semaphore_create(0, NULL, NULL); Task_Params_init(&taskParams); taskParams.priority = Task_numPriorities - 1; /* Highest priority */ taskParams.instance->name = "ti.pm.IpcPower_tskSuspend"; IpcPower_tskSuspend = Task_create(IpcPower_suspendTaskFxn, &taskParams, NULL); #endif Swi_Params_init(&swiParams); swiParams.priority = Swi_numPriorities - 1; /* Max Priority Swi */ suspendResumeSwi = Swi_create(IpcPower_suspendSwi, &swiParams, NULL); /*Power settings for saving/restoring context */ PowerSuspArgs.rendezvousResume = TRUE; PowerSuspArgs.dmaChannel = CPU_COPY; PowerSuspArgs.intMask31_0 = 0x0; #ifndef SMP PowerSuspArgs.intMask63_32 = 0x0; #else PowerSuspArgs.intMask63_32 = WUGEN_MAILBOX_BIT << 16; #endif PowerSuspArgs.intMask79_64 = 0x0; IpcPower_sleepMode(IpcPower_SLEEP_MODE_DEEPSLEEP); IpcPower_getWugen(&wugenEvtMask); #ifdef OMAP5 wugenEvtMask.mevt0 |= OMAP_IPU_WUGEN_INT_MASK0; wugenEvtMask.mevt1 |= OMAP_IPU_WUGEN_INT_MASK1; #else if (MultiProc_self() == MultiProc_getId("IPU2")) { wugenEvtMask.mevt0 |= VAYU_IPU2_WUGEN_INT_MASK0; wugenEvtMask.mevt1 |= VAYU_IPU2_WUGEN_INT_MASK1; } else { wugenEvtMask.mevt0 |= VAYU_IPU1_WUGEN_INT_MASK0; wugenEvtMask.mevt1 |= VAYU_IPU1_WUGEN_INT_MASK1; } #endif IpcPower_setWugen(&wugenEvtMask); } /* * ======== IpcPower_exit ======== */ Void IpcPower_exit() { --curInit; if (curInit == 0) { #ifndef SMP /* Unblock PM suspend task */ Semaphore_post(IpcPower_semSuspend); /* Wait for task completion */ Semaphore_pend(IpcPower_semExit, BIOS_WAIT_FOREVER); /* Delete the suspend task and semaphore */ Task_delete(&IpcPower_tskSuspend); Semaphore_delete(&IpcPower_semSuspend); Semaphore_delete(&IpcPower_semExit); #endif } } /* * ======== IpcPower_suspend ======== */ Void IpcPower_suspend() { Assert_isTrue((curInit > 0) , NULL); #ifndef SMP Semaphore_post(IpcPower_semSuspend); #else Swi_post(suspendResumeSwi); #endif } /* * ======== IpcPower_idle ======== */ Void IpcPower_idle() { #ifndef SMP IpcPower_idleCount++; #else UInt coreId = Core_getId(); IpcPower_idleCount[coreId]++; #endif REG32(M3_SCR_REG) = IpcPower_deepSleep ? SET_DEEPSLEEP : CLR_DEEPSLEEP; asm(" wfi"); } /* * ======== IpcPower_wakeLock ======== */ Void IpcPower_wakeLock() { IpcPower_sleepMode(IpcPower_SLEEP_MODE_WAKELOCK); } /* * ======== IpcPower_wakeUnlock ======== */ Void IpcPower_wakeUnlock() { IpcPower_sleepMode(IpcPower_SLEEP_MODE_WAKEUNLOCK); } /* * ======== IpcPower_hibernateLock ======== */ UInt IpcPower_hibernateLock() { IArg hwiKey; #ifndef SMP UInt coreIdx = Core_getId(); #endif hwiKey = Hwi_disable(); #ifndef SMP IpcPower_hibLocks[coreIdx] += 1; #else IpcPower_hibLocks++; #endif Hwi_restore(hwiKey); #ifndef SMP return (IpcPower_hibLocks[coreIdx]); #else return IpcPower_hibLocks; #endif } /* * ======== IpcPower_hibernateUnlock ======== */ UInt IpcPower_hibernateUnlock() { IArg hwiKey; #ifndef SMP UInt coreIdx = Core_getId(); #endif hwiKey = Hwi_disable(); #ifndef SMP if (IpcPower_hibLocks[coreIdx] > 0) { IpcPower_hibLocks[coreIdx] -= 1; } #else if (IpcPower_hibLocks > 0) { IpcPower_hibLocks--; } #endif Hwi_restore(hwiKey); #ifndef SMP return (IpcPower_hibLocks[coreIdx]); #else return (IpcPower_hibLocks); #endif } /* * ======== IpcPower_canHibernate ======== */ Bool IpcPower_canHibernate() { #ifndef SMP if (IpcPower_hibLocks[0] || IpcPower_hibLocks[1]) { #else if (IpcPower_hibLocks) { #endif return (FALSE); } return (TRUE); } /* * ======== IpcPower_registerCallback ======== */ #define FXNN "IpcPower_registerCallback" Int IpcPower_registerCallback(Int event, IpcPower_CallbackFuncPtr cbck, Ptr data) { IArg hwiKey; IpcPower_CallbackElem **list, *node; BIOS_ThreadType context = BIOS_getThreadType(); if ((context != BIOS_ThreadType_Task) && (context != BIOS_ThreadType_Main)) { Log_print0(Diags_ERROR, FXNN":Invalid context\n"); return (IpcPower_E_FAIL); } list = &IpcPower_callbackList; /* Allocate and update new element */ node = Memory_alloc(NULL, sizeof(IpcPower_CallbackElem), 0, NULL); if (node == NULL) { Log_print0(Diags_ERROR, FXNN":out of memory\n"); return (IpcPower_E_MEMORY); } node->next = NULL; node->event = (IpcPower_Event) event; node->callback = cbck; node->data = data; hwiKey = Hwi_disable(); /* begin: critical section */ while (*list != NULL) { list = &(*list)->next; } *list = node; Hwi_restore(hwiKey); /* end: critical section */ return (IpcPower_S_SUCCESS); } #undef FXNN /* * ======== IpcPower_unregisterCallback ======== */ #define FXNN "IpcPower_unregisterCallback" Int IpcPower_unregisterCallback(Int event, IpcPower_CallbackFuncPtr cbck) { IArg hwiKey; IpcPower_CallbackElem **list, *node; Int status = IpcPower_E_FAIL; BIOS_ThreadType context = BIOS_getThreadType(); if ((context != BIOS_ThreadType_Task) && (context != BIOS_ThreadType_Main)) { Log_print0(Diags_ERROR, FXNN":Invalid context\n"); return (status); } list = &IpcPower_callbackList; node = NULL; hwiKey = Hwi_disable(); /* begin: critical section */ while (*list != NULL) { if ( ((*list)->callback == cbck) && ((*list)->event == event) ) { node = *list; *list = (*list)->next; status = IpcPower_S_SUCCESS; break; } list = &(*list)->next; } Hwi_restore(hwiKey); /* end: critical section */ if (status == IpcPower_S_SUCCESS) { if (node != NULL) { Memory_free(NULL, node, sizeof(IpcPower_CallbackElem)); } else { Log_print0(Diags_ERROR, FXNN":Invalid pointer\n"); } } return (status); } #undef FXNN /* * ======== IpcPower_preSuspend ======== */ Void IpcPower_preSuspend(Void) { IpcPower_suspendCount++; /* Call all user registered suspend callback functions */ IpcPower_callUserFxns(IpcPower_Event_SUSPEND); } /* * ======== IpcPower_postResume ======== */ Void IpcPower_postResume(Void) { /* Restore timer registers */ Timer_restoreRegisters(tickTimerHandle, NULL); Timer_start(tickTimerHandle); /* Call all user registered resume callback functions */ IpcPower_callUserFxns(IpcPower_Event_RESUME); IpcPower_resumeCount++; }