/* * Copyright (c) 2013-2015 Texas Instruments Incorporated - http://www.ti.com * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /* * ======== Build.xdc ======== * metaonly module to support building various package/product libraries * */ /*! * ======== Build ======== */ @Template("./Build.xdt") metaonly module Build { /*! * ======== LibType ======== * IPC library selection options * * This enumeration defines all the IPC library types provided * by the product. You can select the library type by setting * the {@link #libType Build.libType} configuration parameter. * * @field(LibType_Instrumented) The library supplied is prebuilt * with logging and assertions enabled. * * @field(LibType_NonInstrumented) The library supplied is prebuilt * with logging and assertions disabled. * * @field(LibType_Custom) This option builds the IPC library from * sources using the options specified by {@link #customCCOpts}. * Only the modules and APIs that your application uses are * contained in the resulting executable. Program optimization is * performed to reduce the size of the executable and improve * performance. Enough debug information is retained to allow you * to step through the application code in CCS and locate global * variables. * * @field(LibType_Debug) This option is similar to the LibType_Custom * option in that it builds the IPC library from sources and omits * modules and APIs that your code does not use. However, no program * optimization is performed. The resulting executable is fully * debuggable, and you can step into IPC code. The tradeoff is that * the executable is larger and runs slower than builds that use the * LibType_Custom option. * * @field(LibType_PkgLib) This option uses the individual libraries * built by each package of the IPC product. These libraries are * not shipped. You must build the product to generate the package * libraries. See the IPC Install Guides (links in the Release * Note) for details on building the IPC product. * * @see #libType */ enum LibType { LibType_Instrumented, /*! Instrumented */ LibType_NonInstrumented, /*! Non-instrumented */ LibType_Custom, /*! Custom (Optimized) */ LibType_Debug, /*! Custom (Debug) */ LibType_PkgLib /*! Use package library */ }; /*! * ======== libType ======== * IPC library type * * The IPC runtime is provided in the form of a library that is * linked with your application. Several forms of this library are * provided with the IPC product. In addition, there is an option * to build the library from source. This configuration parameter * allows you to select the form of the IPC library to use. * * The default value of libType is taken from the BIOS.libType * configuration parameter. For a complete list of options and * what they offer see {@link #LibType}. */ config LibType libType; /*! * ======== customCCOpts ======== * Compiler options used when building a custom IPC library * * When {@link #libType Build.libType} is set to * {@link #LibType_Custom Build_LibType_Custom} or * {@link #LibType_Debug Build_LibType_Debug}, this string contains * the options passed to the compiler during any re-build of the * IPC sources. * * In addition to the options specified by `Build.customCCOpts`, * several `-D` and `-I` options are also passed to the compiler. * The options specified by `Build.customCCOpts` preceed the `-D` * and `-I` options passed to the compiler on the command line. * * To view the custom compiler options, add the following line * to your config script: * * @p(code) * print("Build.customCCOpts="+Build.customCCOpts); * @p * * When {@link #libType Build.libType} is set to * {@link #LibType_Custom Build_LibType_Custom}, `Build.customCCOpts` * is initialized to create a highly optimized library. * * When {@link #libType Build.libType} is set to * {@link #LibType_Debug Build_LibType_Debug}, `Build.customCCOpts` * is initialized to create a non-optimized library that can be * used to single-step through the APIs with the CCS debugger. * * @a(Warning) * The default value of `Build.customCCOpts`, which is derived from * the target specified by your configuration, includes runtime * model options (such as endianess) that must be the same for all * sources built and linked into your application. You must not * change or add any options that can alter the runtime model * specified by the default value of `Build.customCCOpts`. */ config String customCCOpts; /*! * ======== assertsEnabled ======== * IPC assert checking in custom library enable flag * * When set to true, assert checking code is compiled into * the custom library created when {@link #libType Build.libType} * is set to {@link #LibType_Custom Build_LibType_Custom} or * {@link #LibType_Debug Build_LibType_Debug}. * * When set to false, assert checking code is removed from the * custom library created when Build.libType is set to * Build.LibType_Custom or Build.LibType_Debug. This option can * considerably improve runtime performance as well significantly * reduce the application's code size. * * @see #libType */ config Bool assertsEnabled = true; /*! * ======== logsEnabled ======== * IPC log support in custom library enable flag * * When set to true, IPC execution log code is compiled into * the custom library created when {@link #libType Build.libType} * is set to {@link #LibType_Custom Build_LibType_Custom} or * {@link #LibType_Debug Build_LibType_Debug}. * * When set to false, all log code is removed from the custom * library created when Build.libType = Build.LibType_Custom or * Build.LibType_Debug. This option can considerably improve runtime * performance as well signficantly reduce the application's code * size. * * @see #libType */ config Bool logsEnabled = true; /*! * ======== libDir ======== */ config String libDir = null; /* * ======== getCCOpts ======== * Get the compiler options necessary to build */ metaonly String getCCOpts(String target); /*! * ======== getDefaultCustomCCOpts ======== */ String getDefaultCustomCCOpts(); /*! * ======== getDefs ======== * Get the compiler -D options necessary to build */ String getDefs(); /*! * ======== getCFiles ======== * Get the library C source files. */ String getCFiles(String target); /*! * ======== getAsmFiles ======== * Get the library Asm source files. */ Any getAsmFiles(String target); /* * ======== buildLibs ======== * This function generates the makefile goals for the libraries * produced by a ti.sysbios package. */ function buildLibs(objList, relList, filter, xdcArgs); /*! * ======== getLibs ======== * Common getLibs() for all ipc packages. */ function getLibs(pkg); }