/* * Copyright (c) 2012-2013, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /* * ======== ListMP.xdc ======== * */ import xdc.runtime.Error; import ti.sdo.utils.NameServer; /*! * ======== ListMP ======== * Shared memory linked list * * @p(html) * This module has a common header that can be found in the {@link ti.ipc} * package. Application code should include the common header file (not the * RTSC-generated one): * *
#include <ti/ipc/ListMP.h>* * The RTSC module must be used in the application's RTSC configuration file * (.cfg): * *
ListMP = xdc.useModule('ti.sdo.ipc.ListMP');* * Documentation for all runtime APIs, instance configuration parameters, * error codes macros and type definitions available to the application * integrator can be found in the * Doxygen documenation * for the IPC product. However, the documentation presented on this page * should be referred to for information specific to the RTSC module, such as * module configuration, Errors, and Asserts. * @p */ @InstanceInitError /* Initialization may throw errors */ @InstanceFinalize module ListMP { /*! * ======== BasicView ======== * @_nodoc * ROV view structure representing a ListMP instance. */ metaonly struct BasicView { String label; String type; String gate; } /*! * ======== ElemView ======== * @_nodoc * ROV view structure representing a single list element. */ metaonly struct ElemView { Int index; String srPtr; String addr; } /*! * ======== rovViewInfo ======== * @_nodoc */ @Facet metaonly config xdc.rov.ViewInfo.Instance rovViewInfo = xdc.rov.ViewInfo.create({ viewMap: [ ['Basic', { type: xdc.rov.ViewInfo.INSTANCE, viewInitFxn: 'viewInitBasic', structName: 'BasicView' } ], ['Lists', { type: xdc.rov.ViewInfo.INSTANCE_DATA, viewInitFxn: 'viewInitLists', structName: 'ElemView' } ], ] }); /*! * ======== maxRuntimeEntries ======== * Maximum number of ListMP's that can be dynamically created * and added to the NameServer. */ metaonly config UInt maxRuntimeEntries = NameServer.ALLOWGROWTH; /*! * ======== maxNameLen ======== * Maximum length for names. */ metaonly config UInt maxNameLen = 32; /*! * ======== tableSection ======== * Section name is used to place the names table */ metaonly config String tableSection = null; instance: /*! * ======== gate ======== * GateMP used for critical region management of the shared memory * * Using the default value of NULL will result in the default GateMP * being used for context protection. */ config GateMP.Handle gate = null; /*! @_nodoc * ======== openFlag ======== * Set to 'true' by the {@link #open}. */ config Bool openFlag = false; /*! @_nodoc * ======== sharedAddr ======== * Physical address of the shared memory * * The shared memory that will be used for maintaining shared state * information. This is an optional parameter to create. If value * is null, then the shared memory for the new instance will be * allocated from the heap in {@link #regionId}. */ config Ptr sharedAddr = null; /*! * ======== name ======== * Name of the instance * * The name must be unique among all ListMP instances in the sytem. * When using {@link #regionId} to create a new instance, the name must * not be null. */ config String name = null; /*! * ======== regionId ======== * SharedRegion ID. * * The ID corresponding to the index of the shared region in which this * shared instance is to be placed. This is used in create() only when * {@link #name} is not null. */ config UInt16 regionId = 0; /*! @_nodoc * ======== metaListMP ======== * Used to store elem before the object is initialized. */ metaonly config any metaListMP[]; internal: /* not for client use */ const UInt32 CREATED = 0x12181964; /*! * ======== Elem ======== * Opaque ListMP element * * A field of this type must be placed at the head of client structs. */ @Opaque struct Elem { volatile SharedRegion.SRPtr next; /* volatile for whole_program */ volatile SharedRegion.SRPtr prev; /* volatile for whole_program */ }; /*! * ======== nameSrvPrms ======== * This Params object is used for temporary storage of the * module wide parameters that are for setting the NameServer instance. */ metaonly config NameServer.Params nameSrvPrms; /*! * ======== elemClear ======== * Clears a ListMP element's pointers * * This API is not for removing elements from a ListMP, and * should never be called on an element in a ListMP--only on deListed * elements. * * @param(elem) element to be cleared */ Void elemClear(Elem *elem); /* Initialize shared memory */ Void postInit(Object *obj, Error.Block *eb); /*! Structure of attributes in shared memory */ struct Attrs { Bits32 status; /* Created stamp */ SharedRegion.SRPtr gateMPAddr; /* GateMP SRPtr (shm safe) */ Elem head; /* head of list */ }; /* instance object */ struct Instance_State { Attrs *attrs; /* local pointer to attrs */ Ptr nsKey; /* for removing NS entry */ Ipc.ObjType objType; /* Static/Dynamic? open/creator? */ GateMP.Handle gate; /* Gate for critical regions */ SizeT allocSize; /* Shared memory allocated */ UInt16 regionId; /* SharedRegion ID */ Bool cacheEnabled; /* Whether to do cache calls */ SizeT cacheLineSize; /* The region cache line size */ }; /* module object */ struct Module_State { NameServer.Handle nameServer; }; }