/* * Copyright (c) 2012-2018, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /* * ======== SharedRegion.xdc ======== * */ package ti.sdo.ipc; import xdc.runtime.Error; import xdc.runtime.IHeap; import xdc.rov.ViewInfo; /*! * ======== SharedRegion ======== * Shared memory manager and address translator. * * @p(html) * This module has a common header that can be found in the {@link ti.ipc} * package. Application code should include the common header file (not the * RTSC-generated one): * *
#include <ti/ipc/SharedRegion.h>* * The RTSC module must be used in the application's RTSC configuration file * (.cfg) if runtime APIs will be used in the application: * *
SharedRegion = xdc.useModule('ti.sdo.ipc.SharedRegion');* * Documentation for all runtime APIs, instance configuration parameters, * error codes macros and type definitions available to the application * integrator can be found in the * Doxygen documenation * for the IPC product. However, the documentation presented on this page * should be referred to for information specific to the RTSC module, such as * module configuration, Errors, and Asserts. * @p * * The SharedRegion module is designed to be used in a multi-processor * environment in which memory regions are shared and accessed * across different processors. The module itself does not use any shared * memory, because all module state is stored locally. SharedRegion * APIs use the system gate for thread protection. * * This module creates and stores a local shared memory region table. The * table contains the processor's view for every shared region in the system. * The table must not contain any overlapping regions. Each processor's * view of a particular shared memory region is determined by the region id. * In cases where a processor cannot access a certain shared memory region, * that shared memory region should be left invalid for that processor. * Note: The {@link #numEntries} must be the same on all processors. * * Each shared region contains the following: * @p(blist) * -base: The base address * -len: The length * -name: The name of the region * -isValid: Whether the region is valid * -ownerProcId: The id of the processor which owns the region * -cacheEnable: Whether the region is cacheable * -cacheLineSize: The cache line size * -createHeap: Whether a heap is created for the region. * @p * * A region is added statically using the {@link #setEntryMeta} API. * The length of a region must be the same across all processors. * The owner of the region can be specified. If specified, the owner * manages the shared region. It creates a HeapMemMP instance which spans * the full size of the region. The other processors open the same HeapMemMP * instance. * * Note: Prior to calling Ipc_start(), If a SharedRegion's 'isValid' * is true and 'createHeap' is true then the owner of the SharedRegion * must be the same as the owner of SharedRegion 0. * * An example of a SharedRegion configuration is as follows: * * @p(code) * * var SharedRegion = xdc.useModule('ti.sdo.ipc.SharedRegion'); * SharedRegion.setEntryMeta(0, * { base: 0x80000000, * len: 0x20000, * ownerProcId: 0, * isValid: true, * cacheLineSize: 64, * name: "DDR2", * }); * * @p * * The shared region table along with a shared region pointer (SRPtr) * is used to do address translation at runtime. The shared region * pointer is a 32-bit portable pointer composed of an id and offset. * The most significant bits of a SRPtr are used for the id. * The id corresponds to the index of the entry in the table. * The offset is the offset from the base of the shared memory region. * The number of entries in the table determines the number of bits to * use for the id. Increasing the number of entries increases the * range of ids but decreases the range of the offset. * * Note: Region 0 must be visible by all processors. Region 0 is used for * synchonizing the processors, creating the default GateMP, and * creating Notify and MessageQ transport instances. The HeapMemMP * created in Region 0 is the length of the region minus memory * reserved for creating these internal instances. * * Refer to the doxygen documentation for run-time API documenation. * */ module SharedRegion { /*! * ======== RegionView ======== * @_nodoc */ metaonly struct RegionView { UInt16 id; String base; String end; String len; UInt16 ownerProcId; Bool cacheEnable; Bool isValid; UInt16 cacheLineSize; SizeT reservedSize; Ptr heap; String name; }; /*! * ======== rovViewInfo ======== * @_nodoc */ @Facet metaonly config xdc.rov.ViewInfo.Instance rovViewInfo = xdc.rov.ViewInfo.create({ viewMap: [ ['Regions', { type: xdc.rov.ViewInfo.MODULE_DATA, viewInitFxn: 'viewInitRegions', structName: 'RegionView' } ] ] }); /*! * Definition of shared region pointer type */ typedef Bits32 SRPtr; /*! * Assert raised when the id is larger than numEntries. */ config xdc.runtime.Assert.Id A_idTooLarge = {msg: "A_idTooLarge: id cannot be larger than numEntries"}; /*! * Assert raised when an address is out of the range of the region id. */ config xdc.runtime.Assert.Id A_addrOutOfRange = {msg: "A_addrOutOfRange: Address is out of region id's range"}; /*! * Assert raised when attempting to clear region 0 */ config xdc.runtime.Assert.Id A_region0Clear = {msg: "A_region0Clear: Region 0 cannot be cleared"}; /*! * Assert raised when region zero is invalid */ config xdc.runtime.Assert.Id A_region0Invalid = {msg: "A_region0Invalid: Region zero is invalid"}; /*! * Assert raised when region is invalid */ config xdc.runtime.Assert.Id A_regionInvalid = {msg: "A_regionInvalid: Region is invalid"}; /*! * Assert raised when the trying to reserve too much memory. */ config xdc.runtime.Assert.Id A_reserveTooMuch = {msg: "A_reserveTooMuch: Trying to reserve too much memory"}; /*! * Assert raised when cache enabled but cache line size = 0. */ config xdc.runtime.Assert.Id A_cacheLineSizeIsZero = {msg: "A_cacheLineSizeIsZero: cache line size cannot be zero"}; /*! * Assert raised when a new entry overlaps an existing one. */ config xdc.runtime.Assert.Id A_overlap = {msg: "A_overlap: Shared region overlaps"}; /*! * Assert raised when a valid table entry already exists. */ config xdc.runtime.Assert.Id A_alreadyExists = {msg: "A_alreadyExists: Trying to overwrite an existing valid entry"}; /*! * Assert raised when trying to use a heap for a region that has no heap */ config xdc.runtime.Assert.Id A_noHeap = {msg: "A_noHeap: Region has no heap"}; /*! * ======== Entry ======== * Structure for specifying a region. * * Each region entry should not overlap with any other entry. The * length of a region should be the same across all processors. * * During static configuration, the 'isValid' field can be set to 'false' * to signify a partially completed entry. This should only be done * if the base address of the entry is not known during static * configuration. The entry can be completed and the * 'isValid' field can be set to true at runtime. * * @field(base) The base address. * @field(len) The length. * @field(ownerProcId) MultiProc id of processor that manages region. * @field(isValid) Whether the region is valid or not. * @field(cacheEnable) Whether the region is cacheable. * @field(cacheLineSize) The cache line size for the region. * @field(createHeap) Whether a heap is created for the region. * @field(name) The name associated with the region. */ struct Entry { Ptr base; Ptr len; UInt16 ownerProcId; Bool isValid; Bool cacheEnable; SizeT cacheLineSize; Bool createHeap; String name; }; metaonly struct MetaEntry { String base_symbol; String len_symbol; Ptr base; SizeT len; UInt16 ownerProcId; Bool isValid; Bool cacheEnable; SizeT cacheLineSize; Bool createHeap; String name; }; /*! Specifies the invalid id */ const UInt16 INVALIDREGIONID = 0xFFFF; /*! Specifies the default owner proc id */ const UInt16 DEFAULTOWNERID = ~0; /*! * Worst-case cache line size * * This is the default system cache line size for all modules. * When a module puts structures in shared memory, this value is * used to make sure items are aligned on a cache line boundary. * If no cacheLineSize is specified for a region, it will use this * value. */ config SizeT cacheLineSize = 128; /*! * The number of shared region table entries. * * This value is used for calculating the number of bits for the offset. * Note: This value must be the same across all processors in the system. * Increasing this parameter will increase the footprint and * the time for translating a pointer to a SRPtr. */ config UInt16 numEntries = 4; /*! * Determines whether address translation is required. * * This configuration parameter should be set to 'false' if and only if all * shared memory regions have the same base address for all processors. * If 'false', it results in a fast {@link #getPtr} and {@link #getSRPtr}, * because a SRPtr is equivalent to a Ptr and no translation is done. */ config Bool translate = true; /*! @_nodoc * Value that corresponds to NULL in SRPtr address space. */ config SRPtr INVALIDSRPTR = 0xFFFFFFFF; /*! @_nodoc * ======== attach ======== * Opens a heap, for non-owner processors, for each SharedRegion. * * Function is called in Ipc_attach(). */ Int attach(UInt16 remoteProcId); /*! @_nodoc * ======== clearReservedMemory ======== * Clears the reserve memory for each region in the table. */ Void clearReservedMemory(); /*! @_nodoc * ======== detach ======== * Close the heap, for non-owner processors when detaching from the owner. * * Function is called in Ipc_detach(). */ Int detach(UInt16 remoteProcId); /*! * ======== genSectionInCmd ======== * Enable/Disable generation of output section in linker cmd file * * This function can be called for each shared region to not generate * an output section in the linker command file. By default all shared * region entries generate an output section in the linker command file. * * @param(id) Region id. * @param(gen) TRUE - generate, FALSE - don't generate */ metaonly Void genSectionInCmd(UInt16 id, Bool gen); /*! * ======== getCacheLineSizeMeta ======== * Meta version of Ipc_getCacheLineSize */ metaonly SizeT getCacheLineSizeMeta(UInt16 id); /*! @_nodoc * ======== getIdMeta ======== * Returns the region id for a given local address * * @param(addr) Address to retrieve the shared region pointer. * * @b(returns) region id */ metaonly UInt16 getIdMeta(Ptr addr); /*! @_nodoc * ======== getPtrMeta ======== * Meta version of {@link #getPtr} */ metaonly Ptr getPtrMeta(SRPtr srptr); /*! @_nodoc * ======== getPtrMeta$view ======== * ROV-time version of getPtrMeta * * @param(srptr) Shared region pointer. * * @b(returns) Pointer associated with shared region pointer. */ metaonly Ptr getPtrMeta$view(SRPtr srptr); /*! @_nodoc * ======== getSRPtrMeta ======== * Meta version of {@link #getSRPtr} */ metaonly SRPtr getSRPtrMeta(Ptr addr); /*! @_nodoc * ======== getSRPtrMeta$view ======== * ROV-time version of getSRPtrMeta * * @param(addr) Address to retrieve the shared region pointer. * * @b(returns) Shared region pointer. */ metaonly SRPtr getSRPtrMeta$view(Ptr addr); /*! @_nodoc * ======== isCacheEnabledMeta ======== * Meta version of {@link #isCacheEnabled} */ metaonly Bool isCacheEnabledMeta(UInt16 id); /*! @_nodoc * ======== reserveMemory ======== * Reserves the specified amount of memory from the specified region id. * * Must be called before Ipc_start(). The amount of memory reserved * must be the same on all cores. * The return pointer is the starting address that was reserved. * * @param(id) Region id. * @param(size) Amount of memory to reserve. * * @b(returns) Starting address of memory reserved. */ Ptr reserveMemory(UInt16 id, SizeT size); /*! @_nodoc * ======== resetInternalFields ======== * Reset the internal fields of a region. * * This function is called in Ipc_stop() to reset the reservedSize * and heap handle. It should not be called by the user. * * @param(id) Region id. */ Void resetInternalFields(UInt16 id); /*! * ======== setEntryMeta ======== * Sets the entry at the specified region id in the shared region table. * * The required parameters are base and len. All the other fields will * get their default if not specified. * * @param(id) Region id. * @param(entry) Entry fields about the region. */ metaonly Void setEntryMeta(UInt16 id, MetaEntry metaentry); /*! @_nodoc * ======== start ======== * Creates a heap by owner of region for each SharedRegion. * * Function is called by Ipc_start(). Requires that SharedRegion 0 * be valid before calling start(). */ Int start(); /*! @_nodoc * ======== stop ======== * Undo what was done by start. * * This function is called by Ipc_stop(). It deletes any heap that * was created in start for the owner of any SharedRegion. For * non-owners, it doesn't do anything. */ Int stop(); internal: const UInt32 CREATED = 0x08111963; /* Information stored on a per region basis */ struct Region { Entry entry; SizeT reservedSize; IHeap.Handle heap; }; /* temporary storage of shared regions */ metaonly config Entry entry[]; /* generate linker section for shared regions */ metaonly config Bool genSectionInLinkCmd[]; /* internal to keep track of the number of entries added */ metaonly config UInt entryCount; /* number of bits for the offset for a SRPtr. This value is calculated */ config UInt32 numOffsetBits; /* offset bitmask using for generating a SRPtr */ config UInt32 offsetMask; /* * ======== checkOverlap ======== * Determines if there is an overlap with an existing entry * * @param(base) Base address of the region * @param(len) Size of the region * * @b(returns) Status if successful or not. */ Int checkOverlap(Ptr base, SizeT len); /* * ======== Module State structure ======== * The regions array contains information for each shared region entry. * The size of the table will be determined by the number of entries. */ struct Module_State { Region regions[]; }; }