/* * Copyright (c) 2012-2015 Texas Instruments Incorporated - http://www.ti.com * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /* * ======== NameServer.xdc ======== * */ import xdc.runtime.Error; import xdc.runtime.Assert; import xdc.runtime.IHeap; import ti.sysbios.gates.GateSwi; import xdc.rov.ViewInfo; /*! * ======== NameServer ======== * Manages and serves names to remote/local processor * * @p(html) * This module has a common header that can be found in the {@link ti.ipc} * package. Application code should include the common header file (not the * RTSC-generated one): * *
#include <ti/ipc/NameServer.h>* * The RTSC module must be used in the application's RTSC configuration file * (.cfg) if runtime APIs will be used in the application: * *
NameServer = xdc.useModule('ti.sdo.ipc.NameServer');* * Documentation for all runtime APIs, instance configuration parameters, * error codes macros and type definitions available to the application * integrator can be found in the * Doxygen documenation * for the IPC product. However, the documentation presented on this page * should be referred to for information specific to the RTSC module, such as * module configuration, Errors, and Asserts. * @p * * @a(Note) * This modules reflects upon the {@link ti.sdo.utils.MultiProc#procAddrMode} * configuration parameter. Some internal data structure allocations are * optimized for the given processor address mode. For example, when using * MultiProc.ProcAddrMode_Global, resource is allocated for every processor * in the system. When using MultiProc.ProcAddrMode_Cluster, resources are * only allocated for processors in the cluster. A side-effect is that when * using Cluster mode, name queries cannot be addressed to processors * outside of the cluster. */ @ModuleStartup @InstanceInitError /* Initialization may throw errors */ @InstanceFinalize module NameServer { /*! * ======== BasicView ======== * @_nodoc */ metaonly struct BasicView { String name; Bool checkExisting; UInt maxNameLen; UInt maxValueLen; UInt numStatic; String numDynamic; } /*! * ======== NamesListView ======== * @_nodoc */ metaonly struct NamesListView { String name; String value; UInt len; Ptr nsKey; } /*! * ======== rovViewInfo ======== * @_nodoc */ @Facet metaonly config xdc.rov.ViewInfo.Instance rovViewInfo = xdc.rov.ViewInfo.create({ viewMap: [ ['Basic', { type: xdc.rov.ViewInfo.INSTANCE, viewInitFxn: 'viewInitBasic', structName: 'BasicView' } ], ['NamesValues', { type: xdc.rov.ViewInfo.INSTANCE_DATA, viewInitFxn: 'viewInitData', structName: 'NamesListView' } ] ] }); /*! * Assert raised when the name or value is too long */ config Assert.Id A_invalidLen = { msg: "A_invalidLen: Invalid length" }; /*! * ======== A_invArgument ======== * Assert raised when an argument is invalid */ config Assert.Id A_invArgument = { msg: "A_invArgument: Invalid argument supplied" }; /*! * Error raised if all the entries in the instance Name/Value table * are taken */ config Error.Id E_maxReached = { msg: "E_maxReached: All entries in use. NameServer.maxRuntimeEntries is %d" }; /*! * Error raised when the name already exists in the instance * Name/Value table */ config Error.Id E_entryExists = { msg: "E_entryExists: %s name already in table " }; /*! * Error raised when creation parameters do not match those of an * existing NameServer */ config Error.Id E_paramMismatch = { msg: "E_paramMismatch: parameters do not match existing NameServer %s " }; /*! * Allow dynamic growth of the NameServer instance table * * This value can be used to set the {@link #maxRuntimeEntries}. * This flag tells NameServer to allow dynamic growth * of the table. */ const UInt ALLOWGROWTH = (~0); /*! * Structure of entry in Name/Value table * * This structure is returned from the {@link #getMeta} * API. * * @field(name) Name portion of the name/value pair. * @field(len) Length of the value field. * @field(value) Value portion of the name/value entry. */ metaonly struct Entry { String name; UInt len; UArg value; }; /*! * ======== SetupProxy ======== * NameServer setup proxy */ proxy SetupProxy inherits INameServerRemote; /*! * ======== isRegistered ======== * Determines if a remote driver is registered for the specified id. * * @param(procId) The remote processor id. */ @DirectCall Bool isRegistered(UInt16 procId); /*! * ======== registerRemoteDriver ======== * Register the NameServer remote handle for the specified processor id. * * This function is used by NameServer remote driver to register * themselves with NameServer. Only one remote driver can be registered * with a remote processor. The API returns {@link #Status_FAIL} if there * is already a registered remote driver for the processor id. * * @param(handle) The handle for a NameServer remote driver instance. * @param(procId) The remote processor id. * * @b(returns) Returns {@link #Status_SUCCESS} if successful or * {@link #Status_FAIL} if the processor id has already * been set. */ @DirectCall Int registerRemoteDriver(INameServerRemote.Handle handle, UInt16 procId); /*! * ======== unregisterRemoteDriver ======== * Unregister the NameServer remote handle for the specified processor id. * * This function is used by NameServer Remote implementations to unregister * themselves with NameServer. * * @param(procId) The remote processor id to unregister. */ @DirectCall Void unregisterRemoteDriver(UInt16 procId); /*! * ======== modAddMeta ======== * Add a name/value pair into the specified instance's table during * configuration * * This function adds any length value into the local table. The function * makes sure the name does not already exist in the local table. * * This function should be used by modules when adding into a NameServer * instance. The application configuration file, should * use {@link #addMeta}. * * The function does not query remote processors to make sure the * name is unique. * * @param(instName) NameServer instance name * @param(name) Name portion of the name/value pair * @param(value) Value portion of the name/value pair * @param(len) Length of the value buffer */ metaonly Void modAddMeta(String instName, String name, Any value, UInt len); /*! * ======== getName$view ======== * @_nodoc * Used at ROV time to display reverse-lookup name from 32-bit value and * tableName */ metaonly String getName$view(String tableName, UInt32 value); /*! * ======== getNameByKey$view ======== * @_nodoc * ROV function for retrieving an entry by its address. Throws an exception * if the name was not found */ metaonly String getNameByKey$view(Ptr addr); instance: /*! * Maximum number of name/value pairs that can be dynamically created. * * This parameter allows NameServer to pre-allocate memory. * When NameServer_add or NameServer_addUInt32 is called, no memory * allocation occurs. * * If the number of pairs is not known at configuration time, set this * value to {@link #ALLOWGROWTH}. This instructs NameServer to grow the * table as needed. NameServer will allocate memory from the * {@link #tableHeap} when a name/value pair is added. * * The default is {@link #ALLOWGROWTH}. */ config UInt maxRuntimeEntries = ALLOWGROWTH; /*! * Name/value table is allocated from this heap. * * The instance table and related buffers are allocated out of this heap * during the dynamic create. This heap is also used to allocate new * name/value pairs when {@link #ALLOWGROWTH} for * {@link #maxRuntimeEntries} * * The default is to use the same heap that instances are allocated * from which can be configured via the * NameServer.common$.instanceHeap configuration parameter. */ config IHeap.Handle tableHeap = null; /*! * Name/value table is placed into this section on static creates. * * The instance table and related buffers are placed into this section * during the static create. * * The default is no explicit section placement. */ metaonly config String tableSection = null; /*! * Check if a name already exists in the name/value table. * * When a name/value pair is added during runtime, if this boolean is true, * the table is searched to see if the name already exists. If it does, * the name is not added and the {@link #E_entryExists} error is raised. * * If this flag is false, the table will not be checked to see if the name * already exists. It will simply be added. This mode has better * performance at the expense of potentially having non-unique names in the * table. * * This flag is used for runtime adds only. Adding non-unique names during * configuration results in a build error. */ config Bool checkExisting = true; /*! * Length, in MAUs, of the value field in the table. * * Any value less than sizeof(UInt32) will be rounded up to sizeof(UInt32). */ config UInt maxValueLen = 0; /*! * Length, in MAUs, of the name field in the table. * * The maximum length of the name portion of the name/value * pair. The length includes the null terminator ('\0'). */ config UInt maxNameLen = 16; /*! * ======== metaTable ======== * @_nodoc * Table to hold the statically added name/value pairs until * they ready to be added to the object. */ metaonly config Entry metaTable[]; /*! * ======== create ======== * @_nodoc (Refer to doxygen for ti/ipc/NameServer.h) * Create a NameServer instance * * This function creates a NameServer instance. The name is * used for remote processor queries and diagnostic tools. For * single processor system (e.g. no remote queries), the name * can be NULL. * * @param(name) Name of the instance */ create(String name); /*! * ======== addUInt32Meta ======== * Add a name/value pair into the instance's table during configuration * * This function adds a UInt32 value into the local table. The function * makes sure the name does not already exist in the local table. * * The function does not query remote processors to make sure the * name is unique. * * @param(name) Name portion of the name/value pair * @param(value) Value portion of the name/value pair */ metaonly Void addUInt32Meta(String name, any value); /*! * ======== addMeta ======== * Add a name/value pair into the instance's table during configuration * * This function adds any length value into the local table. The function * makes sure the name does not already exist in the local table. * * This function should be used by within the application configuration * file. XDC modules should use {@link #modAddMeta}. * * The function does not query remote processors to make sure the * name is unique. * * @param(name) Name portion of the name/value pair * @param(value) Value portion of the name/value pair * @param(len) Length of the value buffer */ metaonly Void addMeta(String name, Any value, UInt len); /*! * ======== getMeta ======== * Retrieves the name/value entry * * If the name is found, the entry is returned. The caller can parse the * entry as needed. If the name is not found, null is returned. * * The search only occurs on the local table. * * @param(name) Name in question * * @b(returns) Name/value entry */ metaonly Entry getMeta(String name); /*! * ======== getKey ======== * @_nodoc * Returns a pointer to the TableEntry containing the argument 'val'. * This should only be used internally by Ipc modules during their * initialization process. * * This function can only be used when maxValueLen = sizeof(UInt32) */ @DirectCall Ptr getKey(UInt32 val); internal: /* Used to eliminate code when doing whole-program */ config Bool singleProcessor = true; metaonly typedef Entry EntryMap[]; /*! Structure of entry in Name/Value table */ struct TableEntry { List.Elem elem; String name; UInt len; UArg value; }; /*! * ======== metaModTable ======== * Table to hold the static added name/value pairs until * they ready to be added to the object. */ metaonly config EntryMap metaModTable[string]; /* * ======== postInit ======== * Finish initializing static and dynamic NameServer instances */ Int postInit(Object *obj); /* * ======== findLocal ======== * Searches to the local instance table. * * This is an internal function because it returns an internal structure. */ TableEntry *findLocal(Object *obj, String name); /* * ======== removeLocal ======== * removes an entry from the local instance table. */ Void removeLocal(Object *obj, TableEntry *entry); /* * ======== editLocal ======== * replaces the value of an entry from the local instance table. */ Void editLocal(Object *obj, TableEntry *entry, Ptr newValue); /* instance object */ struct Instance_State { String name; /* Name of the instance */ List.Object freeList; /* Empty entries list */ List.Object nameList; /* Filled entries list */ UInt maxNameLen; /* Max name length */ UInt maxValueLen; /* Max value length */ UInt numStatic; /* Total static entries in table */ UInt numDynamic; /* Total dynamic entries in table */ TableEntry table[]; /* Table */ Char names[]; /* Buffer for names */ UInt8 values[]; /* Buffer for values */ IHeap.Handle tableHeap; /* Heap used to alloc table */ Bool checkExisting; /* check ig name already exists */ UInt32 refCount; /* reference count to this instance */ }; struct Module_State { INameServerRemote.Handle nsRemoteHandle[length]; GateSwi.Handle gate; }; }