/* * Copyright (c) 2012-2013, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /* * ======== OmapRpc.h ======== * OMAP Remote Procedure Call Driver. * */ #ifndef ti_srvmgr_OmapRpc__include #define ti_srvmgr_OmapRpc__include #include #include #if defined (__cplusplus) extern "C" { #endif /*! * @def OmapRpc_S_SUCCESS * @brief Operation is successful. */ #define OmapRpc_S_SUCCESS 0 /*! * @def OmapRpc_E_FAIL * @brief Operation is not successful. */ #define OmapRpc_E_FAIL -1 #define OmapRpc_NUM_PARAMETERS(size) \ ((size)/sizeof(struct OmapRpc_Parameter)) #define OmapRpc_PAYLOAD(ptr, type) \ ((struct type *)&(ptr)[sizeof(struct OmapRpc_MsgHeader)]) #define OmapRpc_PARAM(param, type) ((param).size == sizeof(type) ? (type)(param).data : 0) #define OmapRpc_Stringerize(func) #func #define OmapRpc_dimof(x) (sizeof(x)/sizeof((x)[0])) #define OmapRpc_DESC_EXEC_SYNC (0x0100) #define OmapRpc_DESC_EXEC_ASYNC (0x0200) #define OmapRpc_DESC_SYM_ADD (0x0300) #define OmapRpc_DESC_SYM_IDX (0x0400) #define OmapRpc_DESC_CMD (0x0500) #define OmapRpc_DESC_TYPE_MASK (0x0F00) #define OmapRpc_JOBID_DISCRETE (0) #define OmapRpc_POOLID_DEFAULT (0x8000) #define OmapRpc_SET_FXN_IDX(idx) ((idx) | 0x80000000) #define OmapRpc_FXN_MASK(idx) ((idx) & 0x7FFFFFFF) #define OMAPRPC_MAX_CHANNEL_NAMELEN (64) #define OMAPRPC_MAX_FUNC_NAMELEN (64) #define OMAPRPC_MAX_NUM_PARAMS (10) #define OMAPRPC_MAX_INST_NAMELEN (48) typedef enum OmapRpc_InfoType { /** The function signature */ OmapRpc_InfoType_FUNC_SIGNATURE = 1, /** The number of times a function has been called */ OmapRpc_InfoType_NUM_CALLS, /** The performance information releated to the function */ OmapRpc_InfoType_FUNC_PERFORMANCE, /** @hidden used to define the maximum info type */ OmapRpc_InfoType_MAX } OmapRpc_InfoType; /** The applicable types of messages that the HOST may send the SERVICE. */ typedef enum OmapRpc_MsgType { /** Ask Service for channel information, uses \ref OmapRpc_ChannelInfo */ OmapRpc_MsgType_QUERY_CHAN_INFO = 0, /** The return message from OMAPRPC_MSG_QUERY_CHAN_INFO*/ OmapRpc_MsgType_CHAN_INFO = 1, /** Ask the Service Instance to send information about the Service. * Uses \ref OmapRpc_QueryFunction */ OmapRpc_MsgType_QUERY_FUNCTION = 2, /** The return message from OMAPRPC_QUERY_INSTANCE, * which contains the information about the instance. * Uses \ref OmapRpc_Instance_Info */ OmapRpc_MsgType_FUNCTION_INFO = 3, /** Ask the ServiceMgr to create a new instance of the service. * No secondary data is needed. */ OmapRpc_MsgType_CREATE_INSTANCE = 6, /** The return message from OMAPRPC_CREATE_INSTANCE, * contains the new endpoint address in the OmapRpc_InstanceHandle */ OmapRpc_MsgType_INSTANCE_CREATED = 8, /** Ask the Service Mgr to destroy an instance */ OmapRpc_MsgType_DESTROY_INSTANCE = 4, /** The return message from OMAPRPC_DESTROY_INSTANCE. * contains the old endpoint address in the OmapRpc_InstanceHandle */ OmapRpc_MsgType_INSTANCE_DESTROYED = 7, /** Ask the Service Instance to call a particular function */ OmapRpc_MsgType_CALL_FUNCTION = 5, /** The return values from a function call */ OmapRpc_MsgType_FUNCTION_RETURN = 9, /** Returned from either the ServiceMgr or Service Instance * when an error occurs */ OmapRpc_MsgType_ERROR = 10, /** \hidden used to define the max msg enum, not an actual message */ OmapRpc_MsgType_MAX } OmapRpc_MsgType; typedef enum OmapRpc_ErrorType { /**< No errors to report */ OmapRpc_ErrorType_NONE = 0, /**< Not enough memory exist to process request */ OmapRpc_ErrorType_NOT_ENOUGH_MEMORY, /**< The instance died */ OmapRpc_ErrorType_INSTANCE_DIED, /**< Some resource was unavailable. */ OmapRpc_ErrorType_RESOURCE_UNAVAILABLE, /**< A provided parameter was either out of range, incorrect or NULL */ OmapRpc_ErrorType_BAD_PARAMETER, /**< The requested item is not supported */ OmapRpc_ErrorType_NOT_SUPPORTED, /** @hidden used to define the max error value */ OmapRpc_ErrorType_MAX_VALUE } OmapRpc_ErrorType; typedef struct OmapRpc_CreateInstance { Char name[OMAPRPC_MAX_INST_NAMELEN]; } OmapRpc_CreateInstance; typedef struct OmapRpc_ChannelInfo { UInt32 numFuncs; /**< The number of functions supported on this endpoint */ } OmapRpc_ChannelInfo; typedef struct OmapRpc_FuncPerf { UInt32 clocksPerSec; UInt32 clockCycles; } OmapRpc_FuncPerf; /** The parameter direction as relative to the function it describes */ typedef enum OmapRpc_Direction { OmapRpc_Direction_In = 0, OmapRpc_Direction_Out, OmapRpc_Direction_Bi, OmapRpc_Direction_MAX } OmapRpc_Direction; typedef enum OmapRpc_Param_Type { OmapRpc_Param_VOID = 0, OmapRpc_Param_S08, OmapRpc_Param_U08, OmapRpc_Param_S16, OmapRpc_Param_U16, OmapRpc_Param_S32, OmapRpc_Param_U32, OmapRpc_Param_S64, OmapRpc_Param_U64, OmapRpc_Param_PTR = 0x80, /**< Logically OR'd with lower type to make a pointer to the correct type */ OmapRpc_Param_MAX } OmapRpc_Param_Type; #define OmapRpc_PtrType(type) ((type) | OmapRpc_Param_PTR) typedef struct OmapRpc_ParamSignature { UInt32 direction; /**< @see OmapRpc_Direction */ UInt32 type; /**< @see OmapRpc_Param_Type */ UInt32 count; /**< Used to do some basic sanity checking on array bounds */ } OmapRpc_ParamSignature; /** * This is the data structure that represents the function signature. * @note The first parameter (params[0]) is the return value. */ typedef struct OmapRpc_FuncSignature { Char name[OMAPRPC_MAX_FUNC_NAMELEN]; UInt32 numParam; OmapRpc_ParamSignature params[OMAPRPC_MAX_NUM_PARAMS+1]; } OmapRpc_FuncSignature; /** * \brief Function Query Structure. * \details This is used by the host first to ask the remote side for details * about it's published functions */ typedef struct OmapRpc_QueryFunction { UInt32 infoType; /**< @see OmapRpc_InfoType */ UInt32 funcIndex; /**< The function index to query */ union info { UInt32 numCalls; OmapRpc_FuncPerf performance; OmapRpc_FuncSignature signature; } info; } OmapRpc_QueryFunction; /** @brief The generic OMAPRPC message header. * (actually a copy of omx_msg_hdr which is a copy of an RCM header) */ typedef struct OmapRpc_MsgHeader { UInt32 msgType; /**< @see OmapRpc_MsgType */ UInt32 msgLen; /**< The length of the message data in bytes */ } OmapRpc_MsgHeader; typedef struct OmapRpc_InstanceHandle { UInt32 endpointAddress; UInt32 status; } OmapRpc_InstanceHandle; typedef struct OmapRpc_Error { UInt32 endpointAddress; UInt32 status; } OmapRpc_Error; typedef struct OmapRpc_Parameter { SizeT size; SizeT data; } OmapRpc_Parameter; /** This is actually a frankensteined structure of RCM */ typedef struct OmapRpc_Packet{ UInt16 desc; /**< @see RcmClient_Packet.desc */ UInt16 msgId; /**< @see RcmClient_Packet.msgId */ UInt16 poolId; /**< @see RcmClient_Message.poolId */ UInt16 jobId; /**< @see RcmClient_Message.jobId */ UInt32 fxnIdx; /**< @see RcmClient_Message.fxnIdx */ Int32 result; /**< @see RcmClient_Message.result */ UInt32 dataSize; /**< @see RcmClient_Message.data_size */ } OmapRpc_Packet; /** An OmapRpc Function is really an RCM function */ typedef RcmServer_MsgFxn OmapRpc_Function; /** * \brief The Function Declaration Structure. * \details This structure is used to declare the function signature and their * associated functions */ typedef struct OmapRpc_FuncDeclaration { OmapRpc_Function function; /**< \brief The function pointer */ OmapRpc_FuncSignature signature; /**< \brief The signature of the function */ } OmapRpc_FuncDeclaration; typedef struct OmapRpc_Object *OmapRpc_Handle; typedef Void (*OmapRpc_SrvDelNotifyFxn)(Void); #if 0 OmapRpc_Handle OmapRpc_createChannel(String channelName, UInt16 dstProc, UInt32 port, UInt32 numFuncs, OmapRpc_FuncDeclaration* fxns, OmapRpc_SrvDelNotifyFxn func); #else OmapRpc_Handle OmapRpc_createChannel(String channelName, UInt16 dstProc, UInt32 port, RcmServer_Params *rcmParams, MmType_FxnSigTab *fxnSigTab, OmapRpc_SrvDelNotifyFxn srvDelCBFunc); #endif Int OmapRpc_deleteChannel(OmapRpc_Handle handle); #if defined (__cplusplus) } #endif /* defined (__cplusplus) */ /*@}*/ #endif /* ti_srvmgr_OmapRpc__include */