/* * Copyright (c) 2012-2013, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /*============================================================================ * @file MessageQ.c * * @brief MessageQ module "client" implementation * * This implementation is geared for use in a "client/server" model, whereby * system-wide data is maintained in a "server" component and process- * specific data is handled here. At the moment, this implementation * connects and communicates with LAD for the server connection. * * The MessageQ module supports the structured sending and receiving of * variable length messages. This module can be used for homogeneous or * heterogeneous multi-processor messaging. * * MessageQ provides more sophisticated messaging than other modules. It is * typically used for complex situations such as multi-processor messaging. * * The following are key features of the MessageQ module: * -Writers and readers can be relocated to another processor with no * runtime code changes. * -Timeouts are allowed when receiving messages. * -Readers can determine the writer and reply back. * -Receiving a message is deterministic when the timeout is zero. * -Messages can reside on any message queue. * -Supports zero-copy transfers. * -Can send and receive from any type of thread. * -Notification mechanism is specified by application. * -Allows QoS (quality of service) on message buffer pools. For example, * using specific buffer pools for specific message queues. * * Messages are sent and received via a message queue. A reader is a thread * that gets (reads) messages from a message queue. A writer is a thread that * puts (writes) a message to a message queue. Each message queue has one * reader and can have many writers. A thread may read from or write to multiple * message queues. * * Conceptually, the reader thread owns a message queue. The reader thread * creates a message queue. Writer threads a created message queues to * get access to them. * * Message queues are identified by a system-wide unique name. Internally, * MessageQ uses the NameServermodule for managing * these names. The names are used for opening a message queue. Using * names is not required. * * Messages must be allocated from the MessageQ module. Once a message is * allocated, it can be sent on any message queue. Once a message is sent, the * writer loses ownership of the message and should not attempt to modify the * message. Once the reader receives the message, it owns the message. It * may either free the message or re-use the message. * * Messages in a message queue can be of variable length. The only * requirement is that the first field in the definition of a message must be a * MsgHeader structure. For example: * typedef struct MyMsg { * MessageQ_MsgHeader header; * ... * } MyMsg; * * The MessageQ API uses the MessageQ_MsgHeader internally. Your application * should not modify or directly access the fields in the MessageQ_MsgHeader. * * All messages sent via the MessageQ module must be allocated from a * Heap implementation. The heap can be used for * other memory allocation not related to MessageQ. * * An application can use multiple heaps. The purpose of having multiple * heaps is to allow an application to regulate its message usage. For * example, an application can allocate critical messages from one heap of fast * on-chip memory and non-critical messages from another heap of slower * external memory * * MessageQ does support the usage of messages that allocated via the * alloc function. Please refer to the staticMsgInit * function description for more details. * * In a multiple processor system, MessageQ communications to other * processors via MessageQTransport instances. There must be one and * only one MessageQTransport instance for each processor where communication * is desired. * So on a four processor system, each processor must have three * MessageQTransport instance. * * The user only needs to create the MessageQTransport instances. The instances * are responsible for registering themselves with MessageQ. * This is accomplished via the registerTransport function. * * ============================================================================ */ /* Standard headers */ #include /* Linux specific header files, replacing OSAL: */ #include /* Module level headers */ #include #include #include <_MultiProc.h> #include #include <_MessageQ.h> #include <_log.h> #include #include #include #include #include #include #include #include #include #include #include #include #include /* TI IPC utils: */ #include #include /* ============================================================================= * Macros/Constants * ============================================================================= */ /*! * @brief Name of the reserved NameServer used for MessageQ. */ #define MessageQ_NAMESERVER "MessageQ" /* More magic rpmsg port numbers: */ #define MESSAGEQ_RPMSG_PORT 61 #define MESSAGEQ_RPMSG_MAXSIZE 512 #define RPMSG_RESERVED_ADDRESSES (1024) /* Trace flag settings: */ #define TRACESHIFT 12 #define TRACEMASK 0x1000 /* ============================================================================= * Structures & Enums * ============================================================================= */ /* structure for MessageQ module state */ typedef struct MessageQ_ModuleObject { Int refCount; /*!< Reference count */ NameServer_Handle nameServer; /*!< Handle to the local NameServer used for storing GP objects */ pthread_mutex_t gate; /*!< Handle of gate to be used for local thread safety */ MessageQ_Params defaultInstParams; /*!< Default instance creation parameters */ int ipcFd[MultiProc_MAXPROCESSORS]; /*!< File Descriptors for sending to each remote processor */ int seqNum; /*!< Process-specific sequence number */ } MessageQ_ModuleObject; /*! * @brief Structure for the Handle for the MessageQ. */ typedef struct MessageQ_Object_tag { MessageQ_Params params; /*! Instance specific creation parameters */ MessageQ_QueueId queue; /* Unique id */ int ipcFd; /* File Descriptors to receive from a message queue. */ int unblockFdW; /* Write this fd to unblock the select() call in MessageQ _get() */ int unblockFdR; /* File Descriptor to block on to listen to unblockFdW. */ void *serverHandle; } MessageQ_Object; static Bool verbose = FALSE; /* ============================================================================= * Globals * ============================================================================= */ static MessageQ_ModuleObject MessageQ_state = { .refCount = 0, .nameServer = NULL, }; /*! * @var MessageQ_module * * @brief Pointer to the MessageQ module state. */ MessageQ_ModuleObject * MessageQ_module = &MessageQ_state; /* ============================================================================= * Forward declarations of internal functions * ============================================================================= */ /* This is a helper function to initialize a message. */ static Int transportCreateEndpoint(int * fd, UInt16 queueIndex); static Int transportCloseEndpoint(int fd); static Int transportGet(int fd, MessageQ_Msg * retMsg); static Int transportPut(MessageQ_Msg msg, UInt16 dstId, UInt16 dstProcId); /* ============================================================================= * APIS * ============================================================================= */ /* Function to get default configuration for the MessageQ module. * */ Void MessageQ_getConfig (MessageQ_Config * cfg) { Int status; MessageQDrv_CmdArgs cmdArgs; assert (cfg != NULL); cmdArgs.args.getConfig.config = cfg; status = MessageQDrv_ioctl (CMD_MESSAGEQ_GETCONFIG, &cmdArgs); if (status < 0) { PRINTVERBOSE1("MessageQ_getConfig: API (through IOCTL) failed, \ status=%d\n", status) } return; } /* Function to setup the MessageQ module. */ Int MessageQ_setup (const MessageQ_Config * cfg) { Int status; MessageQDrv_CmdArgs cmdArgs; Int i; cmdArgs.args.setup.config = (MessageQ_Config *) cfg; status = MessageQDrv_ioctl(CMD_MESSAGEQ_SETUP, &cmdArgs); if (status < 0) { PRINTVERBOSE1("MessageQ_setup: API (through IOCTL) failed, \ status=%d\n", status) return status; } MessageQ_module->nameServer = cmdArgs.args.setup.nameServerHandle; MessageQ_module->seqNum = 0; /* Create a default local gate. */ pthread_mutex_init (&(MessageQ_module->gate), NULL); /* Clear ipcFd array. */ for (i = 0; i < MultiProc_MAXPROCESSORS; i++) { MessageQ_module->ipcFd[i] = -1; } return status; } /* * Function to destroy the MessageQ module. */ Int MessageQ_destroy (void) { Int status; MessageQDrv_CmdArgs cmdArgs; status = MessageQDrv_ioctl (CMD_MESSAGEQ_DESTROY, &cmdArgs); if (status < 0) { PRINTVERBOSE1("MessageQ_destroy: API (through IOCTL) failed, \ status=%d\n", status) } return status; } /* Function to initialize the parameters for the MessageQ instance. */ Void MessageQ_Params_init (MessageQ_Params * params) { memcpy (params, &(MessageQ_module->defaultInstParams), sizeof (MessageQ_Params)); return; } /* * Function to create a MessageQ object for receiving. * * Create a file descriptor and bind the source address * (local ProcId/MessageQ ID) in * order to get messages dispatched to this messageQ. */ MessageQ_Handle MessageQ_create (String name, const MessageQ_Params * params) { Int status = MessageQ_S_SUCCESS; MessageQ_Object * obj = NULL; UInt16 queueIndex = 0u; UInt16 procId; MessageQDrv_CmdArgs cmdArgs; int fildes[2]; cmdArgs.args.create.params = (MessageQ_Params *) params; cmdArgs.args.create.name = name; if (name != NULL) { cmdArgs.args.create.nameLen = (strlen (name) + 1); } else { cmdArgs.args.create.nameLen = 0; } status = MessageQDrv_ioctl (CMD_MESSAGEQ_CREATE, &cmdArgs); if (status < 0) { PRINTVERBOSE1("MessageQ_create: API (through IOCTL) failed, \ status=%d\n", status) return NULL; } /* Create the generic obj */ obj = (MessageQ_Object *)calloc(1, sizeof (MessageQ_Object)); if (params != NULL) { /* Populate the params member */ memcpy((Ptr) &obj->params, (Ptr)params, sizeof (MessageQ_Params)); } procId = MultiProc_self(); queueIndex = (MessageQ_QueueIndex)cmdArgs.args.create.queueId; obj->queue = cmdArgs.args.create.queueId; obj->serverHandle = cmdArgs.args.create.handle; PRINTVERBOSE2("MessageQ_create: creating endpoint for: %s, \ queueIndex: %d\n", name, queueIndex) status = transportCreateEndpoint(&obj->ipcFd, queueIndex); if (status < 0) { goto cleanup; } /* * Now, to support MessageQ_unblock() functionality, create an event object. * Writing to this event will unblock the select() call in MessageQ_get(). */ if (pipe(fildes) == -1) { printf ("MessageQ_create: pipe creation failed: %d, %s\n", errno, strerror(errno)); status = MessageQ_E_FAIL; } obj->unblockFdW = fildes[1]; obj->unblockFdR = fildes[0]; cleanup: /* Cleanup if fail: */ if (status < 0) { MessageQ_delete((MessageQ_Handle *)&obj); } return ((MessageQ_Handle) obj); } /* * Function to delete a MessageQ object for a specific slave processor. * * Deletes the file descriptors associated with this MessageQ object. */ Int MessageQ_delete (MessageQ_Handle * handlePtr) { Int status = MessageQ_S_SUCCESS; MessageQ_Object * obj = NULL; MessageQDrv_CmdArgs cmdArgs; obj = (MessageQ_Object *) (*handlePtr); cmdArgs.args.deleteMessageQ.handle = obj->serverHandle; status = MessageQDrv_ioctl (CMD_MESSAGEQ_DELETE, &cmdArgs); if (status < 0) { PRINTVERBOSE1("MessageQ_delete: API (through IOCTL) failed, \ status=%d\n", status) } /* Close the fds used for MessageQ_unblock(): */ close(obj->unblockFdW); close(obj->unblockFdR); /* Close the communication endpoint: */ status = transportCloseEndpoint(obj->ipcFd); /* Now free the obj */ free (obj); *handlePtr = NULL; return (status); } /* * Opens an instance of MessageQ for sending. * * We need not create a tiipc file descriptor here; the file descriptors for * all remote processors were created during MessageQ_attach(), and will be * retrieved during MessageQ_put(). */ Int MessageQ_open (String name, MessageQ_QueueId * queueId) { Int status = MessageQ_S_SUCCESS; status = NameServer_getUInt32 (MessageQ_module->nameServer, name, queueId, NULL); if (status == NameServer_E_NOTFOUND) { /* Set return queue ID to invalid. */ *queueId = MessageQ_INVALIDMESSAGEQ; status = MessageQ_E_NOTFOUND; } else if (status >= 0) { /* Override with a MessageQ status code. */ status = MessageQ_S_SUCCESS; } else { /* Set return queue ID to invalid. */ *queueId = MessageQ_INVALIDMESSAGEQ; /* Override with a MessageQ status code. */ if (status == NameServer_E_TIMEOUT) { status = MessageQ_E_TIMEOUT; } else { status = MessageQ_E_FAIL; } } return (status); } /* Closes previously opened instance of MessageQ module. */ Int MessageQ_close (MessageQ_QueueId * queueId) { Int32 status = MessageQ_S_SUCCESS; /* Nothing more to be done for closing the MessageQ. */ *queueId = MessageQ_INVALIDMESSAGEQ; return (status); } /* * Place a message onto a message queue. * * Calls TransportShm_put(), which handles the sending of the message using the * appropriate kernel interface (socket, device ioctl) call for the remote * procId encoded in the queueId argument. * */ Int MessageQ_put (MessageQ_QueueId queueId, MessageQ_Msg msg) { Int status; UInt16 dstProcId = (UInt16)(queueId >> 16); UInt16 queueIndex = (MessageQ_QueueIndex)(queueId & 0x0000ffff); msg->dstId = queueIndex; msg->dstProc = dstProcId; status = transportPut(msg, queueIndex, dstProcId); return (status); } /* * Gets a message for a message queue and blocks if the queue is empty. * If a message is present, it returns it. Otherwise it blocks * waiting for a message to arrive. * When a message is returned, it is owned by the caller. * * We block using select() on the receiving tiipc file descriptor, then * get the waiting message via a read. * We use the file descriptors stored in the messageQ object via a previous * call to MessageQ_create(). * * Note: We currently do not support messages to be sent between threads on the * lcoal processor. * */ Int MessageQ_get (MessageQ_Handle handle, MessageQ_Msg * msg ,UInt timeout) { Int status = MessageQ_S_SUCCESS; Int tmpStatus; MessageQ_Object * obj = (MessageQ_Object *) handle; int retval; int nfds; fd_set rfds; struct timeval tv; void *timevalPtr; int maxfd = 0; /* Wait (with timeout) and retreive message */ FD_ZERO(&rfds); FD_SET(obj->ipcFd, &rfds); maxfd = obj->ipcFd; /* Wait also on the event fd, which may be written by MessageQ_unblock(): */ FD_SET(obj->unblockFdR, &rfds); if (timeout == MessageQ_FOREVER) { timevalPtr = NULL; } else { /* Timeout given in msec: convert: */ tv.tv_sec = timeout / 1000; tv.tv_usec = (timeout % 1000) * 1000; timevalPtr = &tv; } /* Add one to last fd created: */ nfds = ((maxfd > obj->unblockFdR) ? maxfd : obj->unblockFdR) + 1; retval = select(nfds, &rfds, NULL, NULL, timevalPtr); if (retval) { if (FD_ISSET(obj->unblockFdR, &rfds)) { /* * Our event was signalled by MessageQ_unblock(). * * This is typically done during a shutdown sequence, where * the intention of the client would be to ignore (i.e. not fetch) * any pending messages in the transport's queue. * Thus, we shall not check for nor return any messages. */ *msg = NULL; status = MessageQ_E_UNBLOCKED; } else { if (FD_ISSET(obj->ipcFd, &rfds)) { /* Our transport's fd was signalled: Get the message: */ tmpStatus = transportGet(obj->ipcFd, msg); if (tmpStatus < 0) { printf ("MessageQ_get: tranposrtshm_get failed."); status = MessageQ_E_FAIL; } } } } else if (retval == 0) { *msg = NULL; status = MessageQ_E_TIMEOUT; } return (status); } /* * Return a count of the number of messages in the queue * * TBD: To be implemented. Return -1 for now. */ Int MessageQ_count (MessageQ_Handle handle) { Int count = -1; return (count); } /* Initializes a message not obtained from MessageQ_alloc. */ Void MessageQ_staticMsgInit (MessageQ_Msg msg, UInt32 size) { /* Fill in the fields of the message */ MessageQ_msgInit (msg); msg->heapId = MessageQ_STATICMSG; msg->msgSize = size; } /* * Allocate a message and initialize the needed fields (note some * of the fields in the header are set via other APIs or in the * MessageQ_put function, */ MessageQ_Msg MessageQ_alloc (UInt16 heapId, UInt32 size) { MessageQ_Msg msg = NULL; /* * heapId not used for local alloc (as this is over a copy transport), but * we need to send to other side as heapId is used in BIOS transport: */ msg = (MessageQ_Msg)calloc (1, size); MessageQ_msgInit (msg); msg->msgSize = size; msg->heapId = heapId; return msg; } /* Frees the message back to the heap that was used to allocate it. */ Int MessageQ_free (MessageQ_Msg msg) { UInt32 status = MessageQ_S_SUCCESS; /* Check to ensure this was not allocated by user: */ if (msg->heapId == MessageQ_STATICMSG) { status = MessageQ_E_CANNOTFREESTATICMSG; } else { free (msg); } return status; } /* Register a heap with MessageQ. */ Int MessageQ_registerHeap (Ptr heap, UInt16 heapId) { Int status = MessageQ_S_SUCCESS; /* Do nothing, as this uses a copy transport: */ return status; } /* Unregister a heap with MessageQ. */ Int MessageQ_unregisterHeap (UInt16 heapId) { Int status = MessageQ_S_SUCCESS; /* Do nothing, as this uses a copy transport: */ return status; } /* Unblocks a MessageQ */ Void MessageQ_unblock (MessageQ_Handle handle) { MessageQ_Object * obj = (MessageQ_Object *) handle; char buf = 'n'; int numBytes; /* Write to pipe to awaken any threads blocked on this messageQ: */ numBytes = write(obj->unblockFdW, &buf, 1); } /* Embeds a source message queue into a message. */ Void MessageQ_setReplyQueue (MessageQ_Handle handle, MessageQ_Msg msg) { MessageQ_Object * obj = (MessageQ_Object *) handle; msg->replyId = (UInt16)(obj->queue); msg->replyProc = (UInt16)(obj->queue >> 16); } /* Returns the QueueId associated with the handle. */ MessageQ_QueueId MessageQ_getQueueId (MessageQ_Handle handle) { MessageQ_Object * obj = (MessageQ_Object *) handle; UInt32 queueId; queueId = (obj->queue); return queueId; } /* Sets the tracing of a message */ Void MessageQ_setMsgTrace (MessageQ_Msg msg, Bool traceFlag) { msg->flags = (msg->flags & ~TRACEMASK) | (traceFlag << TRACESHIFT); } /* * Returns the amount of shared memory used by one transport instance. * * The MessageQ module itself does not use any shared memory but the * underlying transport may use some shared memory. */ SizeT MessageQ_sharedMemReq (Ptr sharedAddr) { SizeT memReq = 0u; /* Do nothing, as this is a copy transport. */ return (memReq); } /* * Opens a file descriptor for this remote proc. * * Only opens it if one does not already exist for this procId. * * Note: remoteProcId may be MultiProc_Self() for loopback case. */ Int MessageQ_attach (UInt16 remoteProcId, Ptr sharedAddr) { Int status = MessageQ_S_SUCCESS; int ipcFd; PRINTVERBOSE1("MessageQ_attach: remoteProcId: %d\n", remoteProcId) if (remoteProcId >= MultiProc_MAXPROCESSORS) { status = MessageQ_E_INVALIDPROCID; goto exit; } pthread_mutex_lock (&(MessageQ_module->gate)); /* Only open a fd if one doesn't exist: */ if (MessageQ_module->ipcFd[remoteProcId] == -1) { /* Create a fd for sending messages to the remote proc: */ ipcFd = open("/dev/tiipc", O_RDWR); if (ipcFd < 0) { status = MessageQ_E_FAIL; printf ("MessageQ_attach: open of tiipc device failed: %d, %s\n", errno, strerror(errno)); } else { PRINTVERBOSE1("MessageQ_attach: opened tiipc fd for sending: %d\n", ipcFd) MessageQ_module->ipcFd[remoteProcId] = ipcFd; /* * Connect to the remote endpoint and bind a reserved address as * local endpoint */ Connect(ipcFd, remoteProcId, MESSAGEQ_RPMSG_PORT); } } else { status = MessageQ_E_ALREADYEXISTS; } pthread_mutex_unlock (&(MessageQ_module->gate)); exit: return (status); } /* * Close the fd for this remote proc. * */ Int MessageQ_detach (UInt16 remoteProcId) { Int status = MessageQ_S_SUCCESS; int ipcFd; if (remoteProcId >= MultiProc_MAXPROCESSORS) { status = MessageQ_E_INVALIDPROCID; goto exit; } pthread_mutex_lock (&(MessageQ_module->gate)); ipcFd = MessageQ_module->ipcFd[remoteProcId]; if (close (ipcFd)) { status = MessageQ_E_OSFAILURE; printf("MessageQ_detach: close failed: %d, %s\n", errno, strerror(errno)); } else { PRINTVERBOSE1("MessageQ_detach: closed fd: %d\n", ipcFd) MessageQ_module->ipcFd[remoteProcId] = -1; } pthread_mutex_unlock (&(MessageQ_module->gate)); exit: return (status); } /* * This is a helper function to initialize a message. */ Void MessageQ_msgInit (MessageQ_Msg msg) { msg->reserved0 = 0; /* We set this to distinguish from NameServerMsg */ msg->replyId = (UInt16)MessageQ_INVALIDMESSAGEQ; msg->msgId = MessageQ_INVALIDMSGID; msg->dstId = (UInt16)MessageQ_INVALIDMESSAGEQ; msg->flags = MessageQ_HEADERVERSION | MessageQ_NORMALPRI; msg->srcProc = MultiProc_self(); pthread_mutex_lock(&(MessageQ_module->gate)); msg->seqNum = MessageQ_module->seqNum++; pthread_mutex_unlock(&(MessageQ_module->gate)); } /* * ============================================================================= * Transport: Fxns kept here until need for a transport layer is realized. * ============================================================================= */ /* * ======== transportCreateEndpoint ======== * * Create a communication endpoint to receive messages. */ static Int transportCreateEndpoint(int * fd, UInt16 queueIndex) { Int status = MessageQ_S_SUCCESS; int err; /* Create a fd to the ti-ipc to receive messages for this messageQ */ *fd= open("/dev/tiipc", O_RDWR); if (*fd < 0) { status = MessageQ_E_FAIL; printf ("transportCreateEndpoint: Couldn't open tiipc device: %d, %s\n", errno, strerror(errno)); goto exit; } PRINTVERBOSE1("transportCreateEndpoint: opened fd: %d\n", *fd) err = BindAddr(*fd, (UInt32)queueIndex); if (err < 0) { status = MessageQ_E_FAIL; printf ("transportCreateEndpoint: bind failed: %d, %s\n", errno, strerror(errno)); } exit: return (status); } /* * ======== transportCloseEndpoint ======== * * Close the communication endpoint. */ static Int transportCloseEndpoint(int fd) { Int status = MessageQ_S_SUCCESS; PRINTVERBOSE1("transportCloseEndpoint: closing fd: %d\n", fd) /* Stop communication to this endpoint */ close(fd); return (status); } /* * ======== transportGet ======== * Retrieve a message waiting in the queue. */ static Int transportGet(int fd, MessageQ_Msg * retMsg) { Int status = MessageQ_S_SUCCESS; MessageQ_Msg msg; int ret; int byteCount; tiipc_remote_params remote; /* * We have no way of peeking to see what message size we'll get, so we * allocate a message of max size to receive contents from tiipc * (currently, a copy transport) */ msg = MessageQ_alloc (0, MESSAGEQ_RPMSG_MAXSIZE); if (!msg) { status = MessageQ_E_MEMORY; goto exit; } /* Get message */ byteCount = read(fd, msg, MESSAGEQ_RPMSG_MAXSIZE); if (byteCount < 0) { printf("read failed: %s (%d)\n", strerror(errno), errno); status = MessageQ_E_FAIL; goto exit; } else { /* Update the allocated message size (even though this may waste space * when the actual message is smaller than the maximum rpmsg size, * the message will be freed soon anyway, and it avoids an extra copy). */ msg->msgSize = byteCount; /* * If the message received was statically allocated, reset the * heapId, so the app can free it. */ if (msg->heapId == MessageQ_STATICMSG) { msg->heapId = 0; /* for a copy transport, heap id is 0. */ } } PRINTVERBOSE1("transportGet: read from fd: %d\n", fd) ret = ioctl(fd, TIIPC_IOCGETREMOTE, &remote); PRINTVERBOSE3("\tReceived a msg: byteCount: %d, rpmsg addr: %d, rpmsg \ proc: %d\n", byteCount, remote.remote_addr, remote.remote_proc) PRINTVERBOSE2("\tMessage Id: %d, Message size: %d\n", msg->msgId, msg->msgSize) *retMsg = msg; exit: return (status); } /* * ======== transportPut ======== * * Write to tiipc file descriptor associated with * with this destination procID. */ static Int transportPut(MessageQ_Msg msg, UInt16 dstId, UInt16 dstProcId) { Int status = MessageQ_S_SUCCESS; int ipcFd; int err; /* * Retrieve the tiipc file descriptor associated with this * transport for the destination processor. */ ipcFd = MessageQ_module->ipcFd[dstProcId]; PRINTVERBOSE2("Sending msgId: %d via fd: %d\n", msg->msgId, ipcFd) /* send response message to remote processor */ err = write(ipcFd, msg, msg->msgSize); if (err < 0) { printf ("transportPut: write failed: %d, %s\n", errno, strerror(errno)); status = MessageQ_E_FAIL; } /* * Free the message, as this is a copy transport, we maintain MessageQ * semantics. */ MessageQ_free (msg); return (status); }